diff --git a/radio/1.1/IRadio.hal b/radio/1.1/IRadio.hal
index 44b08feb13194b98f892bcf439e56fcf45fa59d6..ea9b96f676a37d92eb982263a32d9ad9e16bd6fb 100644 (file)
--- a/radio/1.1/IRadio.hal
+++ b/radio/1.1/IRadio.hal
* switch and everytime the framework receives a new certificate.
*
* @param serial Serial number of request.
- * @param carrierKey Carrier specific key to be used for encryption. It must
- * be opaque to the framework. This is the byte-stream representation
- * of the key. This is an external encoded form for the key used when
- * a standard representation of the key is needed outside the Java
- * Virtual Machine, as when transmitting the key to some other party.
- * The key is encoded according to a standard format
- * (such as X.509 SubjectPublicKeyInfo or PKCS#8), and is returned using
- * the getEncoded method.
- * @param keyIdentifier This is an opaque value we're given by the carrier
- * and is returned to the carrier. This is used by the server to
- * help it locate the private key to decrypt the permanent identity.
+ * @param message ImsiEncryptionInfo as defined in types.hal.
+ *
*
* Response callback is
* IRadioResponse.setCarrierInfoForImsiEncryptionResponse()
*/
- oneway setCarrierInfoForImsiEncryption(int32_t serial, vec<uint8_t> carrierKey,
- string keyIdentifier);
+ oneway setCarrierInfoForImsiEncryption(int32_t serial, ImsiEncryptionInfo imsiEncryptionInfo);
/**
* Set SIM card power state.
*/
oneway setSimCardPower_1_1(int32_t serial, CardPowerState powerUp);
+ /**
+ * Starts a network scan
+ *
+ * @param serial Serial number of request.
+ * @param request Defines the radio networks/bands/channels which need to be scanned.
+ *
+ * Response function is IRadioResponse.startNetworkScanResponse()
+ */
+ oneway startNetworkScan(int32_t serial, NetworkScanRequest request);
+
+ /**
+ * Stops ongoing network scan
+ *
+ * @param serial Serial number of request.
+ *
+ * Response function is IRadioResponse.stopNetworkScanResponse()
+ */
+ oneway stopNetworkScan(int32_t serial);
};