Radio Interface changes to allow the modem to query the framework
[android/platform-hardware-interfaces.git] / radio / 1.1 / types.hal
index 245d96c00b6926a4762da3b2b4f7686292339ee9..bdd0338d97191cb779daa2d6910076dad9485e95 100644 (file)
@@ -162,3 +162,23 @@ struct NetworkScanResult {
     RadioError error;                       // The error code of the incremental result
     vec<CellInfo> networkInfos;             // List of network information as CellInfo
 };
     RadioError error;                       // The error code of the incremental result
     vec<CellInfo> networkInfos;             // List of network information as CellInfo
 };
+
+struct ImsiEncryptionInfo {
+    string mcc;                   // MCC of the Carrier.
+    string mnc;                   // MNC of the Carrier.
+    vec<uint8_t> carrierKey;      // Carrier specific key to be used for encryption. It must
+                                  // be opaque to the framework. This is the byte-stream
+                                  // representation of the key. This is an external encoded
+                                  // form for the key used when a standard representation of
+                                  // the key is needed outside the Java Virtual Machine, as
+                                  // when transmitting the key to some other party.
+                                  // The key is encoded according to a standard format
+                                  // (such as X.509 SubjectPublicKeyInfo or PKCS#8), and is
+                                  // returned using the getEncoded method as defined on the
+                                  // java.security.Key interface.
+    string keyIdentifier;         // This is an opaque value we're given by the carrier
+                                  // and is returned to the carrier. This is used by the server to
+                                  // help it locate the private key to decrypt the permanent
+                                  // identity.
+    int64_t expirationTime;       // date-time in UTC when the key will expire.
+};