libhwminijail from hardware/interfaces to libhidl.
authorSteven Moreland <smoreland@google.com>
Wed, 11 Oct 2017 18:18:41 +0000 (11:18 -0700)
committerSteven Moreland <smoreland@google.com>
Wed, 11 Oct 2017 18:18:41 +0000 (11:18 -0700)
commitdbdd88124042f2bc592e912941595341be4047e7
tree68b1a44ba4d8cfbd9ea6cbdbddfb23686c8edcb3
parentc3e80fa01ec895f1e0ba72ffb9ff48ec468e07b9
libhwminijail from hardware/interfaces to libhidl.

This library is not a hardware interface, so it doesn't
belong directly in hardware/interfaces. Moving it to
libhidl because it is intended to be a helper library for
hal implementations that want to use minijail/seccomp.

Test: pass
Change-Id: I3f9503f491788492c6692d6584eb088e47862c7a
minijail/Android.bp [deleted file]
minijail/HardwareMinijail.cpp [deleted file]
minijail/include/hwminijail/HardwareMinijail.h [deleted file]