author | Treehugger Robot <treehugger-gerrit@google.com> | |
Mon, 10 Sep 2018 14:00:13 +0000 (14:00 +0000) | ||
committer | Gerrit Code Review <noreply-gerritcodereview@google.com> | |
Mon, 10 Sep 2018 14:00:13 +0000 (14:00 +0000) |
fastboot/1.0/Android.bp | [new file with mode: 0644] | patch | blob |
fastboot/1.0/IFastboot.hal | [new file with mode: 0644] | patch | blob |
fastboot/1.0/types.hal | [new file with mode: 0644] | patch | blob |
diff --git a/fastboot/1.0/Android.bp b/fastboot/1.0/Android.bp
--- /dev/null
+++ b/fastboot/1.0/Android.bp
@@ -0,0 +1,22 @@
+// This file is autogenerated by hidl-gen -Landroidbp.
+
+hidl_interface {
+ name: "android.hardware.fastboot@1.0",
+ root: "android.hardware",
+ vndk: {
+ enabled: true,
+ },
+ srcs: [
+ "types.hal",
+ "IFastboot.hal",
+ ],
+ interfaces: [
+ "android.hidl.base@1.0",
+ ],
+ types: [
+ "Status",
+ "Result",
+ ],
+ gen_java: false,
+}
+
diff --git a/fastboot/1.0/IFastboot.hal b/fastboot/1.0/IFastboot.hal
--- /dev/null
@@ -0,0 +1,32 @@
+/*
+ * Copyright (C) 2018 The Android Open Source Project
+ *
+ * Licensed under the Apache License, Version 2.0 (the "License");
+ * you may not use this file except in compliance with the License.
+ * You may obtain a copy of the License at
+ *
+ * http://www.apache.org/licenses/LICENSE-2.0
+ *
+ * Unless required by applicable law or agreed to in writing, software
+ * distributed under the License is distributed on an "AS IS" BASIS,
+ * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
+ * See the License for the specific language governing permissions and
+ * limitations under the License.
+ */
+package android.hardware.fastboot@1.0;
+
+/**
+ * IFastboot interface implements vendor specific fastboot commands.
+ */
+interface IFastboot {
+ /**
+ * Returns the file system type of the partition. This is only required for
+ * physical partitions that need to be wiped and reformatted.
+ *
+ * @return type Can be ext4, f2fs or raw.
+ * @return result SUCCESS if the operation is successful,
+ * FAILURE_UNKNOWN if the partition is invalid or does not require
+ * reformatting.
+ */
+ getPartitionType(string partitionName) generates (FileSystemType type, Result result);
+};
diff --git a/fastboot/1.0/types.hal b/fastboot/1.0/types.hal
--- /dev/null
+++ b/fastboot/1.0/types.hal
@@ -0,0 +1,61 @@
+/**
+ * Copyright (C) 2018 The Android Open Source Project
+ *
+ * Licensed under the Apache License, Version 2.0 (the "License");
+ * you may not use this file except in compliance with the License.
+ * You may obtain a copy of the License at
+ *
+ * http://www.apache.org/licenses/LICENSE-2.0
+ *
+ * Unless required by applicable law or agreed to in writing, software
+ * distributed under the License is distributed on an "AS IS" BASIS,
+ * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
+ * See the License for the specific language governing permissions and
+ * limitations under the License.
+ */
+
+package android.hardware.fastboot@1.0;
+
+enum Status : uint32_t {
+ /**
+ * Operation completed without errors.
+ */
+ SUCCESS,
+ /**
+ * Unsupported operation.
+ */
+ NOT_SUPPORTED,
+ /**
+ * Bad argument.
+ */
+ INVALID_ARGUMENT,
+ /**
+ * Operation failed due to unknown reason.
+ */
+ FAILURE_UNKNOWN
+};
+
+enum FileSystemType : uint8_t {
+ /**
+ * Fourth extended file system.
+ */
+ EXT4,
+ /**
+ * Flash Friendly File System.
+ */
+ F2FS,
+ /**
+ * Raw file system.
+ */
+ RAW
+};
+
+struct Result {
+ Status status;
+ /**
+ * Error message pertaining to the status. It must be a failure message for
+ * Status FAILURE_UNKNOWN/NOT_SUPPORTED or an informative message for
+ * Status SUCCESS.
+ */
+ string error;
+};