summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: dbdd881)
raw | patch | inline | side by side (parent: dbdd881)
author | Steven Moreland <smoreland@google.com> | |
Tue, 17 Oct 2017 01:29:46 +0000 (18:29 -0700) | ||
committer | Steven Moreland <smoreland@google.com> | |
Wed, 18 Oct 2017 01:33:26 +0000 (18:33 -0700) |
This light extension example was more of a POC. Now it
matches the suggestions for minor version requirements
and vendor extensions that are spelled out in publically
available documentation.
This includes things like:
- taking advantage of namespacing rather than renaming things
- adding documentation when extension differs from what a minor
version extension should be
- importing things specifically rather than dumping namespaces
into the types.hal file
Test: compilation only -- it doesn't do anything
Change-Id: Ia1bf9baaddcb630cc1b6cd4fe272def0c7c492e9
Fixes: 67787567
matches the suggestions for minor version requirements
and vendor extensions that are spelled out in publically
available documentation.
This includes things like:
- taking advantage of namespacing rather than renaming things
- adding documentation when extension differs from what a minor
version extension should be
- importing things specifically rather than dumping namespaces
into the types.hal file
Test: compilation only -- it doesn't do anything
Change-Id: Ia1bf9baaddcb630cc1b6cd4fe272def0c7c492e9
Fixes: 67787567
index 796e2565f651a31eafbd222b3942ffcccefedcbb..612c2d6db98d5eafbae6deb0460d4091b2aff15f 100644 (file)
name: "android.hardware.tests.extension.light@2.0_hal",
srcs: [
"types.hal",
name: "android.hardware.tests.extension.light@2.0_hal",
srcs: [
"types.hal",
- "IExtLight.hal",
+ "ILight.hal",
],
}
],
}
],
out: [
"android/hardware/tests/extension/light/2.0/types.cpp",
],
out: [
"android/hardware/tests/extension/light/2.0/types.cpp",
- "android/hardware/tests/extension/light/2.0/ExtLightAll.cpp",
+ "android/hardware/tests/extension/light/2.0/LightAll.cpp",
],
}
],
}
out: [
"android/hardware/tests/extension/light/2.0/types.h",
"android/hardware/tests/extension/light/2.0/hwtypes.h",
out: [
"android/hardware/tests/extension/light/2.0/types.h",
"android/hardware/tests/extension/light/2.0/hwtypes.h",
- "android/hardware/tests/extension/light/2.0/IExtLight.h",
- "android/hardware/tests/extension/light/2.0/IHwExtLight.h",
- "android/hardware/tests/extension/light/2.0/BnHwExtLight.h",
- "android/hardware/tests/extension/light/2.0/BpHwExtLight.h",
- "android/hardware/tests/extension/light/2.0/BsExtLight.h",
+ "android/hardware/tests/extension/light/2.0/ILight.h",
+ "android/hardware/tests/extension/light/2.0/IHwLight.h",
+ "android/hardware/tests/extension/light/2.0/BnHwLight.h",
+ "android/hardware/tests/extension/light/2.0/BpHwLight.h",
+ "android/hardware/tests/extension/light/2.0/BsLight.h",
],
}
],
}
":android.hardware.tests.extension.light@2.0_hal",
],
out: [
":android.hardware.tests.extension.light@2.0_hal",
],
out: [
+ "android/hardware/tests/extension/light/V2_0/Brightness.java",
"android/hardware/tests/extension/light/V2_0/Default.java",
"android/hardware/tests/extension/light/V2_0/Default.java",
- "android/hardware/tests/extension/light/V2_0/ExtBrightness.java",
- "android/hardware/tests/extension/light/V2_0/ExtLightState.java",
- "android/hardware/tests/extension/light/V2_0/IExtLight.java",
+ "android/hardware/tests/extension/light/V2_0/LightState.java",
+ "android/hardware/tests/extension/light/V2_0/ILight.java",
],
}
],
}
":android.hardware.tests.extension.light@2.0_hal",
],
out: [
":android.hardware.tests.extension.light@2.0_hal",
],
out: [
- "android/hardware/tests/extension/light/2.0/AExtLight.cpp",
+ "android/hardware/tests/extension/light/2.0/ALight.cpp",
],
}
],
}
":android.hardware.tests.extension.light@2.0_hal",
],
out: [
":android.hardware.tests.extension.light@2.0_hal",
],
out: [
- "android/hardware/tests/extension/light/2.0/AExtLight.h",
+ "android/hardware/tests/extension/light/2.0/ALight.h",
],
}
],
}
similarity index 74%
rename from tests/extension/light/2.0/IExtLight.hal
rename to tests/extension/light/2.0/ILight.hal
index 1515b869c040e05c095eb1c380a461575daad56c..94781c0838654a9df18e35d5aa9fc3e3fec1f3b6 100644 (file)
rename from tests/extension/light/2.0/IExtLight.hal
rename to tests/extension/light/2.0/ILight.hal
index 1515b869c040e05c095eb1c380a461575daad56c..94781c0838654a9df18e35d5aa9fc3e3fec1f3b6 100644 (file)
// vendor partition.
package android.hardware.tests.extension.light@2.0;
// vendor partition.
package android.hardware.tests.extension.light@2.0;
-import android.hardware.light@2.0;
+import android.hardware.light@2.0::ILight;
+import android.hardware.light@2.0::Status;
+import android.hardware.light@2.0::Type;
-interface IExtLight extends android.hardware.light@2.0::ILight {
+interface ILight extends android.hardware.light@2.0::ILight {
/**
* Set the provided lights to the provided values.
*
/**
* Set the provided lights to the provided values.
*
+ * If this was a minor version extension, the recommended
+ * name would be setLight_2_1.
+ *
* @param type logical light to set
* @param state describes what the light should look like.
* @return status result of applying state transformation.
*/
* @param type logical light to set
* @param state describes what the light should look like.
* @return status result of applying state transformation.
*/
- setExtLight(Type type, ExtLightState state) generates (Status status);
-
+ setLightExt(Type type, LightState state) generates (Status status);
};
};
diff --git a/tests/extension/light/2.0/default/Light.cpp b/tests/extension/light/2.0/default/Light.cpp
index d941e73e0068b4bcec4d25d84d8d32334833f354..9df79248a775dcb2740b99e306219185c008aeae 100644 (file)
namespace implementation {
// Methods from ::android::hardware::light::V2_0::ILight follow.
namespace implementation {
// Methods from ::android::hardware::light::V2_0::ILight follow.
-Return<Status> Light::setLight(Type type, const LightState& state) {
+Return<Status> Light::setLight(Type type, const OldLightState& state) {
// Forward types for new methods.
// Forward types for new methods.
- ExtLightState extState {
- .state = state,
- .interpolationOmega =
- static_cast<int32_t>(Default::INTERPOLATION_OMEGA),
- .brightness = // ExtBrightness inherits from Brightness
- static_cast<ExtBrightness>(state.brightnessMode)
- };
+ LightState extState{.state = state,
+ .interpolationOmega = static_cast<int32_t>(Default::INTERPOLATION_OMEGA),
+ .brightness = // Brightness inherits from Brightness
+ static_cast<Brightness>(state.brightnessMode)};
- return setExtLight(type, extState);
+ return setLightExt(type, extState);
}
Return<void> Light::getSupportedTypes(getSupportedTypes_cb _hidl_cb) {
}
Return<void> Light::getSupportedTypes(getSupportedTypes_cb _hidl_cb) {
}
// Methods from ::android::hardware::example::extension::light::V2_0::ILight follow.
}
// Methods from ::android::hardware::example::extension::light::V2_0::ILight follow.
-Return<Status> Light::setExtLight(Type /* type */,
- const ExtLightState& /* state */) {
-
+Return<Status> Light::setLightExt(Type /* type */, const LightState& /* state */) {
// ******************************************************
// Note: awesome proprietary hardware implementation here
// ******************************************************
// ******************************************************
// Note: awesome proprietary hardware implementation here
// ******************************************************
index dc2c5dd5379c09d06da8038a77352e845d74ed4c..d178e75cbcf11db514b24e757c9ef1ecd0313bcf 100644 (file)
#ifndef ANDROID_HARDWARE_TESTS_EXTENSION_LIGHT_V2_0_LIGHT_H
#define ANDROID_HARDWARE_TESTS_EXTENSION_LIGHT_V2_0_LIGHT_H
#ifndef ANDROID_HARDWARE_TESTS_EXTENSION_LIGHT_V2_0_LIGHT_H
#define ANDROID_HARDWARE_TESTS_EXTENSION_LIGHT_V2_0_LIGHT_H
-#include <android/hardware/tests/extension/light/2.0/IExtLight.h>
+#include <android/hardware/tests/extension/light/2.0/ILight.h>
#include <hidl/Status.h>
#include <hidl/MQDescriptor.h>
#include <hidl/Status.h>
#include <hidl/MQDescriptor.h>
namespace V2_0 {
namespace implementation {
namespace V2_0 {
namespace implementation {
-using ::android::hardware::tests::extension::light::V2_0::ExtLightState;
-using ::android::hardware::tests::extension::light::V2_0::IExtLight;
-using ::android::hardware::light::V2_0::ILight;
-using ::android::hardware::light::V2_0::LightState;
+using ::android::hardware::tests::extension::light::V2_0::LightState;
+using ::android::hardware::tests::extension::light::V2_0::ILight;
+// If using a minor version upgrade, we could just reference these as
+// V2_0::LightState vs. V2_1::LightState, but this makes things easier.
+using OldLightState = ::android::hardware::light::V2_0::LightState;
using ::android::hardware::light::V2_0::Status;
using ::android::hardware::light::V2_0::Type;
using ::android::hardware::Return;
using ::android::hardware::Void;
using ::android::hardware::hidl_vec;
using ::android::hardware::light::V2_0::Status;
using ::android::hardware::light::V2_0::Type;
using ::android::hardware::Return;
using ::android::hardware::Void;
using ::android::hardware::hidl_vec;
-using ::android::hardware::hidl_string;
using ::android::sp;
using ::android::sp;
-struct Light : public IExtLight {
+struct Light : public ILight {
// Methods from ::android::hardware::light::V2_0::ILight follow.
// Methods from ::android::hardware::light::V2_0::ILight follow.
- Return<Status> setLight(Type type, const LightState& state) override;
+ Return<Status> setLight(Type type, const OldLightState& state) override;
Return<void> getSupportedTypes(getSupportedTypes_cb _hidl_cb) override;
// Methods from ::android::hardware::example::extension::light::V2_0::ILight follow.
Return<void> getSupportedTypes(getSupportedTypes_cb _hidl_cb) override;
// Methods from ::android::hardware::example::extension::light::V2_0::ILight follow.
- Return<Status> setExtLight(Type type, const ExtLightState& state) override;
-
+ Return<Status> setLightExt(Type type, const LightState& state) override;
};
} // namespace implementation
};
} // namespace implementation
index 1b094796db006a130bf769016a5278cb335ffb14..c05e099f2af7b8422baa9032ddaf2ab17594c082 100644 (file)
package android.hardware.tests.extension.light@2.0;
package android.hardware.tests.extension.light@2.0;
-import android.hardware.light@2.0;
+// If importing something from the same package, the preference is:
+// import @2.0::Foo. However, since this isn't a minor version upgrade
+// we have to use the fully-qualified names here.
+import android.hardware.light@2.0::Brightness;
+import android.hardware.light@2.0::LightState;
enum Default : int32_t {
// for calls to setLight from the framework that don't know about this
enum Default : int32_t {
// for calls to setLight from the framework that don't know about this
* One possibility is renaming an old type. Another possibility is taking
* advantages of the different namespaces.
*/
* One possibility is renaming an old type. Another possibility is taking
* advantages of the different namespaces.
*/
-enum ExtBrightness : Brightness {
+enum Brightness : android.hardware.light@2.0::Brightness {
/**
* Say we're really going to use the phone as a heater.
*/
/**
* Say we're really going to use the phone as a heater.
*/
/**
* Structs can't inherit eachother in hidl. Use composition instead. In this
* case, I won't use inheritence because I want to replace Brightness with
/**
* Structs can't inherit eachother in hidl. Use composition instead. In this
* case, I won't use inheritence because I want to replace Brightness with
- * ExtBrightness.
+ * the new enumeration.
*/
*/
-struct ExtLightState {
- LightState state;
+struct LightState {
+ android.hardware.light@2.0::LightState state;
/**
* This is the secret sauce that will really make this extension shine.
/**
* This is the secret sauce that will really make this extension shine.
/**
* Include new values.
*/
/**
* Include new values.
*/
- ExtBrightness brightness;
+ Brightness brightness;
};
};