]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/commitdiff
Clarifying GnssMeasurement and Clock commments
authorWyattRiley <wyattriley@google.com>
Wed, 15 Aug 2018 01:19:30 +0000 (18:19 -0700)
committerWyattRiley <wyattriley@google.com>
Thu, 4 Oct 2018 16:12:15 +0000 (09:12 -0700)
Change-Id: Ia51b16a2904ab43f67464fc91321fad99a2bb614
Fixes: 77812939
Test: Comments only, verified builds

current.txt
gnss/1.0/IGnssMeasurementCallback.hal

index 327833fd3d370f200f3b50cc0f6a8e2102879e65..b1a651f01f5473fdc28d3326ba081871c522b431 100644 (file)
@@ -386,6 +386,7 @@ cd4330c3196bda1d642a32abfe23a7d64ebfbda721940643af6867af3b3f0aa9 android.hardwar
 
 # ABI preserving changes to HALs during Android Q
 da33234403ff5d60f3473711917b9948e6484a4260b5247acdafb111193a9de2 android.hardware.configstore@1.0::ISurfaceFlingerConfigs
+78886339f2c848cf13c1edd3ebba63f89796b2620d3bf3b5c21d038a53519ba0 android.hardware.gnss@1.0::IGnssMeasurementCallback
 b7ecf29927055ec422ec44bf776223f07d79ad9f92ccf9becf167e62c2607e7a android.hardware.keymaster@4.0::IKeymasterDevice
 574e8f1499436fb4075894dcae0b36682427956ecb114f17f1fe22d116a83c6b android.hardware.neuralnetworks@1.0::IPreparedModel
 1fb32361286b938d48a55c2539c846732afce0b99fe08590f556643125bc13d3 android.hardware.neuralnetworks@1.0::types
index b27c2e0d3558a5a25b1a25dcd70450a2bc756f2e..d3489e65b02edba4a2b288d495509f648ec4588e 100644 (file)
@@ -124,6 +124,12 @@ interface IGnssMeasurementCallback {
         /**
          * A set of flags indicating the validity of the fields in this data
          * structure.
+         *
+         * Fields for which there is no corresponding flag must be filled in
+         * with a valid value.  For convenience, these are marked as mandatory.
+         *
+         * Others fields may have invalid information in them, if not marked as
+         * valid by the corresponding bit in gnssClockFlags.
          */
         bitfield<GnssClockFlags> gnssClockFlags;
 
@@ -155,7 +161,7 @@ interface IGnssMeasurementCallback {
          * Sub-nanosecond accuracy can be provided by means of the 'biasNs' field.
          * The value contains the timeUncertaintyNs in it.
          *
-         * This field is mandatory.
+         * This value is mandatory.
          */
         int64_t timeNs;
 
@@ -172,29 +178,31 @@ interface IGnssMeasurementCallback {
 
         /**
          * The difference between hardware clock ('time' field) inside GNSS receiver
-         * and the true GNSS time since 0000Z, January 6, 1980, in nanoseconds.
+         * and the true GPS time since 0000Z, January 6, 1980, in nanoseconds.
          *
          * The sign of the value is defined by the following equation:
-         *      local estimate of GNSS time = timeNs - (fullBiasNs + biasNs)
-         *
-         * This value is mandatory if the receiver has estimated GNSS time. If the
-         * computed time is for a non-GNSS constellation, the time offset of that
-         * constellation to GNSS has to be applied to fill this value. The error
-         * estimate for the sum of this and the biasNs is the biasUncertaintyNs,
-         * and the caller is responsible for using this uncertainty (it can be very
-         * large before the GNSS time has been solved for.) If the data is available
-         * gnssClockFlags must contain HAS_FULL_BIAS.
+         *      local estimate of GPS time = timeNs - (fullBiasNs + biasNs)
+         *
+         * If receiver has computed time for a non-GPS constellation, the time offset of
+         * that constellation versus GPS time must be applied to fill this value.
+         *
+         * The error estimate for the sum of this and the biasNs is the biasUncertaintyNs.
+         *
+         * If the data is available gnssClockFlags must contain HAS_FULL_BIAS.
+         *
+         * This value is mandatory if the receiver has estimated GPS time.
          */
         int64_t fullBiasNs;
 
         /**
-         * Sub-nanosecond bias.
+         * Sub-nanosecond bias - used with fullBiasNS, see fullBiasNs for details.
+         *
          * The error estimate for the sum of this and the fullBiasNs is the
          * biasUncertaintyNs.
          *
-         * If the data is available gnssClockFlags must contain HAS_BIAS. If GNSS
-         * has computed a position fix. This value is mandatory if the receiver has
-         * estimated GNSS time.
+         * If the data is available gnssClockFlags must contain HAS_BIAS.
+         *
+         * This value is mandatory if the receiver has estimated GPS time.
          */
         double biasNs;
 
@@ -203,9 +211,12 @@ interface IGnssMeasurementCallback {
          * bias) in nanoseconds. The uncertainty is represented as an absolute
          * (single sided) value.
          *
-         * If the data is available gnssClockFlags must contain
-         * HAS_BIAS_UNCERTAINTY. This value is mandatory if the receiver
-         * has estimated GNSS time.
+         * The caller is responsible for using this uncertainty (it can be very
+         * large before the GPS time has been fully resolved.)
+         *
+         * If the data is available gnssClockFlags must contain HAS_BIAS_UNCERTAINTY.
+         *
+         * This value is mandatory if the receiver has estimated GPS time.
          */
         double biasUncertaintyNs;
 
@@ -216,10 +227,9 @@ interface IGnssMeasurementCallback {
          * frequency, and that the (fullBiasNs + biasNs) is growing more positive
          * over time.
          *
-         * The value contains the 'drift uncertainty' in it.
          * If the data is available gnssClockFlags must contain HAS_DRIFT.
          *
-         * This value is mandatory if the receiver has estimated GNSS time.
+         * This value is mandatory if the receiver has estimated GPS time.
          */
         double driftNsps;
 
@@ -228,15 +238,15 @@ interface IGnssMeasurementCallback {
          * second).
          * The uncertainty is represented as an absolute (single sided) value.
          *
-         * If the data is available gnssClockFlags must contain
-         * HAS_DRIFT_UNCERTAINTY. If GNSS has computed a position fix this
-         * field is mandatory and must be populated.
+         * If the data is available gnssClockFlags must contain HAS_DRIFT_UNCERTAINTY.
+         *
+         * This value is mandatory if the receiver has estimated GPS time.
          */
         double driftUncertaintyNsps;
 
         /**
-         * When there are any discontinuities in the HW clock, this field is
-         * mandatory.
+         * This field must be incremented, when there are discontinuities in the
+         * hardware clock.
          *
          * A "discontinuity" is meant to cover the case of a switch from one source
          * of clock to another.  A single free-running crystal oscillator (XO)
@@ -262,6 +272,8 @@ interface IGnssMeasurementCallback {
          * as this avoids the need to use (waste) a GNSS measurement to fully
          * re-solve for the GNSS clock bias and drift, when using the accompanying
          * measurements, from consecutive GnssData reports.
+         *
+         * This value is mandatory.
          */
         uint32_t hwClockDiscontinuityCount;
 
@@ -280,17 +292,26 @@ interface IGnssMeasurementCallback {
         /**
          * A set of flags indicating the validity of the fields in this data
          * structure.
+         *
+         * Fields for which there is no corresponding flag must be filled in
+         * with a valid value.  For convenience, these are marked as mandatory.
+         *
+         * Others fields may have invalid information in them, if not marked as
+         * valid by the corresponding bit in flags.
          */
         bitfield<GnssMeasurementFlags> flags;
 
         /**
          * Satellite vehicle ID number, as defined in GnssSvInfo::svid
-         * This is a mandatory value.
+         *
+         * This value is mandatory.
          */
         int16_t svid;
 
         /**
          * Defines the constellation of the given SV.
+         *
+         * This value is mandatory.
          */
         GnssConstellationType constellation;
 
@@ -302,8 +323,10 @@ interface IGnssMeasurementCallback {
          *      measurement time = GnssClock::timeNs + timeOffsetNs
          *
          * It provides an individual time-stamp for the measurement, and allows
-         * sub-nanosecond accuracy.
-         * This is a mandatory value.
+         * sub-nanosecond accuracy. It may be zero if all measurements are
+         * aligned to a common time.
+         *
+         * This value is mandatory.
          */
         double timeOffsetNs;
 
@@ -313,7 +336,7 @@ interface IGnssMeasurementCallback {
          * Based on the sync state, the 'received GNSS tow' field must be interpreted
          * accordingly.
          *
-         * This is a mandatory value.
+         * This value is mandatory.
          */
         bitfield<GnssMeasurementState> state;
 
@@ -413,7 +436,7 @@ interface IGnssMeasurementCallback {
          * Carrier-to-noise density in dB-Hz, typically in the range [0, 63].
          * It contains the measured C/N0 value for the signal at the antenna port.
          *
-         * This is a mandatory value.
+         * This value is mandatory.
          */
         double cN0DbHz;
 
@@ -449,7 +472,7 @@ interface IGnssMeasurementCallback {
          * 1-Sigma uncertainty of the pseudorangeRateMps.
          * The uncertainty is represented as an absolute (single sided) value.
          *
-         * This is a mandatory value.
+         * This value is mandatory.
          */
         double pseudorangeRateUncertaintyMps;
 
@@ -457,7 +480,7 @@ interface IGnssMeasurementCallback {
          * Accumulated delta range's state. It indicates whether ADR is reset or
          * there is a cycle slip(indicating loss of lock).
          *
-         * This is a mandatory value.
+         * This value is mandatory.
          */
         bitfield<GnssAccumulatedDeltaRangeState> accumulatedDeltaRangeState;