Radio Interface changes to allow the modem to query the framework for the key.
authorpkanwar <pkanwar@google.com>
Tue, 13 Jun 2017 20:30:45 +0000 (20:30 +0000)
committerandroid-build-merger <android-build-merger@google.com>
Tue, 13 Jun 2017 20:30:45 +0000 (20:30 +0000)
am: 1076d5ba87

Change-Id: I7191109616d9fb51e2aac762f9685c91782f9f6b

radio/1.1/Android.mk
radio/1.1/IRadio.hal
radio/1.1/types.hal

index 305b6618baa96bdb48e8344b374c608d3303da46..21c4a6aeaa5f7796effbe43a71118569a8fe179b 100644 (file)
@@ -74,6 +74,25 @@ $(GEN): $(LOCAL_PATH)/types.hal
        $(transform-generated-source)
 LOCAL_GENERATED_SOURCES += $(GEN)
 
+#
+# Build types.hal (ImsiEncryptionInfo)
+#
+GEN := $(intermediates)/android/hardware/radio/V1_1/ImsiEncryptionInfo.java
+$(GEN): $(HIDL)
+$(GEN): PRIVATE_HIDL := $(HIDL)
+$(GEN): PRIVATE_DEPS := $(LOCAL_PATH)/types.hal
+$(GEN): PRIVATE_OUTPUT_DIR := $(intermediates)
+$(GEN): PRIVATE_CUSTOM_TOOL = \
+        $(PRIVATE_HIDL) -o $(PRIVATE_OUTPUT_DIR) \
+        -Ljava \
+        -randroid.hardware:hardware/interfaces \
+        -randroid.hidl:system/libhidl/transport \
+        android.hardware.radio@1.1::types.ImsiEncryptionInfo
+
+$(GEN): $(LOCAL_PATH)/types.hal
+       $(transform-generated-source)
+LOCAL_GENERATED_SOURCES += $(GEN)
+
 #
 # Build types.hal (NetworkScanRequest)
 #
@@ -342,6 +361,25 @@ $(GEN): $(LOCAL_PATH)/types.hal
        $(transform-generated-source)
 LOCAL_GENERATED_SOURCES += $(GEN)
 
+#
+# Build types.hal (ImsiEncryptionInfo)
+#
+GEN := $(intermediates)/android/hardware/radio/V1_1/ImsiEncryptionInfo.java
+$(GEN): $(HIDL)
+$(GEN): PRIVATE_HIDL := $(HIDL)
+$(GEN): PRIVATE_DEPS := $(LOCAL_PATH)/types.hal
+$(GEN): PRIVATE_OUTPUT_DIR := $(intermediates)
+$(GEN): PRIVATE_CUSTOM_TOOL = \
+        $(PRIVATE_HIDL) -o $(PRIVATE_OUTPUT_DIR) \
+        -Ljava \
+        -randroid.hardware:hardware/interfaces \
+        -randroid.hidl:system/libhidl/transport \
+        android.hardware.radio@1.1::types.ImsiEncryptionInfo
+
+$(GEN): $(LOCAL_PATH)/types.hal
+       $(transform-generated-source)
+LOCAL_GENERATED_SOURCES += $(GEN)
+
 #
 # Build types.hal (NetworkScanRequest)
 #
index b3e21e7b582f7d501a4bf4f43f82587685697f21..ea9b96f676a37d92eb982263a32d9ad9e16bd6fb 100644 (file)
@@ -34,23 +34,13 @@ interface IRadio extends @1.0::IRadio {
      * switch and everytime the framework receives a new certificate.
      *
      * @param serial Serial number of request.
-     * @param carrierKey Carrier specific key to be used for encryption. It must
-     *        be opaque to the framework. This is the byte-stream representation
-     *        of the key. This is an external encoded form for the key used when
-     *        a standard representation of the key is needed outside the Java
-     *        Virtual Machine, as when transmitting the key to some other party.
-     *        The key is encoded according to a standard format
-     *        (such as X.509 SubjectPublicKeyInfo or PKCS#8), and is returned using
-     *        the getEncoded method.
-     * @param keyIdentifier This is an opaque value we're given by the carrier
-     *        and is returned to the carrier. This is used by the server to
-     *        help it locate the private key to decrypt the permanent identity.
+     * @param message ImsiEncryptionInfo as defined in types.hal.
+     *
      *
      * Response callback is
      * IRadioResponse.setCarrierInfoForImsiEncryptionResponse()
      */
-     oneway setCarrierInfoForImsiEncryption(int32_t serial, vec<uint8_t> carrierKey,
-             string keyIdentifier);
+     oneway setCarrierInfoForImsiEncryption(int32_t serial, ImsiEncryptionInfo imsiEncryptionInfo);
 
     /**
      * Set SIM card power state.
index 245d96c00b6926a4762da3b2b4f7686292339ee9..bdd0338d97191cb779daa2d6910076dad9485e95 100644 (file)
@@ -162,3 +162,23 @@ struct NetworkScanResult {
     RadioError error;                       // The error code of the incremental result
     vec<CellInfo> networkInfos;             // List of network information as CellInfo
 };
+
+struct ImsiEncryptionInfo {
+    string mcc;                   // MCC of the Carrier.
+    string mnc;                   // MNC of the Carrier.
+    vec<uint8_t> carrierKey;      // Carrier specific key to be used for encryption. It must
+                                  // be opaque to the framework. This is the byte-stream
+                                  // representation of the key. This is an external encoded
+                                  // form for the key used when a standard representation of
+                                  // the key is needed outside the Java Virtual Machine, as
+                                  // when transmitting the key to some other party.
+                                  // The key is encoded according to a standard format
+                                  // (such as X.509 SubjectPublicKeyInfo or PKCS#8), and is
+                                  // returned using the getEncoded method as defined on the
+                                  // java.security.Key interface.
+    string keyIdentifier;         // This is an opaque value we're given by the carrier
+                                  // and is returned to the carrier. This is used by the server to
+                                  // help it locate the private key to decrypt the permanent
+                                  // identity.
+    int64_t expirationTime;       // date-time in UTC when the key will expire.
+};