]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - .clang-format
Merge "Fix IUsb version number in vts test" into pie-vts-dev
[android/platform-hardware-interfaces.git] / .clang-format
2018-07-16 sqianresolve merge conflicts of dfa79a6292a42dd8609053febd8d...
2018-07-12 Pawin Vongmasaresolve merge conflicts of b92f1d2e1be35b331b18589a8cde...
2018-07-12 Kevin Rocard[automerger skipped] Audio VTS: run tear-down hooks...
2018-06-18 sqian[automerger skipped] Fix setBandMode.
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc
2018-05-24 Pawin VongmasaAdd multichannel support
2018-04-24 Iris ChangVTS: fix RadioHidlTest.getAvailableNetworks issue am...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support
2018-03-29 Yuexi Maresolve merge conflicts of a9543fee6b3f5e9609206d3a21a4...
2018-03-29 Yuexi MaMerge "rename VtsHalEvsV1_0Target module to VtsHalEvsV1...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported
2018-03-06 Myles Watsonresolve merge conflicts of 8a28de7a8c3d36e648e90ed2fca2...
2018-03-06 Myles WatsonBluetooth: Relax NO_OP and SCO checks am: 8a28de7a8c
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation
2018-01-25 sqianMerge "Add None into cancelPendingUssd" into oreo-vts...
2018-01-25 sqianMerge "Add None into cancelPendingUssd" into oreo-vts-dev
2018-01-24 Keun Soo YimMerge "DO NOT MERGE Resolve merge conflict for VtsHalCa...
2018-01-24 Ram Mohan MMerge "bug fix: close file pointer" into oreo-vts-dev...
2018-01-24 Kevin RocardAudio policy config: remove cross-module device port...
2018-01-24 Keun Soo YimMerge "DO NOT MERGE Resolve merge conflict for VtsHalCa...
2018-01-24 Ram Mohan MMerge "bug fix: close file pointer" into oreo-vts-dev
2018-01-24 Kevin RocardAudio policy config: remove cross-module device port...
2018-01-24 Android Build Merg... [automerger] Audio HAL: Allow setters to not be impleme...
2018-01-24 Android Build Merg... [automerger] Merge "Audio VTS: HAL can support more...
2018-01-24 Android Build Merg... [automerger] Audio policy config: Device port (type...
2018-01-24 Android Build Merg... [automerger] Audio policy config: allow vendor to exten...
2018-01-24 Android Build Merg... [automerger] Set time delay in the vts test setup am...
2018-01-24 Android Build Merg... [automerger] Loosen speed check for first GPS location...
2018-01-24 Android Build Merg... [automerger] Add tests to validate key length for clear...
2018-01-24 Android Build Merg... [automerger skipped] Add REQUEST_NOT_SUPPORTED / SIM_AB...
2018-01-23 Android Build Merg... [automerger] Fix VTS test which turns off radio. am...
2018-01-23 Android Build Merg... [automerger] VTS: fix VtsHalKeymasterV3_0Target issue...
2018-01-23 Android Build Merg... [automerger] Audio VTS: do not test duplicate policy...
2018-01-23 Kevin RocardAudio HAL: Allow setters to not be implemented
2018-01-23 Android Build Merg... [automerger] Audio VTS: remove expectation of policy...
2018-01-23 Kevin RocardMerge "Audio VTS: HAL can support more than the native...
2018-01-23 Kevin RocardAudio policy config: Device port (type,address) must...
2018-01-23 Kevin RocardAudio policy config: allow vendor to extend module...
2018-01-23 Android Build Merg... [automerger] Allow partially dynamic profile in the...
2018-01-23 Android Build Merg... [automerger] bug fix: restore support for broken flag...
2018-01-23 sqianSet time delay in the vts test setup
2018-01-23 Wyatt RileyLoosen speed check for first GPS location
2018-01-23 Android Build Merg... [automerger] bug fix: handle multiple port settings...
2018-01-23 Android Build Merg... [automerger] Merge "Audio VTS: Look for Audio policy...
2018-01-23 Edwin WongAdd tests to validate key length for clearkey plugin.
2018-01-23 sqianAdd REQUEST_NOT_SUPPORTED / SIM_ABSENT for vts tests
2018-01-23 Sanket PadaweFix VTS test which turns off radio.
2018-01-23 Iris ChangVTS: fix VtsHalKeymasterV3_0Target issue
2018-01-23 Kevin RocardAudio VTS: do not test duplicate policy configuration...
2018-01-23 Kevin RocardAudio VTS: remove expectation of policy configuration...
2018-01-23 Android Build Merg... [automerger] Merge "Don't send more than 2K to addRngEn...
2018-01-23 Android Build Merg... [automerger] bug fix: disable timestamp deviation test...
2018-01-23 Android Build Merg... [automerger] Merge "Allow clearkey tests to run if...
2018-01-23 Android Build Merg... [automerger] bug fix: output colorformat configuration...
2018-01-23 Kevin RocardAllow partially dynamic profile in the audio policy...
2018-01-23 Ram Mohan Mbug fix: restore support for broken flag
2018-01-23 Ram Mohan Mbug fix: handle multiple port settings change events...
2018-01-23 Kevin RocardMerge "Audio VTS: Look for Audio policy config in all...
2018-01-23 Shawn WilldenMerge "Don't send more than 2K to addRngEntropy" into...
2018-01-23 Android Build Merg... [automerger] Merge "bug fix: configure input port buffe...
2018-01-23 Ram Mohan Mbug fix: disable timestamp deviation test for audio...
2018-01-23 Jeff TinkerMerge "Allow clearkey tests to run if no vendor modules...
2018-01-23 Ram Mohan Mbug fix: output colorformat configuration fixed
2018-01-23 Ram Mohan MMerge "bug fix: configure input port buffer size" into...
2018-01-23 Tomasz WasilczykUpdate broadcastradio HAL 1.0 VTS tests.
2018-01-23 Android Build Merg... [automerger] Update broadcastradio HAL 1.0 VTS tests...
2018-01-23 Ram Mohan Mbug fix: handle OMX_EventBufferFlag events
2018-01-23 Peng XuSkip direct report test if sensor is not available
2018-01-23 Shawn WilldenReduce max keymaster message size to 2K
2018-01-23 Android Build Merg... [automerger] bug fix: handle OMX_EventBufferFlag events...
2018-01-23 Ruchi Kandoinfc: NCI 2.0: Add CORE_INIT_CMD for NCI 2.0
2018-01-23 sqianAdd EMPTY_RECORD for getDeviceIdentity
2018-01-23 Kevin RocardAudio policy config xsd: add missing gains and address...
2018-01-23 Android Build Merg... [automerger] Skip direct report test if sensor is not...
2018-01-23 Android Build Merg... [automerger] Reduce max keymaster message size to 2K...
2018-01-23 Android Build Merg... [automerger] nfc: NCI 2.0: Add CORE_INIT_CMD for NCI...
2018-01-23 Android Build Merg... [automerger] Add EMPTY_RECORD for getDeviceIdentity...
2018-01-23 Android Build Merg... [automerger] Audio policy config xsd: add missing gains...
2018-01-23 Android Build Merg... [automerger] Merge "Add corresponding error code to...
2018-01-23 Android Build Merg... [automerger] Merge "supplicant(vts): Remove start/stop...
2018-01-23 Android Build Merg... [automerger] Fixed the HCI ACL Header definitions for...
2018-01-23 Android Build Merg... [automerger] Update VTS tests so that Mediatek pass...
2018-01-23 Android Build Merg... [automerger] Add Sim absent assertion in the 1.0 setup...
2018-01-23 Android Build Merg... [automerger] Fix some VTS for 2017 devices am: 44bd0bb4...
2018-01-23 sqianMerge "Add corresponding error code to fix vts test...
2018-01-23 Roshan PiusMerge "supplicant(vts): Remove start/stop framework...
2018-01-23 Stanley TngFixed the HCI ACL Header definitions for PB and BC...
2018-01-23 Legler WuUpdate VTS tests so that Mediatek pass more VTS for O.
2018-01-23 sqianAdd Sim absent assertion in the 1.0 setup
2018-01-23 Android Build Merg... [automerger] Fix consumerir test bugs am: 43e1c6bc55...
2018-01-23 sqianFix some VTS for 2017 devices
2018-01-23 Android Build Merg... [automerger] Camera: Add support for testing partial...
2018-01-23 Connor O'BrienFix consumerir test bugs
2018-01-23 Android Build Merg... [automerger] Fix ICryptoFactory service am: 8a85370679...
next