]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - OWNERS
Use -Werror in hardware/interfaces/automotive/evs/1.0
[android/platform-hardware-interfaces.git] / OWNERS
2017-08-19 Ram Mohan MMerge "bug fix: close file pointer" into oc-dev
2017-08-19 Ram Mohan MMerge "bug fix: configure input port buffer size" into...
2017-08-19 Ram Mohan MMerge "bug fix: close file pointer" into oc-dev am...
2017-08-19 Ram Mohan MMerge "bug fix: configure input port buffer size" into...
2017-08-18 Jeff TinkerAllow clearkey tests to run if no vendor modules am...
2017-08-18 Jeff TinkerAllow clearkey tests to run if no vendor modules
2017-08-15 Emilian PeevMerge "Camera: Switch 'cancelPictureFail' to 'cancelPic...
2017-08-15 Emilian PeevMerge "Camera: Switch 'cancelPictureFail' to 'cancelPic...
2017-08-15 Emilian PeevMerge "Camera: Switch 'cancelPictureFail' to 'cancelPic...
2017-08-11 Tomasz WasilczykMerge "Update broadcastradio HAL 1.0 VTS tests." into...
2017-08-11 Tomasz WasilczykMerge "Update broadcastradio HAL 1.0 VTS tests." into...
2017-08-10 Myles WatsonMerge "Bluetooth: Check the number of file descriptors...
2017-08-10 Myles WatsonMerge "Bluetooth: Add OWNERS file for default/" into...
2017-08-10 Myles WatsonNFC: Add OWNERS file for default/
2017-08-09 Peng XuMerge "Skip direct report test if sensor is not availab...
2017-08-09 Peng XuMerge "Skip direct report test if sensor is not availab...
2017-08-09 Roshan Piuswifi(vts): Remove a tight loop of toggling wifi state
2017-08-09 Erik KlineMerge "Fix typo in in offload control VTS test" into...
2017-08-08 yinxuMerge "Add the error code "OPERATION_NOT_ALLOWED" and...
2017-08-08 Roshan Piuswifi(vts): Ignore IWifi.stop() returning ERROR_NOT_AVAI...
2017-08-08 Erik KlineMerge "Refactor and expand tetheroffload Control and...
2017-08-08 Tyler WearMerge "Tetheroffload Control and Config VTS" into oc...
2017-08-08 Ram Mohan Mbug fix: handle OMX_EventBufferFlag events am: c8df8940e1
2017-08-08 Ram Mohan Mbug fix: handle OMX_EventBufferFlag events
2017-08-03 Ruchi Kandoinfc: NCI 2.0: Add CORE_INIT_CMD for NCI 2.0 am: 029633dcd0
2017-08-03 Ruchi Kandoinfc: NCI 2.0: Add CORE_INIT_CMD for NCI 2.0
2017-08-03 Chia-I WuMerge "graphics: ignore/reduce spurious vsync in VTS...
2017-08-02 Yin-Chia YehMerge "Camera: reset callback after test done" into...
2017-08-02 sqianresolve merge conflicts of 345a396c to oc-dr1-dev
2017-08-01 Yin-Chia YehMerge "Camera: reset callback after test done" into...
2017-08-01 Shuo QianMerge "Add EMPTY_RECORD for getDeviceIdentity" into...
2017-08-01 Shuo QianMerge "Add corresponding error code to fix vts test...
2017-08-01 Shuo QianMerge "Add corresponding error code to fix vts test...
2017-08-01 Shuo QianMerge "Add corresponding error code to fix vts test...
2017-08-01 Kevin RocardMerge "Audio policy config xsd: add missing gains and...
2017-08-01 Kevin RocardMerge "Audio policy config xsd: add missing gains and...
2017-07-31 Sohani RaoMerge "Wifi Offload HAL: Improve VTS tests for scanConf...
2017-07-31 Emilian PeevMerge "NO PARTIAL RERUN Camera: Update stream consumer...
2017-07-31 Emilian PeevMerge "NO PARTIAL RERUN Camera: Update stream consumer...
2017-07-31 Emilian PeevMerge "Camera: Update stream consumer usage flag" into...
2017-07-31 Yin-Chia YehCamera: fix various VTS issues am: a0dd95d45d -s ours
2017-07-31 Yin-Chia YehCamera: fix various VTS issues
2017-07-29 Nathan HaroldRadioV1_1 VTS Tests: startKeepalive, stopKeepalive
2017-07-28 Shuo QianMerge "Add vts test for setCarrierInfoForImsiEncryption...
2017-07-28 Roshan PiusMerge "wifi(hidl): Modify the SAR power levels interfac...
2017-07-27 Yin-Chia YehMerge "Camera: fix various VTS issues" into oc-dr1-dev
2017-07-26 Yin-Chia YehMerge "Camera: reset callback after test done" into...
2017-07-26 Ying XuMerge "Fix VTS errors of the network scan API" into...
2017-07-26 Zhuoyao ZhangMerge "Move android.hardware.tests.msgq@1.0-impl to...
2017-07-26 Zhuoyao ZhangMove android.hardware.tests.msgq@1.0-impl to system.img
2017-07-26 Zhuoyao ZhangMerge "Move all hidl_test dependencies to the system...
2017-07-25 Eino-Ville TalvalaMerge "Camera: Don't enforce result metadata queue...
2017-07-25 Eino-Ville TalvalaMerge "Camera: Don't enforce result metadata queue...
2017-07-25 Andrew ScullMerge "Weaver: functional VTS tests" into oc-dr1-dev
2017-07-25 Andrew ScullMerge "OemLock functional VTS test." into oc-dr1-dev
2017-07-25 Eino-Ville TalvalaMerge "Camera: Don't enforce result metadata queue...
2017-07-25 Roshan Piussupplicant(vts): Remove start/stop framework am: 80599435bd
2017-07-25 Roshan Piussupplicant(vts): Remove start/stop framework
2017-07-25 Shuo QianMerge "Add Sim absent assertion in the 1.0 setup" into...
2017-07-25 Shuo QianMerge "Add Sim absent assertion in the setup" into...
2017-07-25 Shuo QianMerge "Add Sim absent assertion in the 1.0 setup" into...
2017-07-24 Sanket PadaweMerge "Update VTS tests so that more tests pass for...
2017-07-24 Roshan PiusMerge "supplicant(vts): Remove start/stop framework...
2017-07-22 Stanley TngMerge "Fixed the HCI ACL Header definitions for PB...
2017-07-22 Stanley TngMerge "Fixed the HCI ACL Header definitions for PB...
2017-07-22 Legler WuUpdate VTS tests so that Mediatek pass more VTS for...
2017-07-22 Legler WuUpdate VTS tests so that Mediatek pass more VTS for O.
2017-07-21 Shuo QianMerge "Update IRadioResponse.hal documentation" into...
2017-07-21 Shuo QianMerge "Update IRadioResponse.hal documentation" into...
2017-07-21 Etan CohenMerge "[HAL] Invalidate chip before shutting down legac...
2017-07-21 Shuo QianMerge "Fix some VTS for 2017 devices" into oc-dev am...
2017-07-21 Shuo QianMerge "Fix some VTS for 2017 devices" into oc-dev
2017-07-20 Ying XuMerge " Add VTS code for the network scan API" into...
2017-07-20 Kevin RocardAudio VTS: Change test utility from dyn to static lib
2017-07-19 Chia-I WuMerge "graphics: sideband streams are not buffers"...
2017-07-19 Shuo QianMerge changes from topic 'b/62584347' into oc-dr1-dev
2017-07-18 Roshan PiusMerge "wifi: Add the missing RTT capabilities" into...
2017-07-18 Etan Cohen[VTS][NAN] Restore NAN test: configure for device support
2017-07-18 Keun Soo YimAccept a command line arg (nan_on) in wifi vts
2017-07-17 Shuo QianMerge "Fix some VTS for 2017 devices" into oc-dr1-dev
2017-07-17 Shuo QianMerge "Add RadioIndication for Radio VTS test" into...
2017-07-14 Roshan PiusMerge "supplicant(vts): Remove dependency on libwifi_ha...
2017-07-14 Philip CuadraMerge "Add powerHintAsync functionality" into oc-dr1-dev
2017-07-14 Pawin VongmasaMerge "Print test information to the target device...
2017-07-13 Amit MahajanMerge "Add an empty 1.1 ISap interface." into oc-dr1-dev
2017-07-13 Roshan PiusMerge "wifi(implementation): Set/Reset TX power limit...
2017-07-12 Steven MorelandRemove configstore from the list of O-MR1 HALs.
2017-07-12 Sundong AhnMerge "Configstore HAL is down-revisioned to 1.0" into...
2017-07-12 Sundong AhnConfigstore HAL is down-revisioned to 1.0
2017-07-11 Myles WatsonBluetooth: Change CHECK() to LOG_ALWAYS_FATAL()
2017-07-07 Mikhail NaganovMerge "Revert of "Audio: Add XML schema for audio effec...
2017-07-07 Steven MorelandMerge "Freeze wifi 1.1 interface." into oc-dr1-dev
2017-07-07 Peng XuMerge "Relax accelerometer events norm check" into...
2017-07-06 Roshan PiusMerge changes from topic 'wifi_1_1' into oc-dr1-dev
2017-07-06 Peng QiBT HAL H4 write flow
2017-07-06 Jae ShinMerge "Add structural test VtsHalConfigstoreV1_1Target...
2017-07-05 Etan CohenMerge "[AWARE] Pass through full structure for end...
2017-06-30 Jae ShinMerge "Assert getService does not return nullptr" into...
2017-06-30 Emilian PeevMerge "Camera: Try adding a passthrough legacy service...
2017-06-30 Emilian PeevCamera: Try to test additional types of camera provider...
next