]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - audio
Merge "matrix: Enforce kernel requirements in OTA only when flag is set."
[android/platform-hardware-interfaces.git] / audio /
2018-06-13 Zhuoyao ZhangMerge "Include libhidl-gen-utils to HAL tests"
2018-06-12 Treehugger RobotMerge "Do not install assembled framework matrix to...
2018-06-08 Treehugger RobotMerge "Fix bug in VTS attestation cert verification."
2018-05-17 Treehugger RobotMerge "Audio HAL HIDL wrapper: Fix incorrect conversion...
2018-05-05 Kevin RocardAudio HAL HIDL wrapper: Fix incorrect conversion of...
2018-04-26 Dan StozaMerge "graphics: add libhwc2on{1,fb}adapter"
2018-04-23 Kevin RocardMerge "Audio: setParam improve status_t to Result consi...
2018-04-20 Kevin RocardAudio: setParam improve status_t to Result consistency
2018-03-12 Aniket Kumar Lataaudio: Register Bluetooth service with audio HAL
2018-01-23 Badhri Jagan SridharanMerge "Usb: HIDL: UsbGadget hal"
2018-01-18 Treehugger RobotMerge "Camera: Fix hotplug"
2018-01-18 Treehugger RobotMerge "Update makefiles for audio."
2018-01-17 Steven MorelandUpdate makefiles for audio.
2018-01-04 Treehugger RobotMerge "Remove empty generates clause."
2018-01-02 Treehugger RobotMerge "SIM slot related interface changes"
2017-12-22 Treehugger RobotMerge "Add debug output for lights."
2017-12-21 Mikhail Naganovaudio: Fix StreamOut ownership in default wrapper
2017-12-06 Xin LiDO NOT MERGE: Merge Oreo MR1 into master
2017-12-05 Zhuoyao ZhangMerge "Convert boot, memtrack and power hal to use...
2017-12-04 Zhuoyao ZhangMerge "Convert boot, memtrack and power hal to use...
2017-12-04 Michael SchwartzMerge "Remove IOemHook from matrix in P"
2017-12-02 Howard ChenMerge "Add more test methods to IMemoryTest"
2017-12-02 Howard ChenMerge "Add more test methods to IMemoryTest"
2017-12-01 Dan WillemsenFix problem found with host bionic fortify checks
2017-11-29 Chih-Hung HsiehMerge "Use -Werror in hardware/interfaces/automotive...
2017-11-29 Treehugger RobotMerge "Use -Werror in hardware/interfaces/automotive... android-o-mr1-iot-preview-6
2017-11-29 Kevin RocardAdd the audio team as owner of the audio VTS
2017-11-29 Mikhail NaganovAdd OWNERS for audio-related HAL default implementations
2017-11-29 Daniel Van VeenMerge "Fix inequality typo in StreamIn::getCapturePosition"
2017-11-29 Kevin RocardAdd the audio team as owner of the audio VTS
2017-11-29 Mikhail NaganovAdd OWNERS for audio-related HAL default implementations
2017-11-29 Treehugger RobotMerge "Fix inequality typo in StreamIn::getCapturePosition"
2017-11-29 Steven MorelandMerge "Remove subdirs"
2017-11-29 Treehugger RobotMerge "Remove subdirs"
2017-11-29 Badhri Jagan SridharanMerge "usb: Add owner file"
2017-11-29 Treehugger RobotMerge "usb: Add owner file"
2017-11-29 Steven MorelandMerge "Update tests makefile for change."
2017-11-29 Daniel Van VeenFix inequality typo in StreamIn::getCapturePosition
2017-11-29 Treehugger RobotMerge "Update tests makefile for change."
2017-11-29 Steven MorelandRemove subdirs
2017-11-29 TreeHugger RobotMerge "Remove subdirs" into stage-aosp-master
2017-11-29 Chih-Hung HsiehUse -Werror in hardware/interfaces/biometrics/fingerprint
2017-11-28 Steven MorelandRemove subdirs
2017-11-28 Chih-Hung HsiehMerge "Use -Werror in hardware/interfaces/automotive...
2017-11-28 Treehugger RobotMerge "Use -Werror in hardware/interfaces/automotive...
2017-11-28 Chih-Hung HsiehMerge "Use -Werror in hardware/interfaces"
2017-11-28 Treehugger RobotMerge "Use -Werror in hardware/interfaces"
2017-11-28 Chih-Hung HsiehMerge "Use -Werror in hardware/interfaces/audio"
2017-11-28 Treehugger RobotMerge "Use -Werror in hardware/interfaces/audio"
2017-11-28 Chih-Hung HsiehMerge "Use -Werror in hardware/interfaces/light/2.0"
2017-11-28 Chih-Hung HsiehUse -Werror in hardware/interfaces/automotive/vehicle
2017-11-28 Chih-Hung HsiehUse -Werror in hardware/interfaces/audio
2017-11-28 Steven MorelandMerge "Test for references to typedef'd enum."
2017-11-27 Steven MorelandMerge "Additional tests for enum iteration."
2017-11-22 Jiyong ParkMerge "DO NOT MERGE: android.hardware.graphics.allocato...
2017-11-22 Iris ChangMerge "Fix Keymaster VTS for OpenSSL error code change"
2017-11-20 Badhri Jagan SridharanInitialize usb_count in the setup funtion.
2017-11-17 Ryan CampbellTransfer VTS test ownership.
2017-11-16 Roshan Piuswifi(vts): Skip tests if feature not supported
2017-11-15 Zhuoyao ZhangMerge "Convert Renderscript Hal test to test against...
2017-11-15 Iris ChangMerge "VTS: fix RadioHidlTest.getAvailableNetworks...
2017-11-15 Treehugger RobotMerge "VTS: fix RadioHidlTest.getAvailableNetworks...
2017-11-15 Zhuoyao ZhangConvert GraphicsMapper Hal test to test against each...
2017-11-14 Xin LiMerge commit '1a06284b24f5eb7bb9c1fea0817da8898b3b1bff...
2017-11-14 Yifan HongMerge "Revert "Add micro-vts.sh""
2017-11-13 Yifan HongMerge "Add micro-vts.sh"
2017-11-11 Steven MorelandMerge changes from topic "hidl-soong-plugin"
2017-11-11 Treehugger RobotMerge changes from topic "hidl-soong-plugin"
2017-11-10 Steven MorelandUpdate makefiles for hidl_interface.
2017-11-07 Steven MorelandMerge "Automatic mk -> bp."
2017-11-07 Treehugger RobotMerge "Automatic mk -> bp."
2017-11-03 Steven MorelandAutomatic mk -> bp.
2017-10-19 Sanket PadaweFix VTS test which turns off radio. am: 536818d17a...
2017-10-19 Sanket PadaweFix VTS test which turns off radio. am: 536818d17a...
2017-10-18 Sanket PadaweFix VTS test which turns off radio. am: 536818d17a
2017-10-18 Sanket PadaweFix VTS test which turns off radio. am: 536818d17a
2017-10-18 Sanket PadaweFix VTS test which turns off radio.
2017-10-18 sqianMerge "Add REQUEST_NOT_SUPPORTED / SIM_ABSENT for vts...
2017-10-18 Steven MorelandMerge "Update Light extension example to match docs...
2017-10-18 Steven MorelandMerge "Update Light extension example to match docs...
2017-10-18 Steven MorelandMerge "Update Light extension example to match docs."
2017-10-18 Treehugger RobotMerge "Update Light extension example to match docs."
2017-10-18 Tri VoMerge "Set pipe size to >1MB for debugDump test cases...
2017-10-18 Tri VoMerge "Set pipe size to >1MB for debugDump test cases...
2017-10-18 Tri VoMerge "Set pipe size to >1MB for debugDump test cases."
2017-10-18 Treehugger RobotMerge "Set pipe size to >1MB for debugDump test cases."
2017-10-18 Chih-Hung HsiehUse -Werror in hardware/interfaces am: ceb435f2ba am...
2017-10-18 Chih-Hung HsiehUse -Werror in hardware/interfaces am: ceb435f2ba
2017-10-18 Chih-Hung HsiehUse -Werror in hardware/interfaces
2017-10-17 Tri VoSet pipe size to >1MB for debugDump test cases.
2017-10-17 Ram Mohan MMerge "bug fix: during fatal fails bypass freeNode...
2017-10-17 TreeHugger RobotMerge "bug fix: during fatal fails bypass freeNode...
2017-10-17 Sooraj SasindranMerge "Enhanced network scan request" am: 8e5f008ae6...
2017-10-17 Sooraj SasindranMerge "Enhanced network scan request" am: 8e5f008ae6
2017-10-17 Sooraj SasindranMerge "Enhanced network scan request"
2017-10-17 Erik Klinetetheroffload VTS: fix stopOffload test conditions
2017-10-16 Janis DanisevskisRename libkeymaster to libkeymaster_staging am: 8cd5614...
2017-10-16 Janis Danisevskislibkeymaster1 split to libkeymaster and _portable am...
2017-10-16 Janis DanisevskisRename libkeymaster to libkeymaster_staging am: 8cd5614...
2017-10-16 Janis Danisevskislibkeymaster1 split to libkeymaster and _portable am...
next