]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - audio
Merge "Tolerate 1 sv status in GNSS blacklist VTS test" into pie-vts-dev
[android/platform-hardware-interfaces.git] / audio /
2018-08-28 Treehugger RobotMerge "Tolerate 1 sv status in GNSS blacklist VTS test...
2018-08-28 Treehugger RobotMerge "VTS: Do not require XML for Audio effect V2...
2018-08-28 Treehugger RobotMerge "Camera: Don't hold 'mLock' when closing the...
2018-08-28 Treehugger RobotMerge "Audio VTS was testing wrong uninitialized variab...
2018-08-28 Kevin RocardVTS: Do not require XML for Audio effect V2
2018-08-28 Kevin RocardAudio VTS was testing wrong uninitialized variable...
2018-08-20 Treehugger RobotMerge "Add back keymaster@4.0 hash." into pie-vts-dev
2018-08-20 Yin-Chia Yeh[automerger skipped] resolve merge conflicts of cd02298...
2018-08-20 Kevin RocardEffect VTS: Allow an effect proxy as pre/post processing
2018-08-13 sqianresolve merge conflicts of 898d05a713a693670cd450ff3f50...
2018-08-10 Pawin Vongmasaresolve merge conflicts of b92f1d2e1be35b331b18589a8cde...
2018-08-10 Kevin Rocard[automerger skipped] Audio VTS: run tear-down hooks...
2018-08-10 Kevin RocardAudio VTS: run tear-down hooks in LIFO instead of FIFO
2018-08-10 sqian[automerger skipped] Fix setBandMode. am: ab2b8bf919...
2018-08-02 Yin-Chia Yehresolve merge conflicts of cd02298b46cfb17954555e0f1d32...
2018-07-19 Kevin RocardEffect VTS: Allow an effect proxy as pre/post processing
2018-07-16 sqianresolve merge conflicts of dfa79a6292a42dd8609053febd8d...
2018-07-16 Treehugger RobotMerge "Add NONE for LceService" into oreo-vts-dev
2018-07-12 Pawin Vongmasaresolve merge conflicts of b92f1d2e1be35b331b18589a8cde...
2018-07-12 Kevin Rocard[automerger skipped] Audio VTS: run tear-down hooks...
2018-06-29 Kevin RocardAudio VTS: run tear-down hooks in LIFO instead of FIFO
2018-06-29 Kevin RocardAudio VTS: run tear-down hooks in LIFO instead of FIFO
2018-06-18 sqian[automerger skipped] Fix setBandMode.
2018-06-06 David GrossMerge "Document unspecified dimensions." into pi-dev
2018-06-05 Steve PaikMerge "Add initial values for properties" into pi-dev
2018-05-31 Joshua MccloskeyMerge "Modified tests to account for different director...
2018-05-31 TreeHugger RobotMerge "Minor corrections to the Keymaster4 documentatio...
2018-05-30 TreeHugger RobotMerge "graphics: COLORIMETRIC is optional for HDR modes...
2018-05-30 Yu-Han YangMerge "Update VTS test to blacklist only non-GPS satell...
2018-05-29 TreeHugger RobotMerge "audio hal: Add 'interface' declarations for...
2018-05-25 Mikhail Naganovaudio hal: Add 'interface' declarations for IDeviceFact...
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc am: 5de1ae23f9...
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc am: 5de1ae23f9
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc am: 9886d749d4
2018-05-24 Pawin VongmasaAdd multichannel support
2018-05-24 TreeHugger RobotMerge "Move Keymaster docs into HAL" into pi-dev
2018-05-21 TreeHugger RobotMerge "Remove ConfigFlags" into pi-dev
2018-05-21 TreeHugger RobotMerge "[AWARE] Developer documentation on HAL usage...
2018-05-19 TreeHugger RobotMerge "Update comments for doc comments." into pi-dev
2018-05-18 TreeHugger RobotMerge "Update default config areaId's" into pi-dev
2018-05-18 Steven MorelandUpdate comments for doc comments.
2018-05-18 Kevin RocardMerge "VTS tests should be static" into pi-dev
2018-05-17 Kevin RocardVTS tests should be static
2018-05-11 Chong Zhangcas: do not use hidl_memory if size is > SIZE_MAX
2018-05-10 Chao YanMerge "Added fake VHAL value generator based on JSON...
2018-05-07 Kiran RachuriMerge "Add HVAC properties" into pi-dev
2018-05-05 android-build-team... Merge changes I29bbf6bf,Ib0b03fb6 into pi-dev
2018-05-03 Marissa WallMerge "graphics: add new gralloc1 functions to passthro...
2018-05-02 android-build-team... Merge "Camera: fix first launch api level logic" into...
2018-05-02 Kevin RocardAudio HAL HIDL wrapper: Fix incorrect conversion of...
2018-05-02 Kevin RocardAudio V4 VTS: test setter even if getter is NOT_SUPPORTED
2018-05-01 android-build-team... Merge "matrix: copy kernel configs to subdirectory...
2018-04-30 Gene KarshenboymMerge "Add check for empty RDS_PS." into pi-dev
2018-04-30 Gene KarshenboymMerge "Extend tune workaround time." into pi-dev
2018-04-30 Scott RandolphMerge "Remove ENV_CABIN_TEMPERATURE from VHal" into...
2018-04-30 android-build-team... Merge "Add AUDIO_MICROPHONE_CHANNEL_MAPPING_CNT." into...
2018-04-30 jiabinAdd AUDIO_MICROPHONE_CHANNEL_MAPPING_CNT.
2018-04-27 Michael ButlerMerge "NNAPI: sync NDK and HAL documentation" into...
2018-04-27 Yifan HongMerge "Restore kernel requirements for frozen matrices...
2018-04-27 android-build-team... Merge "Camera: check return value of callback" into...
2018-04-27 Jiabin HuangMerge "Add vts for microphone enumeration APIs." into...
2018-04-26 TreeHugger RobotMerge "Fix wrongly initialized test key." into pi-dev
2018-04-26 Mika RaentoMerge "Update namespace to match framework/ml/nn" into...
2018-04-26 Mika RaentoMerge "Update neuralnetworks/*/types.hal to match impl...
2018-04-26 TreeHugger RobotMerge "Use configArray for HVAC_POWER_ON" into pi-dev
2018-04-26 Scott RandolphMerge "Rename EV_CONNECTOR_TYPE enums" into pi-dev
2018-04-26 Michael Butler[automerger skipped] Relax NeuralNetwork's VTS positive...
2018-04-25 jiabinAdd vts for microphone enumeration APIs.
2018-04-25 Kevin RocardMerge changes I2f70f2ec,I9d77a59e,Ied3a657d,Ib6e9d017...
2018-04-24 Kevin RocardAudio V4: Add missing VTS
2018-04-24 Roshan PiusMerge "wifi(implementation): Use stub for |read_packet_...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris ChangVTS: fix RadioHidlTest.getAvailableNetworks issue am...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Kevin RocardAudio V4: VTS Pause was testing resume
2018-04-24 Kevin RocardAudio V4: factorize analyzeStatus
2018-04-24 Wei WangMerge "dumpstate: add interface into rc file" into...
2018-04-23 Eric LaurentMerge "Audio V4: dump effect HAL using the standard...
2018-04-23 Michael ButlerMerge "NNAPI: Create VTS _relaxed tests for newly added...
2018-04-23 Kevin RocardAudio V4: fix invalid SupportedChannelMasks test
2018-04-23 TreeHugger RobotMerge "Deprecate nfc@1.0 for P." into pi-dev
2018-04-21 TreeHugger RobotMerge changes I41328afc,Ie543519f into pi-dev
2018-04-21 Kevin RocardAudio V4: setMode VTS incorrectly assume 0 was invalid
2018-04-21 Kevin RocardAudio V4: XSD device category was missing hearing aid
2018-04-21 Kevin RocardAudio V4: some legacy getSupported can return NOT_SUPPORTED
2018-04-21 Kevin RocardAudio V4: Improve VTS error messages
2018-04-21 Kevin RocardAudio: setParam improve status_t to Result consistency
2018-04-21 Kevin RocardAudio: make core/4.0/default/Util.h version dependant
2018-04-20 Kevin RocardAudio V4: dump effect HAL using the standard debug()
2018-04-20 Michael ButlerMerge "Update NNAPI OWNERS file -- VTS" into pi-dev
2018-04-20 TreeHugger RobotMerge "Update Android.bp via update-makefiles.sh" into...
2018-04-19 Kevin RocardMerge "Revert "Audio: setParam improve status_t to...
2018-04-19 Kevin RocardRevert "Audio: setParam improve status_t to Result...
2018-04-19 Kevin RocardMerge "Audio: setParam improve status_t to Result consi...
2018-04-19 Pankaj KanwarMerge "persist ringbuffer to flash when vendor hal...
2018-04-18 Scott RandolphMerge "Update VHAL comments to clarify useage" into...
2018-04-18 Mikhail Naganovaudio: Add VTS tests for new interface methods in V4.0
next