]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - bluetooth/1.0/default/service.cpp
Apply clang-format to Bluetooth related HAL code
[android/platform-hardware-interfaces.git] / bluetooth / 1.0 / default / service.cpp
2018-10-24 Jack HeApply clang-format to Bluetooth related HAL code
2017-08-17 Zhuoyao ZhangMove android.hardware.tests.libhwbinder@1.0-impl to...
2017-08-10 yinxuMerge "Add the error code "OPERATION_NOT_ALLOWED" and...
2017-08-10 Myles WatsonMerge "Bluetooth: Check the number of file descriptors"
2017-08-09 Myles WatsonMerge "Bluetooth: Add OWNERS file for default/"
2017-08-09 Myles WatsonNFC: Add OWNERS file for default/
2017-08-09 Justin YunManually update makefile for vndk-sp hidl libs.
2017-08-09 Steven MorelandUpdate makefiles for vndk enabled.
2017-08-08 Shuo QianMerge "Add Owners for radio vts"
2017-08-07 Tri VoUpdate comments for VtsHalTargetTestDefaults.
2017-08-04 Steven MorelandMerge changes from topic 'go-away-static-hidl-java'
2017-08-03 Shuo QianMerge "Add vts test for setCarrierInfoForImsiEncryption"
2017-08-03 Tri VoMerge changes from topic 'vts_deps'
2017-08-03 Ruchi Kandoinfc: NCI 2.0: Add CORE_INIT_CMD for NCI 2.0
2017-08-02 Sundong AhnChange dependency library
2017-07-31 Steven MorelandMerge "Update HIDL makefiles."
2017-07-28 yinxuFix VTS errors of the network scan API
2017-07-24 yinxuMerge " Add VTS code for the network scan API"
2017-07-21 Zhuoyao ZhangMove android.hardware.tests.msgq@1.0-impl to system.img
2017-07-20 Stanley TngMerge "Fixed the HCI ACL Header definitions for PB...
2017-07-20 Steven MorelandMove multithread impl to system.
2017-07-18 sqianresolve merge conflicts of 6ecc54a7 to stage-aosp-master
2017-07-18 Steven MorelandMerge "Move all hidl_test dependencies to the system...
2017-07-17 sqianAdd RadioIndication for Radio VTS test
2017-07-14 Michael ButlerMerge "Added protections to RenderScript VTS class...
2017-07-14 Timur IskhakovInterface for configureRpcThreadpool tests
2017-07-11 sqianAdd radio 1.1 vts test folder.
2017-07-07 Myles WatsonMerge "Bluetooth: Change CHECK() to LOG_ALWAYS_FATAL()"
2017-07-07 Jakub PawlowskiMerge "Make RawAddress into a class (4/4)"
2017-07-07 Jakub PawlowskiMerge "Make RawAddress into a class (4/4)"
2017-07-06 Peng QiBT HAL H4 write flow
2017-06-26 TreeHugger RobotMerge "Revert "EVS: Android.bp -> Android.mk""
2017-06-17 Bailey ForrestMerge "Include missing headers" am: 1bbe51d0b5
2017-06-16 nharoldMerge "Radio Keepalive HAL" am: 95f0176afa
2017-06-16 Ruchi KandoiNfc: Vts: modify WriteInvalidAndThenValidCommand am...
2017-06-16 Ruchi KandoiMerge "Support NCI 2.0 for NFC VTS" am: 7b62681f43
2017-06-14 Chih-hung HsiehMerge "Add OWNERS in hardware/interfaces" am: 37e00854d9
2017-06-14 TreeHugger RobotMerge "Fixed flaky RenderScript VTS Test" into oc-dev
2017-06-13 pkanwarRadio Interface changes to allow the modem to query...
2017-06-11 Pankaj KanwarMerge "Radio Interface changes to allow the modem to...
2017-06-09 Myles WatsonBluetooth: Call vendor cleanup() in Close() am: 9eee83093f
2017-06-06 TreeHugger RobotMerge "Move utility classes in a separate static target"
2017-06-06 TreeHugger RobotMerge "Implemented VTS for Dumpstate HIDL."
2017-06-02 Miao WangMerge "[RenderScript] Use OVERRIDE_RS_DRIVER string...
2017-06-02 Miao WangMerge "[RenderScript] Use OVERRIDE_RS_DRIVER string...
2017-06-01 TreeHugger RobotMerge "Revert "audiohal: Add diagnostics to investigate...
2017-05-31 sqianresolve merge conflicts of 0e50326a to oc-dev-plus...
2017-05-31 TreeHugger RobotMerge "Validate certificate names."
2017-05-31 TreeHugger RobotMerge "Verify that attestation root is a valid self...
2017-05-31 TreeHugger RobotMerge "Check HAL return codes."
2017-05-31 Kevin RocardMerge "Revert "Temporary disable tests failing tests...
2017-05-31 Steven Morelandconfigstore-utils: vendor_available
2017-05-31 Jayant ChowdharyMerge "configstore-utils: vendor_available" into oc-dev
2017-05-31 TreeHugger RobotMerge "GNSS HAL radio group for E911 SUPL" into oc-dev
2017-05-31 TreeHugger RobotMerge "Compile manager-lib shared library"
2017-05-30 TreeHugger RobotMerge "Camera: fix release fence FD leaks" into oc-dev
2017-05-30 TreeHugger RobotMerge "GNSS HAL radio group for E911 SUPL"
2017-05-27 Myles WatsonBluetooth: Remove scheduler-service dependency am:...
2017-05-27 Myles WatsonBluetooth: Remove scheduler-service dependency
2017-05-26 Myles WatsonBluetooth: Remove scheduler-service dependency
2017-05-26 TreeHugger RobotMerge "Fix typos in IEvsEnumerator descriptive comment...
2017-05-23 TreeHugger RobotMerge "graphics: set maxThreads to 4 for the allocator"
2017-05-19 Etan CohenMerge "[WIFI] Remove dependency on vendor-specific...
2017-05-16 Grace ChenMerge "Support different SIM power states"
2017-05-16 TreeHugger RobotMerge changes from topic 'audio-primary-hal-vts-fix...
2017-05-16 Jeff TinkerMerge "Revert "Fix resource leaks in drm hal"" into...
2017-05-15 Zhuoyao ZhangMerge "Omx vts tests." into oc-dev
2017-05-15 TreeHugger RobotMerge "Fix resource leaks in drm hal" into oc-dev
2017-05-12 Steven MorelandMerge "Update makefiles from anywhere."
2017-05-12 Ying XuMerge "Add the new RIL requests to start/stop network...
2017-05-12 Chia-I WuMerge "graphics: set maxThreads to 4 for the composer...
2017-05-12 TreeHugger RobotMerge "Eliminate redundant #includes and a missing...
2017-05-12 TreeHugger RobotMerge "Add evs and vehicle hal to compatibility matrix"
2017-05-12 Myles WatsonBluetooth: Add a second thread for the scheduler am...
2017-05-12 Myles WatsonMerge "Bluetooth: Add a second thread for the scheduler...
2017-05-12 Myles WatsonMerge "Bluetooth: Add a second thread for the scheduler"
2017-05-12 Treehugger RobotMerge "Bluetooth: Add a second thread for the scheduler"
2017-05-12 Myles WatsonBluetooth: Add a second thread for the scheduler
2017-05-12 Myles WatsonBluetooth: Add a second thread for the scheduler
2017-05-11 Myles WatsonBluetooth: Add a second thread for the scheduler
2017-01-24 Keun Soo YimMerge "Use the feature-based precondition checking...
2017-01-23 TreeHugger RobotMerge "Make some of the fields comments more clear...
2017-01-23 TreeHugger RobotMerge "Use MQDescriptor typedefs for cleanup"
2017-01-20 TreeHugger RobotMerge "Camera: binderize camera hal"
2017-01-20 TreeHugger RobotMerge "Vehicle HAL: return ACCESS_DENIED when appropriate"
2017-01-20 Crystal QinMerge "Add the new key purpose to types.hal as well."
2017-01-20 Yuexi MaMerge "vts test project init for radio hal"
2017-01-19 Jim MillerMerge "Fix fingerprint crypto operations."
2017-01-19 Eric LaurentMerge "audio: add support for stub HAL in HIDL mode"
2017-01-19 Roshan Piuswifi(vts): Generate the .vts files
2017-01-19 Roshan Piuswifi(interface): Use the "bitfield" type for masks
2017-01-19 Roshan Piussupplicant(interface): Add sta network idstr & ft key...
2017-01-19 Roshan Piussupplicant(interface): Add missing STA callbacks
2017-01-19 Roshan Piussupplicant(interface): Add various WPS device params
2017-01-19 Roshan Piussupplicant(interface): Add P2P iface methods/cbs
2017-01-19 Roshan PiusMerge changes from topics 'id_str_supplicant_hidl'...
2017-01-19 TreeHugger RobotMerge "Remove useless Android.mk files."
2017-01-19 TreeHugger RobotMerge "Revert "thermal: add getUndefinedTemperature...
2017-01-19 Steven MorelandMerge "Ran update-makefiles.sh."
2017-01-19 TreeHugger RobotMerge "Add boot profiling tests."
next