]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - camera
matrix: nn@1.0-1
[android/platform-hardware-interfaces.git] / camera /
2018-05-07 Kiran RachuriMerge "Add HVAC properties" into pi-dev
2018-05-05 android-build-team... Merge changes I29bbf6bf,Ib0b03fb6 into pi-dev
2018-05-03 Marissa WallMerge "graphics: add new gralloc1 functions to passthro...
2018-05-03 android-build-team... Merge "Camera: Set partial results in result batcher...
2018-05-03 Emilian PeevCamera: Set partial results in result batcher
2018-05-02 android-build-team... Merge "Camera: fix first launch api level logic" into...
2018-05-02 Yin-Chia YehCamera: fix first launch api level logic
2018-04-30 Scott RandolphMerge "Remove ENV_CABIN_TEMPERATURE from VHal" into...
2018-04-30 android-build-team... Merge "Add AUDIO_MICROPHONE_CHANNEL_MAPPING_CNT." into...
2018-04-27 Michael ButlerMerge "NNAPI: sync NDK and HAL documentation" into...
2018-04-27 Yifan HongMerge "Restore kernel requirements for frozen matrices...
2018-04-27 android-build-team... Merge "Camera: check return value of callback" into...
2018-04-27 Yin-Chia YehCamera: check return value of callback
2018-04-26 TreeHugger RobotMerge "Fix wrongly initialized test key." into pi-dev
2018-04-26 Mika RaentoMerge "Update namespace to match framework/ml/nn" into...
2018-04-26 Michael Butler[automerger skipped] Relax NeuralNetwork's VTS positive...
2018-04-25 Kevin RocardMerge changes I2f70f2ec,I9d77a59e,Ied3a657d,Ib6e9d017...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris ChangVTS: fix RadioHidlTest.getAvailableNetworks issue am...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Wei WangMerge "dumpstate: add interface into rc file" into...
2018-04-23 Eric LaurentMerge "Audio V4: dump effect HAL using the standard...
2018-04-23 Michael ButlerMerge "NNAPI: Create VTS _relaxed tests for newly added...
2018-04-21 TreeHugger RobotMerge changes I41328afc,Ie543519f into pi-dev
2018-04-20 Shuo QianMerge "Sim Status Present VTS" into pi-dev
2018-04-20 Michael ButlerMerge "Update NNAPI OWNERS file -- VTS" into pi-dev
2018-04-20 TreeHugger RobotMerge "Update Android.bp via update-makefiles.sh" into...
2018-04-19 Kevin RocardMerge "Revert "Audio: setParam improve status_t to...
2018-04-19 Kevin RocardMerge "Audio: setParam improve status_t to Result consi...
2018-04-19 Pankaj KanwarMerge "persist ringbuffer to flash when vendor hal...
2018-04-18 Scott RandolphMerge "Update VHAL comments to clarify useage" into...
2018-04-18 Michael ButlerUpdate Android.bp via update-makefiles.sh
2018-04-16 Shuo QianMerge "Radio Sap 1.2 default implementation" into pi-dev
2018-04-16 TreeHugger RobotMerge "VTS tests for IWifiStaIface@1.2." into pi-dev
2018-04-13 Michael ButlerMerge "NNAPI: Add execution preference to prepareModel...
2018-04-13 TreeHugger RobotMerge "Add 4.14.0 kernel to all matrices." into pi-dev
2018-04-12 TreeHugger RobotMerge "Add "vendor." prefix to ro.camera.wrapper.hal3Tr...
2018-04-12 Jaekyun SeokAdd "vendor." prefix to ro.camera.wrapper.hal3TrebleMin...
2018-04-11 TreeHugger RobotMerge "VTS for Bluetooth A2DP HAL" into pi-dev
2018-04-11 TreeHugger RobotMerge "[AWARE][VTS] Add VTS tests for the Wi-Fi 1.2...
2018-04-10 Etan CohenMerge "[AWARE] Support a mix of 1.0 and 1.2 Callback...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 TreeHugger RobotMerge "Correct bug in HmacKeySharingTest" into pi-dev
2018-04-10 TreeHugger RobotMerge "Audio V4: Use of EffectFlags over bitfield<Effec...
2018-04-10 TreeHugger RobotMerge "Remove DiskStat checks from VTS Health HAL test...
2018-04-10 TreeHugger RobotMerge "Audio V4: Synchronize the devices between the...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support
2018-04-10 Emilian Peev[automerger skipped] Camera: Allocate graphics buffers...
2018-04-10 Emilian PeevCamera: Allocate graphics buffers via 'IAllocator'
2018-04-10 Emilian PeevCamera: Allocate graphics buffers via 'IAllocator'
2018-04-10 TreeHugger RobotMerge "Camera: Allocate graphics buffers via 'IAllocato...
2018-04-10 TreeHugger RobotMerge "Correct type of appData field" into pi-dev
2018-04-10 TreeHugger RobotMerge "Fix the spec for TENSOR_QUANT8_ASYMM to match...
2018-04-09 Chong ZhangMerge "cas: fix UAF in descrambler" into pi-dev
2018-04-09 Chong Zhang[automerger skipped] Merge "cas: fix UAF in descrambler...
2018-04-09 Chong ZhangMerge "cas: fix UAF in descrambler -- DO NOT MERGE...
2018-04-09 TreeHugger RobotMerge "camera: print the oversized result size" into...
2018-04-09 TreeHugger RobotMerge "configstore policy: add dgetdents64" into pi-dev
2018-04-09 Emilian PeevCamera: Allocate graphics buffers via 'IAllocator'
2018-04-07 Zhijun Hecamera: print the oversized result size
2018-04-06 Yifan HongMerge "health: update readme for writing kmesg" into...
2018-04-06 TreeHugger RobotMerge "Camera: various external camera fixes" into...
2018-04-05 TreeHugger RobotMerge "health 2.0: update readme to uninstall healthd...
2018-04-04 TreeHugger RobotMerge "Correct TripleDes tests." into pi-dev
2018-04-04 TreeHugger RobotMerge "Camera: use finer lock in external camera Output...
2018-04-04 TreeHugger RobotMerge "Camera: Check external camera v4l2 buffer size...
2018-04-03 TreeHugger RobotMerge changes from topic "nfc1.1" into pi-dev
2018-04-03 TreeHugger RobotMerge "Update VHAL types.hal" into pi-dev
2018-04-03 Emilian PeevCamera: Check external camera v4l2 buffer size
2018-04-02 TreeHugger RobotMerge changes Ibab77dce,I0829a91d into pi-dev
2018-04-02 TreeHugger RobotMerge "Update doc in Gnss Hal v1.1" into pi-dev
2018-04-02 Chia-I WuMerge "graphics: add RenderIntent and better HDR suppor...
2018-04-02 TreeHugger RobotMerge "Camera: Validate physical camera related metadat...
2018-03-30 TreeHugger RobotMerge "SetMacAddress in Vendor HAL" into pi-dev
2018-03-30 Enrico GranataMerge "Teach VehiclePropertyStore to not propagate...
2018-03-30 TreeHugger RobotMerge "Support query microphones information." into...
2018-03-30 Brian YoungMerge "Add "Unlocked device required" key API" into...
2018-03-30 Shuzhen WangCamera: Validate physical camera related metadata field...
2018-03-30 TreeHugger RobotMerge "Extend VHAL test property to allow inject events...
2018-03-30 Yuexi Maresolve merge conflicts of e41f291381eaafa2f9d946e85f94...
2018-03-29 TreeHugger RobotMerge "Fix the NNAPI HAL documentation about ADD and...
2018-03-29 Yuexi Maresolve merge conflicts of a9543fee6b3f5e9609206d3a21a4...
2018-03-29 Tom CherryMerge "Add BLOCK_SUSPEND capability for Bluetooth HAL...
2018-03-29 Yuexi Ma[automerger skipped] Merge "rename VtsHalEvsV1_0Target...
2018-03-29 Yuexi Ma[automerger skipped] Merge "rename VtsHalEvsV1_0Target...
2018-03-29 Yuexi MaMerge "rename VtsHalEvsV1_0Target module to VtsHalEvsV1...
2018-03-29 Tomasz WasilczykMerge "Update program list when switching bands." into...
2018-03-29 TreeHugger RobotMerge "Build DEVICE_FRAMEWORK_COMPATIBILITY_MATRIX_FILE...
2018-03-28 Michael ButlerMerge "NN validation tests" into pi-dev
2018-03-28 TreeHugger RobotMerge "Camera: Add Monochrome camera capability" into...
next