]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - compatibility_matrices
Merge "Allow REQUEST_NOT_SUPPORTED as an error for startNetworkScan" into pie-vts-dev
[android/platform-hardware-interfaces.git] / compatibility_matrices /
2018-08-20 Yin-Chia Yeh[automerger skipped] resolve merge conflicts of cd02298...
2018-08-20 Kevin RocardEffect VTS: Allow an effect proxy as pre/post processing
2018-08-13 sqianresolve merge conflicts of 898d05a713a693670cd450ff3f50...
2018-08-11 Michael WrightUpdate power HAL to version 1.3.
2018-08-10 Pawin Vongmasaresolve merge conflicts of b92f1d2e1be35b331b18589a8cde...
2018-08-10 Kevin Rocard[automerger skipped] Audio VTS: run tear-down hooks...
2018-08-10 Kevin RocardAudio VTS: run tear-down hooks in LIFO instead of FIFO
2018-08-10 sqian[automerger skipped] Fix setBandMode. am: ab2b8bf919...
2018-06-06 David GrossMerge "Document unspecified dimensions." into pi-dev
2018-05-30 Yu-Han YangMerge "Update VTS test to blacklist only non-GPS satell...
2018-05-25 TreeHugger RobotMerge "Fix tire pressure sensor property" into pi-dev
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc am: 5de1ae23f9...
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc am: 9886d749d4
2018-05-24 TreeHugger RobotMerge "Move Keymaster docs into HAL" into pi-dev
2018-05-24 TreeHugger RobotMerge "Activate HMAC sharing check." into pi-dev
2018-05-24 TreeHugger RobotMerge "configstore: configstore HAL uprev'ed to 1.1...
2018-05-23 TreeHugger RobotMerge "P requires 4.14.42" into pi-dev
2018-05-23 Jaesoo Leeconfigstore: configstore HAL uprev'ed to 1.1
2018-05-23 Yifan HongP requires 4.14.42
2018-05-21 TreeHugger RobotMerge "Remove ConfigFlags" into pi-dev
2018-05-18 TreeHugger RobotMerge "Update default config areaId's" into pi-dev
2018-05-18 Kevin RocardMerge "VTS tests should be static" into pi-dev
2018-05-17 TreeHugger RobotMerge "Camera: Append non-partial results" into pi-dev
2018-05-16 TreeHugger RobotMerge changes from topic "pi_matrix" into pi-dev
2018-05-16 TreeHugger RobotMerge "Composer 2.2: Fix readback docs" into pi-dev
2018-05-16 TreeHugger RobotMerge "Update kernel minor revision for P." into pi-dev
2018-05-16 Yifan Hongmatrix: broadcastradio@2.0::IBroadcastRadio/.*
2018-05-16 Yifan Hongmatrix: nn@1.0-1
2018-05-16 Yifan Hongmatrix: graphics.mapper@2.0-1
2018-05-16 Yifan Hongmatrix: graphics.composer@2.1-2
2018-05-16 Yifan HongUpdate kernel minor revision for P.
2018-05-11 Chong Zhangcas: do not use hidl_memory if size is > SIZE_MAX
2018-05-10 Chao YanMerge "Added fake VHAL value generator based on JSON...
2018-05-07 Kiran RachuriMerge "Add HVAC properties" into pi-dev
2018-05-05 android-build-team... Merge changes I29bbf6bf,Ib0b03fb6 into pi-dev
2018-05-03 Marissa WallMerge "graphics: add new gralloc1 functions to passthro...
2018-05-02 android-build-team... Merge "Camera: fix first launch api level logic" into...
2018-05-01 android-build-team... Merge "matrix: copy kernel configs to subdirectory...
2018-04-30 Scott RandolphMerge "Remove ENV_CABIN_TEMPERATURE from VHal" into...
2018-04-30 android-build-team... Merge "Add AUDIO_MICROPHONE_CHANNEL_MAPPING_CNT." into...
2018-04-30 Yifan Hongmatrix: copy kernel configs to subdirectory.
2018-04-27 Michael ButlerMerge "NNAPI: sync NDK and HAL documentation" into...
2018-04-27 Yifan HongMerge "Restore kernel requirements for frozen matrices...
2018-04-27 Yifan HongRestore kernel requirements for frozen matrices.
2018-04-26 TreeHugger RobotMerge "Fix wrongly initialized test key." into pi-dev
2018-04-26 Mika RaentoMerge "Update namespace to match framework/ml/nn" into...
2018-04-26 Michael Butler[automerger skipped] Relax NeuralNetwork's VTS positive...
2018-04-25 Kevin RocardMerge changes I2f70f2ec,I9d77a59e,Ied3a657d,Ib6e9d017...
2018-04-24 Roshan PiusMerge "wifi(implementation): Use stub for |read_packet_...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Wei WangMerge "dumpstate: add interface into rc file" into...
2018-04-23 Eric LaurentMerge "Audio V4: dump effect HAL using the standard...
2018-04-23 Michael ButlerMerge "NNAPI: Create VTS _relaxed tests for newly added...
2018-04-23 TreeHugger RobotMerge "Deprecate nfc@1.0 for P." into pi-dev
2018-04-23 Steven MorelandDeprecate nfc@1.0 for P.
2018-04-19 Kevin RocardMerge "Revert "Audio: setParam improve status_t to...
2018-04-19 Kevin RocardMerge "Audio: setParam improve status_t to Result consi...
2018-04-19 Pankaj KanwarMerge "persist ringbuffer to flash when vendor hal...
2018-04-18 Scott RandolphMerge "Update VHAL comments to clarify useage" into...
2018-04-16 Shuo QianMerge "Radio Sap 1.2 default implementation" into pi-dev
2018-04-16 TreeHugger RobotMerge "VTS tests for IWifiStaIface@1.2." into pi-dev
2018-04-13 Michael ButlerMerge "NNAPI: Add execution preference to prepareModel...
2018-04-13 TreeHugger RobotMerge "Add 4.14.0 kernel to all matrices." into pi-dev
2018-04-12 Yifan HongAdd 4.14.0 kernel to all matrices.
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 TreeHugger RobotMerge "Remove DiskStat checks from VTS Health HAL test...
2018-04-10 TreeHugger RobotMerge "Audio V4: Synchronize the devices between the...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Emilian Peev[automerger skipped] Camera: Allocate graphics buffers...
2018-04-09 Chong ZhangMerge "cas: fix UAF in descrambler" into pi-dev
2018-04-09 Chong Zhang[automerger skipped] Merge "cas: fix UAF in descrambler...
2018-04-06 TreeHugger RobotMerge "Camera: various external camera fixes" into...
2018-04-04 TreeHugger RobotMerge "Correct TripleDes tests." into pi-dev
2018-04-04 TreeHugger RobotMerge "Camera: use finer lock in external camera Output...
2018-04-04 TreeHugger RobotMerge "Camera: Check external camera v4l2 buffer size...
2018-04-03 TreeHugger RobotMerge changes from topic "nfc1.1" into pi-dev
2018-04-03 TreeHugger RobotMerge "Freeze current as compatibility_matrix.3.xml...
2018-04-03 Steven MorelandFreeze current as compatibility_matrix.3.xml.
2018-04-03 TreeHugger RobotMerge "Update VHAL types.hal" into pi-dev
2018-04-03 Peiyong LinMerge "[Graphics] Update CommandWriter APIs to common...
2018-04-02 TreeHugger RobotMerge changes Ibab77dce,I0829a91d into pi-dev
2018-04-02 TreeHugger RobotMerge "Update doc in Gnss Hal v1.1" into pi-dev
2018-04-02 Chia-I WuMerge "graphics: add RenderIntent and better HDR suppor...
2018-04-02 Steven MorelandAdd confirmationui to compatibility matrix.
2018-04-02 Steven MorelandAdd automotive.audiocontrol to compatibility matrix.
2018-04-02 TreeHugger RobotMerge "Camera: Validate physical camera related metadat...
2018-04-02 TreeHugger RobotMerge "keymaster: provide instance name to getService...
2018-04-02 Yifan HongMerge "matrix: add radio.config" into pi-dev
2018-03-31 TreeHugger RobotMerge "Update RegState for new CellIdentity types"...
2018-03-30 TreeHugger RobotMerge "SetMacAddress in Vendor HAL" into pi-dev
2018-03-30 TreeHugger RobotMerge "Audio V4: Add metadata update to legacy API...
2018-03-30 TreeHugger RobotMerge "matrix: secure_element use regex eSE[1-9][0...
2018-03-30 Ram PeriathiruvadiMerge "Deprecate DRIVING_STATUS vehicle property."...
2018-03-30 TreeHugger RobotMerge "matrix: radio 1.0-2 IRadio/slot[1-3], ISap/slot1...
2018-03-30 Yifan Hongmatrix: secure_element use regex eSE[1-9][0-9]*
2018-03-30 Enrico GranataMerge "Teach VehiclePropertyStore to not propagate...
2018-03-30 Yifan HongMerge "matrix: add gnss 1.1" into pi-dev
next