]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - compatibility_matrices
Merge "matrix: IR HAL specifies interface/instance"
[android/platform-hardware-interfaces.git] / compatibility_matrices /
2018-08-09 Yifan HongMerge "matrix: IR HAL specifies interface/instance"
2018-08-09 Treehugger RobotMerge "matrix: IR HAL specifies interface/instance"
2018-08-09 Yifan Hongmatrix: IR HAL specifies interface/instance
2018-08-06 Xin LiMerge Android Pie into master
2018-08-02 Shuo QianRevert "Fixed VTS failure in no SIM case"
2018-07-30 Yifan HongMerge "matrix: Enforce kernel requirements in OTA only...
2018-07-30 Yifan HongMerge "matrix: Enforce kernel requirements in OTA only...
2018-07-27 Steven MorelandRemove path from hidl_package_root.
2018-07-27 Yifan Hongmatrix: Enforce kernel requirements in OTA only when...
2018-07-25 Steve MuckleMerge "change kernel config naming convention"
2018-07-25 Treehugger RobotMerge "change kernel config naming convention"
2018-07-24 Steven MorelandMerge "Remove misleading comment in sample dumpstate...
2018-07-24 Steve Mucklechange kernel config naming convention
2018-07-21 Jeff Vander Stoep[automerger skipped] configstore: reduce restrictions...
2018-07-20 Josh Gao[automerger skipped] Merge "Hack around wifi_legacy_hal...
2018-07-17 Hans ChenModified ITestMsgQ hal service interface
2018-07-17 Nirav AtreMerge "Updated HALs to test structs/safe_unions contain...
2018-07-17 Amit MahajanAllow NOT_SUPPORTED for setLinkCapacityReportingCriteri...
2018-07-13 Chih-Hung HsiehMerge "Fix unnecessary copy initialization warnings"
2018-07-13 Nirav AtreMerge "Make safeunion@1.0 test HAL Java-compatible"
2018-07-10 Hsin-Yi ChenMerge "Fix IUsb version number in vts test"
2018-07-06 Nirav AtreMerge "Adding HIDL interface type to safeunion test...
2018-07-03 Ruchi KandoiMerge "Secure_element: vts: Modify openBasicChannel...
2018-06-28 sqianFix missed refactor of serial
2018-06-27 Jack YuFixed VTS failure in no SIM case
2018-06-27 Nirav AtreMerge "Test HAL for HIDL safe_union construct"
2018-06-26 Eric SchwarzenbachCall notify for voiceReg and dataReg VTS tests
2018-06-25 sqianMerge "Add setIndicationFilter response notification...
2018-06-25 Amit MahajanAllow REQUEST_NOT_SUPPORTED as an error for startNetwor...
2018-06-23 sqianAdd REQUEST_NOT_SUPPORTED for changeIccPinForApp and...
2018-06-21 Nathan HaroldSomething fishy in 1.1
2018-06-19 David Grossresolve merge conflicts of ad2db12b3a6d1cd72b50a09ae191...
2018-06-19 David Grossresolve merge conflicts of 2a970cb851cf10115cc876190c03...
2018-06-16 David Gross[automerger skipped] Merge "Document unspecified dimens...
2018-06-15 David GrossMerge "Document unspecified dimensions."
2018-06-15 Jeffrey Vander StoepMerge "Revert "configstore: include crash_dump seccomp...
2018-06-15 Treehugger RobotMerge "Revert "configstore: include crash_dump seccomp...
2018-06-14 Amit MahajanAllow general errors for getImsiForApp().
2018-06-13 Jeff Vander StoepMerge "configstore: include crash_dump seccomp policy"
2018-06-13 Treehugger RobotMerge "configstore: include crash_dump seccomp policy"
2018-06-13 Zhuoyao ZhangMerge "Include libhidl-gen-utils to HAL tests"
2018-06-13 Zhuoyao ZhangMerge "Include libhidl-gen-utils to HAL tests"
2018-06-12 Yifan HongMerge "Do not install assembled framework matrix to...
2018-06-12 Treehugger RobotMerge "Do not install assembled framework matrix to...
2018-06-12 Yifan HongDo not install assembled framework matrix to device.
2018-06-08 Xin LiMerge pi-dev-plus-aosp-without-vendor into stage-aosp...
2018-06-08 Tomasz WasilczykMerge "Fix comments and internal names about SEEK opera...
2018-06-08 Ruchi Kandoi[automerger skipped] Merge "secure_element: vts: Fix...
2018-06-08 Ruchi KandoiMerge "secure_element: vts: Fix openBasicChannel and...
2018-06-07 Emilian PeevCamera: Add only physical ids during multi-camera confi...
2018-06-07 Steven MorelandAdd explicit README for configstore future goals. am...
2018-06-06 David GrossMerge "Document unspecified dimensions." into pi-dev
2018-06-06 David GrossMerge "Document unspecified dimensions." into pi-dev
2018-06-06 Shuzhen WangMerge "Camera: Avoid Metadata re-allocation during...
2018-06-06 huansMerge "SetColorMode is not available for vendor hwc...
2018-06-06 Steve PaikMerge "Add initial values for properties" into pi-dev
2018-06-04 Scott RandolphExplicitly unfreeze the Automotive HALs
2018-06-04 Ray EssickMerge "VtsHalMediaOmx should test functionality only...
2018-06-01 Yu-Han YangMerge "Set lowPowerMode as false in StartAndGetLocation...
2018-05-31 Joshua MccloskeyMerge "Modified tests to account for different director...
2018-05-31 Shawn WilldenMerge "Minor corrections to the Keymaster4 documentatio...
2018-05-31 Chia-I WuMerge "graphics: COLORIMETRIC is optional for HDR modes...
2018-05-30 Yu-Han YangMerge "Update VTS test to blacklist only non-GPS satell...
2018-05-30 Yu-Han YangMerge "Update VTS test to blacklist only non-GPS satell...
2018-05-29 Mikhail NaganovMerge "audio hal: Add 'interface' declarations for...
2018-05-26 Steven MorelandMerge "confirmationui: explicitly declare only one...
2018-05-25 Steve PaikMerge "Fix tire pressure sensor property" into pi-dev
2018-05-25 TreeHugger RobotMerge "Fix tire pressure sensor property" into pi-dev
2018-05-25 Yin-Chia YehMerge "Camera: add FMQ size override logic" into pi-dev
2018-05-25 Shawn WilldenMerge "Fix default keymaster so it doesn't start an...
2018-05-25 Pawin VongmasaAdd multichannel support am: c678d51bdc am: 5de1ae23f9...
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc am: 5de1ae23f9...
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc am: 9886d749d4...
2018-05-24 Shawn WilldenMerge "Move Keymaster docs into HAL" into pi-dev
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc am: 9886d749d4
2018-05-24 TreeHugger RobotMerge "Move Keymaster docs into HAL" into pi-dev
2018-05-24 Shawn WilldenMerge "Activate HMAC sharing check." into pi-dev
2018-05-24 Jaesoo LeeMerge "configstore: configstore HAL uprev'ed to 1.1...
2018-05-24 TreeHugger RobotMerge "Activate HMAC sharing check." into pi-dev
2018-05-24 Yifan HongMerge "P requires 4.14.42" into pi-dev
2018-05-24 TreeHugger RobotMerge "configstore: configstore HAL uprev'ed to 1.1...
2018-05-23 TreeHugger RobotMerge "P requires 4.14.42" into pi-dev
2018-05-23 Jaesoo Leeconfigstore: configstore HAL uprev'ed to 1.1
2018-05-23 Tomasz WasilczykMerge "Improve current program info validation." into...
2018-05-23 Yifan HongP requires 4.14.42
2018-05-23 Yin-Chia YehMerge "Camera: use compact copy when necessary" into...
2018-05-23 Steven MorelandMerge "blank_screen: always exit with _exit()." into...
2018-05-23 Chia-I Wugraphics: fix readback buffer tests
2018-05-22 Scott RandolphFix name of Wheel to VehicleAreaWheel
2018-05-22 Steven Moreland[automerger skipped] Update comments for doc comments...
2018-05-21 Steve PaikMerge "Remove ConfigFlags" into pi-dev
2018-05-21 TreeHugger RobotMerge "Remove ConfigFlags" into pi-dev
2018-05-21 Etan CohenMerge "[AWARE] Developer documentation on HAL usage...
2018-05-19 Steven MorelandMerge "Update comments for doc comments." into pi-dev
2018-05-19 Roshan PiusMerge "wifi(implementation) Modify OWNERS" into pi-dev
2018-05-18 Steve PaikMerge "Update default config areaId's" into pi-dev
2018-05-18 TreeHugger RobotMerge "Update default config areaId's" into pi-dev
2018-05-18 Kevin RocardMerge "VTS tests should be static" into pi-dev
2018-05-18 Kevin RocardMerge "VTS tests should be static" into pi-dev
2018-05-17 Kevin Rocard[automerger skipped] Merge "Audio HAL HIDL wrapper...
next