]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - graphics/allocator/2.0/utils/hal/include/allocator-hal/2.0/AllocatorHal.h
Merge "DRM 1.1: Add VINTF doc"
[android/platform-hardware-interfaces.git] / graphics / allocator / 2.0 / utils / hal / include / allocator-hal / 2.0 / AllocatorHal.h
2018-08-20 Yin-Chia Yeh[automerger skipped] resolve merge conflicts of cd02298...
2018-08-20 Kevin RocardEffect VTS: Allow an effect proxy as pre/post processing
2018-08-13 sqianresolve merge conflicts of 898d05a713a693670cd450ff3f50...
2018-08-10 Pawin Vongmasaresolve merge conflicts of b92f1d2e1be35b331b18589a8cde...
2018-08-10 Kevin Rocard[automerger skipped] Audio VTS: run tear-down hooks...
2018-08-10 Kevin RocardAudio VTS: run tear-down hooks in LIFO instead of FIFO
2018-08-10 sqian[automerger skipped] Fix setBandMode. am: ab2b8bf919...
2018-07-20 Kevin RocardEffect VTS: Allow an effect proxy as pre/post processin...
2018-07-18 sqian[automerger skipped] resolve merge conflicts of eb0f7cd...
2018-07-17 Pawin VongmasaDisable tests for secure audio decoders am: b92f1d2e1b...
2018-07-17 Kevin Rocard[automerger skipped] Audio VTS: run tear-down hooks...
2018-07-16 sqianresolve merge conflicts of ccda8d62963b62e80fe1e303c16e...
2018-07-13 Pawin Vongmasaresolve merge conflicts of b92f1d2e1be35b331b18589a8cde...
2018-07-12 Kevin Rocard[automerger skipped] Audio VTS: run tear-down hooks...
2018-06-29 Kevin RocardAudio VTS: run tear-down hooks in LIFO instead of FIFO...
2018-06-18 sqianFix setBandMode. am: ab2b8bf919 am: d88330667d am:...
2018-06-18 sqian[automerger skipped] Fix setBandMode. am: ab2b8bf919...
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc am: 5de1ae23f9...
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc am: 9886d749d4
2018-05-11 Chong Zhangcas: do not use hidl_memory if size is > SIZE_MAX
2018-04-26 Michael Butler[automerger skipped] Relax NeuralNetwork's VTS positive...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Emilian Peev[automerger skipped] Camera: Allocate graphics buffers...
2018-04-09 Chong Zhang[automerger skipped] Merge "cas: fix UAF in descrambler...
2018-03-30 Yuexi Maresolve merge conflicts of e41f291381eaafa2f9d946e85f94...
2018-03-29 Yuexi Ma[automerger skipped] Merge "rename VtsHalEvsV1_0Target...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-21 Emilian PeevCamera: Remove length check in case of 'getCameraIdList...
2018-03-09 Myles WatsonMerge "resolve merge conflicts of b9492b5fe94cb99b5f799...
2018-03-07 Myles Watsonresolve merge conflicts of 8a28de7a8c3d36e648e90ed2fca2...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-01-31 TreeHugger RobotMerge "android.hardware.media.bufferpool@1.0 HAL"
2018-01-26 TreeHugger RobotMerge "Update emulator protobuf to include status"
2018-01-25 Android Build Merg... Merge "Merge "Add None into cancelPendingUssd" into...
2018-01-25 sqianMerge "Add None into cancelPendingUssd" into oreo-vts...
2018-01-25 TreeHugger RobotMerge "Refactor VHAL"
2018-01-24 Keun Soo YimMerge "DO NOT MERGE Resolve merge conflict for VtsHalCa...
2018-01-24 Ram Mohan MMerge "bug fix: close file pointer" into oreo-vts-dev...
2018-01-24 Kevin RocardAudio policy config: remove cross-module device port...
2018-01-24 Keun Soo YimMerge "DO NOT MERGE Resolve merge conflict for VtsHalCa...
2018-01-24 Ram Mohan MMerge "bug fix: close file pointer" into oreo-vts-dev...
2018-01-24 Kevin RocardAudio policy config: remove cross-module device port...
2018-01-24 Asaf RosenfeldMerge "Adding missing VMS PublisherId functionality...
2018-01-24 TreeHugger RobotMerge "move ringbuffer interactions to wifi hal"
2018-01-24 Android Build Merg... [automerger] Audio HAL: Allow setters to not be impleme...
2018-01-24 Android Build Merg... [automerger] Merge "Audio VTS: HAL can support more...
2018-01-24 Android Build Merg... [automerger] Audio policy config: Device port (type...
2018-01-24 Android Build Merg... [automerger] Audio policy config: allow vendor to exten...
2018-01-24 Android Build Merg... [automerger] Set time delay in the vts test setup am...
2018-01-24 Android Build Merg... [automerger] Loosen speed check for first GPS location...
2018-01-24 Android Build Merg... [automerger] Add tests to validate key length for clear...
2018-01-24 Android Build Merg... [automerger skipped] Add REQUEST_NOT_SUPPORTED / SIM_AB...
2018-01-23 Android Build Merg... Merge "Audio HAL: Allow setters to not be implemented...
2018-01-23 Android Build Merg... Merge "Merge "Audio VTS: HAL can support more than...
2018-01-23 Android Build Merg... Merge "Audio policy config: Device port (type,address...
2018-01-23 Android Build Merg... Merge "Audio policy config: allow vendor to extend...
2018-01-23 Android Build Merg... Merge "Set time delay in the vts test setup am: d4c4a4e...
2018-01-23 Android Build Merg... Merge "Loosen speed check for first GPS location am...
2018-01-23 Android Build Merg... Merge "Add tests to validate key length for clearkey...
2018-01-23 Android Build Merg... Merge changes from topic "am-c310f9b4-18a7-4504-8179...
2018-01-23 Android Build Merg... Merge "Add REQUEST_NOT_SUPPORTED / SIM_ABSENT for vts...
2018-01-23 Android Build Merg... Merge "Fix VTS test which turns off radio. am: 71620817...
2018-01-23 Android Build Merg... Merge "VTS: fix VtsHalKeymasterV3_0Target issue am...
2018-01-23 Android Build Merg... Merge changes from topic "am-c3548d64-0940-4c1d-b786...
2018-01-23 Kevin RocardAudio VTS: do not test duplicate policy configuration...
2018-01-23 Kevin RocardAudio VTS: remove expectation of policy configuration...
2018-01-23 Android Build Merg... [automerger] Audio VTS: do not test duplicate policy...
2018-01-23 Android Build Merg... Merge "Allow partially dynamic profile in the audio...
2018-01-23 Android Build Merg... Merge changes from topic "am-37f5fd31-e121-420d-a199...
2018-01-23 Android Build Merg... Merge "bug fix: restore support for broken flag am...
2018-01-23 Android Build Merg... Merge "bug fix: handle multiple port settings change...
2018-01-23 Android Build Merg... Merge "Merge "Audio VTS: Look for Audio policy config...
2018-01-23 Android Build Merg... Merge "Merge "Don't send more than 2K to addRngEntropy...
2018-01-23 Android Build Merg... [automerger] Allow partially dynamic profile in the...
2018-01-23 Android Build Merg... Merge "bug fix: disable timestamp deviation test for...
2018-01-23 Android Build Merg... Merge changes from topic "am-2bdda567-72b2-4e25-9a99...
2018-01-23 Android Build Merg... Merge "Merge "Allow clearkey tests to run if no vendor...
2018-01-23 Android Build Merg... Merge "bug fix: output colorformat configuration fixed...
2018-01-23 Android Build Merg... Merge "Merge "bug fix: configure input port buffer...
2018-01-23 Android Build Merg... Merge "Update broadcastradio HAL 1.0 VTS tests. am...
2018-01-23 Android Build Merg... Merge changes from topic "am-89fe5346-d048-4a7e-b219...
2018-01-23 Android Build Merg... Merge "bug fix: handle OMX_EventBufferFlag events am...
2018-01-23 Android Build Merg... Merge "Skip direct report test if sensor is not availab...
2018-01-23 Android Build Merg... Merge "Reduce max keymaster message size to 2K am:...
2018-01-23 Android Build Merg... Merge "nfc: NCI 2.0: Add CORE_INIT_CMD for NCI 2.0...
2018-01-23 Android Build Merg... Merge "Add EMPTY_RECORD for getDeviceIdentity am: 40d93...
2018-01-23 Android Build Merg... Merge "Audio policy config xsd: add missing gains and...
2018-01-23 Android Build Merg... [automerger] Merge "Audio VTS: Look for Audio policy...
2018-01-23 Android Build Merg... [automerger] Merge "Don't send more than 2K to addRngEn...
2018-01-23 Android Build Merg... [automerger] bug fix: disable timestamp deviation test...
2018-01-23 Android Build Merg... [automerger] Merge "Allow clearkey tests to run if...
2018-01-23 Android Build Merg... [automerger] bug fix: output colorformat configuration...
2018-01-23 Android Build Merg... [automerger] Merge "bug fix: configure input port buffe...
next