Merge "DRM 1.1: Add VINTF doc"
[android/platform-hardware-interfaces.git] / graphics / composer /
2018-10-24 Bill YiMerge pie-platform-release to aosp-master - DO NOT...
2018-10-24 Treehugger RobotMerge "Clarify C/No reflects the tracked portion of...
2018-10-22 Connor O'BrienMerge "Add statically linked boot HAL impl in recovery"
2018-10-22 Chih-hung HsiehMerge "Fix implicit-fallthrough warnings."
2018-10-22 Chih-hung HsiehMerge "Fix implicit-fallthrough warnings. DO NOT MERGE."
2018-10-22 Treehugger RobotMerge "run vts build rule updater when hal make files...
2018-10-22 Przemyslaw SzczepaniakMerge changes from topic "nnapi-cherrypick-from-master...
2018-10-20 Treehugger RobotMerge "Fix implicit-fallthrough warnings."
2018-10-19 Bill YiMerge pi-dr1-dev to aosp-master
2018-10-19 Chia-I Wugraphics: composer@2.2 does not require mapper@2.1
2018-10-19 Chih-hung HsiehMerge "Fix implicit fallthrough warnings."
2018-10-18 Chia-I Wugraphics: composer@2.2 does not require mapper@2.1
2018-10-17 Steven MorelandMerge "Update makefiles."
2018-10-17 Yifan Hongremoved unused line.
2018-10-16 Yifan HongMerge "compatibility matrices: move to soong"
2018-10-16 chenhgMerge "Avoid segfaults if disconnect USB camera while...
2018-10-16 Jack YuMerge "Restored 'maxConnsTime' and 'maxConns' in data...
2018-10-15 Chih-Hung HsiehFix implicit fallthrough warnings.
2018-10-12 Andreas GampeMerge "Audio: Do not sanitize android.hardware.audio...
2018-10-11 Mikhail NaganovMerge "audio: Add a missing break to EffectsFactory...
2018-10-11 Steven MorelandMerge "Add monostate to optional safe unions."
2018-10-11 Przemyslaw SzczepaniakMerge "Divide BBOX_TRANSFORM into 2 ops."
2018-10-10 Steven MorelandMerge "tests IFoo: WithFmq is more complicated."
2018-10-10 Przemyslaw SzczepaniakMerge changes from topic "nnapi-cherrypick-from-master...
2018-10-10 WyattRileyMerge "Clarifying GnssMeasurement and Clock commments"
2018-10-09 Steven MorelandMerge "tests: IBaz, nasty nesting struct"
2018-10-09 Steven MorelandMerge "IFoo: send struct with fmq."
2018-10-09 Jack HeMerge "VTS: Check return status of initialize and close"
2018-10-08 Steven MorelandMerge "IFoo: remove pointer from u."
2018-10-07 Hridya ValsarajuMerge "Add a command to get the minimum battery voltage...
2018-10-06 Jack YuAdded 1.3 DataProfileInfo
2018-10-03 Kevin RocardAudio VTS: Do not constrain implementation frameCount...
2018-10-03 Kevin RocardAudio VTS: Do not constrain implementation frameCount
2018-10-03 Hridya ValsarajuMerge "Reland "Set vendor: true for boot control HAL""
2018-10-03 Shuo QianMerge "Emergency Function HAL (continued)"
2018-10-03 Yifan HongMerge "health VTS: split Properties test"
2018-10-03 Yifan Honghealth: registerCallback() and getHealthInfo() does...
2018-10-03 Yifan Honghealth: use recursive_mutex.
2018-10-02 Ng Zhi AnSkip hal v1 check after p on low ram devices am: a0eb7e415c
2018-10-02 Hridya ValsarajuMerge "Revert "Set vendor: true for boot control HAL""
2018-10-02 Ng Zhi AnSkip hal v1 check after p on low ram devices
2018-10-02 Hridya ValsarajuMerge "Initialize healthd_mode_ops in recovery default...
2018-10-02 Hridya ValsarajuMerge "Set vendor: true for boot control HAL"
2018-10-01 Chih-Hung HsiehAdd noexcept to move constructors and assignment operators.
2018-10-01 WyattRileyMerge "Allow more time to un-blacklist strongest sateli...
2018-10-01 WyattRileyMerge "Allow more time to un-blacklist strongest sateli...
2018-09-28 Hridya ValsarajuAdd command to check whether off-mode-charging is enabled.
2018-09-28 Hridya ValsarajuAdd command to read fastboot variable 'variant'
2018-09-28 Wei WangAdd atrace HAL 1.0
2018-09-27 jiabinTest getActiveMicrophones API when mic is found on...
2018-09-27 jiabinTest getActiveMicrophones API when mic is found on...
2018-09-26 Rob BarnesFixed minor comment typos in IKeymasterDevice.hal
2018-09-26 Hridya ValsarajuReland "Add command to pass oem commands to HAL"
2018-09-25 Steven MorelandMerge changes from topic "current-on-aosp"
2018-09-25 Miao WangRemove NNAPI 1.2 HAL hash
2018-09-24 Yi KongMerge "Don't use initializer_list as return type"
2018-09-24 Slava ShklyaevSync docs with NeuralNetworks.h
2018-09-24 Przemyslaw SzczepaniakMerge changes from topic "nnapisync_1.2"
2018-09-24 Slava ShklyaevCreate NeuralNetworks HAL v1.2 for new OperationTypes
2018-09-22 Hridya ValsarajuMerge "Revert "Add command to pass oem commands to...
2018-09-21 Yifan HongMerge "health.storage: Add VTS test."
2018-09-21 Yifan Honghealth.storage: Add default implementation.
2018-09-21 Amruth RamachandranMerge "Radio HAL: Add VoPS network support"
2018-09-21 Kevin RocardAudio VTS: Workaround async HIDL destructor by sleeping...
2018-09-21 Yifan HongMerge "health.filesystem::IFileSystem -> health.storage...
2018-09-21 Hridya ValsarajuMerge "Add command to pass oem commands to HAL"
2018-09-20 Kevin RocardAudio VTS: Workaround async HIDL destructor by sleeping
2018-09-18 Kevin RocardMerge "Audio VTS: Always check for Result::isOk()"...
2018-09-18 Kevin RocardMerge "Audio VTS: Always check for Result::isOk()"...
2018-09-14 Steven MorelandMerge "ISafeUnion: add case w/ enum"
2018-09-13 Jeff TinkerMerge "Fix failing drm 1.0 vts tests"
2018-09-13 Yifan HongMerge "health filesystem: update garbageCollect() funct...
2018-09-13 Yifan HongMerge "health filesystem: update garbageCollect() funct...
2018-09-12 Xusong WangFix logics for floating-point comparision in VTS test...
2018-09-12 Xusong WangFix logics for floating-point comparision in VTS test.
2018-09-10 Roberto Pereirakeymaster 3.0: make service use nobody as user and...
2018-09-10 Steven MorelandMerge "Note confusion-causing breaks in HIDL convention."
2018-09-08 Hridya ValsarajuMerge "Get partition file system type from Fastboot...
2018-09-08 Treehugger RobotMerge "Get partition file system type from Fastboot...
2018-09-07 Peiyong LinMerge "[Graphics] Only validate display in PresentOrVal...
2018-09-07 Treehugger RobotMerge "[Graphics] Only validate display in PresentOrVal...
2018-09-07 Baranidharan Muthu... Skip NoUserConfirmation VTS test for Strongbox
2018-09-07 Xusong WangFix logics for floating-point comparision in VTS test.
2018-09-05 Shuo QianMerge "Add IRadioResponse/Indication 1.3 and Emergency...
2018-09-05 Youming YeMerge "Correct the comments for radio hal types"
2018-09-04 Baranidharan Muthu... Merge "Fix KM VTS tests for Strongbox implementations"
2018-08-30 Yin-Chia YehMerge "Camera: support torch control on external camera"
2018-08-30 Emilian Peev[automerger skipped] Merge "Camera: Allow 3% ISO tolera...
2018-08-30 Kevin Rocard[automerger skipped] Merge "Allow getCapturePosition...
2018-08-30 Emilian PeevMerge "Camera: Allow 3% ISO tolerance during ISO burst...
2018-08-30 Kevin RocardMerge "Allow getCapturePosition to return 0 frames...
2018-08-30 Yu-Han Yang[automerger skipped] Merge "Set the floor value of...
2018-08-30 Yu-Han YangMerge "Set the floor value of time estimate as 2017...
2018-08-29 Peiyong LinMerge "[ConfigStore] Clarify hasHDRDisplay spec."
2018-08-29 Peiyong Lin[Graphics] Only validate display in PresentOrValidateDi...
2018-08-29 sqian[automerger skipped] Merge "Fix setAllowedCarrier"...
2018-08-29 sqian[automerger skipped] Merge "Fix setAllowedCarrier"...
2018-08-29 Shawn Willden[automerger skipped] Merge "Change ImportWrappedKeyTest...
2018-08-29 Shawn Willden[automerger skipped] Merge "Require keymaster4 attestat...
2018-08-29 nagendra modadugu[automerger skipped] Merge "keymaster: skip SHA2 digest...
next