]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - health/2.0/README
health: Update README to remove .override [DO NOT MERGE]
[android/platform-hardware-interfaces.git] / health / 2.0 / README
2018-06-18 Yifan Honghealth: Update README to remove .override [DO NOT MERGE]
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc am: 5de1ae23f9...
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc am: 9886d749d4
2018-05-11 Chong Zhangcas: do not use hidl_memory if size is > SIZE_MAX
2018-04-26 Michael Butler[automerger skipped] Relax NeuralNetwork's VTS positive...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Wei WangMerge "dumpstate: add interface into rc file" into...
2018-04-13 TreeHugger RobotMerge "Add 4.14.0 kernel to all matrices." into pi-dev
2018-04-11 TreeHugger RobotMerge "VTS for Bluetooth A2DP HAL" into pi-dev
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 TreeHugger RobotMerge "Remove DiskStat checks from VTS Health HAL test...
2018-04-10 TreeHugger RobotMerge "Audio V4: Synchronize the devices between the...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Emilian Peev[automerger skipped] Camera: Allocate graphics buffers...
2018-04-10 TreeHugger RobotMerge "Correct type of appData field" into pi-dev
2018-04-10 TreeHugger RobotMerge "Fix the spec for TENSOR_QUANT8_ASYMM to match...
2018-04-09 Chong ZhangMerge "cas: fix UAF in descrambler" into pi-dev
2018-04-09 Chong Zhang[automerger skipped] Merge "cas: fix UAF in descrambler...
2018-04-09 TreeHugger RobotMerge "configstore policy: add dgetdents64" into pi-dev
2018-04-06 Yifan HongMerge "health: update readme for writing kmesg" into...
2018-04-06 TreeHugger RobotMerge "Camera: various external camera fixes" into...
2018-04-06 Yifan Honghealth: update readme for writing kmesg
2018-04-05 TreeHugger RobotMerge "health: expand debug info." into pi-dev
2018-04-05 TreeHugger RobotMerge "health 2.0: update readme to uninstall healthd...
2018-04-04 Yifan Honghealth 2.0: update readme to uninstall healthd
2018-03-30 Yuexi Maresolve merge conflicts of e41f291381eaafa2f9d946e85f94...
2018-03-29 Yuexi Ma[automerger skipped] Merge "rename VtsHalEvsV1_0Target...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-21 Emilian PeevCamera: Remove length check in case of 'getCameraIdList...
2018-03-09 Myles WatsonMerge "resolve merge conflicts of b9492b5fe94cb99b5f799...
2018-03-07 Myles Watsonresolve merge conflicts of 8a28de7a8c3d36e648e90ed2fca2...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-06 TreeHugger RobotMerge "External camera: add device config file"
2018-02-06 Scott RandolphMerge "Remove IAudioControlCallback for P"
2018-02-05 Oscar ShuMerge "Followup CL for ringbuffer in wifi_hal"
2018-02-03 TreeHugger RobotMerge "Modify FAN_DIRECTION to be a bit mask"
2018-02-02 TreeHugger RobotMerge "Add vts tests for new drm@1.1 methods"
2018-02-02 Jeff TinkerMerge "Fix incorrect comment in ICryptoFactory.hal"
2018-02-02 TreeHugger RobotMerge "Audio V4: Create audio V4.0 .hal makefiles"
2018-02-02 TreeHugger RobotMerge changes from topic "audio-hal-v4"
2018-02-01 Treehugger RobotMerge "Displaying HD audio indicator for GSM/CDMA calls"
2018-01-31 TreeHugger RobotMerge "Add GNSS VTS test for IGnssDebug.TimeDebug value...
2018-01-31 Miao WangMerge "Create NeuralNetworks HAL v1.1 for new Operation...
2018-01-31 Yifan Honghealth 2.0: update README for typo. am: de542acbbf...
2018-01-31 Ruchi KandoiAdd SecureElement HAL interface am: 241e5aba9e am:...
2018-01-31 Yifan Honghealth 2.0: update README for typo. am: de542acbbf
2018-01-31 Yifan Honghealth: add README. am: 3e6dbcbc30
2018-01-31 Yifan Honghealth 2.0: update README for typo.
2018-01-31 Yifan Honghealth: add README.
2018-01-31 TreeHugger RobotMerge "android.hardware.media.bufferpool@1.0 HAL"
2018-01-30 Yifan Honghealth 2.0: update README for typo.
2018-01-30 Yifan Honghealth: add README.
2018-01-26 TreeHugger RobotMerge "Update emulator protobuf to include status"
2018-01-26 Jack YuMerge "HIDL changes for IWLAN refactoring" am: 4365f2e6...
2018-01-26 Yu-Han YangMerge "Add gnssRequestLocationCb to IGnssCallback.hal...
2018-01-25 Android Build Merg... Merge "Merge "Add None into cancelPendingUssd" into...
2018-01-25 sqianMerge "Add None into cancelPendingUssd" into oreo-vts...
2018-01-25 TreeHugger RobotMerge "Refactor VHAL"
2018-01-24 Zhuoyao ZhangMerge "Convert sensors HAL test to use VtsHalHidlTarget...
2018-01-24 Yifan HongMerge changes from topic "vintf_kernel_ver" am: f3dd36f...
2018-01-24 Keun Soo YimMerge "DO NOT MERGE Resolve merge conflict for VtsHalCa...
2018-01-24 Ram Mohan MMerge "bug fix: close file pointer" into oreo-vts-dev...
2018-01-24 Kevin RocardAudio policy config: remove cross-module device port...
2018-01-24 Keun Soo YimMerge "DO NOT MERGE Resolve merge conflict for VtsHalCa...
2018-01-24 Ram Mohan MMerge "bug fix: close file pointer" into oreo-vts-dev...
2018-01-24 Kevin RocardAudio policy config: remove cross-module device port...
2018-01-24 Eric SchwarzenbachAdd bandwidth to cell info. am: 0f2a7358d6 am: f8db2ebfc9
2018-01-24 Eric SchwarzenbachAdd physical channel configuration indication. am:...
2018-01-24 Eric SchwarzenbachAdd reporting criteria to radio interface. am: 21c6dc35...
2018-01-24 Asaf RosenfeldMerge "Adding missing VMS PublisherId functionality...
2018-01-24 Kevin RocardMerge "Revert "Audio V4: Split system and vendor Audio.h""
2018-01-24 Kevin RocardMerge "Audio V4: Split system and vendor Audio.h"
2018-01-24 TreeHugger RobotMerge "move ringbuffer interactions to wifi hal"
2018-01-24 yinxuMerge "Add default implementation for radio config...
2018-01-24 Steven MorelandMerge "Remove unnecessary group from blank_screen....
2018-01-24 Android Build Merg... [automerger] Audio HAL: Allow setters to not be impleme...
2018-01-24 Android Build Merg... [automerger] Merge "Audio VTS: HAL can support more...
2018-01-24 Android Build Merg... [automerger] Audio policy config: Device port (type...
2018-01-24 Android Build Merg... [automerger] Audio policy config: allow vendor to exten...
2018-01-24 Android Build Merg... [automerger] Set time delay in the vts test setup am...
2018-01-24 Android Build Merg... [automerger] Loosen speed check for first GPS location...
2018-01-24 Android Build Merg... [automerger] Add tests to validate key length for clear...
2018-01-24 Android Build Merg... [automerger skipped] Add REQUEST_NOT_SUPPORTED / SIM_AB...
2018-01-23 Android Build Merg... Merge "Audio HAL: Allow setters to not be implemented...
2018-01-23 Android Build Merg... Merge "Merge "Audio VTS: HAL can support more than...
2018-01-23 Android Build Merg... Merge "Audio policy config: Device port (type,address...
2018-01-23 Android Build Merg... Merge "Audio policy config: allow vendor to extend...
2018-01-23 Android Build Merg... Merge "Set time delay in the vts test setup am: d4c4a4e...
2018-01-23 Android Build Merg... Merge "Loosen speed check for first GPS location am...
2018-01-23 Android Build Merg... Merge "Add tests to validate key length for clearkey...
2018-01-23 Android Build Merg... Merge changes from topic "am-c310f9b4-18a7-4504-8179...
2018-01-23 Android Build Merg... Merge "Add REQUEST_NOT_SUPPORTED / SIM_ABSENT for vts...
2018-01-23 Android Build Merg... Merge "Fix VTS test which turns off radio. am: 71620817...
2018-01-23 Android Build Merg... Merge "VTS: fix VtsHalKeymasterV3_0Target issue am...
2018-01-23 Android Build Merg... Merge changes from topic "am-c3548d64-0940-4c1d-b786...
next