]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - health
Merge "Convert usb service .mk -> .bp."
[android/platform-hardware-interfaces.git] / health /
2017-10-05 Treehugger RobotMerge "Convert usb service .mk -> .bp."
2017-10-05 Treehugger RobotMerge "Vibrator service -> .bp"
2017-10-05 Treehugger RobotMerge "Remove Android.bp subdirs loop."
2017-10-04 Steven MorelandMerge "Update for hidl adapter module defaults."
2017-10-04 Treehugger RobotMerge "Update for hidl adapter module defaults."
2017-10-04 Chih-hung HsiehMerge "Use -Werror in hardware/interfaces"
2017-10-04 Steven MorelandUpdate for hidl adapter module defaults.
2017-10-04 Yifan HongMerge "Add android.hardware.health@2.0 HAL"
2017-10-04 Yifan HongMerge "Add android.hardware.health@2.0 HAL"
2017-10-04 Yifan HongAdd android.hardware.health@2.0 HAL
2017-10-03 Treehugger RobotMerge "Convert to Android.bp; rename libminijail_vendor"
2017-09-26 Steven MorelandMerge "Fix typo in update makefiles."
2017-09-26 Treehugger RobotMerge "Fix typo in update makefiles."
2017-09-26 Steven MorelandFix typo in update makefiles.
2017-09-25 Steven MorelandUpdate makefiles for hidl adapter.
2017-09-25 Steven MorelandUpdate makefiles for hidl adapter.
2017-09-18 Peng XuMerge "Add capability for sensor hal to use wakelock"
2017-09-15 Peng XuMerge "Add OWNERS file for sensors"
2017-08-28 Tri VoVTS tests now static link to HAL def libs.
2017-08-25 Tri VoVTS tests now static link to HAL def libs.
2017-08-19 Ram Mohan MMerge "bug fix: close file pointer" into oc-dev
2017-08-19 Ram Mohan MMerge "bug fix: configure input port buffer size" into...
2017-08-19 Ram Mohan MMerge "bug fix: close file pointer" into oc-dev am...
2017-08-19 Ram Mohan MMerge "bug fix: configure input port buffer size" into...
2017-08-19 Ram Mohan MMerge "bug fix: close file pointer" into oc-dev
2017-08-19 Ram Mohan MMerge "bug fix: configure input port buffer size" into...
2017-08-18 Jeff TinkerAllow clearkey tests to run if no vendor modules am...
2017-08-18 Jeff TinkerAllow clearkey tests to run if no vendor modules
2017-08-18 Jeff TinkerAllow clearkey tests to run if no vendor modules
2017-08-17 Zhuoyao ZhangMove android.hardware.tests.libhwbinder@1.0-impl to...
2017-08-15 Emilian PeevMerge "Camera: Switch 'cancelPictureFail' to 'cancelPic...
2017-08-15 Emilian PeevMerge "Camera: Switch 'cancelPictureFail' to 'cancelPic...
2017-08-15 Emilian PeevMerge "Camera: Switch 'cancelPictureFail' to 'cancelPic...
2017-08-15 Emilian PeevMerge "Camera: Switch 'cancelPictureFail' to 'cancelPic...
2017-08-14 Steven MorelandUpdating all makefiles.
2017-08-14 Steven MorelandUpdating all makefiles.
2017-08-14 Steven MorelandMerge "Updating all makefiles." into oc-dr1-dev-plus...
2017-08-11 Steven MorelandUpdating all makefiles.
2017-08-11 Tomasz WasilczykMerge "Update broadcastradio HAL 1.0 VTS tests." into...
2017-08-11 Tomasz WasilczykMerge "Update broadcastradio HAL 1.0 VTS tests." into...
2017-08-10 yinxuMerge "Add the error code "OPERATION_NOT_ALLOWED" and...
2017-08-10 Myles WatsonMerge "Bluetooth: Check the number of file descriptors"
2017-08-09 Myles WatsonMerge "Bluetooth: Add OWNERS file for default/"
2017-08-09 Myles WatsonNFC: Add OWNERS file for default/
2017-08-09 Peng XuMerge "Skip direct report test if sensor is not availab...
2017-08-09 Peng XuMerge "Skip direct report test if sensor is not availab...
2017-08-09 Justin YunManually update makefile for vndk-sp hidl libs.
2017-08-09 Steven MorelandUpdate makefiles for vndk enabled.
2017-08-08 Shuo QianMerge "Add Owners for radio vts"
2017-08-08 Ram Mohan Mbug fix: handle OMX_EventBufferFlag events
2017-08-08 Ram Mohan Mbug fix: handle OMX_EventBufferFlag events
2017-08-07 Tri VoUpdate comments for VtsHalTargetTestDefaults.
2017-08-04 Steven MorelandMerge changes from topic 'go-away-static-hidl-java'
2017-08-03 Shuo QianMerge "Add vts test for setCarrierInfoForImsiEncryption"
2017-08-03 Tri VoMerge changes from topic 'vts_deps'
2017-08-03 Ruchi Kandoinfc: NCI 2.0: Add CORE_INIT_CMD for NCI 2.0
2017-08-03 Ruchi Kandoinfc: NCI 2.0: Add CORE_INIT_CMD for NCI 2.0
2017-08-03 Ruchi Kandoinfc: NCI 2.0: Add CORE_INIT_CMD for NCI 2.0
2017-08-02 Sundong AhnChange dependency library
2017-08-02 Yin-Chia YehMerge "Camera: reset callback after test done" into...
2017-08-01 Yin-Chia YehMerge "Camera: reset callback after test done" into...
2017-08-01 sqianresolve merge conflicts of 345a396c to oc-dr1-dev
2017-08-01 Shuo QianMerge "Add EMPTY_RECORD for getDeviceIdentity" into...
2017-08-01 Shuo QianMerge "Add corresponding error code to fix vts test...
2017-08-01 Shuo QianMerge "Add corresponding error code to fix vts test...
2017-08-01 Kevin RocardMerge "Audio policy config xsd: add missing gains and...
2017-08-01 Kevin RocardMerge "Audio policy config xsd: add missing gains and...
2017-07-31 Steven MorelandMerge "Update HIDL makefiles."
2017-07-31 Emilian PeevMerge "NO PARTIAL RERUN Camera: Update stream consumer...
2017-07-31 Emilian PeevMerge "NO PARTIAL RERUN Camera: Update stream consumer...
2017-07-31 Yin-Chia YehCamera: fix various VTS issues
2017-07-31 Yin-Chia YehCamera: fix various VTS issues
2017-07-28 yinxuFix VTS errors of the network scan API
2017-07-25 Eino-Ville TalvalaMerge "Camera: Don't enforce result metadata queue...
2017-07-25 Eino-Ville TalvalaMerge "Camera: Don't enforce result metadata queue...
2017-07-25 Roshan Piussupplicant(vts): Remove start/stop framework
2017-07-25 Roshan Piussupplicant(vts): Remove start/stop framework
2017-07-25 Shuo QianMerge "Add Sim absent assertion in the 1.0 setup" into...
2017-07-25 Shuo QianMerge "Add Sim absent assertion in the 1.0 setup" into...
2017-07-24 yinxuMerge " Add VTS code for the network scan API"
2017-07-22 Stanley TngMerge "Fixed the HCI ACL Header definitions for PB...
2017-07-22 Stanley TngMerge "Fixed the HCI ACL Header definitions for PB...
2017-07-22 Legler WuUpdate VTS tests so that Mediatek pass more VTS for O.
2017-07-22 Legler WuUpdate VTS tests so that Mediatek pass more VTS for O.
2017-07-21 Zhuoyao ZhangMove android.hardware.tests.msgq@1.0-impl to system.img
2017-07-21 Shuo QianMerge "Update IRadioResponse.hal documentation" into...
2017-07-21 Shuo QianMerge "Update IRadioResponse.hal documentation" into...
2017-07-21 Shuo QianMerge "Fix some VTS for 2017 devices" into oc-dev
2017-07-21 Shuo QianMerge "Fix some VTS for 2017 devices" into oc-dev
2017-07-20 Stanley TngMerge "Fixed the HCI ACL Header definitions for PB...
2017-07-20 Steven MorelandMove multithread impl to system.
2017-07-18 sqianresolve merge conflicts of 6ecc54a7 to stage-aosp-master
2017-07-18 Steven MorelandMerge "Move all hidl_test dependencies to the system...
2017-07-17 sqianAdd RadioIndication for Radio VTS test
2017-07-14 Michael ButlerMerge "Added protections to RenderScript VTS class...
2017-07-14 Timur IskhakovInterface for configureRpcThreadpool tests
2017-07-11 sqianAdd radio 1.1 vts test folder.
2017-07-07 Myles WatsonMerge "Bluetooth: Change CHECK() to LOG_ALWAYS_FATAL()"
2017-07-07 Jakub PawlowskiMerge "Make RawAddress into a class (4/4)"
2017-07-07 Jakub PawlowskiMerge "Make RawAddress into a class (4/4)"
next