]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - health
matrix: broadcastradio@2.0::IBroadcastRadio/.*
[android/platform-hardware-interfaces.git] / health /
2018-04-26 Michael Butler[automerger skipped] Relax NeuralNetwork's VTS positive...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris ChangVTS: fix RadioHidlTest.getAvailableNetworks issue am...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Wei WangMerge "dumpstate: add interface into rc file" into...
2018-04-19 Kevin RocardMerge "Revert "Audio: setParam improve status_t to...
2018-04-19 Kevin RocardMerge "Audio: setParam improve status_t to Result consi...
2018-04-13 TreeHugger RobotMerge "Add 4.14.0 kernel to all matrices." into pi-dev
2018-04-11 TreeHugger RobotMerge "VTS for Bluetooth A2DP HAL" into pi-dev
2018-04-11 TreeHugger RobotMerge "[AWARE][VTS] Add VTS tests for the Wi-Fi 1.2...
2018-04-10 Etan CohenMerge "[AWARE] Support a mix of 1.0 and 1.2 Callback...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 TreeHugger RobotMerge "Correct bug in HmacKeySharingTest" into pi-dev
2018-04-10 TreeHugger RobotMerge "Audio V4: Use of EffectFlags over bitfield<Effec...
2018-04-10 TreeHugger RobotMerge "Remove DiskStat checks from VTS Health HAL test...
2018-04-10 TreeHugger RobotMerge "Audio V4: Synchronize the devices between the...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support
2018-04-10 Emilian Peev[automerger skipped] Camera: Allocate graphics buffers...
2018-04-10 TreeHugger RobotMerge "Correct type of appData field" into pi-dev
2018-04-10 TreeHugger RobotMerge "Fix the spec for TENSOR_QUANT8_ASYMM to match...
2018-04-09 Chong ZhangMerge "cas: fix UAF in descrambler" into pi-dev
2018-04-09 Chong Zhang[automerger skipped] Merge "cas: fix UAF in descrambler...
2018-04-09 TreeHugger RobotMerge "configstore policy: add dgetdents64" into pi-dev
2018-04-06 Yifan HongMerge "health: update readme for writing kmesg" into...
2018-04-06 TreeHugger RobotMerge "Camera: various external camera fixes" into...
2018-04-06 Yifan Honghealth: update readme for writing kmesg
2018-04-05 TreeHugger RobotMerge "health: expand debug info." into pi-dev
2018-04-05 TreeHugger RobotMerge "health 2.0: update readme to uninstall healthd...
2018-04-04 Yifan Honghealth: expand debug info.
2018-04-04 Yifan Honghealth 2.0: update readme to uninstall healthd
2018-04-03 Hridya ValsarajuRemove DiskStat checks from VTS Health HAL test
2018-03-30 Yuexi Maresolve merge conflicts of e41f291381eaafa2f9d946e85f94...
2018-03-29 Yuexi Maresolve merge conflicts of a9543fee6b3f5e9609206d3a21a4...
2018-03-29 Yuexi Ma[automerger skipped] Merge "rename VtsHalEvsV1_0Target...
2018-03-29 Yuexi Ma[automerger skipped] Merge "rename VtsHalEvsV1_0Target...
2018-03-29 Yuexi MaMerge "rename VtsHalEvsV1_0Target module to VtsHalEvsV1...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported
2018-03-21 Emilian PeevCamera: Remove length check in case of 'getCameraIdList...
2018-03-09 Myles WatsonMerge "resolve merge conflicts of b9492b5fe94cb99b5f799...
2018-03-07 Myles Watsonresolve merge conflicts of 8a28de7a8c3d36e648e90ed2fca2...
2018-03-07 Myles Watsonresolve merge conflicts of b9492b5fe94cb99b5f79964a4931...
2018-03-06 Myles Watsonresolve merge conflicts of 8a28de7a8c3d36e648e90ed2fca2...
2018-03-06 Myles WatsonBluetooth: Relax NO_OP and SCO checks am: 8a28de7a8c
2018-03-02 CassieMerge "Add VTS test for getCellInfoList_1_2" am: 6a8364...
2018-03-02 chenhgMerge "configstore: allow to USE_CONTEXT_PRIORITY by...
2018-03-02 yinxuAdd vts response functions for Radio Response 1.2 am...
2018-03-01 Myles WatsonBluetooth: Relax NO_OP and SCO checks am: 72382e3014...
2018-03-01 Jack YuAdded new VTS test cases for v1.2 data call APIs am...
2018-02-28 Ruchi KandoiMerge "Add init() as a part of Secure Element VTS test...
2018-02-28 Eric SchwarzenbachAdd VTS tests for 1.2 reporting criteria am: 8bdc4e04e2...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation
2018-02-24 Zhuoyao ZhangMerge "Convert tv input hal test to use VtsHalHidlTarge...
2018-02-24 Connor O'BrienMerge "Fix boot VTS GetSuffix test" am: 5cd16a71f5...
2018-02-23 Eric SchwarzenbachMerge "Update documentation for currentPhysicalChannelC...
2018-02-23 TreeHugger RobotMerge "camera: Add OisSamples synthetic key"
2018-02-23 TreeHugger RobotMerge "Revert "Restore "Add "Unlocked device required...
2018-02-22 CassieMerge "Dot allow error OPERATION_NOT_ALLOWED and REQUES...
2018-02-22 Treehugger RobotMerge "Dot allow error OPERATION_NOT_ALLOWED and REQUES...
2018-02-22 TreeHugger RobotMerge "ConfirmationUI VTS tests"
2018-02-21 Zhuoyao ZhangMerge "Convert evs hal test to use VtsHalHidlTargetTest...
2018-02-21 Zhuoyao ZhangMerge "Convert evs hal test to use VtsHalHidlTargetTest...
2018-02-21 Yin-Chia YehMerge "Camera: avoid copying of HalRequest"
2018-02-21 TreeHugger RobotMerge "Call deleteAidingData to clean up after injectBe...
2018-02-21 Andrew ScullMerge "AuthSecret: make method oneway"
2018-02-21 Yin-Chia YehMerge "Camera: implement external camera dumpState...
2018-02-20 Zhuoyao ZhangMerge "Convert drm hal test to use VtsHalHidlTargetTest...
2018-02-16 TreeHugger RobotMerge "Audio HAL V4: Add Hearing aid output device"
2018-02-16 Chong ZhangMerge "MediaCas: use HidlMemory to avoid handle leaks"
2018-02-16 Kevin RocardMerge "Audio HAL V4: Switch back to 32 bit AudioDevice"
2018-02-16 TreeHugger RobotMerge "Fix LTE Timing Advance Doc String"
2018-02-16 TreeHugger RobotMerge "Camera: implement external camera flush"
2018-02-16 Eric SchwarzenbachFix comments for link capacity and signal strength...
2018-02-16 TreeHugger RobotMerge "Refactor NN API VTS tests and add v1.1 tests"
2018-02-16 Eric SchwarzenbachMerge "Use new AccessNetwork type in the reporting...
2018-02-16 Brian YoungMerge "Restore "Add "Unlocked device required" paramete...
2018-02-16 nharoldMerge "Fixes to Align TdScdma Reports with All Others...
2018-02-16 Treehugger RobotMerge "Use new AccessNetwork type in the reporting...
2018-02-16 nharoldMerge "Update WcdmaSignalStrength to add RAT-specific...
2018-02-16 Zhuoyao ZhangMerge "Convert thermal hal test to use VtsHalHidlTarget...
2018-02-16 Zhuoyao ZhangMerge "Convert nfc hal test to use VtsHalHidlTargetTest...
next