]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - neuralnetworks
Merge "configstore: include crash_dump seccomp policy"
[android/platform-hardware-interfaces.git] / neuralnetworks /
2018-06-13 Zhuoyao ZhangMerge "Include libhidl-gen-utils to HAL tests"
2018-06-08 Treehugger RobotMerge "Fix bug in VTS attestation cert verification."
2018-05-17 Treehugger RobotMerge "Audio HAL HIDL wrapper: Fix incorrect conversion...
2018-05-09 Mika RaentoUpdate namespace to match framework/ml/nn
2018-05-09 Michael ButlerNNAPI: sync NDK and HAL documentation
2018-05-09 Mika RaentoUpdate neuralnetworks/*/types.hal to match impl
2018-04-27 android-build-prod... Merge "HWC2On1Adapter: Fix fd leak in Layer::dump"
2018-04-27 android-build-prod... Merge "Replace hidl_enum_{iterator -> range}."
2018-04-26 Dan StozaMerge "graphics: add libhwc2on{1,fb}adapter"
2018-04-25 Steven MorelandReplace hidl_enum_{iterator -> range}.
2018-04-23 Kevin RocardMerge "Audio: setParam improve status_t to Result consi...
2018-04-21 Treehugger RobotMerge "Mark configstore-utils as double_loadable"
2018-04-18 Michael ButlerMerge changes from topic "nnapi-aosp-sync"
2018-04-18 Michael ButlerNNAPI: Add execution preference to prepareModel (HAL)
2018-04-18 Michael ButlerSync NNAPI Operand and Operation documentation fixes
2018-04-18 Miao WangFix the spec for TENSOR_QUANT8_ASYMM to match our valid...
2018-04-18 Miao WangFix the NNAPI HAL documentation about ADD and MUL
2018-04-18 Michael ButlerNN validation tests
2018-04-18 David GrossAdd validation tests for consistency of model inputs...
2018-04-17 Pirama Arumuga NainarDisable arm32 asan for VtsHalNeuralnetworksV1_1TargetTest
2018-04-13 nharoldMerge "Add a Test for RadioBandMode to Ensure Auto...
2018-04-12 David GrossFix documentation.
2018-03-05 Treehugger RobotMerge changes from topic "cp_nnapi" android-o-mr1-iot-preview-7 android-p-preview-1
2018-03-05 Michael ButlerRelax NeuralNetwork's VTS positive and negative base...
2018-03-05 David GrossAdd Capabilities::relaxedFloat32toFloat16Performance...
2018-03-05 Miao WangMinor modification to allow relaxed precision test
2018-03-05 Michael ButlerNNAPI narrow evaluation for P -- HAL
2018-03-05 Miao WangRefactor NN API VTS tests and add v1.1 tests
2018-03-05 Michael ButlerAdd README to NeuralNetworks HAL
2018-02-02 Treehugger RobotMerge "Remove extra space."
2018-02-02 Treehugger RobotMerge "Create NeuralNetworks HAL v1.1 for new Operation...
2018-01-31 Michael ButlerCreate NeuralNetworks HAL v1.1 for new OperationTypes
2017-12-06 Xin LiDO NOT MERGE: Merge Oreo MR1 into master
2017-12-05 Zhuoyao ZhangMerge "Convert boot, memtrack and power hal to use...
2017-12-04 Michael SchwartzMerge "Remove IOemHook from matrix in P"
2017-12-03 Steven MorelandUpdating makefiles for hidl_interface.
2017-12-02 Howard ChenMerge "Add more test methods to IMemoryTest"
2017-12-01 Dan WillemsenFix problem found with host bionic fortify checks
2017-11-29 Chih-Hung HsiehMerge "Use -Werror in hardware/interfaces/automotive...
2017-11-29 Kevin RocardAdd the audio team as owner of the audio VTS
2017-11-29 Mikhail NaganovAdd OWNERS for audio-related HAL default implementations
2017-11-29 Daniel Van VeenMerge "Fix inequality typo in StreamIn::getCapturePosition"
2017-11-29 Steven MorelandMerge "Remove subdirs"
2017-11-29 Badhri Jagan SridharanMerge "usb: Add owner file"
2017-11-29 Steven MorelandMerge "Update tests makefile for change."
2017-11-29 TreeHugger RobotMerge "Remove subdirs" into stage-aosp-master
2017-11-29 Chih-Hung HsiehUse -Werror in hardware/interfaces/biometrics/fingerprint
2017-11-28 Steven MorelandRemove subdirs
2017-11-28 Chih-Hung HsiehMerge "Use -Werror in hardware/interfaces/automotive...
2017-11-28 Chih-Hung HsiehMerge "Use -Werror in hardware/interfaces"
2017-11-28 Chih-Hung HsiehMerge "Use -Werror in hardware/interfaces/audio"
2017-11-28 Chih-Hung HsiehMerge "Use -Werror in hardware/interfaces/light/2.0"
2017-11-28 Chih-Hung HsiehUse -Werror in hardware/interfaces/automotive/vehicle
2017-11-28 Steven MorelandMerge "Test for references to typedef'd enum."
2017-11-27 Steven MorelandMerge "Additional tests for enum iteration."
2017-11-22 Jiyong ParkMerge "DO NOT MERGE: android.hardware.graphics.allocato...
2017-11-22 Iris ChangMerge "Fix Keymaster VTS for OpenSSL error code change"
2017-11-20 Badhri Jagan SridharanInitialize usb_count in the setup funtion.
2017-11-17 Ryan CampbellTransfer VTS test ownership.
2017-11-16 Roshan Piuswifi(vts): Skip tests if feature not supported
2017-11-15 Zhuoyao ZhangMerge "Convert Renderscript Hal test to test against...
2017-11-15 Iris ChangMerge "VTS: fix RadioHidlTest.getAvailableNetworks...
2017-11-15 Zhuoyao ZhangConvert GraphicsMapper Hal test to test against each...
2017-11-14 Xin LiMerge commit '1a06284b24f5eb7bb9c1fea0817da8898b3b1bff...
2017-10-19 Sanket PadaweFix VTS test which turns off radio. am: 536818d17a...
2017-10-18 Sanket PadaweFix VTS test which turns off radio. am: 536818d17a
2017-10-18 Steven MorelandMerge "Update Light extension example to match docs...
2017-10-18 Tri VoMerge "Set pipe size to >1MB for debugDump test cases...
2017-10-18 Chih-Hung HsiehUse -Werror in hardware/interfaces am: ceb435f2ba am...
2017-10-17 TreeHugger RobotMerge "bug fix: during fatal fails bypass freeNode...
2017-10-17 Sooraj SasindranMerge "Enhanced network scan request" am: 8e5f008ae6...
2017-10-16 Janis DanisevskisRename libkeymaster to libkeymaster_staging am: 8cd5614...
2017-10-16 Janis Danisevskislibkeymaster1 split to libkeymaster and _portable am...
2017-10-15 Steven MorelandMerge changes from topic "hidl-test" am: 240f9e1476...
2017-10-15 Zhuoyao ZhangStatic link test lib shims with test -impl libs. am...
2017-10-15 Tri VoMerge "Use a pipe instead of tmp for debugDump tests...
2017-10-15 Steven MorelandMerge "Remove invalid annotations from IBaz." am: e322e...
2017-10-15 Tri VoMerge "Change tmp dir to /data/system/users/0/fpdata...
2017-10-15 sqianMerge "Refactor radio folder for 1.0 and 1.1" am: bf758...
2017-10-15 sqianRefactor radio folder for 1.0 and 1.1 am: 8735a7d935
2017-10-12 Peng XuEnlarge buffer size for direct report testing am: 3c01f...
2017-10-12 Peng XuEnlarge buffer size for direct report testing am: 3c01f...
2017-10-12 Yifan HongMerge "health@2.0: IHealthInfoCallback expands HealthIn...
2017-10-11 Steven Morelandlibhwminijail from hardware/interfaces to libhidl....
2017-10-11 TreeHugger RobotMerge "Added VTS tests for requiresSecureDecoderCompone...
2017-10-11 Steven MorelandUpdate for Soong java makefiles. am: c3e80fa01e am...
2017-10-11 Mikhail NaganovAudio VTS: Allow 4GB buffer prepareToWrite/Read to...
2017-10-11 Mikhail NaganovAudio VTS: Allow 4GB buffer prepareToWrite/Read to...
2017-10-11 TreeHugger RobotMerge "cas-vts: use MemoryDealer to allocate shared...
2017-10-10 TreeHugger RobotMerge "Legacy wrapper: Use arbitrary limit on buffer...
2017-10-10 Iris ChangVTS: fix VtsHalKeymasterV3_0Target issue am: 926a8e7440...
2017-10-10 Iris ChangVTS: fix VtsHalKeymasterV3_0Target issue am: 926a8e7440
2017-10-10 I-Jui (Ray) SungMerge "Refactor test harness for generated VTS tests...
2017-10-10 TreeHugger RobotMerge "Refactor test harness for generated VTS tests...
2017-10-09 I-Jui (Ray) SungRefactor test harness for generated VTS tests
2017-10-07 TreeHugger RobotMerge "omxvts: exit gracefully during fatal fails"...
2017-10-06 Peng XuMerge "Replace sys_nice capability with rlimit rtprio...
2017-10-06 TreeHugger RobotMerge "Added VTS tests for MediaCas - II" into oc-mr1-dev
2017-10-06 Yifan HongMerge changes from topic "health2-hal" am: 116fb89f70...
2017-10-06 Iris ChangMerge "VTS: fix VtsHalKeymasterV3_0Target issue" am...
next