]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - nfc
Merge "matrix: add gnss 1.1" into pi-dev
[android/platform-hardware-interfaces.git] / nfc /
2018-03-30 Yifan HongMerge changes from topic "check_unused_hals" am: 61cbaa8dd7
2018-03-30 Yuexi Maresolve merge conflicts of e41f291381eaafa2f9d946e85f94...
2018-03-29 Yuexi Maresolve merge conflicts of a9543fee6b3f5e9609206d3a21a4...
2018-03-29 Tom CherryMerge "Add BLOCK_SUSPEND capability for Bluetooth HAL...
2018-03-29 Yuexi Ma[automerger skipped] Merge "rename VtsHalEvsV1_0Target...
2018-03-29 Yuexi Ma[automerger skipped] Merge "rename VtsHalEvsV1_0Target...
2018-03-29 Yuexi MaMerge "rename VtsHalEvsV1_0Target module to VtsHalEvsV1...
2018-03-29 Yifan HongMerge "Build DEVICE_FRAMEWORK_COMPATIBILITY_MATRIX_FILE...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported
2018-03-26 Yuexi Maresolve merge conflicts of 07ff5f43761273cadfbbe67aad5b...
2018-03-26 Tom Cherry[automerger skipped]Merge "Add capabilities to wifi...
2018-03-24 Lloyd Pique[automerger skipped]Merge "Fix crash on hotplug disconn...
2018-03-23 Tom CherryMerge "Add capabilities to bluetooth HAL service" am...
2018-03-23 Tom CherryMerge "Add capabilities to wifi HAL service" into pi-dev
2018-03-22 Yuexi Ma[automerger skipped]rename VtsHalEvsV1_0Target module...
2018-03-21 Emilian PeevCamera: Remove length check in case of 'getCameraIdList...
2018-03-19 Jeff Vander Stoepconfigstore: whitelist getpid call for arm64 am: 0979cc5dd9
2018-03-19 TreeHugger RobotMerge changes I20310606,Ic23b7fb2 into pi-dev
2018-03-17 Steven Morelandblank_screen: shut off all lights am: b944d69508
2018-03-17 Steven Morelandlight service: mark as shutdown critical am: b25202527e
2018-03-13 Aniket Kumar Lataaudio: Register Bluetooth service with audio HAL am...
2018-03-13 Sunny KapdiBluetooth: A2DP offload HIDL am: 9526c2ff73
2018-03-12 TreeHugger RobotMerge "Implement Gnss::start() and Gnss::stop()" into...
2018-03-12 Ruchi KandoiAdd VTS Test for getConfig() in NFC 1.1 am: 4cd374a6c4
2018-03-12 Ruchi KandoiNFC 1.1: Add getConfigs() method am: d128c87f70
2018-03-12 Ruchi KandoiAdd VTS Test for getConfig() in NFC 1.1
2018-03-12 Ruchi KandoiNFC 1.1: Add getConfigs() method
2018-03-12 TreeHugger RobotMerge "Camera: Do not forward capture_result in error...
2018-03-10 TreeHugger RobotMerge "Add VTS test for automotive AudioControl HAL...
2018-03-09 Ruchi KandoiAdd VTS Test for getConfig() in NFC 1.1
2018-03-09 Ruchi KandoiNFC 1.1: Add getConfigs() method
2018-03-09 Ruchi KandoiAdd VTS Test for getConfig() in NFC 1.1
2018-03-09 Ruchi KandoiNFC 1.1: Add getConfigs() method
2018-03-09 Ruchi KandoiAdd VTS Test for getConfig() in NFC 1.1
2018-03-09 Ruchi KandoiNFC 1.1: Add getConfigs() method
2018-03-09 Myles WatsonMerge "resolve merge conflicts of b9492b5fe94cb99b5f799...
2018-03-07 Myles Watsonresolve merge conflicts of 8a28de7a8c3d36e648e90ed2fca2...
2018-03-07 Myles Watsonresolve merge conflicts of b9492b5fe94cb99b5f79964a4931...
2018-03-06 Myles Watsonresolve merge conflicts of 8a28de7a8c3d36e648e90ed2fca2...
2018-03-06 Myles WatsonBluetooth: Relax NO_OP and SCO checks am: 8a28de7a8c
2018-03-06 Michael ButlerMerge changes from topic "cp_nnapi" am: 7df64ea2fd
2018-03-06 David GrossAdd Capabilities::relaxedFloat32toFloat16Performance...
2018-03-06 Miao WangMinor modification to allow relaxed precision test...
2018-03-06 Michael ButlerNNAPI narrow evaluation for P -- HAL am: e0d9b167a6
2018-03-06 Miao WangRefactor NN API VTS tests and add v1.1 tests am: 4862d612ad
2018-03-06 Michael ButlerAdd README to NeuralNetworks HAL am: 5f57913184
2018-03-02 CassieMerge "Add VTS test for getCellInfoList_1_2" am: 6a8364...
2018-03-02 chenhgMerge "configstore: allow to USE_CONTEXT_PRIORITY by...
2018-03-02 yinxuAdd vts response functions for Radio Response 1.2 am...
2018-03-01 Myles WatsonBluetooth: Relax NO_OP and SCO checks am: 72382e3014...
2018-03-01 Jack YuAdded new VTS test cases for v1.2 data call APIs am...
2018-02-28 Ruchi KandoiMerge "Add init() as a part of Secure Element VTS test...
2018-02-28 Eric SchwarzenbachAdd VTS tests for 1.2 reporting criteria am: 8bdc4e04e2...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation
2018-02-24 Zhuoyao ZhangMerge "Convert tv input hal test to use VtsHalHidlTarge...
2018-02-24 Connor O'BrienMerge "Fix boot VTS GetSuffix test" am: 5cd16a71f5...
2018-02-23 Eric SchwarzenbachMerge "Update documentation for currentPhysicalChannelC...
2018-02-23 TreeHugger RobotMerge "camera: Add OisSamples synthetic key"
2018-02-23 TreeHugger RobotMerge "Revert "Restore "Add "Unlocked device required...
2018-02-22 CassieMerge "Dot allow error OPERATION_NOT_ALLOWED and REQUES...
2018-02-22 Treehugger RobotMerge "Dot allow error OPERATION_NOT_ALLOWED and REQUES...
2018-02-22 TreeHugger RobotMerge "ConfirmationUI VTS tests"
2018-02-21 Zhuoyao ZhangMerge "Convert evs hal test to use VtsHalHidlTargetTest...
2018-02-21 Zhuoyao ZhangMerge "Convert evs hal test to use VtsHalHidlTargetTest...
2018-02-21 Yin-Chia YehMerge "Camera: avoid copying of HalRequest"
2018-02-21 TreeHugger RobotMerge "Call deleteAidingData to clean up after injectBe...
2018-02-21 Andrew ScullMerge "AuthSecret: make method oneway"
2018-02-21 Yin-Chia YehMerge "Camera: implement external camera dumpState...
2018-02-20 Zhuoyao ZhangMerge "Convert drm hal test to use VtsHalHidlTargetTest...
2018-02-16 TreeHugger RobotMerge "Audio HAL V4: Add Hearing aid output device"
2018-02-16 Chong ZhangMerge "MediaCas: use HidlMemory to avoid handle leaks"
2018-02-16 Kevin RocardMerge "Audio HAL V4: Switch back to 32 bit AudioDevice"
2018-02-16 TreeHugger RobotMerge "Fix LTE Timing Advance Doc String"
2018-02-16 TreeHugger RobotMerge "Camera: implement external camera flush"
2018-02-16 Eric SchwarzenbachFix comments for link capacity and signal strength...
2018-02-16 TreeHugger RobotMerge "Refactor NN API VTS tests and add v1.1 tests"
2018-02-16 Eric SchwarzenbachMerge "Use new AccessNetwork type in the reporting...
2018-02-16 Brian YoungMerge "Restore "Add "Unlocked device required" paramete...
2018-02-16 nharoldMerge "Fixes to Align TdScdma Reports with All Others...
2018-02-16 Treehugger RobotMerge "Use new AccessNetwork type in the reporting...
2018-02-16 nharoldMerge "Update WcdmaSignalStrength to add RAT-specific...
2018-02-16 Zhuoyao ZhangMerge "Convert thermal hal test to use VtsHalHidlTarget...
2018-02-16 Zhuoyao ZhangMerge "Convert nfc hal test to use VtsHalHidlTargetTest...
2018-02-16 Zhuoyao ZhangMerge "Convert health hal test to use VtsHalHidlTargetT...
2018-02-15 Zhuoyao ZhangMerge "Convert nfc hal test to use VtsHalHidlTargetTest...
2018-02-15 Zhuoyao ZhangMerge "Convert nfc hal test to use VtsHalHidlTargetTest...
2018-02-15 nharoldMerge "Fixes to Align TdScdma Reports with All Others"
2018-02-15 nharoldMerge "Update WcdmaSignalStrength to add RAT-specific...
2018-02-15 Zhuoyao ZhangMerge "Convert thermal hal test to use VtsHalHidlTarget...
2018-02-15 Zhuoyao ZhangMerge "Convert nfc hal test to use VtsHalHidlTargetTest...
next