]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - secure_element
Merge "Camera: Don't hold 'mLock' when closing the camera session" into pie-vts-dev
[android/platform-hardware-interfaces.git] / secure_element /
2018-08-20 Yin-Chia Yeh[automerger skipped] resolve merge conflicts of cd02298...
2018-08-20 Kevin RocardEffect VTS: Allow an effect proxy as pre/post processing
2018-08-13 sqianresolve merge conflicts of 898d05a713a693670cd450ff3f50...
2018-08-10 Pawin Vongmasaresolve merge conflicts of b92f1d2e1be35b331b18589a8cde...
2018-08-10 Kevin Rocard[automerger skipped] Audio VTS: run tear-down hooks...
2018-08-10 Kevin RocardAudio VTS: run tear-down hooks in LIFO instead of FIFO
2018-08-10 sqian[automerger skipped] Fix setBandMode. am: ab2b8bf919...
2018-06-07 TreeHugger RobotMerge "Fix comments and internal names about SEEK opera...
2018-06-07 TreeHugger RobotMerge "secure_element: vts: Fix openBasicChannel and...
2018-06-07 Ruchi Kandoisecure_element: vts: Fix openBasicChannel and transmit...
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc am: 5de1ae23f9...
2018-05-24 Pawin VongmasaAdd multichannel support am: c678d51bdc am: 9886d749d4
2018-05-11 Chong Zhangcas: do not use hidl_memory if size is > SIZE_MAX
2018-04-26 Michael Butler[automerger skipped] Relax NeuralNetwork's VTS positive...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 Peng XuMerge "Ignore meta sensor events when checking values...
2018-04-10 TreeHugger RobotMerge "Remove DiskStat checks from VTS Health HAL test...
2018-04-10 TreeHugger RobotMerge "Audio V4: Synchronize the devices between the...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Srinivas Dasari[WIFI][VTS]: Check for the Logger capability Support...
2018-04-10 Emilian Peev[automerger skipped] Camera: Allocate graphics buffers...
2018-04-09 Chong ZhangMerge "cas: fix UAF in descrambler" into pi-dev
2018-04-09 Chong Zhang[automerger skipped] Merge "cas: fix UAF in descrambler...
2018-04-06 TreeHugger RobotMerge "Camera: various external camera fixes" into...
2018-04-04 TreeHugger RobotMerge "Correct TripleDes tests." into pi-dev
2018-04-04 TreeHugger RobotMerge "Camera: use finer lock in external camera Output...
2018-04-03 TreeHugger RobotMerge "Update VHAL types.hal" into pi-dev
2018-04-02 TreeHugger RobotMerge "Update doc in Gnss Hal v1.1" into pi-dev
2018-04-02 TreeHugger RobotMerge "Camera: Validate physical camera related metadat...
2018-04-02 TreeHugger RobotMerge "keymaster: provide instance name to getService...
2018-04-02 Yifan HongMerge "matrix: add radio.config" into pi-dev
2018-03-31 Tomasz WasilczykMerge "Clear out ambiguity in broadcastradio@2.0 commen...
2018-03-31 TreeHugger RobotMerge "secure_element: VTS: Remove MANAGE_CHANNEL comma...
2018-03-30 Ruchi Kandoisecure_element: VTS: Remove MANAGE_CHANNEL commands...
2018-03-30 Yuexi Maresolve merge conflicts of e41f291381eaafa2f9d946e85f94...
2018-03-29 Yuexi Ma[automerger skipped] Merge "rename VtsHalEvsV1_0Target...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-21 Emilian PeevCamera: Remove length check in case of 'getCameraIdList...
2018-03-09 Myles WatsonMerge "resolve merge conflicts of b9492b5fe94cb99b5f799...
2018-03-07 Myles Watsonresolve merge conflicts of 8a28de7a8c3d36e648e90ed2fca2...
2018-03-02 Yin-Chia YehMerge "Camera: add profiling traces"
2018-03-02 Treehugger RobotMerge "configstore: allow to USE_CONTEXT_PRIORITY by...
2018-03-01 TreeHugger RobotMerge "Use std::unordered_map for mTagToTypeMap"
2018-03-01 Yin-Chia YehMerge "Camera: add external camera fps control"
2018-03-01 TreeHugger RobotMerge "audio: Initialize processstate with vndbinder"
2018-02-28 TreeHugger RobotMerge "Add boilerplate default implementation for Gnss...
2018-02-28 Ruchi KandoiMerge "Add init() as a part of Secure Element VTS test...
2018-02-28 Ruchi KandoiMerge "Add init() as a part of Secure Element VTS test...
2018-02-28 Ruchi KandoiMerge "Add init() as a part of Secure Element VTS test"
2018-02-28 Treehugger RobotMerge "Add init() as a part of Secure Element VTS test"
2018-02-26 Ruchi KandoiAdd init() as a part of Secure Element VTS test
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-24 Polina Bondarenkothermal: fix VTS test for default implementation am...
2018-02-06 TreeHugger RobotMerge "External camera: add device config file"
2018-02-06 Steve PaikMerge "Add ENGINE_OIL_LEVEL, PARKING_BRAKE_AUTO_APPLY"
2018-02-06 Scott RandolphMerge "Remove IAudioControlCallback for P"
2018-02-05 Oscar ShuMerge "Followup CL for ringbuffer in wifi_hal"
2018-02-05 TreeHugger RobotMerge "Camera: fix external camera FD double close"
2018-02-03 TreeHugger RobotMerge "Modify FAN_DIRECTION to be a bit mask"
2018-02-02 Roshan PiusMerge "wpa/hostapd(interface): Add terminate method"
2018-02-02 TreeHugger RobotMerge "Add vts tests for new drm@1.1 methods"
2018-02-02 Jeff TinkerMerge "Fix incorrect comment in ICryptoFactory.hal"
2018-02-02 Ruchi KandoiMerge "Add VTS Test for Secure Element HAL" am: 6a75cdb...
2018-02-02 Ruchi KandoiMerge "Add VTS Test for Secure Element HAL" am: 6a75cdbe96
2018-02-02 TreeHugger RobotMerge "Audio V4: Create audio V4.0 .hal makefiles"
2018-02-02 TreeHugger RobotMerge changes from topic "audio-hal-v4"
2018-02-02 Treehugger RobotMerge "Create NeuralNetworks HAL v1.1 for new Operation...
2018-02-02 Ruchi KandoiMerge "Add VTS Test for Secure Element HAL"
2018-02-01 Treehugger RobotMerge "Displaying HD audio indicator for GSM/CDMA calls"
2018-02-01 Chia-I WuMerge changes from topic "gralloc-mapper-cleanup"
2018-02-01 Ruchi KandoiMerge "Add VTS Test for Secure Element HAL"
2018-01-31 TreeHugger RobotMerge "Add GNSS VTS test for IGnssDebug.TimeDebug value...
2018-01-31 Ruchi KandoiAdd VTS Test for Secure Element HAL
2018-01-31 Miao WangMerge "Create NeuralNetworks HAL v1.1 for new Operation...
2018-01-31 Ruchi KandoiAdd SecureElement HAL interface am: 241e5aba9e am:...
2018-01-31 Ruchi KandoiAdd SecureElement HAL interface am: 241e5aba9e
2018-01-31 Ruchi KandoiAdd SecureElement HAL interface
2018-01-26 Ruchi KandoiAdd SecureElement HAL interface