]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/history - wifi
Add 4.14.0 kernel to all matrices.
[android/platform-hardware-interfaces.git] / wifi /
2018-04-06 TreeHugger RobotMerge "Camera: various external camera fixes" into...
2018-04-04 TreeHugger RobotMerge "Correct TripleDes tests." into pi-dev
2018-04-04 TreeHugger RobotMerge "Camera: use finer lock in external camera Output...
2018-04-03 TreeHugger RobotMerge "Update VHAL types.hal" into pi-dev
2018-04-02 TreeHugger RobotMerge "Update doc in Gnss Hal v1.1" into pi-dev
2018-04-02 TreeHugger RobotMerge "Camera: Validate physical camera related metadat...
2018-04-02 Yifan HongMerge "matrix: add radio.config" into pi-dev
2018-03-31 Tomasz WasilczykMerge "Clear out ambiguity in broadcastradio@2.0 commen...
2018-03-31 TreeHugger RobotMerge "secure_element: VTS: Remove MANAGE_CHANNEL comma...
2018-03-31 TreeHugger RobotMerge "Update RegState for new CellIdentity types"...
2018-03-30 TreeHugger RobotMerge "SetMacAddress in Vendor HAL" into pi-dev
2018-03-30 Enrico GranataMerge "Teach VehiclePropertyStore to not propagate...
2018-03-30 TreeHugger RobotMerge "Support query microphones information." into...
2018-03-30 Yuexi Maresolve merge conflicts of e41f291381eaafa2f9d946e85f94...
2018-03-29 Yuexi Maresolve merge conflicts of a9543fee6b3f5e9609206d3a21a4...
2018-03-29 Tom CherryMerge "Add BLOCK_SUSPEND capability for Bluetooth HAL...
2018-03-29 Yuexi Ma[automerger skipped] Merge "rename VtsHalEvsV1_0Target...
2018-03-29 Yuexi Ma[automerger skipped] Merge "rename VtsHalEvsV1_0Target...
2018-03-29 Yuexi MaMerge "rename VtsHalEvsV1_0Target module to VtsHalEvsV1...
2018-03-29 Treehugger RobotMerge "rename VtsHalEvsV1_0Target module to VtsHalEvsV1...
2018-03-29 Tomasz WasilczykMerge "Update program list when switching bands." into...
2018-03-28 Michael ButlerMerge "NN validation tests" into pi-dev
2018-03-28 TreeHugger RobotMerge "Camera: Add Monochrome camera capability" into...
2018-03-28 TreeHugger RobotMerge "matrix: camera HAL uses [^/]+/[0-9]+ instance...
2018-03-28 TreeHugger RobotMerge "Audio V4: Add V2 XML in V4 effect" into pi-dev
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 TreeHugger RobotMerge "matrix: NN HAL uses .* instance." into pi-dev
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported am:...
2018-03-28 Yifan HongMerge "matrix: radio HAL uses slot[0-9]+ instance....
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported
2018-03-28 Roshan Piuswifi(vts): Skip tests if feature not supported
2018-03-28 Keun Soo YimMerge "Add more drm@1.1 VTS structure tests" into pi-dev
2018-03-28 Ahmed ElArabawyMerge changes from topic "propagate_eap_failure" into...
2018-03-27 Jong Wook KimSetMacAddress in Vendor HAL
2018-03-27 TreeHugger RobotMerge "Camera2: Add distortion correction support"...
2018-03-27 Ahmed ElArabawyWiFi: Add vts tests for ISupplicantStaIface 1.1
2018-03-27 Ahmed ElArabawyWiFi: supplicant HAL: Modify onEapFailure Callback
2018-03-27 Tom CherryMerge "Add capabilities to bluetooth HAL service" into...
2018-03-27 Bernie InnocentiMerge "Wire readApfPacketFilterData() to the legacy...
2018-03-26 TreeHugger RobotMerge "Add Vendor comand to ConfirmationUI support...
2018-03-26 David GrossMerge "Add validation tests for consistency of model...
2018-03-26 TreeHugger RobotMerge "Fix AP_POWER_BOOTUP_REASON to be static" into...
2018-03-26 Bernie InnocentiWire readApfPacketFilterData() to the legacy hal
2018-03-23 Enrico GranataMerge "Make toInt() a little bit shorter by moving...
2018-03-23 Tom CherryMerge "Add capabilities to wifi HAL service" into pi-dev
2018-03-23 Tom CherryAdd capabilities to wifi HAL service
2018-03-21 Roshan Piuswifi(vts): Skip tests if feature not supported
2018-03-21 Emilian PeevCamera: Remove length check in case of 'getCameraIdList...
2018-03-19 TreeHugger RobotMerge changes I20310606,Ic23b7fb2 into pi-dev
2018-03-12 TreeHugger RobotMerge "Implement Gnss::start() and Gnss::stop()" into...
2018-03-09 TreeHugger RobotMerge "Only allow audio V4 for devices targeting level...
2018-03-09 Carmen JacksonMerge "Add hwcomposer to the system-background cpuset...
2018-03-09 Etan CohenMerge "[RTT][AWARE] Support new legacy error codes...
2018-03-09 Myles WatsonMerge "resolve merge conflicts of b9492b5fe94cb99b5f799...
2018-03-08 Etan Cohen[RTT][AWARE] Support new legacy error codes for Aware RTT
2018-03-07 Myles Watsonresolve merge conflicts of 8a28de7a8c3d36e648e90ed2fca2...
2018-03-07 Myles Watsonresolve merge conflicts of b9492b5fe94cb99b5f79964a4931...
2018-03-07 TreeHugger RobotMerge changes from topic "audio-hal-v4-pi-dev" into...
2018-03-07 TreeHugger RobotMerge "supplicant/hostapd(vts): Test for terminate...
2018-03-06 Roshan Piussupplicant/hostapd(vts): Test for terminate
2018-03-06 Myles Watsonresolve merge conflicts of 8a28de7a8c3d36e648e90ed2fca2...
2018-03-06 Ahmed ElArabawyMerge "WiFi: Wait for driver to be ready before operati...
2018-03-06 Ahmed ElArabawyWiFi: Wait for driver to be ready before operation
2018-03-06 Myles WatsonBluetooth: Relax NO_OP and SCO checks am: 8a28de7a8c
2018-03-05 Bernie InnocentiMerge "Add a wifi hal interface to read-back the APF...
2018-03-02 Bernie InnocentiAdd a wifi hal interface to read-back the APF memory.
2018-03-02 TreeHugger RobotMerge "Add functional tests for bad input to 1.2"
2018-03-02 Kevin RocardMerge "Audio V4: Add owner files for implementations"
2018-03-02 Yin-Chia YehMerge "Camera: add profiling traces"
2018-03-02 TreeHugger RobotMerge "wifi(implementation): Remove support for STA...
2018-03-02 Roshan Piuswifi(implementation): Remove support for STA + STA...
2018-03-02 CassieMerge "Add VTS test for getCellInfoList_1_2" am: 6a8364...
2018-03-02 CassieMerge "Add VTS test for getCellInfoList_1_2" am: 6a83645f64
2018-03-02 Zhuoyao ZhangMerge "Convert auth secret hal test to use VtsHalHidlTa...
2018-03-02 chenhgMerge "configstore: allow to USE_CONTEXT_PRIORITY by...
2018-03-02 chenhgMerge "configstore: allow to USE_CONTEXT_PRIORITY by...
2018-03-02 yinxuAdd vts response functions for Radio Response 1.2 am...
2018-03-02 yinxuAdd vts response functions for Radio Response 1.2 am...
2018-03-01 Ahmed ElArabawyMerge "WiFi: Add VTS for Wifi HAL V1.2"
2018-03-01 TreeHugger RobotMerge "Use std::unordered_map for mTagToTypeMap"
2018-03-01 Myles WatsonBluetooth: Relax NO_OP and SCO checks am: 72382e3014...
2018-03-01 Myles WatsonBluetooth: Relax NO_OP and SCO checks am: 72382e3014
2018-03-01 Ahmed ElArabawyWiFi: Add VTS for Wifi HAL V1.2
2018-03-01 Yin-Chia YehMerge "Camera: add external camera fps control"
2018-03-01 TreeHugger RobotMerge "audio: Initialize processstate with vndbinder"
2018-03-01 Jack YuAdded new VTS test cases for v1.2 data call APIs am...
2018-03-01 Jack YuAdded new VTS test cases for v1.2 data call APIs am...
2018-02-28 TreeHugger RobotMerge "Add boilerplate default implementation for Gnss...
2018-02-28 Ruchi KandoiMerge "Add init() as a part of Secure Element VTS test...
2018-02-28 Ruchi KandoiMerge "Add init() as a part of Secure Element VTS test...
2018-02-28 Eric SchwarzenbachAdd VTS tests for 1.2 reporting criteria am: 8bdc4e04e2...
2018-02-28 Eric SchwarzenbachAdd VTS tests for 1.2 reporting criteria am: 8bdc4e04e2
2018-02-28 Roshan PiusMerge "supplicant 1.0 (vts): Add ifaces at init for...
2018-02-27 TreeHugger RobotMerge "Update documentation of gnssRequestLocationCb"
2018-02-27 Michael ButlerMerge "Relax NeuralNetwork's VTS positive and negative...
2018-02-27 Roshan Piussupplicant 1.0 (vts): Add ifaces at init for 1.1 HAL...
2018-02-27 Ecco ParkMerge "wpa_supplicant(sta_network): Support encrypted...
next