Merge "Apply clang-format to Bluetooth related HAL code"
Merge pie-platform-release to aosp-master - DO NOT MERGE
Change-Id: I052cfae991c063eb5631e681be600d2da8111fc6
Change-Id: I052cfae991c063eb5631e681be600d2da8111fc6
Merge "Clarify C/No reflects the tracked portion of a GnssMeasurement"
Apply clang-format to Bluetooth related HAL code
- cp system/bt/.clang-format hardware/interfaces/bluetooth/
- modify hardware/interfaces/bluetooth/.clang-format to match context
- find . -type f \( -iname \*.cpp -o -iname \*.h -o -iname \*.cc \) | xargs clang-format --style=file -i
Test: make
Change-Id: I82e4f26e1efeb715aff7de8a15c3db06e02967a4
- cp system/bt/.clang-format hardware/interfaces/bluetooth/
- modify hardware/interfaces/bluetooth/.clang-format to match context
- find . -type f \( -iname \*.cpp -o -iname \*.h -o -iname \*.cc \) | xargs clang-format --style=file -i
Test: make
Change-Id: I82e4f26e1efeb715aff7de8a15c3db06e02967a4
Merge "Add statically linked boot HAL impl in recovery"
Merge "Fix implicit-fallthrough warnings."
Merge "Fix implicit-fallthrough warnings. DO NOT MERGE."
Merge "Allow implicit-fallthrough warnings locally."
Merge "run vts build rule updater when hal make files are updated"
Allow implicit-fallthrough warnings locally. DO NOT MERGE.
It will be a global error by default.
This change is not needed for goog/master.
Test: make checkbuild
Bug: 112564944
Change-Id: Ie90ad1f59f6922da6cecd4a0ac136b1e42b6d482
Exempt-From-Owner-Approval: do not block on new warnings
It will be a global error by default.
This change is not needed for goog/master.
Test: make checkbuild
Bug: 112564944
Change-Id: Ie90ad1f59f6922da6cecd4a0ac136b1e42b6d482
Exempt-From-Owner-Approval: do not block on new warnings
Allow implicit-fallthrough warnings locally.
It will be a global error by default.
Test: make checkbuild
Bug: 112564944
Change-Id: I3e914835fcb4ee97662ab51136f143e665d0ba01
Exempt-From-Owner-Approval: do not block on new warnings
It will be a global error by default.
Test: make checkbuild
Bug: 112564944
Change-Id: I3e914835fcb4ee97662ab51136f143e665d0ba01
Exempt-From-Owner-Approval: do not block on new warnings
Merge changes from topic "nnapi-cherrypick-from-master-and-pi-dev-to-aosp2"
* changes:
Adds TENSOR_FLOAT16 operand type.
Add TENSOR_QUANT16_ASYMM to operand types
Add new OperandType BOOL.
Add HAL entry to allow querying device impl version.
* changes:
Adds TENSOR_FLOAT16 operand type.
Add TENSOR_QUANT16_ASYMM to operand types
Add new OperandType BOOL.
Add HAL entry to allow querying device impl version.
Merge "Fix implicit-fallthrough warnings."
Fix implicit-fallthrough warnings. DO NOT MERGE.
These changes are not needed in goog/master.
Test: make checkbuild
Bug: 112564944
Change-Id: I4f1727d9b33108d34d314787460aa1d2298ae5b2
These changes are not needed in goog/master.
Test: make checkbuild
Bug: 112564944
Change-Id: I4f1727d9b33108d34d314787460aa1d2298ae5b2
Fix implicit-fallthrough warnings.
Test: make checkbuild
Bug: 112564944
Change-Id: Ib93559a5c1512861f9746cd28d8b19073ce92aa8
Test: make checkbuild
Bug: 112564944
Change-Id: Ib93559a5c1512861f9746cd28d8b19073ce92aa8
Fix implicit-fallthrough warnings.
Test: make checkbuild
Bug: 112564944
Change-Id: Ifc8b7444b95d667b0d185c7d45b3f15278d4af2f
Test: make checkbuild
Bug: 112564944
Change-Id: Ifc8b7444b95d667b0d185c7d45b3f15278d4af2f
Clarify C/No reflects the tracked portion of a GnssMeasurement
Test: Comment updates only. Verified it builds.
Bug: 117942478
Change-Id: Ia069fbdb396b5bfc76d3dbeabd0c54622f568ade
Fixes: 117942478
Test: Comment updates only. Verified it builds.
Bug: 117942478
Change-Id: Ia069fbdb396b5bfc76d3dbeabd0c54622f568ade
Fixes: 117942478
run vts build rule updater when hal make files are updated
Test: ./update-makefiles.sh
Bug: 117826861
Change-Id: I7c7b22ecff1a373cd905fedd96bdaa12e1a558f0
Test: ./update-makefiles.sh
Bug: 117826861
Change-Id: I7c7b22ecff1a373cd905fedd96bdaa12e1a558f0
Add statically linked boot HAL impl in recovery
The default Treble boot HAL implementation currently can only work in
recovery on devices that specifically build their libhardware
implementation as a shared library for recovery.
This CL adds the option to statically link the libhardware
implementation in recovery instead of finding it using
hw_get_module(). This new approach allows devices that define
PRODUCT_STATIC_BOOT_CONTROL_HAL to begin using the Treble HAL in
recovery without requiring device-specific changes.
A previous version of this CL broke some device builds by omitting
libbase.recovery from LOCAL_SHARED_LIBRARIES. This version fixes that
issue.
Test: adb sideload succeeds
Bug: 78598708
Change-Id: I1c2ef7fa59575ac7975129f7544f741459b8540e
Signed-off-by: Connor O'Brien <connoro@google.com>
The default Treble boot HAL implementation currently can only work in
recovery on devices that specifically build their libhardware
implementation as a shared library for recovery.
This CL adds the option to statically link the libhardware
implementation in recovery instead of finding it using
hw_get_module(). This new approach allows devices that define
PRODUCT_STATIC_BOOT_CONTROL_HAL to begin using the Treble HAL in
recovery without requiring device-specific changes.
A previous version of this CL broke some device builds by omitting
libbase.recovery from LOCAL_SHARED_LIBRARIES. This version fixes that
issue.
Test: adb sideload succeeds
Bug: 78598708
Change-Id: I1c2ef7fa59575ac7975129f7544f741459b8540e
Signed-off-by: Connor O'Brien <connoro@google.com>
Merge pi-dr1-dev to aosp-master
Change-Id: Ida0bc98526f4fc7a1c20f5bbd3210b2f6156d459
Change-Id: Ida0bc98526f4fc7a1c20f5bbd3210b2f6156d459
graphics: composer@2.2 does not require mapper@2.1
am: 0eafa742c6
Change-Id: I6f045113a3c0218a4b8f2c8e794892a21c1fc306
am: 0eafa742c6
Change-Id: I6f045113a3c0218a4b8f2c8e794892a21c1fc306
Adds TENSOR_FLOAT16 operand type.
Bug: 113563458
Test: VtsHalNeuralnetworksV1_2TargetTest --hal_service_instance=android.hardware.neuralnetworks@1.2::IDevice/sample-all
Change-Id: If12ceff428e1b1a90ef99b7353f0df60d4ef8010
Merged-In: If12ceff428e1b1a90ef99b7353f0df60d4ef8010
(cherry picked from commit 19d63453d4c2723c3fad4ce7f852f548d761278e)
Bug: 113563458
Test: VtsHalNeuralnetworksV1_2TargetTest --hal_service_instance=android.hardware.neuralnetworks@1.2::IDevice/sample-all
Change-Id: If12ceff428e1b1a90ef99b7353f0df60d4ef8010
Merged-In: If12ceff428e1b1a90ef99b7353f0df60d4ef8010
(cherry picked from commit 19d63453d4c2723c3fad4ce7f852f548d761278e)
Add TENSOR_QUANT16_ASYMM to operand types
Add new OperandType::TENSOR_QUANT16_ASYMM.
Add VTS validation for the new type.
Bug: 113561892
Test: NeuralNetworksTest_static
Test: VtsHalNeuralnetworksV1_0TargetTest
Test: VtsHalNeuralnetworksV1_1TargetTest
Test: VtsHalNeuralnetworksV1_2TargetTest
Change-Id: I4f9ed6a33d5d3ec227e9f335df71954c73edf344
Merged-In: I4f9ed6a33d5d3ec227e9f335df71954c73edf344
(cherry picked from commit 5d7c99527e7bad07d6ab5413bcfd14cec5df5f31)
Add new OperandType::TENSOR_QUANT16_ASYMM.
Add VTS validation for the new type.
Bug: 113561892
Test: NeuralNetworksTest_static
Test: VtsHalNeuralnetworksV1_0TargetTest
Test: VtsHalNeuralnetworksV1_1TargetTest
Test: VtsHalNeuralnetworksV1_2TargetTest
Change-Id: I4f9ed6a33d5d3ec227e9f335df71954c73edf344
Merged-In: I4f9ed6a33d5d3ec227e9f335df71954c73edf344
(cherry picked from commit 5d7c99527e7bad07d6ab5413bcfd14cec5df5f31)
Add new OperandType BOOL.
- Add new enum OperandType::BOOL.
- Add v1.2 Operand, OperandType.
- Add VTS validation tests for BOOL.
Bug: 117423393
Test: NeuralNetworksTest_static
Test: VtsHalNeuralnetworksV1_2TargetTest
Change-Id: I420e2afeb09b881a499eee6b138c1f26e9874f5a
Merged-In: I420e2afeb09b881a499eee6b138c1f26e9874f5a
(cherry picked from commit abad9eac448cc61582a9a658a231010358051b97)
- Add new enum OperandType::BOOL.
- Add v1.2 Operand, OperandType.
- Add VTS validation tests for BOOL.
Bug: 117423393
Test: NeuralNetworksTest_static
Test: VtsHalNeuralnetworksV1_2TargetTest
Change-Id: I420e2afeb09b881a499eee6b138c1f26e9874f5a
Merged-In: I420e2afeb09b881a499eee6b138c1f26e9874f5a
(cherry picked from commit abad9eac448cc61582a9a658a231010358051b97)
Add HAL entry to allow querying device impl version.
Bug: 111425781
Bug: 112661050
Test: mm
Test: NeuralNetworksTest_static
Change-Id: I32527fa09e45459bc9759f5b679646073cf96785
Merged-In: I32527fa09e45459bc9759f5b679646073cf96785
(cherry picked from commit 44b029b181b554931367c670f8bd026ceacc0536)
Bug: 111425781
Bug: 112661050
Test: mm
Test: NeuralNetworksTest_static
Change-Id: I32527fa09e45459bc9759f5b679646073cf96785
Merged-In: I32527fa09e45459bc9759f5b679646073cf96785
(cherry picked from commit 44b029b181b554931367c670f8bd026ceacc0536)
Merge "Fix implicit fallthrough warnings."
am: 591171a659
Change-Id: I6fc2f638f3e7559a1ec2face4c8ec2dab51506be
am: 591171a659
Change-Id: I6fc2f638f3e7559a1ec2face4c8ec2dab51506be
Merge "Fix implicit fallthrough warnings."
graphics: composer@2.2 does not require mapper@2.1
Fix composer@2.2 VTS to not require mapper@2.1. We will need a
better test infra before things get too complex.
Bug: 112248843
Test: manual
Change-Id: Ia71a102742fd26f14e8edf3f43f3351786350ccd
Merged-In: Ia71a102742fd26f14e8edf3f43f3351786350ccd
Fix composer@2.2 VTS to not require mapper@2.1. We will need a
better test infra before things get too complex.
Bug: 112248843
Test: manual
Change-Id: Ia71a102742fd26f14e8edf3f43f3351786350ccd
Merged-In: Ia71a102742fd26f14e8edf3f43f3351786350ccd
Merge "Update makefiles."
Update makefiles.
Some of these were out of date.
Bug: N/A
Test: N/A
Change-Id: I25a2706b95e199f5728cda5a5e4e2b23c60a8d40
Some of these were out of date.
Bug: N/A
Test: N/A
Change-Id: I25a2706b95e199f5728cda5a5e4e2b23c60a8d40
Fix implicit fallthrough warnings.
Test: make checkbuild
Bug: 112564944
Change-Id: Ib2b337146de86e4abe40ded5932196f1b8b698c6
Test: make checkbuild
Bug: 112564944
Change-Id: Ib2b337146de86e4abe40ded5932196f1b8b698c6
removed unused line.
Test: builds
Change-Id: I6df9338de150e35147c191a551b1e5eb538db32e
Test: builds
Change-Id: I6df9338de150e35147c191a551b1e5eb538db32e
Merge "compatibility matrices: move to soong"
am: 9cfddb6282
Change-Id: I3e88b69a9ed6f57c1b5d011349473b3c568bc74f
am: 9cfddb6282
Change-Id: I3e88b69a9ed6f57c1b5d011349473b3c568bc74f
Merge "Avoid segfaults if disconnect USB camera while preview."
am: 4dce57e459
Change-Id: I08b09d87cbaf4ed3c18ccbd5cd28b3de8fa4c8e4
am: 4dce57e459
Change-Id: I08b09d87cbaf4ed3c18ccbd5cd28b3de8fa4c8e4
Merge "compatibility matrices: move to soong"
Merge "Avoid segfaults if disconnect USB camera while preview."
Merge "Restored 'maxConnsTime' and 'maxConns' in data profile"
am: bcb0c1b49a
Change-Id: I376197118faadef4175ed97be87ed50b4573e919
am: bcb0c1b49a
Change-Id: I376197118faadef4175ed97be87ed50b4573e919
Merge "Restored 'maxConnsTime' and 'maxConns' in data profile"
compatibility matrices: move to soong
* Kernel config requirements are built as
separate rules in kernel/configs. All kernel requirements
(including minlts and configs) are represented there.
* device framework compatibility matrix and final
framework compatibility matrix need special environment
variables, so they are not generic enough to be written
in the soong rule.
See compatibility_matrices/Android.bp for sample usages.
Test: builds and compare output before change
Change-Id: I53bf88362314f96487ca243c9292570b7931f24b
* Kernel config requirements are built as
separate rules in kernel/configs. All kernel requirements
(including minlts and configs) are represented there.
* device framework compatibility matrix and final
framework compatibility matrix need special environment
variables, so they are not generic enough to be written
in the soong rule.
See compatibility_matrices/Android.bp for sample usages.
Test: builds and compare output before change
Change-Id: I53bf88362314f96487ca243c9292570b7931f24b
Fix implicit fallthrough warnings.
am: 40b77ef6b5
Change-Id: I0eee7ff35ef8943847d6966720a2c5477fc21fd0
am: 40b77ef6b5
Change-Id: I0eee7ff35ef8943847d6966720a2c5477fc21fd0
Fix implicit fallthrough warnings.
Test: make checkbuild
Bug: 112564944
Change-Id: Iaaa0e2c325e860572d058ae27a7ad7dc00134564
Test: make checkbuild
Bug: 112564944
Change-Id: Iaaa0e2c325e860572d058ae27a7ad7dc00134564
Restored 'maxConnsTime' and 'maxConns' in data profile
These two fields are still needed for some carriers. Should
not be removed in 1.3. Reverted back to what we have in 1.0.
Test: Telephony sanity tests
Bug: 73659459
Change-Id: I33e7b9b0cb26b56fc3c0e011557657136cb38a6c
These two fields are still needed for some carriers. Should
not be removed in 1.3. Reverted back to what we have in 1.0.
Test: Telephony sanity tests
Bug: 73659459
Change-Id: I33e7b9b0cb26b56fc3c0e011557657136cb38a6c
Avoid segfaults if disconnect USB camera while preview.
BUG: 117575807
Test: manual test by disconnect USB camera while preview.
Change-Id: Ia74b03e7f2a672efd9e9dfd651b5894529daeeee
BUG: 117575807
Test: manual test by disconnect USB camera while preview.
Change-Id: Ia74b03e7f2a672efd9e9dfd651b5894529daeeee
Merge "Audio: Do not sanitize android.hardware.audio@2.0-service"
am: f06fb17cd7
Change-Id: I743c1afaae84f560879cab6afba0fe31978ef871
am: f06fb17cd7
Change-Id: I743c1afaae84f560879cab6afba0fe31978ef871
5 years agoMerge "Audio: Do not sanitize android.hardware.audio@2.0-service" android-o-mr1-iot-release-smart-display-r3
Merge "Audio: Do not sanitize android.hardware.audio@2.0-service"
Merge "audio: Add a missing break to EffectsFactory::getAllDescriptors"
am: ef84854472
Change-Id: I47effe88ae8467f8570556ad56ced648abddc4d7
am: ef84854472
Change-Id: I47effe88ae8467f8570556ad56ced648abddc4d7
Merge "audio: Add a missing break to EffectsFactory::getAllDescriptors"
Merge "Add monostate to optional safe unions."
am: 17c437eac1
Change-Id: I28c1b888c3611262dbbbb48f5b3886b7e41ac56d
am: 17c437eac1
Change-Id: I28c1b888c3611262dbbbb48f5b3886b7e41ac56d
Merge "Add monostate to optional safe unions."
audio: Add a missing break to EffectsFactory::getAllDescriptors
Would the legacy HAL return -ENOENT while retrieving an effect,
the enumeration has to be aborted, and the effects queried so far
need to be returned. A missing 'break' was causing returning
no effects at all.
Bug: 117567478
Test: make
Change-Id: I7cc05004f88b39272d06d2ed33a0693f8e1e3d04
Merged-In: I7cc05004f88b39272d06d2ed33a0693f8e1e3d04
Would the legacy HAL return -ENOENT while retrieving an effect,
the enumeration has to be aborted, and the effects queried so far
need to be returned. A missing 'break' was causing returning
no effects at all.
Bug: 117567478
Test: make
Change-Id: I7cc05004f88b39272d06d2ed33a0693f8e1e3d04
Merged-In: I7cc05004f88b39272d06d2ed33a0693f8e1e3d04
Add monostate to optional safe unions.
Bug: 116156870
Test: hidl_test, hidl_test_java
Change-Id: Ie17a80dee982775e267a39086016071ac2361fb5
Bug: 116156870
Test: hidl_test, hidl_test_java
Change-Id: Ie17a80dee982775e267a39086016071ac2361fb5
Merge "Divide BBOX_TRANSFORM into 2 ops."
am: 76c45692bf
Change-Id: Ic45409f36b1084c32c14ec708cda52b9c760865e
am: 76c45692bf
Change-Id: Ic45409f36b1084c32c14ec708cda52b9c760865e
Merge "Divide BBOX_TRANSFORM into 2 ops."
Audio: Do not sanitize android.hardware.audio@2.0-service
Until the underlying bug is fixed, do not produce a sanitized
binary.
Bug: 117506164
Bug: 117580200
Test: m && SANITIZE_TARGET=address m
Change-Id: I4e6d1206512513c687f7ae065d2974c55c617b61
Until the underlying bug is fixed, do not produce a sanitized
binary.
Bug: 117506164
Bug: 117580200
Test: m && SANITIZE_TARGET=address m
Change-Id: I4e6d1206512513c687f7ae065d2974c55c617b61
Merge "tests IFoo: WithFmq is more complicated."
am: da1d79bf07
Change-Id: I2256aaad4016dc2ed6176bff8e9bf897f53b52ae
am: da1d79bf07
Change-Id: I2256aaad4016dc2ed6176bff8e9bf897f53b52ae
Merge "tests IFoo: WithFmq is more complicated."
Divide BBOX_TRANSFORM into 2 ops.
Divide BBOX_TRANSFORM op into 2 ops
- AXIS_ALIGNED_BBOX_TRANSFORM
- ROTATED_BBOX_TRANSFORM
Rotated bounding boxes use different tensor format than axis-aligned
bounding boxes, and it would be less confusing if they were represented
by a separate operator code.
Bug: 113562630
Test: NeuralNetworksTest_static
Test: VtsHalNeuralnetworksV1_xTargetTest with sample driver
Change-Id: Ie08f2e0d0da77f6750766a394969653478d054d5
Merged-In: Ie08f2e0d0da77f6750766a394969653478d054d5
(cherry picked from commit d2bae1c268f8ef8e313441450e226d68ab515d9a)
Divide BBOX_TRANSFORM op into 2 ops
- AXIS_ALIGNED_BBOX_TRANSFORM
- ROTATED_BBOX_TRANSFORM
Rotated bounding boxes use different tensor format than axis-aligned
bounding boxes, and it would be less confusing if they were represented
by a separate operator code.
Bug: 113562630
Test: NeuralNetworksTest_static
Test: VtsHalNeuralnetworksV1_xTargetTest with sample driver
Change-Id: Ie08f2e0d0da77f6750766a394969653478d054d5
Merged-In: Ie08f2e0d0da77f6750766a394969653478d054d5
(cherry picked from commit d2bae1c268f8ef8e313441450e226d68ab515d9a)
Merge changes from topic "nnapi-cherrypick-from-master-and-pi-dev-to-aosp"
am: f59720c6b8
Change-Id: I636b34bce6c154c72f1eb732a23d8473b17f7efd
am: f59720c6b8
Change-Id: I636b34bce6c154c72f1eb732a23d8473b17f7efd
Merge changes from topic "nnapi-cherrypick-from-master-and-pi-dev-to-aosp"
* changes:
Update OWNERS
Fix indexing bug in NNAPI
Attach a bug to syncing docs
Reserve enums for new NNAPI ops.
Add new op PAD_V2
Add new ops ARGMAX and ARGMIN
* changes:
Update OWNERS
Fix indexing bug in NNAPI
Attach a bug to syncing docs
Reserve enums for new NNAPI ops.
Add new op PAD_V2
Add new ops ARGMAX and ARGMIN
Merge "Clarifying GnssMeasurement and Clock commments"
am: 3a5649ddd5
Change-Id: I0c94fe09746981e8ec52880e4dbe56dbdd9a6d0e
am: 3a5649ddd5
Change-Id: I0c94fe09746981e8ec52880e4dbe56dbdd9a6d0e
Merge "Clarifying GnssMeasurement and Clock commments"
tests IFoo: WithFmq is more complicated.
When an interface is in the struct, scatter gather isn't used.
Bug: 117239572
Test: hidl_test
Change-Id: I749dd7cce85d220c1908ad583b1744c799a105cc
When an interface is in the struct, scatter gather isn't used.
Bug: 117239572
Test: hidl_test
Change-Id: I749dd7cce85d220c1908ad583b1744c799a105cc
Merge "tests: IBaz, nasty nesting struct"
am: b035e3a246
Change-Id: I744b3504199a7a6a11b52599368574c575526f21
am: b035e3a246
Change-Id: I744b3504199a7a6a11b52599368574c575526f21
Merge "tests: IBaz, nasty nesting struct"
Merge "IFoo: send struct with fmq."
am: 7daf2659ea
Change-Id: I56b079caffb4b72afdb44f1fdfb98239eea22f5f
am: 7daf2659ea
Change-Id: I56b079caffb4b72afdb44f1fdfb98239eea22f5f
Merge "IFoo: send struct with fmq."
tests: IBaz, nasty nesting struct
toString is broken in some cases because of recursive definitions. This
exercises that case.
Bug: 117342189
Test: hidl_test
Test: m android.hardware.tests.baz@1.0 android.hardware.tests.baz-V1.0-java
(this runs hidl-gen on this for both Java and C++ output)
Test: manually inspected output
Change-Id: Ic09ac133345f2d83d6f83d3d0af1f63e7e3250ee
toString is broken in some cases because of recursive definitions. This
exercises that case.
Bug: 117342189
Test: hidl_test
Test: m android.hardware.tests.baz@1.0 android.hardware.tests.baz-V1.0-java
(this runs hidl-gen on this for both Java and C++ output)
Test: manually inspected output
Change-Id: Ic09ac133345f2d83d6f83d3d0af1f63e7e3250ee
Merge "VTS: Check return status of initialize and close"
am: 5956e27299
Change-Id: I4b496d9a896b1a55fa213d20c0bf01dd73863869
am: 5956e27299
Change-Id: I4b496d9a896b1a55fa213d20c0bf01dd73863869
Merge "VTS: Check return status of initialize and close"
Update OWNERS
Test: none
Change-Id: I96db4de3f34837c9f3174fd01e7d06d3355617f3
Merged-In: I96db4de3f34837c9f3174fd01e7d06d3355617f3
(cherry picked from commit 6653e69dc6385805909df504a93776aae6a6f639)
Test: none
Change-Id: I96db4de3f34837c9f3174fd01e7d06d3355617f3
Merged-In: I96db4de3f34837c9f3174fd01e7d06d3355617f3
(cherry picked from commit 6653e69dc6385805909df504a93776aae6a6f639)
Fix indexing bug in NNAPI
Bug: 114365802
Test: n/a
Change-Id: I87173528b58f66175c99e7c7e2e66daa307b04da
Merged-In: I87173528b58f66175c99e7c7e2e66daa307b04da
(cherry picked from commit 4a211d836457e22788010ddd58c8c2f6dd3cfbe7)
Bug: 114365802
Test: n/a
Change-Id: I87173528b58f66175c99e7c7e2e66daa307b04da
Merged-In: I87173528b58f66175c99e7c7e2e66daa307b04da
(cherry picked from commit 4a211d836457e22788010ddd58c8c2f6dd3cfbe7)
Attach a bug to syncing docs
Bug: 116445845
Test: none
Change-Id: I841b1dc503d70efddb8175b75d9d3efe8078eeb1
Merged-In: I841b1dc503d70efddb8175b75d9d3efe8078eeb1
(cherry picked from commit 7f9f46159183b02d53ca8d6bbe728e5610c2ea5a)
Bug: 116445845
Test: none
Change-Id: I841b1dc503d70efddb8175b75d9d3efe8078eeb1
Merged-In: I841b1dc503d70efddb8175b75d9d3efe8078eeb1
(cherry picked from commit 7f9f46159183b02d53ca8d6bbe728e5610c2ea5a)
Reserve enums for new NNAPI ops.
Test: NeuralNetworksTest_static
Bug: 114365802
Change-Id: I3b379fe3f0336b92ef602bbb12a4bd4a150c573c
Merged-In: I3b379fe3f0336b92ef602bbb12a4bd4a150c573c
(cherry picked from commit 5a9362eb2d1378636fd8bf604f6536eb2a268d2c)
Test: NeuralNetworksTest_static
Bug: 114365802
Change-Id: I3b379fe3f0336b92ef602bbb12a4bd4a150c573c
Merged-In: I3b379fe3f0336b92ef602bbb12a4bd4a150c573c
(cherry picked from commit 5a9362eb2d1378636fd8bf604f6536eb2a268d2c)
Add new op PAD_V2
Bug: 113561890
Test: NeuralNetworksTest_static
Change-Id: I34351d6ff5fae0a13e3e883ca42210c534418ff3
Merged-In: I34351d6ff5fae0a13e3e883ca42210c534418ff3
(cherry picked from commit ffe467e6d863b2b555171df7b2f46676ad46200e)
Bug: 113561890
Test: NeuralNetworksTest_static
Change-Id: I34351d6ff5fae0a13e3e883ca42210c534418ff3
Merged-In: I34351d6ff5fae0a13e3e883ca42210c534418ff3
(cherry picked from commit ffe467e6d863b2b555171df7b2f46676ad46200e)
Add new ops ARGMAX and ARGMIN
Bug: 113558658
Test: NeuralNetworksTest_static
Change-Id: I8862d4062181689ce69ab65aa07c1b6af07ba567
Merged-In: I8862d4062181689ce69ab65aa07c1b6af07ba567
(cherry picked from commit cc31bd6622f5e01ab640916fbb26433dd4ff9db2)
Bug: 113558658
Test: NeuralNetworksTest_static
Change-Id: I8862d4062181689ce69ab65aa07c1b6af07ba567
Merged-In: I8862d4062181689ce69ab65aa07c1b6af07ba567
(cherry picked from commit cc31bd6622f5e01ab640916fbb26433dd4ff9db2)
VTS: Check return status of initialize and close
Test: atest VtsHalBluetoothV1_0TargetTest
Change-Id: I579c4d5f4c6e24b358c67c3dc8a8a8ceb1f936e2
Test: atest VtsHalBluetoothV1_0TargetTest
Change-Id: I579c4d5f4c6e24b358c67c3dc8a8a8ceb1f936e2
IFoo: send struct with fmq.
Bug: 117239572
Test: hidl_test
Change-Id: I968916a9d62e1c8f7a237bd24e6b4267dd013366
Bug: 117239572
Test: hidl_test
Change-Id: I968916a9d62e1c8f7a237bd24e6b4267dd013366
Merge "IFoo: remove pointer from u."
am: 999693e4e8
Change-Id: I83c607457dbcf46833e2a2fdc50626e1da0a338a
am: 999693e4e8
Change-Id: I83c607457dbcf46833e2a2fdc50626e1da0a338a
Merge "IFoo: remove pointer from u."
Merge "Add a command to get the minimum battery voltage required for flashing"
am: b99e695e91
Change-Id: Ic6c443e27d84db54fea6e5cda2241c068ebf53cf
am: b99e695e91
Change-Id: Ic6c443e27d84db54fea6e5cda2241c068ebf53cf
Merge "Add a command to get the minimum battery voltage required for flashing"
Add a command to get the minimum battery voltage required for flashing
Bug: 79480454
Test: fastboot getvar battery-soc-ok
Change-Id: I6141993972a3084fe3620d81f707999e1264b997
Merged-In: I6141993972a3084fe3620d81f707999e1264b997
(cherry picked from commit 83f5631deb5169d7b6f897679956bc11d13e6e0b)
Bug: 79480454
Test: fastboot getvar battery-soc-ok
Change-Id: I6141993972a3084fe3620d81f707999e1264b997
Merged-In: I6141993972a3084fe3620d81f707999e1264b997
(cherry picked from commit 83f5631deb5169d7b6f897679956bc11d13e6e0b)
Added 1.3 DataProfileInfo
1. Deprecated the fields 'mvnoType', 'mvnoMatchData', 'maxConnsTime',
and 'maxConns'.
2. Added a new flag 'preferred' indicating if this data profile
is preferred for default data connection setup.
3. Move modemCognative flag from setupDataCall and setInitialAttachApn
into the struct DataProfileInfo and rename it to 'persistent'.
4. Removed isRoaming flag in setupDataCall, setInitialAttachApn, and
setDataProfile.
Test: Telephony sanity tests
Bug: 73659459
Change-Id: Ia28715e85755b47a1ee870b5c90e5505a7fd8c4a
1. Deprecated the fields 'mvnoType', 'mvnoMatchData', 'maxConnsTime',
and 'maxConns'.
2. Added a new flag 'preferred' indicating if this data profile
is preferred for default data connection setup.
3. Move modemCognative flag from setupDataCall and setInitialAttachApn
into the struct DataProfileInfo and rename it to 'persistent'.
4. Removed isRoaming flag in setupDataCall, setInitialAttachApn, and
setDataProfile.
Test: Telephony sanity tests
Bug: 73659459
Change-Id: Ia28715e85755b47a1ee870b5c90e5505a7fd8c4a
IFoo: remove pointer from u.
pointer needs a fixup (to abort) since they can't be used in remote
transactions, so removing it from the union here.
Bug: 117322722
Test: hidl_test
Change-Id: Ie582f6b79a8176ca1585bf4b1f43ae9d5d97fa92
pointer needs a fixup (to abort) since they can't be used in remote
transactions, so removing it from the union here.
Bug: 117322722
Test: hidl_test
Change-Id: Ie582f6b79a8176ca1585bf4b1f43ae9d5d97fa92
Clarifying GnssMeasurement and Clock commments
Change-Id: Ia51b16a2904ab43f67464fc91321fad99a2bb614
Fixes: 77812939
Test: Comments only, verified builds
Change-Id: Ia51b16a2904ab43f67464fc91321fad99a2bb614
Fixes: 77812939
Test: Comments only, verified builds
Audio VTS: Do not constrain implementation frameCount am: 069bc45044
am: 5596e985d4
Change-Id: Idf051c458d74057425ec3c13227fa31190535e18
am: 5596e985d4
Change-Id: Idf051c458d74057425ec3c13227fa31190535e18
Audio VTS: Do not constrain implementation frameCount
am: 069bc45044
Change-Id: I3ec1df7f581e5b11e0d394139c1421109c16fc19
am: 069bc45044
Change-Id: I3ec1df7f581e5b11e0d394139c1421109c16fc19
Merge "Reland "Set vendor: true for boot control HAL""
am: 9ba23d0c78
Change-Id: I4fa44112bf00e1ccb96e8fd7de606fb7ebbe2cd5
am: 9ba23d0c78
Change-Id: I4fa44112bf00e1ccb96e8fd7de606fb7ebbe2cd5
Merge "Reland "Set vendor: true for boot control HAL""
Reland "Set vendor: true for boot control HAL"
This reverts commit f8169cc2bc23db9be612da42d241267cdccbed40.
Bug: 117072247
Change-Id: Ib80966e31ed92d316217844d0399e6f6ba5fdd2c
This reverts commit f8169cc2bc23db9be612da42d241267cdccbed40.
Bug: 117072247
Change-Id: Ib80966e31ed92d316217844d0399e6f6ba5fdd2c
Merge "Emergency Function HAL (continued)"
am: f461463b39
Change-Id: I6c0105193a38b477fdfa7e8b88343bd5b8bb2f14
am: f461463b39
Change-Id: I6c0105193a38b477fdfa7e8b88343bd5b8bb2f14
Merge "Emergency Function HAL (continued)"
Merge "health VTS: split Properties test"
am: f8a8873ee6
Change-Id: I4a951a54f052e8f1891e4aeb406307c59f25d3e3
am: f8a8873ee6
Change-Id: I4a951a54f052e8f1891e4aeb406307c59f25d3e3
health: registerCallback() and getHealthInfo() does not notify all callbacks
am: e9fc235eb4
Change-Id: I839443bed06f0007b93d1032c61d28d3955d79a3
am: e9fc235eb4
Change-Id: I839443bed06f0007b93d1032c61d28d3955d79a3
Merge "health VTS: split Properties test"
Audio VTS: Do not constrain implementation frameCount
The test was assuming Stream::getFrameCount() would return the
AudioConfig::frameCount used to create the stream, similarly
to the sampleRate or the channelMask.
Nevertheless this is not the case as the AudioConfig::frameCount
field is not to used by Stream::openOutputStream (nor Input) as
the buffer size is chosen by the HAL, not the framework.
Thus the test can not assume the frameCount chosen by the HAL and
must not test for a particular value.
Test: atest VtsHalAudioV4_0TargetTest
Bug: 116169974
Change-Id: Ibbf0825f540957e01e7c512d851cb9628991f4c4
Signed-off-by: Kevin Rocard <krocard@google.com>
The test was assuming Stream::getFrameCount() would return the
AudioConfig::frameCount used to create the stream, similarly
to the sampleRate or the channelMask.
Nevertheless this is not the case as the AudioConfig::frameCount
field is not to used by Stream::openOutputStream (nor Input) as
the buffer size is chosen by the HAL, not the framework.
Thus the test can not assume the frameCount chosen by the HAL and
must not test for a particular value.
Test: atest VtsHalAudioV4_0TargetTest
Bug: 116169974
Change-Id: Ibbf0825f540957e01e7c512d851cb9628991f4c4
Signed-off-by: Kevin Rocard <krocard@google.com>