android/platform-hardware-interfaces.git
2 years agoMerge "Add IRadioResponse/Indication 1.3 and Emergency Function HAL" android-o-mr1-iot-release-1.0.4
Shuo Qian [Wed, 5 Sep 2018 18:44:31 +0000 (18:44 +0000)]
Merge "Add IRadioResponse/Indication 1.3 and Emergency Function HAL"

2 years agoMerge "Correct the comments for radio hal types"
Youming Ye [Wed, 5 Sep 2018 16:53:27 +0000 (16:53 +0000)]
Merge "Correct the comments for radio hal types"

2 years agoAdd IRadioResponse/Indication 1.3 and Emergency Function HAL
sqian [Thu, 30 Aug 2018 03:26:03 +0000 (20:26 -0700)]
Add IRadioResponse/Indication 1.3 and Emergency Function HAL

- Add IRadioResponse/Indication in 1.3
- Add Emergency Functions:
1) getCurrentEmergencyNumberList/getCurrentEmergencyNumberListResponse
2) emergencyDial/emergencyDialResponse
3) currentEmergencyNumberList
4) EmergencyNumber/EmergencyServiceCategory

Test: compile (will add VTS later)
Bug: 112657134
Change-Id: Iafe12d5fd0e4c28fcf6e4d8e61cfb954db7fa68a

2 years agoCorrect the comments for radio hal types
Youming Ye [Fri, 17 Aug 2018 20:53:52 +0000 (13:53 -0700)]
Correct the comments for radio hal types

The type of mcc and mnc is String instead of Int now. They should be an
empty string if unknown. Also added a test case for their values.

Bug: 111703979
Test: Vts
Change-Id: Ie0426453dc426ccc6cf203b315806e78511ce14d

2 years agoMerge "Fix KM VTS tests for Strongbox implementations"
Treehugger Robot [Tue, 4 Sep 2018 10:44:18 +0000 (10:44 +0000)]
Merge "Fix KM VTS tests for Strongbox implementations"

2 years agoMerge "Camera: support torch control on external camera"
Treehugger Robot [Thu, 30 Aug 2018 19:02:26 +0000 (19:02 +0000)]
Merge "Camera: support torch control on external camera"

2 years agoMerge "Camera: Allow 3% ISO tolerance during ISO burst VTS" into pie-vts-dev
Emilian Peev [Thu, 30 Aug 2018 17:23:00 +0000 (10:23 -0700)]
Merge "Camera: Allow 3% ISO tolerance during ISO burst VTS" into pie-vts-dev
am: 391eb588cf

Change-Id: Id897eee2251eee92267b4e32f7d245aca3eb1e88

2 years agoMerge "Allow getCapturePosition to return 0 frames for unprepared streams" into pie...
Kevin Rocard [Thu, 30 Aug 2018 17:22:35 +0000 (10:22 -0700)]
Merge "Allow getCapturePosition to return 0 frames for unprepared streams" into pie-vts-dev
am: 137194ef5e

Change-Id: Ibef9acb447f71a94c27ad62ffd93b87126637143

2 years agoMerge "Camera: Allow 3% ISO tolerance during ISO burst VTS" into pie-vts-dev
Treehugger Robot [Thu, 30 Aug 2018 17:15:35 +0000 (17:15 +0000)]
Merge "Camera: Allow 3% ISO tolerance during ISO burst VTS" into pie-vts-dev

2 years agoMerge "Allow getCapturePosition to return 0 frames for unprepared streams" into pie...
Treehugger Robot [Thu, 30 Aug 2018 17:15:19 +0000 (17:15 +0000)]
Merge "Allow getCapturePosition to return 0 frames for unprepared streams" into pie-vts-dev

2 years agoMerge "Set the floor value of time estimate as 2017 Jan 01 00:00:00 GMT" into pie...
Yu-Han Yang [Thu, 30 Aug 2018 00:11:15 +0000 (17:11 -0700)]
Merge "Set the floor value of time estimate as 2017 Jan 01 00:00:00 GMT" into pie-vts-dev
am: 4e0c7c1760

Change-Id: Ia8b0d2e61772da26e399d5a6d029159eb70b88d7

2 years agoMerge "Set the floor value of time estimate as 2017 Jan 01 00:00:00 GMT" into pie...
Treehugger Robot [Wed, 29 Aug 2018 23:59:34 +0000 (23:59 +0000)]
Merge "Set the floor value of time estimate as 2017 Jan 01 00:00:00 GMT" into pie-vts-dev

2 years agoMerge "[ConfigStore] Clarify hasHDRDisplay spec."
Treehugger Robot [Wed, 29 Aug 2018 22:34:02 +0000 (22:34 +0000)]
Merge "[ConfigStore] Clarify hasHDRDisplay spec."

2 years ago[automerger skipped] Merge "Fix setAllowedCarrier" into pie-vts-dev
sqian [Wed, 29 Aug 2018 18:54:50 +0000 (11:54 -0700)]
[automerger skipped] Merge "Fix setAllowedCarrier" into pie-vts-dev
am: 052f207b42  -s ours

Change-Id: Ic6f3763761f13361d21d14594042011e797099f1

2 years agoMerge "Fix setAllowedCarrier" into pie-vts-dev
Treehugger Robot [Wed, 29 Aug 2018 18:44:58 +0000 (18:44 +0000)]
Merge "Fix setAllowedCarrier" into pie-vts-dev

2 years agoCamera: Allow 3% ISO tolerance during ISO burst VTS
Emilian Peev [Tue, 26 Jun 2018 08:17:33 +0000 (09:17 +0100)]
Camera: Allow 3% ISO tolerance during ISO burst VTS

The advertised ISO ranges may not be entirely supported on
some devices. Expect a 3% tolerance when comparing the applied
results versus the expected ISO value.

Bug: 80025874
Test: run vts --skip-all-system-status-check --skip-preconditions
--primary-abi-only --module VtsHalCameraProviderV2_4Target -l INFO

Merged-In: Ibd2758e48a0924e81877e35dd27433669274fdb3
Change-Id: Ibd2758e48a0924e81877e35dd27433669274fdb3
(cherry picked from commit 0fdd7cdc0eab249e0f0615fad1034231c09987dd)

2 years agoSet the floor value of time estimate as 2017 Jan 01 00:00:00 GMT
Yu-Han Yang [Thu, 14 Jun 2018 21:17:58 +0000 (14:17 -0700)]
Set the floor value of time estimate as 2017 Jan 01 00:00:00 GMT

- The VTS test checks if the time estimate is a sane value. Thus, any
arbitrary sane value is acceptable. Here we make it consistent to
IGnssDebug.hal, where a comment mentions 2017 Jan 1 as an example of
the value.

Bug: 110094003
Test: make vts, and tested on device.
Merged-In: Ic4f6b597a718ea3e98a67c7939f9e6930d44d224
Change-Id: Ic4f6b597a718ea3e98a67c7939f9e6930d44d224
(cherry picked from commit 5fa43c83e90ccd0f852c89feb0e071aad195d7b2)
(cherry picked from commit 4f0d19ebff1f4a3eb565d8432f44b561ebd4abe2)

2 years agoAllow getCapturePosition to return 0 frames for unprepared streams
Kevin Rocard [Thu, 21 Jun 2018 21:10:58 +0000 (14:10 -0700)]
Allow getCapturePosition to return 0 frames for unprepared streams

For device supporting getCapturePosition,
VTS only allowed unprepared stream to return INVALID_STATE.
Now also allow for the stream to return 0 frames similarly to the other
non started states.

Test: vts-tradefed run commandAndExit vts --module VtsHalAudioV2_0Target
Bug: 110367728
Cherry-piked from: d01dc3edac9e92981e7ae419d0e7622f753acf94
Merged-In: Ibdf8df8cb8809e98c40a50035371df6893fe4da4
Change-Id: Ibdf8df8cb8809e98c40a50035371df6893fe4da4
Signed-off-by: Kevin Rocard <krocard@google.com>
(cherry picked from commit 6c9c6e62c193461ed0de4666d0995631ba39e009)

2 years ago[automerger skipped] Merge "Change ImportWrappedKeyTest back to SHA1" into pie-vts-dev
Shawn Willden [Wed, 29 Aug 2018 08:13:11 +0000 (01:13 -0700)]
[automerger skipped] Merge "Change ImportWrappedKeyTest back to SHA1" into pie-vts-dev
am: e7300721a0  -s ours

Change-Id: Ie8af40cfea7a0893f9f90d4c42a7cf8513e38818

2 years ago[automerger skipped] Merge "Require keymaster4 attestations to contain the right...
Shawn Willden [Wed, 29 Aug 2018 08:12:55 +0000 (01:12 -0700)]
[automerger skipped] Merge "Require keymaster4 attestations to contain the right version." into pie-vts-dev
am: 516718071b  -s ours

Change-Id: I15537d95bc28ff14aa3942d932378e99d5793f42

2 years ago[automerger skipped] Merge "keymaster: skip SHA2 digest tests for strongbox" into...
nagendra modadugu [Wed, 29 Aug 2018 08:12:38 +0000 (01:12 -0700)]
[automerger skipped] Merge "keymaster: skip SHA2 digest tests for strongbox" into pie-vts-dev
am: 86104dcc18  -s ours

Change-Id: Ib420f757159aaf8bbf462f98d88be3808d84c7d1

2 years ago[automerger skipped] Merge changes Ic41afbd0,Ibe264d08 into pie-vts-dev
nagendra modadugu [Wed, 29 Aug 2018 08:12:17 +0000 (01:12 -0700)]
[automerger skipped] Merge changes Ic41afbd0,Ibe264d08 into pie-vts-dev
am: e101aa87a3  -s ours

Change-Id: Ifff697b20cb2e0c9f89594fe965dde3545447175

2 years agoMerge "Fixing Keymaster documentation." into pie-vts-dev
Eran Messeri [Wed, 29 Aug 2018 08:11:55 +0000 (01:11 -0700)]
Merge "Fixing Keymaster documentation." into pie-vts-dev
am: 33f7970672

Change-Id: I0bd196af03f96817cbd23620b109e7665456f586

2 years agoMerge "Change ImportWrappedKeyTest back to SHA1" into pie-vts-dev
Treehugger Robot [Wed, 29 Aug 2018 08:07:09 +0000 (08:07 +0000)]
Merge "Change ImportWrappedKeyTest back to SHA1" into pie-vts-dev

2 years agoMerge "Require keymaster4 attestations to contain the right version." into pie-vts-dev
Treehugger Robot [Wed, 29 Aug 2018 08:06:55 +0000 (08:06 +0000)]
Merge "Require keymaster4 attestations to contain the right version." into pie-vts-dev

2 years agoMerge "keymaster: skip SHA2 digest tests for strongbox" into pie-vts-dev
Treehugger Robot [Wed, 29 Aug 2018 08:06:40 +0000 (08:06 +0000)]
Merge "keymaster: skip SHA2 digest tests for strongbox" into pie-vts-dev

2 years agoMerge changes Ic41afbd0,Ibe264d08 into pie-vts-dev
Treehugger Robot [Wed, 29 Aug 2018 08:06:38 +0000 (08:06 +0000)]
Merge changes Ic41afbd0,Ibe264d08 into pie-vts-dev

* changes:
  keymaster: spec does not require that update produce output
  Fix attestation test.

2 years agoMerge "Fixing Keymaster documentation." into pie-vts-dev
Treehugger Robot [Wed, 29 Aug 2018 08:06:31 +0000 (08:06 +0000)]
Merge "Fixing Keymaster documentation." into pie-vts-dev

2 years ago[automerger skipped] Allow general errors for getImsiForApp().
Amit Mahajan [Wed, 29 Aug 2018 02:51:27 +0000 (19:51 -0700)]
[automerger skipped] Allow general errors for getImsiForApp().
am: 1f3d0a68a4  -s ours

Change-Id: I2b7df276429ce16a63e00ed5f3e2654bbb9c63ed

2 years agoFix setAllowedCarrier
sqian [Tue, 31 Jul 2018 16:23:24 +0000 (09:23 -0700)]
Fix setAllowedCarrier

If function is not supported or executed successfully, do not
expect its effect on cardStatus.

Bug: 112008372
Test: run vts
Change-Id: I4532a39af2cfcf0e44eafe29c3c7f6779ae101f5
Merged-In: I4532a39af2cfcf0e44eafe29c3c7f6779ae101f5
(cherry picked from commit 44b129f7288016a4113f5e6ff059d63987d63385)

2 years agoAllow general errors for getImsiForApp().
Amit Mahajan [Tue, 12 Jun 2018 22:23:39 +0000 (15:23 -0700)]
Allow general errors for getImsiForApp().

This is to match it with other 1.0 tests where general errors are
allowed. For newer tests we have decided to not allow these errors,
but a failure for this old test is reported when run with SIM
present.

Test: run vts -m VtsHalRadioV1_0Target
Bug: 109889468
Change-Id: If36083b7832706a50805932e8ba08e4eb397f3fe
Merged-In: If36083b7832706a50805932e8ba08e4eb397f3fe
(cherry picked from commit 817848e59e18334a30f623ef143cf182716fd3fa)

2 years ago[automerger skipped] Merge "Loose startNetworkScan cases" into pie-vts-dev
sqian [Tue, 28 Aug 2018 23:51:22 +0000 (16:51 -0700)]
[automerger skipped] Merge "Loose startNetworkScan cases" into pie-vts-dev
am: 3c233d344c  -s ours

Change-Id: Ie83195654dc60810651b9cd883d1a5f1f360f5fa

2 years ago[automerger skipped] Merge "Fix missed refactor of serial" into pie-vts-dev
sqian [Tue, 28 Aug 2018 23:47:55 +0000 (16:47 -0700)]
[automerger skipped] Merge "Fix missed refactor of serial" into pie-vts-dev
am: d4f9ad2c59  -s ours

Change-Id: I95f73d92932ffa352b6299c7bb8d5fe4ec71e023

2 years ago[automerger skipped] Merge "Allow NOT_SUPPORTED for setLinkCapacityReportingCriteria...
Amit Mahajan [Tue, 28 Aug 2018 23:47:35 +0000 (16:47 -0700)]
[automerger skipped] Merge "Allow NOT_SUPPORTED for setLinkCapacityReportingCriteria on GERAN." into pie-vts-dev
am: 429da8656e  -s ours

Change-Id: Ie29dbb55092bcfecc0f01a4ba3405ea8dd8db518

2 years agoMerge "Loose startNetworkScan cases" into pie-vts-dev
Treehugger Robot [Tue, 28 Aug 2018 23:47:27 +0000 (23:47 +0000)]
Merge "Loose startNetworkScan cases" into pie-vts-dev

2 years ago[automerger skipped] Merge "Allow REQUEST_NOT_SUPPORTED as an error for startNetworkS...
Amit Mahajan [Tue, 28 Aug 2018 23:47:16 +0000 (16:47 -0700)]
[automerger skipped] Merge "Allow REQUEST_NOT_SUPPORTED as an error for startNetworkScan" into pie-vts-dev
am: 00cdcb77f8  -s ours

Change-Id: Ie8c2baaacc0369048448d608ab002c1369b9b68f

2 years agoMerge "Fix missed refactor of serial" into pie-vts-dev
Treehugger Robot [Tue, 28 Aug 2018 23:42:41 +0000 (23:42 +0000)]
Merge "Fix missed refactor of serial" into pie-vts-dev

2 years agoMerge "Allow NOT_SUPPORTED for setLinkCapacityReportingCriteria on GERAN." into pie...
Treehugger Robot [Tue, 28 Aug 2018 23:40:57 +0000 (23:40 +0000)]
Merge "Allow NOT_SUPPORTED for setLinkCapacityReportingCriteria on GERAN." into pie-vts-dev

2 years agoMerge "Allow REQUEST_NOT_SUPPORTED as an error for startNetworkScan" into pie-vts-dev
Treehugger Robot [Tue, 28 Aug 2018 23:37:53 +0000 (23:37 +0000)]
Merge "Allow REQUEST_NOT_SUPPORTED as an error for startNetworkScan" into pie-vts-dev

2 years ago[automerger skipped] Secure_element: vts: Modify openBasicChannel as per OMAPI standard
Ruchi Kandoi [Tue, 28 Aug 2018 22:56:05 +0000 (15:56 -0700)]
[automerger skipped] Secure_element: vts: Modify openBasicChannel as per OMAPI standard
am: ecdec18c73  -s ours

Change-Id: I84c5b1003063990e4d70941344a0b920b28a2867

2 years agoLoose startNetworkScan cases
sqian [Fri, 3 Aug 2018 23:19:29 +0000 (16:19 -0700)]
Loose startNetworkScan cases

startNetworkScan:
Some vendor may not support the required manual GSM search
functionality.

startNetworkScan_GoodRequest1 and startNetworkScan_GoodRequest2:
Some vendor may not support max search time of 360s.

Test: sanity
Bug: 109765420
Merged-In: I456847815057d76561bfb3e840016619ac753476
Change-Id: I456847815057d76561bfb3e840016619ac753476
(cherry picked from commit 12f7d6127b301b140ee81696fed19f81a7ea50c6)

2 years agoFix missed refactor of serial
sqian [Wed, 27 Jun 2018 19:12:26 +0000 (12:12 -0700)]
Fix missed refactor of serial

Bug: 109822806
Test: run vts
Merged-In: If88384699dbb4c2ddd1c580d2b35be38afd0f8e8
Change-Id: If88384699dbb4c2ddd1c580d2b35be38afd0f8e8
(cherry picked from commit c0e2e2b071df5cdff10193556163e2975f0b682c)

2 years agoAllow NOT_SUPPORTED for setLinkCapacityReportingCriteria on GERAN.
Amit Mahajan [Mon, 25 Jun 2018 21:16:37 +0000 (14:16 -0700)]
Allow NOT_SUPPORTED for setLinkCapacityReportingCriteria on GERAN.

Test: run vts -m VtsHalRadioV1_2Target
Bug: 110716988
Merged-In: I9a5f014d498db00d818870cbd73e119f66562ef1
Change-Id: I9a5f014d498db00d818870cbd73e119f66562ef1
(cherry picked from commit c7896501db413c9a0fa44d2697da4079610075d8)

2 years agoAllow REQUEST_NOT_SUPPORTED as an error for startNetworkScan
Amit Mahajan [Fri, 15 Jun 2018 18:16:28 +0000 (11:16 -0700)]
Allow REQUEST_NOT_SUPPORTED as an error for startNetworkScan

We are trying to tighten the APIs. However for this case since the
documentation was not updated, we are allowing NOT_SUPPORTED for
now and will be cleaned up in a later release.

Test: run vts -m VtsHalRadioV1_2Target
Bug: 110118713
Merged-In: Id9dd3d7bac99bed36ceb9c906189f1fea78d5a2c
Change-Id: Id9dd3d7bac99bed36ceb9c906189f1fea78d5a2c
(cherry picked from commit a7587b5a7fdace0d193ad333e6f5cda8b995570b)

2 years agoSecure_element: vts: Modify openBasicChannel as per OMAPI standard
Ruchi Kandoi [Mon, 2 Jul 2018 20:20:34 +0000 (13:20 -0700)]
Secure_element: vts: Modify openBasicChannel as per OMAPI standard

CHANNEL_NOT_AVAILABLE should be returned when opening basic channel
is not permitted on the secure element

Test: Test with SIM1 HAL
Bug: 110945797
Merged-In: I2dd4eafaf4c534b49a37690a9baadcc5ac93190c
Change-Id: I2dd4eafaf4c534b49a37690a9baadcc5ac93190c
(cherry picked from commit ec5aa6af4d8b330af6c8599830942e29294aa688)

2 years agoChange ImportWrappedKeyTest back to SHA1
Shawn Willden [Mon, 6 Aug 2018 23:23:23 +0000 (17:23 -0600)]
Change ImportWrappedKeyTest back to SHA1

Change I5f877b2a1ac66026a876e145416ba078d486e4b5 inadvertently changed
the digest used for ImportWrappedKey, breaking the test.  This CL
reverts that portion of the change.

Test: VtsHalKeymasterV4_0TargetTest
Bug: 112279922
Merged-In: Ib8e2e7793ba46ae0d29d8407bb730a35bdb5ea98
Change-Id: Ib8e2e7793ba46ae0d29d8407bb730a35bdb5ea98
(cherry picked from commit 0dba88861267b2b37355b41504b9d1e0d89bbe0f)

2 years agoRequire keymaster4 attestations to contain the right version.
Shawn Willden [Tue, 31 Jul 2018 19:47:37 +0000 (13:47 -0600)]
Require keymaster4 attestations to contain the right version.

Note that devices with KM4 will fail to pass VTS after this
lands, until the fix from Qualcomm arrives.

Test: VtsHalKeymasterV4_0TargetTest
Bug: 112040197
Merged-In: Ie2cd917af704b9f19de3537297b3a7e4f0c861e9
Change-Id: Ie2cd917af704b9f19de3537297b3a7e4f0c861e9
(cherry picked from commit 4e006c2b92be6ac71927b975b6725ddadf0b3342)

2 years agokeymaster: skip SHA2 digest tests for strongbox
nagendra modadugu [Mon, 23 Jul 2018 17:32:28 +0000 (10:32 -0700)]
keymaster: skip SHA2 digest tests for strongbox

Strongbox is not required to support SHA-2 digests,
so skip the related tests.

Bug: 109771020
Merged-In: I5f877b2a1ac66026a876e145416ba078d486e4b5
Change-Id: I5f877b2a1ac66026a876e145416ba078d486e4b5
(cherry picked from commit 8cec80be1fc3d2d30fe095fa009dfa83cb7651ce)

2 years agokeymaster: spec does not require that update produce output
nagendra modadugu [Tue, 26 Jun 2018 02:56:35 +0000 (19:56 -0700)]
keymaster: spec does not require that update produce output

Remove out of spec enforcement on the amount of data returned
by update, as this is not specified in the HAL.

Bug: 109771020
Test: yes it is
Merged-In: Ic41afbd01d51faf48d3c0fe090409ebcd257cc1e
Change-Id: Ic41afbd01d51faf48d3c0fe090409ebcd257cc1e
(cherry picked from commit 7b75f015a7a7ebc40722fd4f36c9ca70e7e58e59)

2 years agoFix attestation test.
Shawn Willden [Wed, 20 Jun 2018 04:10:03 +0000 (22:10 -0600)]
Fix attestation test.

Bug: 77588764
Test: VtsHalKeymasterV4_0TargetTest
Merged-In: Ibe264d08ae7b3333a6949761a92759f5305b3fcb
Change-Id: Ibe264d08ae7b3333a6949761a92759f5305b3fcb
(cherry picked from commit d898d0a4223df75225cfdf23e6f184166933cdb3)

2 years ago[automerger skipped] Merge changes Ia3b96e83,I80d924cc into pie-vts-dev
sqian [Tue, 28 Aug 2018 22:10:52 +0000 (15:10 -0700)]
[automerger skipped] Merge changes Ia3b96e83,I80d924cc into pie-vts-dev
am: 0b1461687f  -s ours

Change-Id: I8a2912ea0ea9fc396f3d6513db7c466f5cdec0c5

2 years agoFixing Keymaster documentation.
Eran Messeri [Tue, 19 Jun 2018 16:12:04 +0000 (17:12 +0100)]
Fixing Keymaster documentation.

Keymaster HAL documentation documents the bootPatchLevel as having
tag 718, while types.hal indicates the tag value for it is actually
719.

Test: N/A
Bug: 78104779
Merged-In: I0dde0b3c863081f2594e20466d8e82866a5f2d2e
Change-Id: I0dde0b3c863081f2594e20466d8e82866a5f2d2e
(cherry picked from commit ae8da1b70ad563edb79f4f7429b704b54c1a9e19)

2 years agoMerge changes Ia3b96e83,I80d924cc into pie-vts-dev
Treehugger Robot [Tue, 28 Aug 2018 22:06:22 +0000 (22:06 +0000)]
Merge changes Ia3b96e83,I80d924cc into pie-vts-dev

* changes:
  Add REQUEST_NOT_SUPPORTED for pin and pin2 Icc VTS
  Add SIM_PUK2 for Icc VTS tests

2 years agoImprove VTS GNSS 1.1 reliability.
WyattRiley [Tue, 28 Aug 2018 21:22:11 +0000 (14:22 -0700)]
Improve VTS GNSS 1.1 reliability.
am: 2d86da7b28

Change-Id: I401190490a49bdf529d5fd697216cdf5b051729d

2 years agoDelete time/position in InjectDelete instead of Delete_all
Yu-Han Yang [Tue, 28 Aug 2018 21:21:56 +0000 (14:21 -0700)]
Delete time/position in InjectDelete instead of Delete_all
am: 66fb7a1b88

Change-Id: I6651f1f2e181ad2022ae2cdc6b9f6c1d4a4d0d06

2 years agoInject last location in InjectBestLocation VTS test
Yu-Han Yang [Tue, 28 Aug 2018 21:21:40 +0000 (14:21 -0700)]
Inject last location in InjectBestLocation VTS test
am: 75b0c4bba2

Change-Id: I934dd9ac9a49d1813f10f6d2f31739c3a6a6babf

2 years agoImprove VTS GNSS 1.1 reliability.
WyattRiley [Thu, 28 Jun 2018 22:05:14 +0000 (15:05 -0700)]
Improve VTS GNSS 1.1 reliability.

Allow VTS test for low power mode to handle
certain vendor issues that supply one extra location
at the start of low power mode.

Allow more time for GNSS first fix, and warmup as
needed given limited VTS access to AGPS.

Bug: 110626730
Bug: 110987651
Test: (TODO) Passes on device.
Merged-In: Ieeefd7fcd45890b03dffbbee965e1d9b17805c4c
Change-Id: Ieeefd7fcd45890b03dffbbee965e1d9b17805c4c
(cherry picked from commit 5ea5dda2c33f9d2f1db77d6b4493f0eb356c2937)

2 years agoDelete time/position in InjectDelete instead of Delete_all
Yu-Han Yang [Mon, 2 Jul 2018 17:41:28 +0000 (10:41 -0700)]
Delete time/position in InjectDelete instead of Delete_all

- DELETE_ALL will delete XTRA.

Bug: 110626730
Test: run VTS test on device.
Merged-In: I4f01430f24f92238193d3de6b6fbb31e81e9f006
Change-Id: I4f01430f24f92238193d3de6b6fbb31e81e9f006
(cherry picked from commit 84cff99b2fcae8757704b0384552aebe290165ed)

2 years agoInject last location in InjectBestLocation VTS test
Yu-Han Yang [Fri, 29 Jun 2018 23:21:32 +0000 (16:21 -0700)]
Inject last location in InjectBestLocation VTS test

Bug: 110626730
Test: run VTS on device.
Merged-In: I6f57dd7f9164dacf011f25412e55fcd22821aca0
Change-Id: I6f57dd7f9164dacf011f25412e55fcd22821aca0
(cherry picked from commit bb372e5984a612cb6972e837662d64a90785fbd8)

2 years agoMerge "Tolerate 1 sv status in GNSS blacklist VTS test" into pie-vts-dev
Yu-Han Yang [Tue, 28 Aug 2018 19:25:47 +0000 (12:25 -0700)]
Merge "Tolerate 1 sv status in GNSS blacklist VTS test" into pie-vts-dev
am: a9ad41d1ad

Change-Id: I0bce1b24e7472bebd96614bc502a863bca020e8f

2 years agoMerge "VTS: Do not require XML for Audio effect V2" into pie-vts-dev
Kevin Rocard [Tue, 28 Aug 2018 19:25:23 +0000 (12:25 -0700)]
Merge "VTS: Do not require XML for Audio effect V2" into pie-vts-dev
am: 5e6dd1288e

Change-Id: If389674923030e041dfdb95cd99cd0316603c917

2 years agoMerge "Camera: Don't hold 'mLock' when closing the camera session" into pie-vts-dev
Emilian Peev [Tue, 28 Aug 2018 19:24:48 +0000 (12:24 -0700)]
Merge "Camera: Don't hold 'mLock' when closing the camera session" into pie-vts-dev
am: 75ceb36b27

Change-Id: I3b3d8c2051dd89b0993bd17af77a6a19cd7792b6

2 years agoMerge "Tolerate 1 sv status in GNSS blacklist VTS test" into pie-vts-dev
Treehugger Robot [Tue, 28 Aug 2018 19:14:59 +0000 (19:14 +0000)]
Merge "Tolerate 1 sv status in GNSS blacklist VTS test" into pie-vts-dev

2 years agoMerge "VTS: Do not require XML for Audio effect V2" into pie-vts-dev
Treehugger Robot [Tue, 28 Aug 2018 19:13:44 +0000 (19:13 +0000)]
Merge "VTS: Do not require XML for Audio effect V2" into pie-vts-dev

2 years agoMerge "Camera: Don't hold 'mLock' when closing the camera session" into pie-vts-dev
Treehugger Robot [Tue, 28 Aug 2018 19:11:28 +0000 (19:11 +0000)]
Merge "Camera: Don't hold 'mLock' when closing the camera session" into pie-vts-dev

2 years agoMerge "Audio VTS was testing wrong uninitialized variable due to typo" into pie-vts-dev
Kevin Rocard [Tue, 28 Aug 2018 19:03:40 +0000 (12:03 -0700)]
Merge "Audio VTS was testing wrong uninitialized variable due to typo" into pie-vts-dev
am: b3e86d489a

Change-Id: I13b546ec0e8785040e4096a7658474f2eff6c90e

2 years agoAdd VTS test to verify scheduling capability
Vishal Agarwal [Tue, 28 Aug 2018 19:01:04 +0000 (12:01 -0700)]
Add VTS test to verify scheduling capability
am: 2910e64d24

Change-Id: Ife2f3b299e9c3762d5aad18007b28e62da4fe20f

2 years ago[automerger skipped] Add setIndicationFilter response notification in 1.2 VTS
sqian [Tue, 28 Aug 2018 19:00:28 +0000 (12:00 -0700)]
[automerger skipped] Add setIndicationFilter response notification in 1.2 VTS
am: 388883a3ec  -s ours

Change-Id: Iddbbd11134cc9c05320cec945d513126e6662641

2 years agoMerge "Audio VTS was testing wrong uninitialized variable due to typo" into pie-vts-dev
Treehugger Robot [Tue, 28 Aug 2018 18:48:10 +0000 (18:48 +0000)]
Merge "Audio VTS was testing wrong uninitialized variable due to typo" into pie-vts-dev

2 years agoCamera: support torch control on external camera
Yin-Chia Yeh [Tue, 28 Aug 2018 17:52:43 +0000 (10:52 -0700)]
Camera: support torch control on external camera

Claim torch API support though there is no device
actually has a flash unit. This is to workaround
an issue in camera service where it falls back
to legacy camera HAL1 control if the device does
not report torch API support (and external camera
HAL does not implement HAL1)

Test: CtsVerifier FlashLight test
Bug: 113336515
Change-Id: I945b35fecfed3b2698b1e9bb1d8faad8699258d2

2 years agoTolerate 1 sv status in GNSS blacklist VTS test
Yu-Han Yang [Mon, 2 Jul 2018 17:48:08 +0000 (10:48 -0700)]
Tolerate 1 sv status in GNSS blacklist VTS test

Bug: 110969497
Test: run VTS test on device.
Merged-In: I26345bb62513da8530cb48672e5f59a915817cb4
Change-Id: I26345bb62513da8530cb48672e5f59a915817cb4
(cherry picked from commit 91cc8f4832882e8fa9baa04d717184636a57314d)

2 years agoVTS: Do not require XML for Audio effect V2
Kevin Rocard [Thu, 19 Jul 2018 20:31:47 +0000 (13:31 -0700)]
VTS: Do not require XML for Audio effect V2

In O, the Audio effect V2 HAL allows not to have an audio effect XML
configuration but to use a .conf format.

In P, before this patch, the Audio effect V2 HAL _requires_ to have an
audio effect XML configuration and forbids the use of a .conf format.

This is discouraged by Treble as it means that an unchanged HAL V2
implementation that was compatible with O VTS will not be with P VTS.

As a result, revert to the Oreo behavior for Audio Effect V2 VTS.

Note that the audio effect V4 VTS is not changed by this patch and
still requires an audio effect XML configuration.
Aka device _updating_ to P will not have to upgrade to XML but new
devices lunching on P are still required to have an audio effect
XML configuration.

This commit only changes VTS code.

Test: cd hardware/interfaces/audio/effect/
      mmm 2.0/vts/functional 4.0/vts/functional && adb sync data
      adb push *.0/xml/audio_effects_conf_V*.xsd /data/local/tmp/
      adb shell
      cd /data/nativetest64
      OPS=--gtest_filter=CheckConfig.audioEffectsConfigurationValidation
      VtsHalAudioEffectV2_0TargetTest/VtsHalAudioEffectV2_0TargetTest $OPS
      VtsHalAudioEffectV4_0TargetTest/VtsHalAudioEffectV4_0TargetTest $OPS
      rm /{odm,vendor,system}/etc/audio_effects.xml || true
      VtsHalAudioEffectV2_0TargetTest/VtsHalAudioEffectV2_0TargetTest $OPS
      ! VtsHalAudioEffectV4_0TargetTest/VtsHalAudioEffectV4_0TargetTest $OPS
Bug: 111421676
Change-Id: Ifb15d65ae4aa65759c8ebaa91cbc8c02234030dc
Merged-In: Ifb15d65ae4aa65759c8ebaa91cbc8c02234030dc
Signed-off-by: Kevin Rocard <krocard@google.com>
(cherry picked from commit b41b575475f3c93fe30216b9cdb2db441b92854b)

2 years agoCamera: Don't hold 'mLock' when closing the camera session
Emilian Peev [Thu, 26 Jul 2018 12:00:08 +0000 (13:00 +0100)]
Camera: Don't hold 'mLock' when closing the camera session

After flushing the camera requests don't try to close the
camera session while still holding 'mLock'. Different Hals
could still try and return additional results which then will
get blocked on 'mLock'. Closing the session could potentially
introduce a deadlock if the Hal implementation waits for any
of the result calls to return.

Bug: 111836165
Test: vts-tradefed run commandAndExit vts --skip-all-system-status-check
--skip-preconditions --module VtsHalCameraProviderV2_4Target -l INFO

Change-Id: I0f309f435cc76db3f9b6ba500da65a232b014717
Merged-In: I0f309f435cc76db3f9b6ba500da65a232b014717
(cherry picked from commit 8e920568371136b011c79e6c1d15bcb4c047d0a3)

2 years agoFix KM VTS tests for Strongbox implementations
Baranidharan Muthukumaran [Fri, 24 Aug 2018 20:31:35 +0000 (13:31 -0700)]
Fix KM VTS tests for Strongbox implementations

Modify RSA keysize used in various tests
to ensure both TEE and Strongbox implementations
can be validated.
Skip invalid keysizes that Strongbox does not
support.

Test: Patches the strongbox tests
Bug: 112189538
Change-Id: I46ab01ce9b8224403e2a334a894967761d6799c9
Signed-off-by: Max Bires <jbires@google.com>
2 years agoAudio VTS was testing wrong uninitialized variable due to typo
Kevin Rocard [Fri, 29 Jun 2018 01:00:05 +0000 (18:00 -0700)]
Audio VTS was testing wrong uninitialized variable due to typo

The test was testing a uninitialized variable instead of testing
the result of the tested method.

Bug: 110963314
Test: vts-tradefed run commandAndExit vts --module VtsHalAudioV2_0Target
Merged-In: I9a212eef690ae627fd7f7dbfaf4a0b4047c491b3
Change-Id: I9a212eef690ae627fd7f7dbfaf4a0b4047c491b3
Signed-off-by: Kevin Rocard <krocard@google.com>
(cherry picked from commit 72641e7ad014a011562c3fd16444b919d32aeb63)

2 years agoAdd VTS test to verify scheduling capability
Vishal Agarwal [Wed, 6 Jun 2018 01:42:01 +0000 (18:42 -0700)]
Add VTS test to verify scheduling capability

2018+ devices must support GNSS capability scheduling
Test results: go/vts-review-bucket/pi-dev/4267645

Bug: 109642198
Test: atest VtsHalGnssV1_0TargetTest
Merged-In: I7394674abca8f8c40ab30403be6b41bbbb279956
Change-Id: I7394674abca8f8c40ab30403be6b41bbbb279956
(cherry picked from commit e3ff41fc12fb7a80ee533e4459035ef4545c174d)

2 years agoAdd setIndicationFilter response notification in 1.2 VTS
sqian [Thu, 7 Jun 2018 05:35:20 +0000 (22:35 -0700)]
Add setIndicationFilter response notification in 1.2 VTS

Test: compile
Bug: 109822806
Merged-In: I95102a148a26cab80235cc68ad83143a9bb6eb39
Change-Id: I95102a148a26cab80235cc68ad83143a9bb6eb39
(cherry picked from commit 0ff41b94b30a0db0ce4a6a5b29600ced5853a762)

2 years ago[ConfigStore] Clarify hasHDRDisplay spec.
Peiyong Lin [Thu, 23 Aug 2018 01:01:07 +0000 (18:01 -0700)]
[ConfigStore] Clarify hasHDRDisplay spec.

BUG: 111505327
Test: Build, flash and boot

Change-Id: Ie22d4c7b069a918f039a60317a213dc6a7efb205
Merged-In: Ie22d4c7b069a918f039a60317a213dc6a7efb205

2 years agoAdd REQUEST_NOT_SUPPORTED for pin and pin2 Icc VTS
sqian [Thu, 12 Jul 2018 23:30:24 +0000 (16:30 -0700)]
Add REQUEST_NOT_SUPPORTED for pin and pin2 Icc VTS

Bug: 111222834
Test: sanity
Change-Id: Ia3b96e83d6173c2c80bdbf7763a876883b167af9
Merged-In: Ia3b96e83d6173c2c80bdbf7763a876883b167af9
(cherry picked from commit c0a06f34c88cf9dc017be6178113b35c3c7fc67e)

2 years agoAdd SIM_PUK2 for Icc VTS tests
sqian [Mon, 9 Jul 2018 21:45:12 +0000 (14:45 -0700)]
Add SIM_PUK2 for Icc VTS tests

Add SIM_PUK2 for supplyIccPin2ForApp and changeIccPin2ForApp if sim
card is in the puk2 state.

Bug: 111211929
Test: sanity
Change-Id: I80d924cc4a61565887cbd2a65ee5927a42ad656e
Merged-In: I80d924cc4a61565887cbd2a65ee5927a42ad656e
(cherry picked from commit 4ed0a216adc3bc9460d11d302ba53db9707ded44)

2 years ago[automerger skipped] Add docs for setSignalStrengthReportingCriteria
Nathan Harold [Tue, 21 Aug 2018 03:44:31 +0000 (20:44 -0700)]
[automerger skipped] Add docs for setSignalStrengthReportingCriteria
am: dd06d73cab  -s ours

Change-Id: Ia23dd5a7f2a354a6ada49458a4497a46cdd9cfff

2 years agoAdd docs for setSignalStrengthReportingCriteria
Nathan Harold [Thu, 21 Jun 2018 18:46:42 +0000 (11:46 -0700)]
Add docs for setSignalStrengthReportingCriteria

Because setSignalStrengthReportingCriteria only
supports a single measurement quantity, provide
further clarification on the applicability of the
API and how it may be used in various situations.

Bug: 110121199
Test: compilation - docstring-only change
Merged-In: If4236070fbc03368e5a78b0cf502cdc4a529a6ed
Change-Id: If4236070fbc03368e5a78b0cf502cdc4a529a6ed
(cherry picked from commit 529d2fffa02451406f013b354fd7c07164f619b1)

2 years agoMerge "Add back keymaster@4.0 hash." into pie-vts-dev
Steven Moreland [Tue, 21 Aug 2018 00:20:49 +0000 (17:20 -0700)]
Merge "Add back keymaster@4.0 hash." into pie-vts-dev
am: 6a20e646e4

Change-Id: Id5a125e9a6563a71873e9edcc746c36bc8594c87

2 years agoMerge "Add back keymaster@4.0 hash." into pie-vts-dev
Treehugger Robot [Mon, 20 Aug 2018 23:44:03 +0000 (23:44 +0000)]
Merge "Add back keymaster@4.0 hash." into pie-vts-dev

2 years ago[automerger skipped] resolve merge conflicts of cd02298b46cfb17954555e0f1d324f63085aa...
Yin-Chia Yeh [Mon, 20 Aug 2018 18:32:43 +0000 (11:32 -0700)]
[automerger skipped] resolve merge conflicts of cd02298b46cfb17954555e0f1d324f63085aa204 to oreo-mr1-vts-dev am: 79cea44239  -s ours
am: 46a5d4f73b

Change-Id: Ie798e2e248a6eea4c8a705d3bd8063f054c79205

2 years ago[automerger skipped] resolve merge conflicts of cd02298b46cfb17954555e0f1d324f63085aa...
Yin-Chia Yeh [Mon, 20 Aug 2018 18:29:40 +0000 (11:29 -0700)]
[automerger skipped] resolve merge conflicts of cd02298b46cfb17954555e0f1d324f63085aa204 to oreo-mr1-vts-dev
am: 79cea44239  -s ours

Change-Id: I17d4a58573074b7746a9d35be04414f9227ec47e

2 years agoEffect VTS: Allow an effect proxy as pre/post processing am: 0f0328fc4e
Kevin Rocard [Mon, 20 Aug 2018 18:21:39 +0000 (11:21 -0700)]
Effect VTS: Allow an effect proxy as pre/post processing am: 0f0328fc4e
am: a3268e954d

Change-Id: Ic9afa418ca68ed98368ab4696c4d3a3e5e8ccbdb

2 years agoMerge "Fix base class of WifiHidlEnvironment_1_2" into pie-vts-dev
Hsin-Yi Chen [Mon, 20 Aug 2018 18:14:25 +0000 (11:14 -0700)]
Merge "Fix base class of WifiHidlEnvironment_1_2" into pie-vts-dev
am: a73a8c9b2b

Change-Id: I18081c95710d4d505991628994df7a9ebbdc99df

2 years ago[automerger skipped] Merge "Fix IUsb version number in vts test" into pie-vts-dev
Hsin-Yi Chen [Mon, 20 Aug 2018 18:14:00 +0000 (11:14 -0700)]
[automerger skipped] Merge "Fix IUsb version number in vts test" into pie-vts-dev
am: 0a55878d1e  -s ours

Change-Id: I612a4597b8689a232e75e97a634aa535ca0730a2

2 years agoEffect VTS: Allow an effect proxy as pre/post processing
Kevin Rocard [Mon, 20 Aug 2018 18:13:35 +0000 (11:13 -0700)]
Effect VTS: Allow an effect proxy as pre/post processing
am: 0f0328fc4e

Change-Id: I570e2a73de01900cf39b5d08cfed370ee17a0e38

2 years agoAdd back keymaster@4.0 hash.
Steven Moreland [Mon, 20 Aug 2018 17:46:48 +0000 (10:46 -0700)]
Add back keymaster@4.0 hash.

This was changed after this branch was released. The originally
released hash needs to be restored since that is what partners
are building with.

Bug: 112688384
Bug: 78104779
Test: m android.hardware.keymaster@4.0 (tests hashes)
Change-Id: I0f59a493d7f17a13402d992495d1a259f6257077
(cherry picked from commit ec720564dbdef01d14fcf46c46ea18294440358b)

2 years agoMerge "Fix matrix dep on kernel configs"
Treehugger Robot [Fri, 17 Aug 2018 23:51:59 +0000 (23:51 +0000)]
Merge "Fix matrix dep on kernel configs"

2 years agoMerge changes from topic "share-buffer"
Treehugger Robot [Fri, 17 Aug 2018 23:03:44 +0000 (23:03 +0000)]
Merge changes from topic "share-buffer"

* changes:
  Audio default HAL: hidl_memory size must be positive
  Aaudio: Implement app shareable flag instead of -size hack

2 years agoFix matrix dep on kernel configs
Yifan Hong [Fri, 17 Aug 2018 22:45:03 +0000 (15:45 -0700)]
Fix matrix dep on kernel configs

Use global instead of rule variables.

Test: make a change in kernel configs, existing out files
are changed.

Change-Id: Ic731356b4533bc10743d3711309ab16de1d3bd78

2 years agoChange ImportWrappedKeyTest back to SHA1
Shawn Willden [Mon, 6 Aug 2018 23:23:23 +0000 (17:23 -0600)]
Change ImportWrappedKeyTest back to SHA1

Change I5f877b2a1ac66026a876e145416ba078d486e4b5 inadvertently changed
the digest used for ImportWrappedKey, breaking the test.  This CL
reverts that portion of the change.

Test: VtsHalKeymasterV4_0TargetTest
Bug: 112279922
Bug: 80246122
Change-Id: Ib8e2e7793ba46ae0d29d8407bb730a35bdb5ea98

2 years agoRequire KM4 attestations contain the right version
Shawn Willden [Tue, 31 Jul 2018 19:47:37 +0000 (13:47 -0600)]
Require KM4 attestations contain the right version

Note that devices with KM4 will fail to pass VTS after this
lands, until the fix from Qualcomm arrives.

Test: VtsHalKeymasterV4_0TargetTest
Bug: 112040197
Bug: 80246122
Change-Id: Ie2cd917af704b9f19de3537297b3a7e4f0c861e9

2 years agokeymaster: skip SHA2 digest tests for strongbox
nagendra modadugu [Mon, 23 Jul 2018 17:32:28 +0000 (10:32 -0700)]
keymaster: skip SHA2 digest tests for strongbox

Strongbox is not required to support SHA-2 digests,
so skip the related tests.

Bug: 109771020
Bug: 80246122
Test: This is the test
Change-Id: I5f877b2a1ac66026a876e145416ba078d486e4b5

2 years agokeymaster spec doesn't require update to output
nagendra modadugu [Tue, 26 Jun 2018 02:56:35 +0000 (19:56 -0700)]
keymaster spec doesn't require update to output

Remove out of spec enforcement on the amount of data returned
by update, as this is not specified in the HAL.

Bug: 109771020
Bug: 80246122
Test: yes it is
Change-Id: Ic41afbd01d51faf48d3c0fe090409ebcd257cc1e

2 years agoFix attestation test.
Shawn Willden [Wed, 20 Jun 2018 04:10:03 +0000 (22:10 -0600)]
Fix attestation test.

Bug: 77588764
Bug: 80246122
Test: VtsHalKeymasterV4_0TargetTest
Change-Id: Ibe264d08ae7b3333a6949761a92759f5305b3fcb

2 years agoMerge "Fix base class of WifiHidlEnvironment_1_2" into pie-vts-dev
Treehugger Robot [Thu, 16 Aug 2018 15:43:19 +0000 (15:43 +0000)]
Merge "Fix base class of WifiHidlEnvironment_1_2" into pie-vts-dev