]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/platform-hardware-interfaces.git/shortlog
android/platform-hardware-interfaces.git
2018-05-16 Yifan HongUpdate kernel minor revision for P.
2018-05-16 android-build... Snap for 4784261 from e9a39e2714c7311fb88b38f509a967646...
2018-05-15 Kiran RachuriUpdate types.hal comments
2018-05-14 android-build... Snap for 4779114 from 5acc0b1fa3b2793a85465d4342388c5c8...
2018-05-14 Lorenzo ColittiMerge changes I819a2942,Ife0607e7 into pi-dev
2018-05-13 android-build... Snap for 4778776 from 68995cb341a4617f3a09bff033e26e473...
2018-05-12 Kourosh Derakshancamera: Adding 64-bit version of Camera Provider
2018-05-11 NickAdd feature flag to disable wifi AP on the watch.
2018-05-11 Chong Zhangcas: do not use hidl_memory if size is > SIZE_MAX
2018-05-11 TreeHugger... Merge "Add utility method to perform HMAC agreement...
2018-05-11 Lorenzo ColittiFix OffloadControlHidlTestBase.AdditionalStopsWithInitR...
2018-05-11 Lorenzo ColittiAdd debugging to VtsHalTetherOffloadControl test.
2018-05-11 Pawin VongmasaAdd multichannel support
2018-05-11 Shawn WilldenAdd utility method to perform HMAC agreement
2018-05-10 Chao YanMerge "Added fake VHAL value generator based on JSON...
2018-05-10 Chong Zhangcas: do not use hidl_memory if size is > SIZE_MAX
2018-05-10 Chao YanAdded fake VHAL value generator based on JSON file
2018-05-08 android-build... Snap for 4767765 from 73bfa71121f882493ca63265926b8e797...
2018-05-07 Kiran RachuriMerge "Add HVAC properties" into pi-dev
2018-05-06 android-build... Snap for 4765094 from 8f3b492c83fb2a01e95e3edc8a4bda147...
2018-05-05 Kiran RachuriAdd HVAC properties
2018-05-05 android-build... Merge changes I29bbf6bf,Ib0b03fb6 into pi-dev
2018-05-03 Marissa WallMerge "graphics: add new gralloc1 functions to passthro...
2018-05-03 Marissa Wallgraphics: add new gralloc1 functions to passthrough
2018-05-03 android-build... Merge "Camera: Set partial results in result batcher...
2018-05-03 Emilian PeevCamera: Set partial results in result batcher
2018-05-03 android-build... Snap for 4759746 from 3d5a6411222f0b8b47a16b3442f6417bb...
2018-05-02 android-build... Merge "Camera: fix first launch api level logic" into...
2018-05-02 Yin-Chia YehCamera: fix first launch api level logic
2018-05-02 Kevin RocardAudio HAL HIDL wrapper: Fix incorrect conversion of...
2018-05-02 Kevin RocardAudio V4 VTS: test setter even if getter is NOT_SUPPORTED
2018-05-01 android-build... Snap for 4754571 from 14bdba8865098afc35515ef73c5f8fa3f...
2018-05-01 android-build... Merge "matrix: copy kernel configs to subdirectory...
2018-04-30 Gene KarshenboymMerge "Add check for empty RDS_PS." into pi-dev
2018-04-30 Gene KarshenboymMerge "Extend tune workaround time." into pi-dev
2018-04-30 Scott RandolphMerge "Remove ENV_CABIN_TEMPERATURE from VHal" into...
2018-04-30 android-build... Merge "Add AUDIO_MICROPHONE_CHANNEL_MAPPING_CNT." into...
2018-04-30 Yifan Hongmatrix: copy kernel configs to subdirectory.
2018-04-30 jiabinAdd AUDIO_MICROPHONE_CHANNEL_MAPPING_CNT.
2018-04-30 Tomasz WasilczykAdd check for empty RDS_PS.
2018-04-30 Tomasz WasilczykExtend tune workaround time.
2018-04-29 android-build... Snap for 4751833 from 89802f742382863ea26e7761bf773b0d4...
2018-04-27 Michael ButlerMerge "NNAPI: sync NDK and HAL documentation" into...
2018-04-27 Yifan HongMerge "Restore kernel requirements for frozen matrices...
2018-04-27 Michael ButlerNNAPI: sync NDK and HAL documentation
2018-04-27 android-build... Merge "Camera: check return value of callback" into...
2018-04-27 Yin-Chia YehCamera: check return value of callback
2018-04-27 Jiabin HuangMerge "Add vts for microphone enumeration APIs." into...
2018-04-27 Yifan HongRestore kernel requirements for frozen matrices.
2018-04-26 Janis DanisevskisFix for bug in Fix for wrongly initialized test key
2018-04-26 TreeHugger... Merge "Fix wrongly initialized test key." into pi-dev
2018-04-26 Janis DanisevskisFix wrongly initialized test key.
2018-04-26 Mika RaentoMerge "Update namespace to match framework/ml/nn" into...
2018-04-26 Mika RaentoMerge "Update neuralnetworks/*/types.hal to match impl...
2018-04-26 android-build... Snap for 4745538 from 7fa25dee8f24c7e8b22f7e499efe1acab...
2018-04-26 Scott RandolphRemove ENV_CABIN_TEMPERATURE from VHal
2018-04-26 TreeHugger... Merge "Use configArray for HVAC_POWER_ON" into pi-dev
2018-04-26 Scott RandolphMerge "Rename EV_CONNECTOR_TYPE enums" into pi-dev
2018-04-26 Steve PaikUse configArray for HVAC_POWER_ON
2018-04-26 Michael Butler[automerger skipped] Relax NeuralNetwork's VTS positive...
2018-04-25 Michael ButlerRelax NeuralNetwork's VTS positive and negative base...
2018-04-25 Michael ButlerRelax NeuralNetwork's VTS positive and negative base...
2018-04-25 Chia-I Wugraphics: allow re-saturation for any legacy dataspace
2018-04-25 Steve PaikRename EV_CONNECTOR_TYPE enums
2018-04-25 jiabinAdd vts for microphone enumeration APIs.
2018-04-25 Mika RaentoUpdate neuralnetworks/*/types.hal to match impl
2018-04-25 android-build... Snap for 4742838 from adf9e18c01c3bf25858aacc380c16aa46...
2018-04-25 Kevin RocardMerge changes I2f70f2ec,I9d77a59e,Ied3a657d,Ib6e9d017...
2018-04-24 Kevin RocardAudio V4: Add missing VTS
2018-04-24 Roshan PiusMerge "wifi(implementation): Use stub for |read_packet_...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris ChangVTS: fix RadioHidlTest.getAvailableNetworks issue am...
2018-04-24 Iris Chang[automerger skipped] VTS: fix RadioHidlTest.getAvailabl...
2018-04-24 Iris ChangVTS: fix RadioHidlTest.getAvailableNetworks issue
2018-04-24 android-build... Snap for 4739962 from a088ab45707ce6f368f8171a3512197b1...
2018-04-24 Kevin RocardAudio V4: VTS Pause was testing resume
2018-04-24 Kevin RocardAudio V4: factorize analyzeStatus
2018-04-24 Wei WangMerge "dumpstate: add interface into rc file" into...
2018-04-23 Eric LaurentMerge "Audio V4: dump effect HAL using the standard...
2018-04-23 Michael ButlerMerge "NNAPI: Create VTS _relaxed tests for newly added...
2018-04-23 Kevin RocardAudio V4: fix invalid SupportedChannelMasks test
2018-04-23 Michael ButlerNNAPI: Create VTS _relaxed tests for newly added tests
2018-04-23 TreeHugger... Merge "Deprecate nfc@1.0 for P." into pi-dev
2018-04-23 Steven MorelandDeprecate nfc@1.0 for P.
2018-04-22 android-build... Snap for 4736748 from 63abd8fdbc05ba5534141ae93816572e2...
2018-04-21 TreeHugger... Merge changes I41328afc,Ie543519f into pi-dev
2018-04-21 Kevin RocardAudio V4: setMode VTS incorrectly assume 0 was invalid
2018-04-21 Kevin RocardAudio V4: XSD device category was missing hearing aid
2018-04-21 Kevin RocardAudio V4: some legacy getSupported can return NOT_SUPPORTED
2018-04-21 Kevin RocardAudio V4: Improve VTS error messages
2018-04-21 Kevin RocardAudio: setParam improve status_t to Result consistency
2018-04-21 Kevin RocardAudio: make core/4.0/default/Util.h version dependant
2018-04-20 Roshan Piuswifi(implementation): Use stub for |read_packet_filter|
2018-04-20 Kevin RocardAudio V4: dump effect HAL using the standard debug()
2018-04-20 Shuo QianMerge "Sim Status Present VTS" into pi-dev
2018-04-20 Michael ButlerMerge "Update NNAPI OWNERS file -- VTS" into pi-dev
2018-04-20 Michael ButlerUpdate NNAPI OWNERS file -- VTS
next