summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: d5f825c)
raw | patch | inline | side by side (parent: d5f825c)
author | David Anderson <dvander@google.com> | |
Mon, 30 Jul 2018 19:54:53 +0000 (12:54 -0700) | ||
committer | David Anderson <dvander@google.com> | |
Mon, 30 Jul 2018 21:48:13 +0000 (14:48 -0700) |
When host fastboot sends sparse blocks to the device, it tries to only
send blocks in multiples of 1024 bytes. If a block is not aligned to this
size, the excess bytes are prepended to the next write operation. This
is implemented by doing the write in two steps: first the previous
excess from the last write (plus new data up to alignment), then a
second write for the aligned remainder of the new data.
This logic has a bug if the final block plus the previous excess data
contains >= 1024 but < 2048 bytes. In this case the first write will
drain 1024 bytes from the data, and the second write will not have 1024
bytes to write. Instead of retaining this data for the next write, it
tries to write 0 chunks (and thus 0 bytes), which hangs the ioctl() call.
Bug: N/A
Test: "fastboot flash super super.img" where super.img is generated by
lpmake, containing system and product_services partitions and
images.
Change-Id: I9e8523c976ec84d5a57b36a28f4b1ca800edb7e7
send blocks in multiples of 1024 bytes. If a block is not aligned to this
size, the excess bytes are prepended to the next write operation. This
is implemented by doing the write in two steps: first the previous
excess from the last write (plus new data up to alignment), then a
second write for the aligned remainder of the new data.
This logic has a bug if the final block plus the previous excess data
contains >= 1024 but < 2048 bytes. In this case the first write will
drain 1024 bytes from the data, and the second write will not have 1024
bytes to write. Instead of retaining this data for the next write, it
tries to write 0 chunks (and thus 0 bytes), which hangs the ioctl() call.
Bug: N/A
Test: "fastboot flash super super.img" where super.img is generated by
lpmake, containing system and product_services partitions and
images.
Change-Id: I9e8523c976ec84d5a57b36a28f4b1ca800edb7e7
fastboot/fastboot_driver.cpp | patch | blob | history |
index c308420552ade7003af8776f6b9e01c39d94d542..aabc620d431a00cd7d663ae9cd870973e30b849a 100644 (file)
}
RetCode FastBootDriver::SendBuffer(const void* buf, size_t size) {
+ if (!size) {
+ return SUCCESS;
+ }
+
// Write the buffer
ssize_t tmp = transport->Write(buf, size);