summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 4f9d34e)
raw | patch | inline | side by side (parent: 4f9d34e)
author | Vasily Khoruzhick <anarsoul@gmail.com> | |
Tue, 6 Nov 2018 04:24:28 +0000 (20:24 -0800) | ||
committer | Jagan Teki <jagan@amarulasolutions.com> | |
Tue, 13 Nov 2018 16:37:39 +0000 (22:07 +0530) |
A64 and H6 support automatic delay calibration and Linux driver uses it
instead of hardcoded delays. Add support for it to u-boot driver.
Fixes eMMC instability on Pinebook
Signed-off-by: Vasily Khoruzhick <anarsoul@gmail.com>
Acked-by: Maxime Ripard <maxime.ripard@bootlin.com>
Tested-by: Maxime Ripard <maxime.ripard@bootlin.com>
Reviewed-by: Andre Przywara <andre.przywara@arm.com>
Cc: Vagrant Cascadian <vagrant@debian.org>
Reviewed-by: Jagan Teki <jagan@openedev.com>
instead of hardcoded delays. Add support for it to u-boot driver.
Fixes eMMC instability on Pinebook
Signed-off-by: Vasily Khoruzhick <anarsoul@gmail.com>
Acked-by: Maxime Ripard <maxime.ripard@bootlin.com>
Tested-by: Maxime Ripard <maxime.ripard@bootlin.com>
Reviewed-by: Andre Przywara <andre.przywara@arm.com>
Cc: Vagrant Cascadian <vagrant@debian.org>
Reviewed-by: Jagan Teki <jagan@openedev.com>
arch/arm/include/asm/arch-sunxi/mmc.h | patch | blob | history | |
drivers/mmc/sunxi_mmc.c | patch | blob | history |
index d98c53faaa1f0cf166e771cf1719c141b4f593a5..f2deafddd20203e30dfb91d2ba050b2f0bc0ac08 100644 (file)
u32 cbda; /* 0x94 */
u32 res2[26];
#if defined(CONFIG_SUNXI_GEN_SUN6I) || defined(CONFIG_MACH_SUN50I_H6)
- u32 res3[64];
+ u32 res3[17];
+ u32 samp_dl;
+ u32 res4[46];
#endif
u32 fifo; /* 0x100 / 0x200 FIFO access address */
};
#define SUNXI_MMC_COMMON_CLK_GATE (1 << 16)
#define SUNXI_MMC_COMMON_RESET (1 << 18)
+#define SUNXI_MMC_CAL_DL_SW_EN (0x1 << 7)
+
struct mmc *sunxi_mmc_init(int sdc_no);
#endif /* _SUNXI_MMC_H */
index 39f15eb4236c252f9e24b71894452e3be28bddc8..147eb9b4d5f9c3c49f92a414b85c7ee4442da5c3 100644 (file)
--- a/drivers/mmc/sunxi_mmc.c
+++ b/drivers/mmc/sunxi_mmc.c
{
unsigned int pll, pll_hz, div, n, oclk_dly, sclk_dly;
bool new_mode = false;
+ bool calibrate = false;
u32 val = 0;
if (IS_ENABLED(CONFIG_MMC_SUNXI_HAS_NEW_MODE) && (priv->mmc_no == 2))
new_mode = true;
+#if defined(CONFIG_MACH_SUN50I) || defined(CONFIG_MACH_SUN50I_H6)
+ calibrate = true;
+#endif
+
/*
* The MMC clock has an extra /2 post-divider when operating in the new
* mode.
val = CCM_MMC_CTRL_MODE_SEL_NEW;
setbits_le32(&priv->reg->ntsr, SUNXI_MMC_NTSR_MODE_SEL_NEW);
#endif
- } else {
+ } else if (!calibrate) {
+ /*
+ * Use hardcoded delay values if controller doesn't support
+ * calibration
+ */
val = CCM_MMC_CTRL_OCLK_DLY(oclk_dly) |
CCM_MMC_CTRL_SCLK_DLY(sclk_dly);
}
rval &= ~SUNXI_MMC_CLK_DIVIDER_MASK;
writel(rval, &priv->reg->clkcr);
+#if defined(CONFIG_MACH_SUN50I) || defined(CONFIG_MACH_SUN50I_H6)
+ /* A64 supports calibration of delays on MMC controller and we
+ * have to set delay of zero before starting calibration.
+ * Allwinner BSP driver sets a delay only in the case of
+ * using HS400 which is not supported by mainline U-Boot or
+ * Linux at the moment
+ */
+ writel(SUNXI_MMC_CAL_DL_SW_EN, &priv->reg->samp_dl);
+#endif
+
/* Re-enable Clock */
rval |= SUNXI_MMC_CLK_ENABLE;
writel(rval, &priv->reg->clkcr);