]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - android/vendor-ti-am57x.git/blobdiff - sgx_km/eurasia_km/services4/srvkm/include/perproc.h
sgx_km: Build SGX KM from source
[android/vendor-ti-am57x.git] / sgx_km / eurasia_km / services4 / srvkm / include / perproc.h
diff --git a/sgx_km/eurasia_km/services4/srvkm/include/perproc.h b/sgx_km/eurasia_km/services4/srvkm/include/perproc.h
new file mode 100644 (file)
index 0000000..124f2f2
--- /dev/null
@@ -0,0 +1,141 @@
+/*************************************************************************/ /*!
+@Title          Handle Manager API
+@Copyright      Copyright (c) Imagination Technologies Ltd. All Rights Reserved
+@Description   Perprocess data
+@License        Dual MIT/GPLv2
+
+The contents of this file are subject to the MIT license as set out below.
+
+Permission is hereby granted, free of charge, to any person obtaining a copy
+of this software and associated documentation files (the "Software"), to deal
+in the Software without restriction, including without limitation the rights
+to use, copy, modify, merge, publish, distribute, sublicense, and/or sell
+copies of the Software, and to permit persons to whom the Software is
+furnished to do so, subject to the following conditions:
+
+The above copyright notice and this permission notice shall be included in
+all copies or substantial portions of the Software.
+
+Alternatively, the contents of this file may be used under the terms of
+the GNU General Public License Version 2 ("GPL") in which case the provisions
+of GPL are applicable instead of those above.
+
+If you wish to allow use of your version of this file only under the terms of
+GPL, and not to allow others to use your version of this file under the terms
+of the MIT license, indicate your decision by deleting the provisions above
+and replace them with the notice and other provisions required by GPL as set
+out in the file called "GPL-COPYING" included in this distribution. If you do
+not delete the provisions above, a recipient may use your version of this file
+under the terms of either the MIT license or GPL.
+
+This License is also included in this distribution in the file called
+"MIT-COPYING".
+
+EXCEPT AS OTHERWISE STATED IN A NEGOTIATED AGREEMENT: (A) THE SOFTWARE IS
+PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR IMPLIED, INCLUDING
+BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR
+PURPOSE AND NONINFRINGEMENT; AND (B) IN NO EVENT SHALL THE AUTHORS OR
+COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER LIABILITY, WHETHER
+IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN
+CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE SOFTWARE.
+*/ /**************************************************************************/
+#ifndef __PERPROC_H__
+#define __PERPROC_H__
+
+#if defined (__cplusplus)
+extern "C" {
+#endif
+
+#include "img_types.h"
+#include "resman.h"
+
+#include "handle.h"
+
+typedef struct _PVRSRV_PER_PROCESS_DATA_
+{
+       IMG_UINT32              ui32PID;
+       IMG_HANDLE              hBlockAlloc;
+       PRESMAN_CONTEXT         hResManContext;
+       IMG_HANDLE              hPerProcData;
+       PVRSRV_HANDLE_BASE      *psHandleBase;
+#if defined (PVR_SECURE_HANDLES)
+       /* Handles are being allocated in batches */
+       IMG_BOOL                bHandlesBatched;
+#endif  /* PVR_SECURE_HANDLES */
+       IMG_UINT32              ui32RefCount;
+
+       /* True if the process is the initialisation server. */
+       IMG_BOOL                bInitProcess;
+#if defined(PDUMP)
+       /* True if pdump data from the process is 'persistent' */
+       IMG_BOOL                bPDumpPersistent;
+#if defined(SUPPORT_PDUMP_MULTI_PROCESS)
+       /* True if this process is marked for pdumping. This flag is
+        * significant in a multi-app environment.
+        */
+       IMG_BOOL                bPDumpActive;
+#endif /* SUPPORT_PDUMP_MULTI_PROCESS */
+#endif
+       /*
+        * OS specific data can be stored via this handle.
+        * See osperproc.h for a generic mechanism for initialising
+        * this field.
+        */
+       IMG_HANDLE              hOsPrivateData;
+} PVRSRV_PER_PROCESS_DATA;
+
+PVRSRV_PER_PROCESS_DATA *PVRSRVPerProcessData(IMG_UINT32 ui32PID);
+
+PVRSRV_ERROR PVRSRVPerProcessDataConnect(IMG_UINT32    ui32PID, IMG_UINT32 ui32Flags);
+IMG_VOID PVRSRVPerProcessDataDisconnect(IMG_UINT32     ui32PID);
+
+PVRSRV_ERROR PVRSRVPerProcessDataInit(IMG_VOID);
+PVRSRV_ERROR PVRSRVPerProcessDataDeInit(IMG_VOID);
+
+#ifdef INLINE_IS_PRAGMA
+#pragma inline(PVRSRVFindPerProcessData)
+#endif
+static INLINE
+PVRSRV_PER_PROCESS_DATA *PVRSRVFindPerProcessData(IMG_VOID)
+{
+       return PVRSRVPerProcessData(OSGetCurrentProcessIDKM());
+}
+
+
+#ifdef INLINE_IS_PRAGMA
+#pragma inline(PVRSRVProcessPrivateData)
+#endif
+static INLINE
+IMG_HANDLE PVRSRVProcessPrivateData(PVRSRV_PER_PROCESS_DATA *psPerProc)
+{
+       return (psPerProc != IMG_NULL) ? psPerProc->hOsPrivateData : IMG_NULL;
+}
+
+
+#ifdef INLINE_IS_PRAGMA
+#pragma inline(PVRSRVPerProcessPrivateData)
+#endif
+static INLINE
+IMG_HANDLE PVRSRVPerProcessPrivateData(IMG_UINT32 ui32PID)
+{
+       return PVRSRVProcessPrivateData(PVRSRVPerProcessData(ui32PID));
+}
+
+#ifdef INLINE_IS_PRAGMA
+#pragma inline(PVRSRVFindPerProcessPrivateData)
+#endif
+static INLINE
+IMG_HANDLE PVRSRVFindPerProcessPrivateData(IMG_VOID)
+{
+       return PVRSRVProcessPrivateData(PVRSRVFindPerProcessData());
+}
+
+#if defined (__cplusplus)
+}
+#endif
+
+#endif /* __PERPROC_H__ */
+
+/******************************************************************************
+ End of file (perproc.h)
+******************************************************************************/