1 /******************************************************************************
2 @file stream_private.h
4 @brief TIMAC 2.0 API Internal "stream" implimentation details
6 Group: WCS LPC
7 $Target Devices: Linux: AM335x, Embedded Devices: CC1310, CC1350$
9 ******************************************************************************
10 $License: BSD3 2016 $
12 Copyright (c) 2015, Texas Instruments Incorporated
13 All rights reserved.
15 Redistribution and use in source and binary forms, with or without
16 modification, are permitted provided that the following conditions
17 are met:
19 * Redistributions of source code must retain the above copyright
20 notice, this list of conditions and the following disclaimer.
22 * Redistributions in binary form must reproduce the above copyright
23 notice, this list of conditions and the following disclaimer in the
24 documentation and/or other materials provided with the distribution.
26 * Neither the name of Texas Instruments Incorporated nor the names of
27 its contributors may be used to endorse or promote products derived
28 from this software without specific prior written permission.
30 THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
31 AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
32 THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
33 PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
34 CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
35 EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
36 PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
37 OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
38 WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
39 OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
40 EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
41 ******************************************************************************
42 $Release Name: TI-15.4Stack Linux x64 SDK$
43 $Release Date: July 14, 2016 (2.00.00.30)$
44 *****************************************************************************/
46 /*
47 * OVERVIEW
48 * ========
49 *
50 * The STREAM implimentations share a number of "common" features
51 * This header file describes the common items shared across all
52 * streams, it is not intended for use by general code
53 * it should only be used by code that is implimenting a stream.
54 */
56 #if !defined(STREAM_PRIVATE_H)
57 #define STREAM_PRIVATE_H
60 #if !defined(_STREAM_IMPLIMENTOR_)
61 #error This file should only be included by stream implimentation code.
62 #endif
64 /* forward decloration */
65 struct io_stream_funcs;
67 /*!
68 * @struct io_stream - represents byte stream, emulates the stdio FILE
69 *
70 * To create a stream, call one of the STREAM_CREATE_foobar() functions
71 * where foobar is the type of interface you wish to access.
72 */
73 struct io_stream {
74 /*! check value, used to verify this is an io-stream */
75 const int *check_ptr;
77 /*! stream specific funcs (method functions, specific to stream type)*/
78 const struct io_stream_funcs *pFuncs;
80 /*! for use internal by stream specific funcs */
81 intptr_t opaque_ptr;
83 /*! for use internal by the io stream to handle unget operations */
84 int unget_buf;
86 /* set to true when an error occurs. */
87 bool is_error;
89 /*! for use by the rd callback */
90 intptr_t rd_rdy_cookie;
92 /*! this callback is called when data is put into the rx fifo */
93 void (*rd_rdy_cb)(struct io_stream *pIO, int nAvail);
94 };
96 /*!
97 * @struct io_stream_funcs
98 *
99 * @brief Functions (methods) that backend various streams
100 */
101 struct io_stream_funcs {
102 /*! Name for debug purposes */
103 const char *name;
105 /*! close the stream, does not always release resources */
106 void (*close_fn)(struct io_stream *pIO);
108 /*!
109 * @brief write bytes to the stream
110 * @param pIO stream - the io stream to use
111 * @param pData - data buffer holding the data
112 * @param nbytes - number of bytes to write
113 * @param timeout_mSecs - timeout in milliseconds (see timeout mSec rule)
114 *
115 * @return -1 on error, 0..actual number of bytes written
116 */
117 int (*wr_fn)(struct io_stream *pIO, const void *pData, size_t n, int timeout_mSecs);
119 /*!
120 * @brief read bytes from the stream
121 * @param pIO stream - the io stream to use
122 * @param pData - data buffer to put data into
123 * @param nbytes - number of bytes to read
124 * @param timeout_mSecs - timeout in milliseconds (see timeout mSec rule)
125 *
126 * @return -1 on error, 0..actual number of bytes read
127 */
128 int (*rd_fn)(struct io_stream *pIO, void *pData, size_t n, int timeout_mSecs);
130 /*!
131 * @brief Determine if the io stream is readable
132 *
133 * @param pIO - the io stream
134 * @param timeout_mSec - the timeout for the poll operation
135 * @return true if it is, false if not
136 */
137 bool (*poll_fn)(struct io_stream *pIO, int timeout_mSec);
139 /*!
140 * @brief Flush all buffered IO to the device
141 *
142 * @param pIO - the io stream
143 *
144 * @return negative error, 0 success
145 */
146 int (*flush_fn)(struct io_stream *pIO);
148 /*!
149 * @brief clear underlying errors.
150 *
151 * @param pIO - the io stream
152 */
153 void (*clear_fn)(struct io_stream *pIO);
154 };
156 /*!
157 * @brief Create & Initialize a io_stream properly
158 * @param pFuncs - set of method functions for this stream.
159 * @param opaque - the opaque parameter for the method functions
160 *
161 * @returns NULL on error, or an initialized io stream
162 *
163 * To return the "handle" to the caller, cast the "io_stream" pointer
164 * to an intptr_t.
165 */
166 struct io_stream *STREAM_createPrivate(const struct io_stream_funcs *pFuncs, intptr_t opaque);
168 /*!
169 * @brief Release resources (memory) in the io_stream structure
170 * @param pIO - io stream from STREAM_CreatePrivate()
171 */
172 void STREAM_destroyPrivate(struct io_stream *pIO);
174 /*!
175 * @brief convert an handle into an io_stream structure pointer.
176 * @param h - public version (handle) of an IO stream
177 * @returns NULL if h is invalid, or a proper structure pointer.
178 */
179 struct io_stream *STREAM_hToStruct(intptr_t h);
181 /*
182 * @brief convert an io_stream structure pointer into a public handle
183 * @param pIO - the io stream to convert.
184 * @returns proper value for the IO stream
185 */
186 intptr_t STREAM_structToH(struct io_stream *pIO);
188 #endif
190 /*
191 * ========================================
192 * Texas Instruments Micro Controller Style
193 * ========================================
194 * Local Variables:
195 * mode: c
196 * c-file-style: "bsd"
197 * tab-width: 4
198 * c-basic-offset: 4
199 * indent-tabs-mode: nil
200 * End:
201 * vim:set filetype=c tabstop=4 shiftwidth=4 expandtab=true
202 */