1 # accepts
3 [![NPM Version][npm-image]][npm-url]
4 [![NPM Downloads][downloads-image]][downloads-url]
5 [![Node.js Version][node-version-image]][node-version-url]
6 [![Build Status][travis-image]][travis-url]
7 [![Test Coverage][coveralls-image]][coveralls-url]
9 Higher level content negotiation based on [negotiator](https://www.npmjs.com/package/negotiator). Extracted from [koa](https://www.npmjs.com/package/koa) for general use.
11 In addition to negotiator, it allows:
13 - Allows types as an array or arguments list, ie `(['text/html', 'application/json'])` as well as `('text/html', 'application/json')`.
14 - Allows type shorthands such as `json`.
15 - Returns `false` when no types match
16 - Treats non-existent headers as `*`
18 ## Installation
20 ```sh
21 npm install accepts
22 ```
24 ## API
26 ```js
27 var accepts = require('accepts')
28 ```
30 ### accepts(req)
32 Create a new `Accepts` object for the given `req`.
34 #### .charset(charsets)
36 Return the first accepted charset. If nothing in `charsets` is accepted,
37 then `false` is returned.
39 #### .charsets()
41 Return the charsets that the request accepts, in the order of the client's
42 preference (most preferred first).
44 #### .encoding(encodings)
46 Return the first accepted encoding. If nothing in `encodings` is accepted,
47 then `false` is returned.
49 #### .encodings()
51 Return the encodings that the request accepts, in the order of the client's
52 preference (most preferred first).
54 #### .language(languages)
56 Return the first accepted language. If nothing in `languages` is accepted,
57 then `false` is returned.
59 #### .languages()
61 Return the languages that the request accepts, in the order of the client's
62 preference (most preferred first).
64 #### .type(types)
66 Return the first accepted type (and it is returned as the same text as what
67 appears in the `types` array). If nothing in `types` is accepted, then `false`
68 is returned.
70 The `types` array can contain full MIME types or file extensions. Any value
71 that is not a full MIME types is passed to `require('mime-types').lookup`.
73 #### .types()
75 Return the types that the request accepts, in the order of the client's
76 preference (most preferred first).
78 ## Examples
80 ### Simple type negotiation
82 This simple example shows how to use `accepts` to return a different typed
83 respond body based on what the client wants to accept. The server lists it's
84 preferences in order and will get back the best match between the client and
85 server.
87 ```js
88 var accepts = require('accepts')
89 var http = require('http')
91 function app(req, res) {
92 var accept = accepts(req)
94 // the order of this list is significant; should be server preferred order
95 switch(accept.type(['json', 'html'])) {
96 case 'json':
97 res.setHeader('Content-Type', 'application/json')
98 res.write('{"hello":"world!"}')
99 break
100 case 'html':
101 res.setHeader('Content-Type', 'text/html')
102 res.write('<b>hello, world!</b>')
103 break
104 default:
105 // the fallback is text/plain, so no need to specify it above
106 res.setHeader('Content-Type', 'text/plain')
107 res.write('hello, world!')
108 break
109 }
111 res.end()
112 }
114 http.createServer(app).listen(3000)
115 ```
117 You can test this out with the cURL program:
118 ```sh
119 curl -I -H'Accept: text/html' http://localhost:3000/
120 ```
122 ## License
124 [MIT](LICENSE)
126 [npm-image]: https://img.shields.io/npm/v/accepts.svg
127 [npm-url]: https://npmjs.org/package/accepts
128 [node-version-image]: https://img.shields.io/node/v/accepts.svg
129 [node-version-url]: http://nodejs.org/download/
130 [travis-image]: https://img.shields.io/travis/jshttp/accepts/master.svg
131 [travis-url]: https://travis-ci.org/jshttp/accepts
132 [coveralls-image]: https://img.shields.io/coveralls/jshttp/accepts/master.svg
133 [coveralls-url]: https://coveralls.io/r/jshttp/accepts
134 [downloads-image]: https://img.shields.io/npm/dm/accepts.svg
135 [downloads-url]: https://npmjs.org/package/accepts