]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - apps/tidep0084.git/blob - example/iot-gateway/node_modules/aws-iot-device-sdk/node_modules/mqtt/node_modules/mqtt-connection/CONTRIBUTING.md
Updated to use the latest TI 15.4-Stack v2.1.0 from the SimpleLink CC13x0 SDK v1.30.
[apps/tidep0084.git] / example / iot-gateway / node_modules / aws-iot-device-sdk / node_modules / mqtt / node_modules / mqtt-connection / CONTRIBUTING.md
1 # mqtt-packet is an OPEN Open Source Project
3 -----------------------------------------
5 ## What?
7 Individuals making significant and valuable contributions are given commit-access to the project to contribute as they see fit. This project is more like an open wiki than a standard guarded open source project.
9 ## Rules
11 There are a few basic ground-rules for contributors:
13 1. **No `--force` pushes** or modifying the Git history in any way.
14 1. **Non-master branches** ought to be used for ongoing work.
15 1. **External API changes and significant modifications** ought to be subject to an **internal pull-request** to solicit feedback from other contributors.
16 1. Internal pull-requests to solicit feedback are *encouraged* for any other non-trivial contribution but left to the discretion of the contributor.
17 1. Contributors should attempt to adhere to the prevailing code-style.
19 ## Releases
21 Declaring formal releases remains the prerogative of the project maintainer.
23 ## Changes to this arrangement
25 This is an experiment and feedback is welcome! This document may also be subject to pull-requests or changes by contributors where you believe you have something valuable to add or change.
27 -----------------------------------------