2 # Engine.IO client
4 [![Build Status](https://secure.travis-ci.org/socketio/engine.io-client.svg)](http://travis-ci.org/socketio/engine.io-client)
5 [![NPM version](https://badge.fury.io/js/engine.io-client.svg)](http://badge.fury.io/js/engine.io-client)
7 This is the client for [Engine.IO](http://github.com/socketio/engine.io),
8 the implementation of transport-based cross-browser/cross-device
9 bi-directional communication layer for [Socket.IO](http://github.com/socketio/socket.io).
11 ## How to use
13 ### Standalone
15 You can find an `engine.io.js` file in this repository, which is a
16 standalone build you can use as follows:
18 ```html
19 <script src="/path/to/engine.io.js"></script>
20 <script>
21 // eio = Socket
22 var socket = eio('ws://localhost');
23 socket.on('open', function(){
24 socket.on('message', function(data){});
25 socket.on('close', function(){});
26 });
27 </script>
28 ```
30 ### With browserify
32 Engine.IO is a commonjs module, which means you can include it by using
33 `require` on the browser and package using [browserify](http://browserify.org/):
35 1. install the client package
37 ```bash
38 $ npm install engine.io-client
39 ```
41 1. write your app code
43 ```js
44 var socket = require('engine.io-client')('ws://localhost');
45 socket.on('open', function(){
46 socket.on('message', function(data){});
47 socket.on('close', function(){});
48 });
49 ```
51 1. build your app bundle
53 ```bash
54 $ browserify app.js > bundle.js
55 ```
57 1. include on your page
59 ```html
60 <script src="/path/to/bundle.js"></script>
61 ```
63 ### Sending and receiving binary
65 ```html
66 <script src="/path/to/engine.io.js"></script>
67 <script>
68 var socket = new eio.Socket('ws://localhost/');
69 socket.binaryType = 'blob';
70 socket.on('open', function () {
71 socket.send(new Int8Array(5));
72 socket.on('message', function(blob){});
73 socket.on('close', function(){ });
74 });
75 </script>
76 ```
78 ### Node.JS
80 Add `engine.io-client` to your `package.json` and then:
82 ```js
83 var socket = require('engine.io-client')('ws://localhost');
84 socket.on('open', function(){
85 socket.on('message', function(data){});
86 socket.on('close', function(){});
87 });
88 ```
90 ### Node.js with certificates
91 ```js
92 var opts = {
93 key: fs.readFileSync('test/fixtures/client.key'),
94 cert: fs.readFileSync('test/fixtures/client.crt'),
95 ca: fs.readFileSync('test/fixtures/ca.crt')
96 };
98 var socket = require('engine.io-client')('ws://localhost', opts);
99 socket.on('open', function(){
100 socket.on('message', function(data){});
101 socket.on('close', function(){});
102 });
103 ```
105 ### Node.js with extraHeaders
106 ```js
107 var opts = {
108 extraHeaders: {
109 'X-Custom-Header-For-My-Project': 'my-secret-access-token',
110 'Cookie': 'user_session=NI2JlCKF90aE0sJZD9ZzujtdsUqNYSBYxzlTsvdSUe35ZzdtVRGqYFr0kdGxbfc5gUOkR9RGp20GVKza; path=/; expires=Tue, 07-Apr-2015 18:18:08 GMT; secure; HttpOnly'
111 }
112 };
114 var socket = require('engine.io-client')('ws://localhost', opts);
115 socket.on('open', function(){
116 socket.on('message', function(data){});
117 socket.on('close', function(){});
118 });
119 ```
121 ## Features
123 - Lightweight
124 - Runs on browser and node.js seamlessly
125 - Transports are independent of `Engine`
126 - Easy to debug
127 - Easy to unit test
128 - Runs inside HTML5 WebWorker
129 - Can send and receive binary data
130 - Receives as ArrayBuffer or Blob when in browser, and Buffer or ArrayBuffer
131 in Node
132 - When XHR2 or WebSockets are used, binary is emitted directly. Otherwise
133 binary is encoded into base64 strings, and decoded when binary types are
134 supported.
135 - With browsers that don't support ArrayBuffer, an object { base64: true,
136 data: dataAsBase64String } is emitted on the `message` event.
138 ## API
140 ### Socket
142 The client class. Mixes in [Emitter](http://github.com/component/emitter).
143 Exposed as `eio` in the browser standalone build.
145 #### Properties
147 - `protocol` _(Number)_: protocol revision number
148 - `binaryType` _(String)_ : can be set to 'arraybuffer' or 'blob' in browsers,
149 and `buffer` or `arraybuffer` in Node. Blob is only used in browser if it's
150 supported.
152 #### Events
154 - `open`
155 - Fired upon successful connection.
156 - `message`
157 - Fired when data is received from the server.
158 - **Arguments**
159 - `String` | `ArrayBuffer`: utf-8 encoded data or ArrayBuffer containing
160 binary data
161 - `close`
162 - Fired upon disconnection. In compliance with the WebSocket API spec, this event may be
163 fired even if the `open` event does not occur (i.e. due to connection error or `close()`).
164 - `error`
165 - Fired when an error occurs.
166 - `flush`
167 - Fired upon completing a buffer flush
168 - `drain`
169 - Fired after `drain` event of transport if writeBuffer is empty
170 - `upgradeError`
171 - Fired if an error occurs with a transport we're trying to upgrade to.
172 - `upgrade`
173 - Fired upon upgrade success, after the new transport is set
174 - `ping`
175 - Fired upon _flushing_ a ping packet (ie: actual packet write out)
176 - `pong`
177 - Fired upon receiving a pong packet.
179 #### Methods
181 - **constructor**
182 - Initializes the client
183 - **Parameters**
184 - `String` uri
185 - `Object`: optional, options object
186 - **Options**
187 - `agent` (`http.Agent`): `http.Agent` to use, defaults to `false` (NodeJS only)
188 - `upgrade` (`Boolean`): defaults to true, whether the client should try
189 to upgrade the transport from long-polling to something better.
190 - `forceJSONP` (`Boolean`): forces JSONP for polling transport.
191 - `jsonp` (`Boolean`): determines whether to use JSONP when
192 necessary for polling. If disabled (by settings to false) an error will
193 be emitted (saying "No transports available") if no other transports
194 are available. If another transport is available for opening a
195 connection (e.g. WebSocket) that transport
196 will be used instead.
197 - `forceBase64` (`Boolean`): forces base 64 encoding for polling transport even when XHR2 responseType is available and WebSocket even if the used standard supports binary.
198 - `enablesXDR` (`Boolean`): enables XDomainRequest for IE8 to avoid loading bar flashing with click sound. default to `false` because XDomainRequest has a flaw of not sending cookie.
199 - `timestampRequests` (`Boolean`): whether to add the timestamp with each
200 transport request. Note: polling requests are always stamped unless this
201 option is explicitly set to `false` (`false`)
202 - `timestampParam` (`String`): timestamp parameter (`t`)
203 - `policyPort` (`Number`): port the policy server listens on (`843`)
204 - `path` (`String`): path to connect to, default is `/engine.io`
205 - `transports` (`Array`): a list of transports to try (in order).
206 Defaults to `['polling', 'websocket']`. `Engine`
207 always attempts to connect directly with the first one, provided the
208 feature detection test for it passes.
209 - `rememberUpgrade` (`Boolean`): defaults to false.
210 If true and if the previous websocket connection to the server succeeded,
211 the connection attempt will bypass the normal upgrade process and will initially
212 try websocket. A connection attempt following a transport error will use the
213 normal upgrade process. It is recommended you turn this on only when using
214 SSL/TLS connections, or if you know that your network does not block websockets.
215 - `pfx` (`String`): Certificate, Private key and CA certificates to use for SSL. Can be used in Node.js client environment to manually specify certificate information.
216 - `key` (`String`): Private key to use for SSL. Can be used in Node.js client environment to manually specify certificate information.
217 - `passphrase` (`String`): A string of passphrase for the private key or pfx. Can be used in Node.js client environment to manually specify certificate information.
218 - `cert` (`String`): Public x509 certificate to use. Can be used in Node.js client environment to manually specify certificate information.
219 - `ca` (`String`|`Array`): An authority certificate or array of authority certificates to check the remote host against.. Can be used in Node.js client environment to manually specify certificate information.
220 - `ciphers` (`String`): A string describing the ciphers to use or exclude. Consult the [cipher format list](http://www.openssl.org/docs/apps/ciphers.html#CIPHER_LIST_FORMAT) for details on the format. Can be used in Node.js client environment to manually specify certificate information.
221 - `rejectUnauthorized` (`Boolean`): If true, the server certificate is verified against the list of supplied CAs. An 'error' event is emitted if verification fails. Verification happens at the connection level, before the HTTP request is sent. Can be used in Node.js client environment to manually specify certificate information.
222 - `perMessageDeflate` (`Object|Boolean`): parameters of the WebSocket permessage-deflate extension
223 (see [ws module](https://github.com/einaros/ws) api docs). Set to `false` to disable. (`true`)
224 - `threshold` (`Number`): data is compressed only if the byte size is above this value. This option is ignored on the browser. (`1024`)
225 - `extraHeaders` (`Object`): Headers that will be passed for each request to the server (via xhr-polling and via websockets). These values then can be used during handshake or for special proxies. Can only be used in Node.js client environment.
226 - `send`
227 - Sends a message to the server
228 - **Parameters**
229 - `String` | `ArrayBuffer` | `ArrayBufferView` | `Blob`: data to send
230 - `Object`: optional, options object
231 - `Function`: optional, callback upon `drain`
232 - **Options**
233 - `compress` (`Boolean`): whether to compress sending data. This option is ignored and forced to be `true` on the browser. (`true`)
234 - `close`
235 - Disconnects the client.
237 ### Transport
239 The transport class. Private. _Inherits from EventEmitter_.
241 #### Events
243 - `poll`: emitted by polling transports upon starting a new request
244 - `pollComplete`: emitted by polling transports upon completing a request
245 - `drain`: emitted by polling transports upon a buffer drain
247 ## Tests
249 `engine.io-client` is used to test
250 [engine](http://github.com/socketio/engine.io). Running the `engine.io`
251 test suite ensures the client works and vice-versa.
253 Browser tests are run using [zuul](https://github.com/defunctzombie/zuul). You can
254 run the tests locally using the following command.
256 ```
257 ./node_modules/.bin/zuul --local 8080 -- test/index.js
258 ```
260 Additionally, `engine.io-client` has a standalone test suite you can run
261 with `make test` which will run node.js and browser tests. You must have zuul setup with
262 a saucelabs account.
264 ## Support
266 The support channels for `engine.io-client` are the same as `socket.io`:
267 - irc.freenode.net **#socket.io**
268 - [Google Groups](http://groups.google.com/group/socket_io)
269 - [Website](http://socket.io)
271 ## Development
273 To contribute patches, run tests or benchmarks, make sure to clone the
274 repository:
276 ```bash
277 git clone git://github.com/socketio/engine.io-client.git
278 ```
280 Then:
282 ```bash
283 cd engine.io-client
284 npm install
285 ```
287 See the `Tests` section above for how to run tests before submitting any patches.
289 ## License
291 MIT - Copyright (c) 2014 Automattic, Inc.