1 # minimist
3 parse argument options
5 This module is the guts of optimist's argument parser without all the
6 fanciful decoration.
8 [![browser support](https://ci.testling.com/substack/minimist.png)](http://ci.testling.com/substack/minimist)
10 [![build status](https://secure.travis-ci.org/substack/minimist.png)](http://travis-ci.org/substack/minimist)
12 # example
14 ``` js
15 var argv = require('minimist')(process.argv.slice(2));
16 console.dir(argv);
17 ```
19 ```
20 $ node example/parse.js -a beep -b boop
21 { _: [], a: 'beep', b: 'boop' }
22 ```
24 ```
25 $ node example/parse.js -x 3 -y 4 -n5 -abc --beep=boop foo bar baz
26 { _: [ 'foo', 'bar', 'baz' ],
27 x: 3,
28 y: 4,
29 n: 5,
30 a: true,
31 b: true,
32 c: true,
33 beep: 'boop' }
34 ```
36 # methods
38 ``` js
39 var parseArgs = require('minimist')
40 ```
42 ## var argv = parseArgs(args, opts={})
44 Return an argument object `argv` populated with the array arguments from `args`.
46 `argv._` contains all the arguments that didn't have an option associated with
47 them.
49 Numeric-looking arguments will be returned as numbers unless `opts.string` or
50 `opts.boolean` is set for that argument name.
52 Any arguments after `'--'` will not be parsed and will end up in `argv._`.
54 options can be:
56 * `opts.string` - a string or array of strings argument names to always treat as
57 strings
58 * `opts.boolean` - a boolean, string or array of strings to always treat as
59 booleans. if `true` will treat all double hyphenated arguments without equal signs
60 as boolean (e.g. affects `--foo`, not `-f` or `--foo=bar`)
61 * `opts.alias` - an object mapping string names to strings or arrays of string
62 argument names to use as aliases
63 * `opts.default` - an object mapping string argument names to default values
64 * `opts.stopEarly` - when true, populate `argv._` with everything after the
65 first non-option
66 * `opts['--']` - when true, populate `argv._` with everything before the `--`
67 and `argv['--']` with everything after the `--`. Here's an example:
68 * `opts.unknown` - a function which is invoked with a command line parameter not
69 defined in the `opts` configuration object. If the function returns `false`, the
70 unknown option is not added to `argv`.
72 ```
73 > require('./')('one two three -- four five --six'.split(' '), { '--': true })
74 { _: [ 'one', 'two', 'three' ],
75 '--': [ 'four', 'five', '--six' ] }
76 ```
78 Note that with `opts['--']` set, parsing for arguments still stops after the
79 `--`.
81 # install
83 With [npm](https://npmjs.org) do:
85 ```
86 npm install minimist
87 ```
89 # license
91 MIT