diff --git a/example/ibm-frontend/public/dist/jquery/jqplot.barRenderer.js b/example/ibm-frontend/public/dist/jquery/jqplot.barRenderer.js
--- /dev/null
@@ -0,0 +1,801 @@
+/**
+ * jqPlot
+ * Pure JavaScript plotting plugin using jQuery
+ *
+ * Version: 1.0.9
+ * Revision: d96a669
+ *
+ * Copyright (c) 2009-2016 Chris Leonello
+ * jqPlot is currently available for use in all personal or commercial projects
+ * under both the MIT (http://www.opensource.org/licenses/mit-license.php) and GPL
+ * version 2.0 (http://www.gnu.org/licenses/gpl-2.0.html) licenses. This means that you can
+ * choose the license that best suits your project and use it accordingly.
+ *
+ * Although not required, the author would appreciate an email letting him
+ * know of any substantial use of jqPlot. You can reach the author at:
+ * chris at jqplot dot com or see http://www.jqplot.com/info.php .
+ *
+ * If you are feeling kind and generous, consider supporting the project by
+ * making a donation at: http://www.jqplot.com/donate.php .
+ *
+ * sprintf functions contained in jqplot.sprintf.js by Ash Searle:
+ *
+ * version 2007.04.27
+ * author Ash Searle
+ * http://hexmen.com/blog/2007/03/printf-sprintf/
+ * http://hexmen.com/js/sprintf.js
+ * The author (Ash Searle) has placed this code in the public domain:
+ * "This code is unrestricted: you are free to use it however you like."
+ *
+ */
+(function($) {
+
+ // Class: $.jqplot.BarRenderer
+ // A plugin renderer for jqPlot to draw a bar plot.
+ // Draws series as a line.
+
+ $.jqplot.BarRenderer = function(){
+ $.jqplot.LineRenderer.call(this);
+ };
+
+ $.jqplot.BarRenderer.prototype = new $.jqplot.LineRenderer();
+ $.jqplot.BarRenderer.prototype.constructor = $.jqplot.BarRenderer;
+
+ // called with scope of series.
+ $.jqplot.BarRenderer.prototype.init = function(options, plot) {
+ // Group: Properties
+ //
+ // prop: barPadding
+ // Number of pixels between adjacent bars at the same axis value.
+ this.barPadding = 8;
+ // prop: barMargin
+ // Number of pixels between groups of bars at adjacent axis values.
+ this.barMargin = 10;
+ // prop: barDirection
+ // 'vertical' = up and down bars, 'horizontal' = side to side bars
+ this.barDirection = 'vertical';
+ // prop: barWidth
+ // Width of the bar in pixels (auto by devaul). null = calculated automatically.
+ this.barWidth = null;
+ // prop: shadowOffset
+ // offset of the shadow from the slice and offset of
+ // each succesive stroke of the shadow from the last.
+ this.shadowOffset = 2;
+ // prop: shadowDepth
+ // number of strokes to apply to the shadow,
+ // each stroke offset shadowOffset from the last.
+ this.shadowDepth = 5;
+ // prop: shadowAlpha
+ // transparency of the shadow (0 = transparent, 1 = opaque)
+ this.shadowAlpha = 0.08;
+ // prop: waterfall
+ // true to enable waterfall plot.
+ this.waterfall = false;
+ // prop: groups
+ // group bars into this many groups
+ this.groups = 1;
+ // prop: varyBarColor
+ // true to color each bar of a series separately rather than
+ // have every bar of a given series the same color.
+ // If used for non-stacked multiple series bar plots, user should
+ // specify a separate 'seriesColors' array for each series.
+ // Otherwise, each series will set their bars to the same color array.
+ // This option has no Effect for stacked bar charts and is disabled.
+ this.varyBarColor = false;
+ // prop: highlightMouseOver
+ // True to highlight slice when moused over.
+ // This must be false to enable highlightMouseDown to highlight when clicking on a slice.
+ this.highlightMouseOver = true;
+ // prop: highlightMouseDown
+ // True to highlight when a mouse button is pressed over a slice.
+ // This will be disabled if highlightMouseOver is true.
+ this.highlightMouseDown = false;
+ // prop: highlightColors
+ // an array of colors to use when highlighting a bar.
+ this.highlightColors = [];
+ // prop: transposedData
+ // NOT IMPLEMENTED YET. True if this is a horizontal bar plot and
+ // x and y values are "transposed". Tranposed, or "swapped", data is
+ // required prior to rev. 894 builds of jqPlot with horizontal bars.
+ // Allows backward compatability of bar renderer horizontal bars with
+ // old style data sets.
+ this.transposedData = true;
+ this.renderer.animation = {
+ show: false,
+ direction: 'down',
+ speed: 3000,
+ _supported: true
+ };
+ this._type = 'bar';
+
+ // if user has passed in highlightMouseDown option and not set highlightMouseOver, disable highlightMouseOver
+ if (options.highlightMouseDown && options.highlightMouseOver == null) {
+ options.highlightMouseOver = false;
+ }
+
+ //////
+ // This is probably wrong here.
+ // After going back and forth on whether renderer should be the thing
+ // or extend the thing, it seems that it it best if it is a property
+ // on the thing. This should be something that is commonized
+ // among series renderers in the future.
+ //////
+ $.extend(true, this, options);
+
+ // really should probably do this
+ $.extend(true, this.renderer, options);
+ // fill is still needed to properly draw the legend.
+ // bars have to be filled.
+ this.fill = true;
+
+ // if horizontal bar and animating, reset the default direction
+ if (this.barDirection === 'horizontal' && this.rendererOptions.animation && this.rendererOptions.animation.direction == null) {
+ this.renderer.animation.direction = 'left';
+ }
+
+ if (this.waterfall) {
+ this.fillToZero = false;
+ this.disableStack = true;
+ }
+
+ if (this.barDirection == 'vertical' ) {
+ this._primaryAxis = '_xaxis';
+ this._stackAxis = 'y';
+ this.fillAxis = 'y';
+ }
+ else {
+ this._primaryAxis = '_yaxis';
+ this._stackAxis = 'x';
+ this.fillAxis = 'x';
+ }
+ // index of the currenty highlighted point, if any
+ this._highlightedPoint = null;
+ // total number of values for all bar series, total number of bar series, and position of this series
+ this._plotSeriesInfo = null;
+ // Array of actual data colors used for each data point.
+ this._dataColors = [];
+ this._barPoints = [];
+
+ // set the shape renderer options
+ var opts = {lineJoin:'miter', lineCap:'round', fill:true, isarc:false, strokeStyle:this.color, fillStyle:this.color, closePath:this.fill};
+ this.renderer.shapeRenderer.init(opts);
+ // set the shadow renderer options
+ var sopts = {lineJoin:'miter', lineCap:'round', fill:true, isarc:false, angle:this.shadowAngle, offset:this.shadowOffset, alpha:this.shadowAlpha, depth:this.shadowDepth, closePath:this.fill};
+ this.renderer.shadowRenderer.init(sopts);
+
+ plot.postInitHooks.addOnce(postInit);
+ plot.postDrawHooks.addOnce(postPlotDraw);
+ plot.eventListenerHooks.addOnce('jqplotMouseMove', handleMove);
+ plot.eventListenerHooks.addOnce('jqplotMouseDown', handleMouseDown);
+ plot.eventListenerHooks.addOnce('jqplotMouseUp', handleMouseUp);
+ plot.eventListenerHooks.addOnce('jqplotClick', handleClick);
+ plot.eventListenerHooks.addOnce('jqplotRightClick', handleRightClick);
+ };
+
+ // called with scope of series
+ function barPreInit(target, data, seriesDefaults, options) {
+ if (this.rendererOptions.barDirection == 'horizontal') {
+ this._stackAxis = 'x';
+ this._primaryAxis = '_yaxis';
+ }
+ if (this.rendererOptions.waterfall == true) {
+ this._data = $.extend(true, [], this.data);
+ var sum = 0;
+ var pos = (!this.rendererOptions.barDirection || this.rendererOptions.barDirection === 'vertical' || this.transposedData === false) ? 1 : 0;
+ for(var i=0; i<this.data.length; i++) {
+ sum += this.data[i][pos];
+ if (i>0) {
+ this.data[i][pos] += this.data[i-1][pos];
+ }
+ }
+ this.data[this.data.length] = (pos == 1) ? [this.data.length+1, sum] : [sum, this.data.length+1];
+ this._data[this._data.length] = (pos == 1) ? [this._data.length+1, sum] : [sum, this._data.length+1];
+ }
+ if (this.rendererOptions.groups > 1) {
+ this.breakOnNull = true;
+ var l = this.data.length;
+ var skip = parseInt(l/this.rendererOptions.groups, 10);
+ var count = 0;
+ for (var i=skip; i<l; i+=skip) {
+ this.data.splice(i+count, 0, [null, null]);
+ this._plotData.splice(i+count, 0, [null, null]);
+ this._stackData.splice(i+count, 0, [null, null]);
+ count++;
+ }
+ for (i=0; i<this.data.length; i++) {
+ if (this._primaryAxis == '_xaxis') {
+ this.data[i][0] = i+1;
+ this._plotData[i][0] = i+1;
+ this._stackData[i][0] = i+1;
+ }
+ else {
+ this.data[i][1] = i+1;
+ this._plotData[i][1] = i+1;
+ this._stackData[i][1] = i+1;
+ }
+ }
+ }
+ }
+
+ $.jqplot.preSeriesInitHooks.push(barPreInit);
+
+ // needs to be called with scope of series, not renderer.
+ $.jqplot.BarRenderer.prototype.calcSeriesNumbers = function() {
+ var nvals = 0;
+ var nseries = 0;
+ var paxis = this[this._primaryAxis];
+ var s, series, pos;
+ // loop through all series on this axis
+ for (var i=0; i < paxis._series.length; i++) {
+ series = paxis._series[i];
+ if (series === this) {
+ pos = i;
+ }
+ // is the series rendered as a bar?
+ if (series.renderer.constructor == $.jqplot.BarRenderer) {
+ // gridData may not be computed yet, use data length insted
+ nvals += series.data.length;
+ nseries += 1;
+ }
+ }
+ // return total number of values for all bar series, total number of bar series, and position of this series
+ return [nvals, nseries, pos];
+ };
+
+ $.jqplot.BarRenderer.prototype.setBarWidth = function() {
+ // need to know how many data values we have on the approprate axis and figure it out.
+ var i;
+ var nvals = 0;
+ var nseries = 0;
+ var paxis = this[this._primaryAxis];
+ var s, series, pos;
+ var temp = this._plotSeriesInfo = this.renderer.calcSeriesNumbers.call(this);
+ nvals = temp[0];
+ nseries = temp[1];
+ var nticks = paxis.numberTicks;
+ var nbins = (nticks-1)/2;
+ // so, now we have total number of axis values.
+ if (paxis.name == 'xaxis' || paxis.name == 'x2axis') {
+ if (this._stack) {
+ this.barWidth = (paxis._offsets.max - paxis._offsets.min) / nvals * nseries - this.barMargin;
+ }
+ else {
+ this.barWidth = ((paxis._offsets.max - paxis._offsets.min)/nbins - this.barPadding * (nseries-1) - this.barMargin*2)/nseries;
+ // this.barWidth = (paxis._offsets.max - paxis._offsets.min) / nvals - this.barPadding - this.barMargin/nseries;
+ }
+ }
+ else {
+ if (this._stack) {
+ this.barWidth = (paxis._offsets.min - paxis._offsets.max) / nvals * nseries - this.barMargin;
+ }
+ else {
+ this.barWidth = ((paxis._offsets.min - paxis._offsets.max)/nbins - this.barPadding * (nseries-1) - this.barMargin*2)/nseries;
+ // this.barWidth = (paxis._offsets.min - paxis._offsets.max) / nvals - this.barPadding - this.barMargin/nseries;
+ }
+ }
+ return [nvals, nseries];
+ };
+
+ function computeHighlightColors (colors) {
+ var ret = [];
+ for (var i=0; i<colors.length; i++){
+ var rgba = $.jqplot.getColorComponents(colors[i]);
+ var newrgb = [rgba[0], rgba[1], rgba[2]];
+ var sum = newrgb[0] + newrgb[1] + newrgb[2];
+ for (var j=0; j<3; j++) {
+ // when darkening, lowest color component can be is 60.
+ newrgb[j] = (sum > 570) ? newrgb[j] * 0.8 : newrgb[j] + 0.3 * (255 - newrgb[j]);
+ newrgb[j] = parseInt(newrgb[j], 10);
+ }
+ ret.push('rgb('+newrgb[0]+','+newrgb[1]+','+newrgb[2]+')');
+ }
+ return ret;
+ }
+
+ function getStart(sidx, didx, comp, plot, axis) {
+ // check if sign change
+ var seriesIndex = sidx,
+ prevSeriesIndex = sidx - 1,
+ start,
+ prevVal,
+ aidx = (axis === 'x') ? 0 : 1;
+
+ // is this not the first series?
+ if (seriesIndex > 0) {
+ prevVal = plot.series[prevSeriesIndex]._plotData[didx][aidx];
+
+ // is there a sign change
+ if ((comp * prevVal) < 0) {
+ start = getStart(prevSeriesIndex, didx, comp, plot, axis);
+ }
+
+ // no sign change.
+ else {
+ start = plot.series[prevSeriesIndex].gridData[didx][aidx];
+ }
+
+ }
+
+ // if first series, return value at 0
+ else {
+
+ start = (aidx === 0) ? plot.series[seriesIndex]._xaxis.series_u2p(0) : plot.series[seriesIndex]._yaxis.series_u2p(0);
+ }
+
+ return start;
+ }
+
+
+ $.jqplot.BarRenderer.prototype.draw = function(ctx, gridData, options, plot) {
+ var i;
+ // Ughhh, have to make a copy of options b/c it may be modified later.
+ var opts = $.extend({}, options);
+ var shadow = (opts.shadow != undefined) ? opts.shadow : this.shadow;
+ var showLine = (opts.showLine != undefined) ? opts.showLine : this.showLine;
+ var fill = (opts.fill != undefined) ? opts.fill : this.fill;
+ var xaxis = this.xaxis;
+ var yaxis = this.yaxis;
+ var xp = this._xaxis.series_u2p;
+ var yp = this._yaxis.series_u2p;
+ var pointx, pointy;
+ // clear out data colors.
+ this._dataColors = [];
+ this._barPoints = [];
+
+ if (this.barWidth == null || this.rendererOptions.barWidth == null) {//check pull request https://bitbucket.org/cleonello/jqplot/pull-request/61/fix-for-issue-513/diff
+ this.renderer.setBarWidth.call(this);
+ }
+
+ var temp = this._plotSeriesInfo = this.renderer.calcSeriesNumbers.call(this);
+ var nvals = temp[0];
+ var nseries = temp[1];
+ var pos = temp[2];
+ var points = [];
+
+ if (this._stack) {
+ this._barNudge = 0;
+ }
+ else {
+ this._barNudge = (-Math.abs(nseries/2 - 0.5) + pos) * (this.barWidth + this.barPadding);
+ }
+ if (showLine) {
+ var negativeColors = new $.jqplot.ColorGenerator(this.negativeSeriesColors);
+ var positiveColors = new $.jqplot.ColorGenerator(this.seriesColors);
+ var negativeColor = negativeColors.get(this.index);
+ if (! this.useNegativeColors) {
+ negativeColor = opts.fillStyle;
+ }
+ var positiveColor = opts.fillStyle;
+ var base;
+ var xstart;
+ var ystart;
+
+ if (this.barDirection == 'vertical') {
+ for (var i=0; i<gridData.length; i++) {
+ if (!this._stack && this.data[i][1] == null) {
+ continue;
+ }
+ points = [];
+ base = gridData[i][0] + this._barNudge;
+
+ // stacked
+ if (this._stack && this._prevGridData.length) {
+ ystart = getStart(this.index, i, this._plotData[i][1], plot, 'y');
+ }
+
+ // not stacked
+ else {
+ if (this.fillToZero) {
+ ystart = this._yaxis.series_u2p(0);
+ }
+ else if (this.waterfall && i > 0 && i < this.gridData.length-1) {
+ ystart = this.gridData[i-1][1];
+ }
+ else if (this.waterfall && i == 0 && i < this.gridData.length-1) {
+ if (this._yaxis.min <= 0 && this._yaxis.max >= 0) {
+ ystart = this._yaxis.series_u2p(0);
+ }
+ else if (this._yaxis.min > 0) {
+ ystart = ctx.canvas.height;
+ }
+ else {
+ ystart = 0;
+ }
+ }
+ else if (this.waterfall && i == this.gridData.length - 1) {
+ if (this._yaxis.min <= 0 && this._yaxis.max >= 0) {
+ ystart = this._yaxis.series_u2p(0);
+ }
+ else if (this._yaxis.min > 0) {
+ ystart = ctx.canvas.height;
+ }
+ else {
+ ystart = 0;
+ }
+ }
+ else {
+ ystart = ctx.canvas.height;
+ }
+ }
+ if ((this.fillToZero && this._plotData[i][1] < 0) || (this.waterfall && this._data[i][1] < 0)) {
+ if (this.varyBarColor && !this._stack) {
+ if (this.useNegativeColors) {
+ opts.fillStyle = negativeColors.next();
+ }
+ else {
+ opts.fillStyle = positiveColors.next();
+ }
+ }
+ else {
+ opts.fillStyle = negativeColor;
+ }
+ }
+ else {
+ if (this.varyBarColor && !this._stack) {
+ opts.fillStyle = positiveColors.next();
+ }
+ else {
+ opts.fillStyle = positiveColor;
+ }
+ }
+
+ if (!this.fillToZero || this._plotData[i][1] >= 0) {
+ points.push([base-this.barWidth/2, ystart]);
+ points.push([base-this.barWidth/2, gridData[i][1]]);
+ points.push([base+this.barWidth/2, gridData[i][1]]);
+ points.push([base+this.barWidth/2, ystart]);
+ }
+ // for negative bars make sure points are always ordered clockwise
+ else {
+ points.push([base-this.barWidth/2, gridData[i][1]]);
+ points.push([base-this.barWidth/2, ystart]);
+ points.push([base+this.barWidth/2, ystart]);
+ points.push([base+this.barWidth/2, gridData[i][1]]);
+ }
+ this._barPoints.push(points);
+ // now draw the shadows if not stacked.
+ // for stacked plots, they are predrawn by drawShadow
+ if (shadow && !this._stack) {
+ var sopts = $.extend(true, {}, opts);
+ // need to get rid of fillStyle on shadow.
+ delete sopts.fillStyle;
+ this.renderer.shadowRenderer.draw(ctx, points, sopts);
+ }
+ var clr = opts.fillStyle || this.color;
+ this._dataColors.push(clr);
+ this.renderer.shapeRenderer.draw(ctx, points, opts);
+ }
+ }
+
+ else if (this.barDirection == 'horizontal'){
+ for (var i=0; i<gridData.length; i++) {
+ if (!this._stack && this.data[i][0] == null) {
+ continue;
+ }
+ points = [];
+ base = gridData[i][1] - this._barNudge;
+ xstart;
+
+ if (this._stack && this._prevGridData.length) {
+ xstart = getStart(this.index, i, this._plotData[i][0], plot, 'x');
+ }
+ // not stacked
+ else {
+ if (this.fillToZero) {
+ xstart = this._xaxis.series_u2p(0);
+ }
+ else if (this.waterfall && i > 0 && i < this.gridData.length-1) {
+ xstart = this.gridData[i-1][0];
+ }
+ else if (this.waterfall && i == 0 && i < this.gridData.length-1) {
+ if (this._xaxis.min <= 0 && this._xaxis.max >= 0) {
+ xstart = this._xaxis.series_u2p(0);
+ }
+ else if (this._xaxis.min > 0) {
+ xstart = 0;
+ }
+ else {
+ xstart = 0;
+ }
+ }
+ else if (this.waterfall && i == this.gridData.length - 1) {
+ if (this._xaxis.min <= 0 && this._xaxis.max >= 0) {
+ xstart = this._xaxis.series_u2p(0);
+ }
+ else if (this._xaxis.min > 0) {
+ xstart = 0;
+ }
+ else {
+ xstart = ctx.canvas.width;
+ }
+ }
+ else {
+ xstart = 0;
+ }
+ }
+ if ((this.fillToZero && this._plotData[i][0] < 0) || (this.waterfall && this._data[i][0] < 0)) {
+ if (this.varyBarColor && !this._stack) {
+ if (this.useNegativeColors) {
+ opts.fillStyle = negativeColors.next();
+ }
+ else {
+ opts.fillStyle = positiveColors.next();
+ }
+ }
+ else {
+ opts.fillStyle = negativeColor;
+ }
+ }
+ else {
+ if (this.varyBarColor && !this._stack) {
+ opts.fillStyle = positiveColors.next();
+ }
+ else {
+ opts.fillStyle = positiveColor;
+ }
+ }
+
+
+ if (!this.fillToZero || this._plotData[i][0] >= 0) {
+ points.push([xstart, base + this.barWidth / 2]);
+ points.push([xstart, base - this.barWidth / 2]);
+ points.push([gridData[i][0], base - this.barWidth / 2]);
+ points.push([gridData[i][0], base + this.barWidth / 2]);
+ }
+ else {
+ points.push([gridData[i][0], base + this.barWidth / 2]);
+ points.push([gridData[i][0], base - this.barWidth / 2]);
+ points.push([xstart, base - this.barWidth / 2]);
+ points.push([xstart, base + this.barWidth / 2]);
+ }
+
+ this._barPoints.push(points);
+ // now draw the shadows if not stacked.
+ // for stacked plots, they are predrawn by drawShadow
+ if (shadow && !this._stack) {
+ var sopts = $.extend(true, {}, opts);
+ delete sopts.fillStyle;
+ this.renderer.shadowRenderer.draw(ctx, points, sopts);
+ }
+ var clr = opts.fillStyle || this.color;
+ this._dataColors.push(clr);
+ this.renderer.shapeRenderer.draw(ctx, points, opts);
+ }
+ }
+ }
+
+ if (this.highlightColors.length == 0) {
+ this.highlightColors = $.jqplot.computeHighlightColors(this._dataColors);
+ }
+
+ else if (typeof(this.highlightColors) == 'string') {
+ var temp = this.highlightColors;
+ this.highlightColors = [];
+ for (var i=0; i<this._dataColors.length; i++) {
+ this.highlightColors.push(temp);
+ }
+ }
+
+ };
+
+
+ // for stacked plots, shadows will be pre drawn by drawShadow.
+ $.jqplot.BarRenderer.prototype.drawShadow = function(ctx, gridData, options, plot) {
+ var i;
+ var opts = (options != undefined) ? options : {};
+ var shadow = (opts.shadow != undefined) ? opts.shadow : this.shadow;
+ var showLine = (opts.showLine != undefined) ? opts.showLine : this.showLine;
+ var fill = (opts.fill != undefined) ? opts.fill : this.fill;
+ var xaxis = this.xaxis;
+ var yaxis = this.yaxis;
+ var xp = this._xaxis.series_u2p;
+ var yp = this._yaxis.series_u2p;
+ var pointx, points, pointy, nvals, nseries, pos;
+
+ if (this._stack && this.shadow) {
+ if (this.barWidth == null) {
+ this.renderer.setBarWidth.call(this);
+ }
+
+ var temp = this._plotSeriesInfo = this.renderer.calcSeriesNumbers.call(this);
+ nvals = temp[0];
+ nseries = temp[1];
+ pos = temp[2];
+
+ if (this._stack) {
+ this._barNudge = 0;
+ }
+ else {
+ this._barNudge = (-Math.abs(nseries/2 - 0.5) + pos) * (this.barWidth + this.barPadding);
+ }
+ if (showLine) {
+
+ if (this.barDirection == 'vertical') {
+ for (var i=0; i<gridData.length; i++) {
+ if (this.data[i][1] == null) {
+ continue;
+ }
+ points = [];
+ var base = gridData[i][0] + this._barNudge;
+ var ystart;
+
+ if (this._stack && this._prevGridData.length) {
+ ystart = getStart(this.index, i, this._plotData[i][1], plot, 'y');
+ }
+ else {
+ if (this.fillToZero) {
+ ystart = this._yaxis.series_u2p(0);
+ }
+ else {
+ ystart = ctx.canvas.height;
+ }
+ }
+
+ points.push([base-this.barWidth/2, ystart]);
+ points.push([base-this.barWidth/2, gridData[i][1]]);
+ points.push([base+this.barWidth/2, gridData[i][1]]);
+ points.push([base+this.barWidth/2, ystart]);
+ this.renderer.shadowRenderer.draw(ctx, points, opts);
+ }
+ }
+
+ else if (this.barDirection == 'horizontal'){
+ for (var i=0; i<gridData.length; i++) {
+ if (this.data[i][0] == null) {
+ continue;
+ }
+ points = [];
+ var base = gridData[i][1] - this._barNudge;
+ var xstart;
+
+ if (this._stack && this._prevGridData.length) {
+ xstart = getStart(this.index, i, this._plotData[i][0], plot, 'x');
+ }
+ else {
+ if (this.fillToZero) {
+ xstart = this._xaxis.series_u2p(0);
+ }
+ else {
+ xstart = 0;
+ }
+ }
+
+ points.push([xstart, base+this.barWidth/2]);
+ points.push([gridData[i][0], base+this.barWidth/2]);
+ points.push([gridData[i][0], base-this.barWidth/2]);
+ points.push([xstart, base-this.barWidth/2]);
+ this.renderer.shadowRenderer.draw(ctx, points, opts);
+ }
+ }
+ }
+
+ }
+ };
+
+ function postInit(target, data, options) {
+ for (var i=0; i<this.series.length; i++) {
+ if (this.series[i].renderer.constructor == $.jqplot.BarRenderer) {
+ // don't allow mouseover and mousedown at same time.
+ if (this.series[i].highlightMouseOver) {
+ this.series[i].highlightMouseDown = false;
+ }
+ }
+ }
+ }
+
+ // called within context of plot
+ // create a canvas which we can draw on.
+ // insert it before the eventCanvas, so eventCanvas will still capture events.
+ function postPlotDraw() {
+ // Memory Leaks patch
+ if (this.plugins.barRenderer && this.plugins.barRenderer.highlightCanvas) {
+
+ this.plugins.barRenderer.highlightCanvas.resetCanvas();
+ this.plugins.barRenderer.highlightCanvas = null;
+ }
+
+ this.plugins.barRenderer = {highlightedSeriesIndex:null};
+ this.plugins.barRenderer.highlightCanvas = new $.jqplot.GenericCanvas();
+
+ this.eventCanvas._elem.before(this.plugins.barRenderer.highlightCanvas.createElement(this._gridPadding, 'jqplot-barRenderer-highlight-canvas', this._plotDimensions, this));
+ this.plugins.barRenderer.highlightCanvas.setContext();
+ this.eventCanvas._elem.bind('mouseleave', {plot:this}, function (ev) { unhighlight(ev.data.plot); });
+ }
+
+ function highlight (plot, sidx, pidx, points) {
+ var s = plot.series[sidx];
+ var canvas = plot.plugins.barRenderer.highlightCanvas;
+ canvas._ctx.clearRect(0,0,canvas._ctx.canvas.width, canvas._ctx.canvas.height);
+ s._highlightedPoint = pidx;
+ plot.plugins.barRenderer.highlightedSeriesIndex = sidx;
+ var opts = {fillStyle: s.highlightColors[pidx]};
+ s.renderer.shapeRenderer.draw(canvas._ctx, points, opts);
+ canvas = null;
+ }
+
+ function unhighlight (plot) {
+ var canvas = plot.plugins.barRenderer.highlightCanvas;
+ canvas._ctx.clearRect(0,0, canvas._ctx.canvas.width, canvas._ctx.canvas.height);
+ for (var i=0; i<plot.series.length; i++) {
+ plot.series[i]._highlightedPoint = null;
+ }
+ plot.plugins.barRenderer.highlightedSeriesIndex = null;
+ plot.target.trigger('jqplotDataUnhighlight');
+ canvas = null;
+ }
+
+
+ function handleMove(ev, gridpos, datapos, neighbor, plot) {
+ if (neighbor) {
+ var ins = [neighbor.seriesIndex, neighbor.pointIndex, neighbor.data];
+ var evt1 = jQuery.Event('jqplotDataMouseOver');
+ evt1.pageX = ev.pageX;
+ evt1.pageY = ev.pageY;
+ plot.target.trigger(evt1, ins);
+ if (plot.series[ins[0]].show && plot.series[ins[0]].highlightMouseOver &&
+ !(ins[0] == plot.plugins.barRenderer.highlightedSeriesIndex && ins[1] == plot.series[ins[0]]._highlightedPoint)) {
+ var evt = jQuery.Event('jqplotDataHighlight');
+ evt.which = ev.which;
+ evt.pageX = ev.pageX;
+ evt.pageY = ev.pageY;
+ plot.target.trigger(evt, ins);
+ highlight (plot, neighbor.seriesIndex, neighbor.pointIndex, neighbor.points);
+ }
+ }
+ else if (neighbor == null) {
+ unhighlight (plot);
+ }
+ }
+
+ function handleMouseDown(ev, gridpos, datapos, neighbor, plot) {
+ if (neighbor) {
+ var ins = [neighbor.seriesIndex, neighbor.pointIndex, neighbor.data];
+ if (plot.series[ins[0]].highlightMouseDown && !(ins[0] == plot.plugins.barRenderer.highlightedSeriesIndex && ins[1] == plot.series[ins[0]]._highlightedPoint)) {
+ var evt = jQuery.Event('jqplotDataHighlight');
+ evt.which = ev.which;
+ evt.pageX = ev.pageX;
+ evt.pageY = ev.pageY;
+ plot.target.trigger(evt, ins);
+ highlight (plot, neighbor.seriesIndex, neighbor.pointIndex, neighbor.points);
+ }
+ }
+ else if (neighbor == null) {
+ unhighlight (plot);
+ }
+ }
+
+ function handleMouseUp(ev, gridpos, datapos, neighbor, plot) {
+ var idx = plot.plugins.barRenderer.highlightedSeriesIndex;
+ if (idx != null && plot.series[idx].highlightMouseDown) {
+ unhighlight(plot);
+ }
+ }
+
+ function handleClick(ev, gridpos, datapos, neighbor, plot) {
+ if (neighbor) {
+ var ins = [neighbor.seriesIndex, neighbor.pointIndex, neighbor.data];
+ var evt = jQuery.Event('jqplotDataClick');
+ evt.which = ev.which;
+ evt.pageX = ev.pageX;
+ evt.pageY = ev.pageY;
+ plot.target.trigger(evt, ins);
+ }
+ }
+
+ function handleRightClick(ev, gridpos, datapos, neighbor, plot) {
+ if (neighbor) {
+ var ins = [neighbor.seriesIndex, neighbor.pointIndex, neighbor.data];
+ var idx = plot.plugins.barRenderer.highlightedSeriesIndex;
+ if (idx != null && plot.series[idx].highlightMouseDown) {
+ unhighlight(plot);
+ }
+ var evt = jQuery.Event('jqplotDataRightClick');
+ evt.which = ev.which;
+ evt.pageX = ev.pageX;
+ evt.pageY = ev.pageY;
+ plot.target.trigger(evt, ins);
+ }
+ }
+
+
+})(jQuery);