]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - apps/tidep0084.git/blobdiff - example/iot-gateway/node_modules/bytebuffer/src/types/floats/float32.js
Updated Sensor To Cloud design to have an easy to use setup GUI on the
[apps/tidep0084.git] / example / iot-gateway / node_modules / bytebuffer / src / types / floats / float32.js
diff --git a/example/iot-gateway/node_modules/bytebuffer/src/types/floats/float32.js b/example/iot-gateway/node_modules/bytebuffer/src/types/floats/float32.js
deleted file mode 100644 (file)
index ab5f4a7..0000000
+++ /dev/null
@@ -1,81 +0,0 @@
-//? if (FLOAT32) {
-// types/floats/float32
-//? if (!NODE && !DATAVIEW) {
-
-//? include("ieee754.js");
-//? }
-
-/**
- * Writes a 32bit float.
- * @param {number} value Value to write
- * @param {number=} offset Offset to write to. Will use and increase {@link ByteBuffer#offset} by `4` if omitted.
- * @returns {!ByteBuffer} this
- * @expose
- */
-ByteBufferPrototype.writeFloat32 = function(value, offset) {
-    //? RELATIVE();
-    if (!this.noAssert) {
-        if (typeof value !== 'number')
-            throw TypeError("Illegal value: "+value+" (not a number)");
-        //? ASSERT_OFFSET();
-    }
-    //? ENSURE_CAPACITY(4);
-    //? if (NODE) { // FIXME: Is there any way to inline the following in a sane way?
-    this.littleEndian
-        ? this.buffer.writeFloatLE(value, offset, true)
-        : this.buffer.writeFloatBE(value, offset, true);
-    //? } else if (DATAVIEW)
-    this.view.setFloat32(offset, value, this.littleEndian);
-    //? else
-    ieee754_write(this.view, value, offset, this.littleEndian, 23, 4);
-    //? RELATIVE(4);
-    return this;
-};
-//? if (ALIASES) {
-
-/**
- * Writes a 32bit float. This is an alias of {@link ByteBuffer#writeFloat32}.
- * @function
- * @param {number} value Value to write
- * @param {number=} offset Offset to write to. Will use and increase {@link ByteBuffer#offset} by `4` if omitted.
- * @returns {!ByteBuffer} this
- * @expose
- */
-ByteBufferPrototype.writeFloat = ByteBufferPrototype.writeFloat32;
-//? }
-
-/**
- * Reads a 32bit float.
- * @param {number=} offset Offset to read from. Will use and increase {@link ByteBuffer#offset} by `4` if omitted.
- * @returns {number}
- * @expose
- */
-ByteBufferPrototype.readFloat32 = function(offset) {
-    //? RELATIVE();
-    if (!this.noAssert) {
-        //? ASSERT_OFFSET(4);
-    }
-    //? if (NODE) {
-    var value = this.littleEndian
-        ? this.buffer.readFloatLE(offset, true)
-        : this.buffer.readFloatBE(offset, true);
-    //? } else if (DATAVIEW)
-    var value = this.view.getFloat32(offset, this.littleEndian);
-    //? else
-    var value = ieee754_read(this.view, offset, this.littleEndian, 23, 4);
-    //? RELATIVE(4);
-    return value;
-};
-//? if (ALIASES) {
-
-/**
- * Reads a 32bit float. This is an alias of {@link ByteBuffer#readFloat32}.
- * @function
- * @param {number=} offset Offset to read from. Will use and increase {@link ByteBuffer#offset} by `4` if omitted.
- * @returns {number}
- * @expose
- */
-ByteBufferPrototype.readFloat = ByteBufferPrototype.readFloat32;
-//? }
-
-//? }
\ No newline at end of file