diff --git a/prebuilt/iot-gateway/node_modules/mime-db/README.md b/prebuilt/iot-gateway/node_modules/mime-db/README.md
+++ /dev/null
@@ -1,82 +0,0 @@
-# mime-db
-
-[![NPM Version][npm-version-image]][npm-url]
-[![NPM Downloads][npm-downloads-image]][npm-url]
-[![Node.js Version][node-image]][node-url]
-[![Build Status][travis-image]][travis-url]
-[![Coverage Status][coveralls-image]][coveralls-url]
-
-This is a database of all mime types.
-It consists of a single, public JSON file and does not include any logic,
-allowing it to remain as un-opinionated as possible with an API.
-It aggregates data from the following sources:
-
-- http://www.iana.org/assignments/media-types/media-types.xhtml
-- http://svn.apache.org/repos/asf/httpd/httpd/trunk/docs/conf/mime.types
-- http://hg.nginx.org/nginx/raw-file/default/conf/mime.types
-
-## Installation
-
-```bash
-npm install mime-db
-```
-
-### Database Download
-
-If you're crazy enough to use this in the browser, you can just grab the
-JSON file using [RawGit](https://rawgit.com/). It is recommended to replace
-`master` with [a release tag](https://github.com/jshttp/mime-db/tags) as the
-JSON format may change in the future.
-
-```
-https://cdn.rawgit.com/jshttp/mime-db/master/db.json
-```
-
-## Usage
-
-```js
-var db = require('mime-db');
-
-// grab data on .js files
-var data = db['application/javascript'];
-```
-
-## Data Structure
-
-The JSON file is a map lookup for lowercased mime types.
-Each mime type has the following properties:
-
-- `.source` - where the mime type is defined.
- If not set, it's probably a custom media type.
- - `apache` - [Apache common media types](http://svn.apache.org/repos/asf/httpd/httpd/trunk/docs/conf/mime.types)
- - `iana` - [IANA-defined media types](http://www.iana.org/assignments/media-types/media-types.xhtml)
- - `nginx` - [nginx media types](http://hg.nginx.org/nginx/raw-file/default/conf/mime.types)
-- `.extensions[]` - known extensions associated with this mime type.
-- `.compressible` - whether a file of this type can be gzipped.
-- `.charset` - the default charset associated with this type, if any.
-
-If unknown, every property could be `undefined`.
-
-## Contributing
-
-To edit the database, only make PRs against `src/custom.json` or
-`src/custom-suffix.json`.
-
-To update the build, run `npm run build`.
-
-## Adding Custom Media Types
-
-The best way to get new media types included in this library is to register
-them with the IANA. The community registration procedure is outlined in
-[RFC 6838 section 5](http://tools.ietf.org/html/rfc6838#section-5). Types
-registered with the IANA are automatically pulled into this library.
-
-[npm-version-image]: https://img.shields.io/npm/v/mime-db.svg
-[npm-downloads-image]: https://img.shields.io/npm/dm/mime-db.svg
-[npm-url]: https://npmjs.org/package/mime-db
-[travis-image]: https://img.shields.io/travis/jshttp/mime-db/master.svg
-[travis-url]: https://travis-ci.org/jshttp/mime-db
-[coveralls-image]: https://img.shields.io/coveralls/jshttp/mime-db/master.svg
-[coveralls-url]: https://coveralls.io/r/jshttp/mime-db?branch=master
-[node-image]: https://img.shields.io/node/v/mime-db.svg
-[node-url]: http://nodejs.org/download/