diff --git a/prebuilt/iot-gateway/node_modules/on-finished/README.md b/prebuilt/iot-gateway/node_modules/on-finished/README.md
+++ /dev/null
@@ -1,154 +0,0 @@
-# on-finished
-
-[![NPM Version][npm-image]][npm-url]
-[![NPM Downloads][downloads-image]][downloads-url]
-[![Node.js Version][node-version-image]][node-version-url]
-[![Build Status][travis-image]][travis-url]
-[![Test Coverage][coveralls-image]][coveralls-url]
-
-Execute a callback when a HTTP request closes, finishes, or errors.
-
-## Install
-
-```sh
-$ npm install on-finished
-```
-
-## API
-
-```js
-var onFinished = require('on-finished')
-```
-
-### onFinished(res, listener)
-
-Attach a listener to listen for the response to finish. The listener will
-be invoked only once when the response finished. If the response finished
-to an error, the first argument will contain the error. If the response
-has already finished, the listener will be invoked.
-
-Listening to the end of a response would be used to close things associated
-with the response, like open files.
-
-Listener is invoked as `listener(err, res)`.
-
-```js
-onFinished(res, function (err, res) {
- // clean up open fds, etc.
- // err contains the error is request error'd
-})
-```
-
-### onFinished(req, listener)
-
-Attach a listener to listen for the request to finish. The listener will
-be invoked only once when the request finished. If the request finished
-to an error, the first argument will contain the error. If the request
-has already finished, the listener will be invoked.
-
-Listening to the end of a request would be used to know when to continue
-after reading the data.
-
-Listener is invoked as `listener(err, req)`.
-
-```js
-var data = ''
-
-req.setEncoding('utf8')
-res.on('data', function (str) {
- data += str
-})
-
-onFinished(req, function (err, req) {
- // data is read unless there is err
-})
-```
-
-### onFinished.isFinished(res)
-
-Determine if `res` is already finished. This would be useful to check and
-not even start certain operations if the response has already finished.
-
-### onFinished.isFinished(req)
-
-Determine if `req` is already finished. This would be useful to check and
-not even start certain operations if the request has already finished.
-
-## Special Node.js requests
-
-### HTTP CONNECT method
-
-The meaning of the `CONNECT` method from RFC 7231, section 4.3.6:
-
-> The CONNECT method requests that the recipient establish a tunnel to
-> the destination origin server identified by the request-target and,
-> if successful, thereafter restrict its behavior to blind forwarding
-> of packets, in both directions, until the tunnel is closed. Tunnels
-> are commonly used to create an end-to-end virtual connection, through
-> one or more proxies, which can then be secured using TLS (Transport
-> Layer Security, [RFC5246]).
-
-In Node.js, these request objects come from the `'connect'` event on
-the HTTP server.
-
-When this module is used on a HTTP `CONNECT` request, the request is
-considered "finished" immediately, **due to limitations in the Node.js
-interface**. This means if the `CONNECT` request contains a request entity,
-the request will be considered "finished" even before it has been read.
-
-There is no such thing as a response object to a `CONNECT` request in
-Node.js, so there is no support for for one.
-
-### HTTP Upgrade request
-
-The meaning of the `Upgrade` header from RFC 7230, section 6.1:
-
-> The "Upgrade" header field is intended to provide a simple mechanism
-> for transitioning from HTTP/1.1 to some other protocol on the same
-> connection.
-
-In Node.js, these request objects come from the `'upgrade'` event on
-the HTTP server.
-
-When this module is used on a HTTP request with an `Upgrade` header, the
-request is considered "finished" immediately, **due to limitations in the
-Node.js interface**. This means if the `Upgrade` request contains a request
-entity, the request will be considered "finished" even before it has been
-read.
-
-There is no such thing as a response object to a `Upgrade` request in
-Node.js, so there is no support for for one.
-
-## Example
-
-The following code ensures that file descriptors are always closed
-once the response finishes.
-
-```js
-var destroy = require('destroy')
-var http = require('http')
-var onFinished = require('on-finished')
-
-http.createServer(function onRequest(req, res) {
- var stream = fs.createReadStream('package.json')
- stream.pipe(res)
- onFinished(res, function (err) {
- destroy(stream)
- })
-})
-```
-
-## License
-
-[MIT](LICENSE)
-
-[npm-image]: https://img.shields.io/npm/v/on-finished.svg
-[npm-url]: https://npmjs.org/package/on-finished
-[node-version-image]: https://img.shields.io/node/v/on-finished.svg
-[node-version-url]: http://nodejs.org/download/
-[travis-image]: https://img.shields.io/travis/jshttp/on-finished/master.svg
-[travis-url]: https://travis-ci.org/jshttp/on-finished
-[coveralls-image]: https://img.shields.io/coveralls/jshttp/on-finished/master.svg
-[coveralls-url]: https://coveralls.io/r/jshttp/on-finished?branch=master
-[downloads-image]: https://img.shields.io/npm/dm/on-finished.svg
-[downloads-url]: https://npmjs.org/package/on-finished