summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 0412b73)
raw | patch | inline | side by side (parent: 0412b73)
author | Pali Rohár <pali@kernel.org> | |
Wed, 21 Oct 2020 09:50:40 +0000 (11:50 +0200) | ||
committer | Pali Rohár <pali@kernel.org> | |
Wed, 21 Oct 2020 10:05:25 +0000 (12:05 +0200) |
Currently a3k target is misusing ${DOIMAGETOOL} target for building flash
and UART images. It is not used for building image tool.
So move ${DOIMAGETOOL} target from common marvell include file into a8k
include file and add correct invocation of ${MAKE} into a3k for building
flash and UART images.
Part of this change is also checks that MV_DDR_PATH for a3k was specified
by user as this option is required for building a3k flash and UART images.
Signed-off-by: Pali Rohár <pali@kernel.org>
Change-Id: I5ae9d08b8505460933f17836c9b6435fd6e51bb6
and UART images. It is not used for building image tool.
So move ${DOIMAGETOOL} target from common marvell include file into a8k
include file and add correct invocation of ${MAKE} into a3k for building
flash and UART images.
Part of this change is also checks that MV_DDR_PATH for a3k was specified
by user as this option is required for building a3k flash and UART images.
Signed-off-by: Pali Rohár <pali@kernel.org>
Change-Id: I5ae9d08b8505460933f17836c9b6435fd6e51bb6
plat/marvell/armada/a3k/common/a3700_common.mk | patch | blob | history | |
plat/marvell/armada/a8k/common/a8k_common.mk | patch | blob | history | |
plat/marvell/marvell.mk | patch | blob | history |
diff --git a/plat/marvell/armada/a3k/common/a3700_common.mk b/plat/marvell/armada/a3k/common/a3700_common.mk
index 8f65e92b31bf825eb2ca7cd9ddfe8b5a80b5e239..2050d59b63e0ed056073c81f6a2e50d30d17846f 100644 (file)
$(shell truncate -s %128K ${BUILD_PLAT}/bl1.bin)
$(shell cat ${BUILD_PLAT}/bl1.bin ${BUILD_PLAT}/${FIP_NAME} > ${BUILD_PLAT}/${BOOT_IMAGE})
$(shell truncate -s %4 ${BUILD_PLAT}/${BOOT_IMAGE})
+ $(if $(value MV_DDR_PATH),,$(error "Platform '${PLAT}' for target '$@' requires MV_DDR_PATH. Please set MV_DDR_PATH to point to the right directory"))
+ ${Q}${MAKE} --no-print-directory -C ${DOIMAGEPATH} WTMI_IMG=$(WTMI_IMG) MV_DDR_PATH=$(MV_DDR_PATH)
$(shell truncate -s %4 $(WTMI_IMG))
@echo
@echo "Building uart images"
diff --git a/plat/marvell/armada/a8k/common/a8k_common.mk b/plat/marvell/armada/a8k/common/a8k_common.mk
index a807891e511a48361974c9a1654580f3f981ad38..c8273265e8f2c62307402fa01de6c0039f033621 100644 (file)
# SPDX-License-Identifier: BSD-3-Clause
# https://spdx.org/licenses
-include tools/marvell/doimage/doimage.mk
-
PLAT_FAMILY := a8k
PLAT_INCLUDE_BASE := include/plat/marvell/armada/$(PLAT_FAMILY)
PLAT_COMMON_BASE := plat/marvell/armada/a8k/common
DOIMAGETOOL ?= ${DOIMAGEPATH}/doimage
include plat/marvell/marvell.mk
+include tools/marvell/doimage/doimage.mk
+
+ifeq (${MARVELL_SECURE_BOOT},1)
+DOIMAGE_SEC_FLAGS := -c $(DOIMAGE_SEC)
+DOIMAGE_LIBS_CHECK = \
+ if ! [ -d "/usr/include/mbedtls" ]; then \
+ echo "****************************************" >&2; \
+ echo "Missing mbedTLS installation! " >&2; \
+ echo "Please download it from \"tls.mbed.org\"" >&2; \
+ echo "Alternatively on Debian/Ubuntu system install" >&2; \
+ echo "\"libmbedtls-dev\" package" >&2; \
+ echo "Make sure to use version 2.1.0 or later" >&2; \
+ echo "****************************************" >&2; \
+ exit 1; \
+ else if ! [ -f "/usr/include/libconfig.h" ]; then \
+ echo "********************************************************" >&2; \
+ echo "Missing Libconfig installation!" >&2; \
+ echo "Please download it from \"www.hyperrealm.com/libconfig/\"" >&2; \
+ echo "Alternatively on Debian/Ubuntu system install packages" >&2; \
+ echo "\"libconfig8\" and \"libconfig8-dev\"" >&2; \
+ echo "********************************************************" >&2; \
+ exit 1; \
+ fi \
+ fi
+else #MARVELL_SECURE_BOOT
+DOIMAGE_LIBS_CHECK =
+DOIMAGE_SEC_FLAGS =
+endif #MARVELL_SECURE_BOOT
ROM_BIN_EXT ?= $(BUILD_PLAT)/ble.bin
DOIMAGE_FLAGS += -b $(ROM_BIN_EXT) $(NAND_DOIMAGE_FLAGS) $(DOIMAGE_SEC_FLAGS)
include ${BLE_PATH}/ble.mk
$(eval $(call MAKE_BL,e))
+mrvl_clean:
+ @echo " Doimage CLEAN"
+ ${Q}${MAKE} PLAT=${PLAT} --no-print-directory -C ${DOIMAGEPATH} clean
+
+${DOIMAGETOOL}: mrvl_clean
+ @$(DOIMAGE_LIBS_CHECK)
+ ${Q}${MAKE} --no-print-directory -C ${DOIMAGEPATH}
+
mrvl_flash: ${BUILD_PLAT}/${FIP_NAME} ${DOIMAGETOOL} ${BUILD_PLAT}/ble.bin
$(shell truncate -s %128K ${BUILD_PLAT}/bl1.bin)
$(shell cat ${BUILD_PLAT}/bl1.bin ${BUILD_PLAT}/${FIP_NAME} > ${BUILD_PLAT}/${BOOT_IMAGE})
index 82457536d3f8f2ebf1719afc2226143d0ed19863..b6a2b9995b8fd4a62da318cb53fe3a2ebbfc0e97 100644 (file)
--- a/plat/marvell/marvell.mk
+++ b/plat/marvell/marvell.mk
# Set board to work with DDR 32bit
DDR32 := 0
$(eval $(call add_define,DDR32))
-
-ifeq (${MARVELL_SECURE_BOOT},1)
-DOIMAGE_SEC_FLAGS := -c $(DOIMAGE_SEC)
-DOIMAGE_LIBS_CHECK = \
- if ! [ -d "/usr/include/mbedtls" ]; then \
- echo "****************************************" >&2; \
- echo "Missing mbedTLS installation! " >&2; \
- echo "Please download it from \"tls.mbed.org\"" >&2; \
- echo "Alternatively on Debian/Ubuntu system install" >&2; \
- echo "\"libmbedtls-dev\" package" >&2; \
- echo "Make sure to use version 2.1.0 or later" >&2; \
- echo "****************************************" >&2; \
- exit 1; \
- else if ! [ -f "/usr/include/libconfig.h" ]; then \
- echo "********************************************************" >&2; \
- echo "Missing Libconfig installation!" >&2; \
- echo "Please download it from \"www.hyperrealm.com/libconfig/\"" >&2; \
- echo "Alternatively on Debian/Ubuntu system install packages" >&2; \
- echo "\"libconfig8\" and \"libconfig8-dev\"" >&2; \
- echo "********************************************************" >&2; \
- exit 1; \
- fi \
- fi
-else #MARVELL_SECURE_BOOT
-DOIMAGE_LIBS_CHECK =
-DOIMAGE_SEC_FLAGS =
-endif #MARVELL_SECURE_BOOT
-
-mrvl_clean:
- @echo " Doimage CLEAN"
- ${Q}${MAKE} PLAT=${PLAT} --no-print-directory -C ${DOIMAGEPATH} clean
-
-${DOIMAGETOOL}: mrvl_clean
- @$(DOIMAGE_LIBS_CHECK)
- ${Q}${MAKE} --no-print-directory -C ${DOIMAGEPATH} VERSION=$(SUBVERSION) WTMI_IMG=$(WTMI_IMG)
-
-