Fix crash when a local deauth occurs (squash)
[build-utilities/hostap.git] / COPYING
1 wpa_supplicant and hostapd
2 --------------------------
4 Copyright (c) 2002-2012, Jouni Malinen <j@w1.fi> and contributors
5 All Rights Reserved.
8 See the README file for the current license terms.
10 This software was previously distributed under BSD/GPL v2 dual license
11 terms that allowed either of those license alternatives to be
12 selected. As of February 11, 2012, the project has chosen to use only
13 the BSD license option for future distribution. As such, the GPL v2
14 license option is no longer used. It should be noted that the BSD
15 license option (the one with advertisement clause removed) is compatible
16 with GPL and as such, does not prevent use of this software in projects
17 that use GPL.
19 Some of the files may still include pointers to GPL version 2 license
20 terms. However, such copyright and license notifications are maintained
21 only for attribution purposes and any distribution of this software
22 after February 11, 2012 is no longer under the GPL v2 option.