34dad3034268c667c4db124442431f3dcd50a254
[build-utilities/hostap.git] / hostapd / README
1 hostapd - user space IEEE 802.11 AP and IEEE 802.1X/WPA/WPA2/EAP
2           Authenticator and RADIUS authentication server
3 ================================================================
5 Copyright (c) 2002-2012, Jouni Malinen <j@w1.fi> and contributors
6 All Rights Reserved.
8 This program is licensed under the BSD license (the one with
9 advertisement clause removed).
11 If you are submitting changes to the project, please see CONTRIBUTIONS
12 file for more instructions.
16 License
17 -------
19 This software may be distributed, used, and modified under the terms of
20 BSD license:
22 Redistribution and use in source and binary forms, with or without
23 modification, are permitted provided that the following conditions are
24 met:
26 1. Redistributions of source code must retain the above copyright
27    notice, this list of conditions and the following disclaimer.
29 2. Redistributions in binary form must reproduce the above copyright
30    notice, this list of conditions and the following disclaimer in the
31    documentation and/or other materials provided with the distribution.
33 3. Neither the name(s) of the above-listed copyright holder(s) nor the
34    names of its contributors may be used to endorse or promote products
35    derived from this software without specific prior written permission.
37 THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
38 "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
39 LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
40 A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
41 OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
42 SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
43 LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
44 DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
45 THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
46 (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
47 OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
51 Introduction
52 ============
54 Originally, hostapd was an optional user space component for Host AP
55 driver. It adds more features to the basic IEEE 802.11 management
56 included in the kernel driver: using external RADIUS authentication
57 server for MAC address based access control, IEEE 802.1X Authenticator
58 and dynamic WEP keying, RADIUS accounting, WPA/WPA2 (IEEE 802.11i/RSN)
59 Authenticator and dynamic TKIP/CCMP keying.
61 The current version includes support for other drivers, an integrated
62 EAP server (i.e., allow full authentication without requiring
63 an external RADIUS authentication server), and RADIUS authentication
64 server for EAP authentication.
67 Requirements
68 ------------
70 Current hardware/software requirements:
71 - drivers:
72         Host AP driver for Prism2/2.5/3.
73         (http://hostap.epitest.fi/)
74         Please note that station firmware version needs to be 1.7.0 or newer
75         to work in WPA mode.
77         madwifi driver for cards based on Atheros chip set (ar521x)
78         (http://sourceforge.net/projects/madwifi/)
79         Please note that you will need to add the correct path for
80         madwifi driver root directory in .config (see defconfig file for
81         an example: CFLAGS += -I<path>)
83         mac80211-based drivers that support AP mode (with driver=nl80211).
84         This includes drivers for Atheros (ath9k) and Broadcom (b43)
85         chipsets.
87         Any wired Ethernet driver for wired IEEE 802.1X authentication
88         (experimental code)
90         FreeBSD -current (with some kernel mods that have not yet been
91         committed when hostapd v0.3.0 was released)
92         BSD net80211 layer (e.g., Atheros driver)
95 Build configuration
96 -------------------
98 In order to be able to build hostapd, you will need to create a build
99 time configuration file, .config that selects which optional
100 components are included. See defconfig file for example configuration
101 and list of available options.
105 IEEE 802.1X
106 ===========
108 IEEE Std 802.1X-2001 is a standard for port-based network access
109 control. In case of IEEE 802.11 networks, a "virtual port" is used
110 between each associated station and the AP. IEEE 802.11 specifies
111 minimal authentication mechanism for stations, whereas IEEE 802.1X
112 introduces a extensible mechanism for authenticating and authorizing
113 users.
115 IEEE 802.1X uses elements called Supplicant, Authenticator, Port
116 Access Entity, and Authentication Server. Supplicant is a component in
117 a station and it performs the authentication with the Authentication
118 Server. An access point includes an Authenticator that relays the packets
119 between a Supplicant and an Authentication Server. In addition, it has a
120 Port Access Entity (PAE) with Authenticator functionality for
121 controlling the virtual port authorization, i.e., whether to accept
122 packets from or to the station.
124 IEEE 802.1X uses Extensible Authentication Protocol (EAP). The frames
125 between a Supplicant and an Authenticator are sent using EAP over LAN
126 (EAPOL) and the Authenticator relays these frames to the Authentication
127 Server (and similarly, relays the messages from the Authentication
128 Server to the Supplicant). The Authentication Server can be colocated with the
129 Authenticator, in which case there is no need for additional protocol
130 for EAP frame transmission. However, a more common configuration is to
131 use an external Authentication Server and encapsulate EAP frame in the
132 frames used by that server. RADIUS is suitable for this, but IEEE
133 802.1X would also allow other mechanisms.
135 Host AP driver includes PAE functionality in the kernel driver. It
136 is a relatively simple mechanism for denying normal frames going to
137 or coming from an unauthorized port. PAE allows IEEE 802.1X related
138 frames to be passed between the Supplicant and the Authenticator even
139 on an unauthorized port.
141 User space daemon, hostapd, includes Authenticator functionality. It
142 receives 802.1X (EAPOL) frames from the Supplicant using the wlan#ap
143 device that is also used with IEEE 802.11 management frames. The
144 frames to the Supplicant are sent using the same device.
146 The normal configuration of the Authenticator would use an external
147 Authentication Server. hostapd supports RADIUS encapsulation of EAP
148 packets, so the Authentication Server should be a RADIUS server, like
149 FreeRADIUS (http://www.freeradius.org/). The Authenticator in hostapd
150 relays the frames between the Supplicant and the Authentication
151 Server. It also controls the PAE functionality in the kernel driver by
152 controlling virtual port authorization, i.e., station-AP
153 connection, based on the IEEE 802.1X state.
155 When a station would like to use the services of an access point, it
156 will first perform IEEE 802.11 authentication. This is normally done
157 with open systems authentication, so there is no security. After
158 this, IEEE 802.11 association is performed. If IEEE 802.1X is
159 configured to be used, the virtual port for the station is set in
160 Unauthorized state and only IEEE 802.1X frames are accepted at this
161 point. The Authenticator will then ask the Supplicant to authenticate
162 with the Authentication Server. After this is completed successfully,
163 the virtual port is set to Authorized state and frames from and to the
164 station are accepted.
166 Host AP configuration for IEEE 802.1X
167 -------------------------------------
169 The user space daemon has its own configuration file that can be used to
170 define AP options. Distribution package contains an example
171 configuration file (hostapd/hostapd.conf) that can be used as a basis
172 for configuration. It includes examples of all supported configuration
173 options and short description of each option. hostapd should be started
174 with full path to the configuration file as the command line argument,
175 e.g., './hostapd /etc/hostapd.conf'. If you have more that one wireless
176 LAN card, you can use one hostapd process for multiple interfaces by
177 giving a list of configuration files (one per interface) in the command
178 line.
180 hostapd includes a minimal co-located IEEE 802.1X server which can be
181 used to test IEEE 802.1X authentication. However, it should not be
182 used in normal use since it does not provide any security. This can be
183 configured by setting ieee8021x and minimal_eap options in the
184 configuration file.
186 An external Authentication Server (RADIUS) is configured with
187 auth_server_{addr,port,shared_secret} options. In addition,
188 ieee8021x and own_ip_addr must be set for this mode. With such
189 configuration, the co-located Authentication Server is not used and EAP
190 frames will be relayed using EAPOL between the Supplicant and the
191 Authenticator and RADIUS encapsulation between the Authenticator and
192 the Authentication Server. Other than this, the functionality is similar
193 to the case with the co-located Authentication Server.
195 Authentication Server and Supplicant
196 ------------------------------------
198 Any RADIUS server supporting EAP should be usable as an IEEE 802.1X
199 Authentication Server with hostapd Authenticator. FreeRADIUS
200 (http://www.freeradius.org/) has been successfully tested with hostapd
201 Authenticator and both Xsupplicant (http://www.open1x.org) and Windows
202 XP Supplicants. EAP/TLS was used with Xsupplicant and
203 EAP/MD5-Challenge with Windows XP.
205 http://www.missl.cs.umd.edu/wireless/eaptls/ has useful information
206 about using EAP/TLS with FreeRADIUS and Xsupplicant (just replace
207 Cisco access point with Host AP driver, hostapd daemon, and a Prism2
208 card ;-). http://www.freeradius.org/doc/EAP-MD5.html has information
209 about using EAP/MD5 with FreeRADIUS, including instructions for WinXP
210 configuration. http://www.denobula.com/EAPTLS.pdf has a HOWTO on
211 EAP/TLS use with WinXP Supplicant.
213 Automatic WEP key configuration
214 -------------------------------
216 EAP/TLS generates a session key that can be used to send WEP keys from
217 an AP to authenticated stations. The Authenticator in hostapd can be
218 configured to automatically select a random default/broadcast key
219 (shared by all authenticated stations) with wep_key_len_broadcast
220 option (5 for 40-bit WEP or 13 for 104-bit WEP). In addition,
221 wep_key_len_unicast option can be used to configure individual unicast
222 keys for stations. This requires support for individual keys in the
223 station driver.
225 WEP keys can be automatically updated by configuring rekeying. This
226 will improve security of the network since same WEP key will only be
227 used for a limited period of time. wep_rekey_period option sets the
228 interval for rekeying in seconds.
231 WPA/WPA2
232 ========
234 Features
235 --------
237 Supported WPA/IEEE 802.11i features:
238 - WPA-PSK ("WPA-Personal")
239 - WPA with EAP (e.g., with RADIUS authentication server) ("WPA-Enterprise")
240 - key management for CCMP, TKIP, WEP104, WEP40
241 - RSN/WPA2 (IEEE 802.11i), including PMKSA caching and pre-authentication
243 WPA
244 ---
246 The original security mechanism of IEEE 802.11 standard was not
247 designed to be strong and has proved to be insufficient for most
248 networks that require some kind of security. Task group I (Security)
249 of IEEE 802.11 working group (http://www.ieee802.org/11/) has worked
250 to address the flaws of the base standard and has in practice
251 completed its work in May 2004. The IEEE 802.11i amendment to the IEEE
252 802.11 standard was approved in June 2004 and this amendment is likely
253 to be published in July 2004.
255 Wi-Fi Alliance (http://www.wi-fi.org/) used a draft version of the
256 IEEE 802.11i work (draft 3.0) to define a subset of the security
257 enhancements that can be implemented with existing wlan hardware. This
258 is called Wi-Fi Protected Access<TM> (WPA). This has now become a
259 mandatory component of interoperability testing and certification done
260 by Wi-Fi Alliance. Wi-Fi provides information about WPA at its web
261 site (http://www.wi-fi.org/OpenSection/protected_access.asp).
263 IEEE 802.11 standard defined wired equivalent privacy (WEP) algorithm
264 for protecting wireless networks. WEP uses RC4 with 40-bit keys,
265 24-bit initialization vector (IV), and CRC32 to protect against packet
266 forgery. All these choices have proven to be insufficient: key space is
267 too small against current attacks, RC4 key scheduling is insufficient
268 (beginning of the pseudorandom stream should be skipped), IV space is
269 too small and IV reuse makes attacks easier, there is no replay
270 protection, and non-keyed authentication does not protect against bit
271 flipping packet data.
273 WPA is an intermediate solution for the security issues. It uses
274 Temporal Key Integrity Protocol (TKIP) to replace WEP. TKIP is a
275 compromise on strong security and possibility to use existing
276 hardware. It still uses RC4 for the encryption like WEP, but with
277 per-packet RC4 keys. In addition, it implements replay protection,
278 keyed packet authentication mechanism (Michael MIC).
280 Keys can be managed using two different mechanisms. WPA can either use
281 an external authentication server (e.g., RADIUS) and EAP just like
282 IEEE 802.1X is using or pre-shared keys without need for additional
283 servers. Wi-Fi calls these "WPA-Enterprise" and "WPA-Personal",
284 respectively. Both mechanisms will generate a master session key for
285 the Authenticator (AP) and Supplicant (client station).
287 WPA implements a new key handshake (4-Way Handshake and Group Key
288 Handshake) for generating and exchanging data encryption keys between
289 the Authenticator and Supplicant. This handshake is also used to
290 verify that both Authenticator and Supplicant know the master session
291 key. These handshakes are identical regardless of the selected key
292 management mechanism (only the method for generating master session
293 key changes).
296 IEEE 802.11i / WPA2
297 -------------------
299 The design for parts of IEEE 802.11i that were not included in WPA has
300 finished (May 2004) and this amendment to IEEE 802.11 was approved in
301 June 2004. Wi-Fi Alliance is using the final IEEE 802.11i as a new
302 version of WPA called WPA2. This includes, e.g., support for more
303 robust encryption algorithm (CCMP: AES in Counter mode with CBC-MAC)
304 to replace TKIP and optimizations for handoff (reduced number of
305 messages in initial key handshake, pre-authentication, and PMKSA caching).
307 Some wireless LAN vendors are already providing support for CCMP in
308 their WPA products. There is no "official" interoperability
309 certification for CCMP and/or mixed modes using both TKIP and CCMP, so
310 some interoperability issues can be expected even though many
311 combinations seem to be working with equipment from different vendors.
312 Testing for WPA2 is likely to start during the second half of 2004.
314 hostapd configuration for WPA/WPA2
315 ----------------------------------
317 TODO
319 # Enable WPA. Setting this variable configures the AP to require WPA (either
320 # WPA-PSK or WPA-RADIUS/EAP based on other configuration). For WPA-PSK, either
321 # wpa_psk or wpa_passphrase must be set and wpa_key_mgmt must include WPA-PSK.
322 # For WPA-RADIUS/EAP, ieee8021x must be set (but without dynamic WEP keys),
323 # RADIUS authentication server must be configured, and WPA-EAP must be included
324 # in wpa_key_mgmt.
325 # This field is a bit field that can be used to enable WPA (IEEE 802.11i/D3.0)
326 # and/or WPA2 (full IEEE 802.11i/RSN):
327 # bit0 = WPA
328 # bit1 = IEEE 802.11i/RSN (WPA2)
329 #wpa=1
331 # WPA pre-shared keys for WPA-PSK. This can be either entered as a 256-bit
332 # secret in hex format (64 hex digits), wpa_psk, or as an ASCII passphrase
333 # (8..63 characters) that will be converted to PSK. This conversion uses SSID
334 # so the PSK changes when ASCII passphrase is used and the SSID is changed.
335 #wpa_psk=0123456789abcdef0123456789abcdef0123456789abcdef0123456789abcdef
336 #wpa_passphrase=secret passphrase
338 # Set of accepted key management algorithms (WPA-PSK, WPA-EAP, or both). The
339 # entries are separated with a space.
340 #wpa_key_mgmt=WPA-PSK WPA-EAP
342 # Set of accepted cipher suites (encryption algorithms) for pairwise keys
343 # (unicast packets). This is a space separated list of algorithms:
344 # CCMP = AES in Counter mode with CBC-MAC [RFC 3610, IEEE 802.11i]
345 # TKIP = Temporal Key Integrity Protocol [IEEE 802.11i]
346 # Group cipher suite (encryption algorithm for broadcast and multicast frames)
347 # is automatically selected based on this configuration. If only CCMP is
348 # allowed as the pairwise cipher, group cipher will also be CCMP. Otherwise,
349 # TKIP will be used as the group cipher.
350 #wpa_pairwise=TKIP CCMP
352 # Time interval for rekeying GTK (broadcast/multicast encryption keys) in
353 # seconds.
354 #wpa_group_rekey=600
356 # Time interval for rekeying GMK (master key used internally to generate GTKs
357 # (in seconds).
358 #wpa_gmk_rekey=86400
360 # Enable IEEE 802.11i/RSN/WPA2 pre-authentication. This is used to speed up
361 # roaming be pre-authenticating IEEE 802.1X/EAP part of the full RSN
362 # authentication and key handshake before actually associating with a new AP.
363 #rsn_preauth=1
365 # Space separated list of interfaces from which pre-authentication frames are
366 # accepted (e.g., 'eth0' or 'eth0 wlan0wds0'. This list should include all
367 # interface that are used for connections to other APs. This could include
368 # wired interfaces and WDS links. The normal wireless data interface towards
369 # associated stations (e.g., wlan0) should not be added, since
370 # pre-authentication is only used with APs other than the currently associated
371 # one.
372 #rsn_preauth_interfaces=eth0