1 ##### hostapd configuration file ##############################################
2 # Empty lines and lines starting with # are ignored
4 # Example configuration file for wired authenticator. See hostapd.conf for
5 # more details.
7 interface=eth0
8 driver=wired
9 logger_stdout=-1
10 logger_stdout_level=1
11 debug=2
12 dump_file=/tmp/hostapd.dump
14 ieee8021x=1
15 eap_reauth_period=3600
17 use_pae_group_addr=1
20 ##### RADIUS configuration ####################################################
21 # for IEEE 802.1X with external Authentication Server, IEEE 802.11
22 # authentication with external ACL for MAC addresses, and accounting
24 # The own IP address of the access point (used as NAS-IP-Address)
25 own_ip_addr=127.0.0.1
27 # Optional NAS-Identifier string for RADIUS messages. When used, this should be
28 # a unique to the NAS within the scope of the RADIUS server. For example, a
29 # fully qualified domain name can be used here.
30 nas_identifier=ap.example.com
32 # RADIUS authentication server
33 auth_server_addr=127.0.0.1
34 auth_server_port=1812
35 auth_server_shared_secret=radius
37 # RADIUS accounting server
38 acct_server_addr=127.0.0.1
39 acct_server_port=1813
40 acct_server_shared_secret=radius