2f67c734c9014fdcdda60c68d8ea848d8e5ed181
1 <!DOCTYPE HTML PUBLIC "-//W3C//DTD HTML 4.01//EN" "http://www.w3.org/TR/html4/strict.dtd">
2 <html>
3 <head>
4 <title>Host AP Linux driver for Intersil Prism2/2.5/3 wireless LAN cards and WPA Supplicant</title>
5 <meta name="description" content="Linux driver for Host AP mode of Intersil Prism2/2.5/3 and WPA Supplicant">
6 <meta name="keywords" content="Host AP, hostap, Prism2, Linux driver for Prism2, Linux access point, software access point, hostapd, IEEE 802.11, IEEE 802.1X, WPA, WPA2, WPA Supplicant, wpa_supplicant, IEEE 802.11i, TKIP, CCMP, EAP-PEAP, EAP-TLS, IEEE 802.1X Supplicant, IEEE 802.1aa, EAPOL, RSN, pre-authentication, PMKSA caching, BSD hostapd, FreeBSD hostapd, RADIUS, authentication server, wireless">
7 <meta http-equiv="Content-Type" content="text/html; charset=iso-8859-1">
8 </head>
10 <body>
11 <h2>Host AP driver for Intersil Prism2/2.5/3, hostapd, and WPA Supplicant</h2>
13 <h3><a name="intro">Introduction</a></h3>
15 <p>This project includes three main components:</p>
16 <ul>
17 <li>Host AP - Linux driver for Prism2/2.5/3</li>
18 <li><a href="hostapd/">hostapd</a> - user space daemon for access points,
19 including, e.g., IEEE 802.1X/WPA/EAP Authenticator for number of Linux and
20 BSD drivers, RADIUS client, integrated EAP server, and RADIUS
21 authentication server</li>
22 <li><a href="wpa_supplicant/">wpa_supplicant</a> user space IEEE 802.1X/WPA
23 supplicant (wireless client) for number of Linux, BSD, and Windows
24 drivers</li>
25 </ul>
27 <p>
28 Host AP is a Linux driver for wireless LAN cards based on Intersil's
29 Prism2/2.5/3 chipset. The driver supports a so called Host AP mode, i.e., it
30 takes care of IEEE 802.11 management functions in the host computer
31 and acts as an access point. This does not require any special
32 firmware for the wireless LAN card. In addition to this, it has
33 support for normal station operations in BSS and possible also in
34 IBSS. WPA and RSN (WPA2) is supported when used with accompanied tools,
35 wpa_supplicant (WPA/RSN Supplicant) and hostapd (WPA/RSN Authenticator). All
36 these programs have been designed for both desktop/laptop computers and
37 embedded systems.
38 </p>
40 <p>
41 Intersil's station firmware for Prism2 chipset supports a so called
42 Host AP mode in which the firmware takes care of time critical tasks
43 like beacon sending and frame acknowledging, but leaves other
44 management tasks to host computer driver. This driver implements basic
45 functionality needed to initialize and configure Prism2-based cards,
46 to send and receive frames, and to gather statistics. In addition, it
47 includes an implementation of following IEEE 802.11 functions:
48 authentication (and deauthentication), association (reassociation, and
49 disassociation), data transmission between two wireless stations,
50 power saving (PS) mode signaling and frame buffering for PS
51 stations. The driver has also various features for development
52 debugging and for researching IEEE 802.11 environments like access to
53 hardware configuration records, I/O registers, and frames with 802.11
54 headers.
55 </p>
57 <p>
58 When used with a user space daemon, the combination of the Host AP
59 driver and hostapd daemon includes additional features. These include
60 support for IEEE 802.1X and dynamic WEP rekeying, RADIUS Accounting,
61 RADIUS-based ACL for IEEE 802.11 authentication, minimal IAPP (IEEE
62 802.11f), WPA, IEEE 802.11i/RSN/WPA2.
63 </p>
65 <p>
66 <a href="http://www.hpl.hp.com/personal/Jean_Tourrilhes/Linux/Wireless.html">Linux
67 Wireless LAN Howto</a> has some useful information about wireless LAN support
68 in Linux. In addition, it includes information about which cards are
69 Prism2-based (and can thus be used in Host AP mode).
70 </p>
72 <h3><a name="wpa_supplicant">WPA/RSN Supplicant (wpa_supplicant)</a></h3>
74 <p>More information is available on <a
75 href="wpa_supplicant/">wpa_supplicant's own page</a>.</p>
77 <p>Supported WPA/IEEE 802.11i features:</p>
78 <ul>
79 <li>WPA-PSK ("WPA-Personal")</li>
80 <li>WPA with EAP (e.g., with RADIUS authentication server) ("WPA-Enterprise")</li>
81 <li>key management for CCMP, TKIP, WEP104, WEP40</li>
82 <li>WPA and full IEEE 802.11i/RSN/WPA2</li>
83 <li>RSN: PMKSA caching, pre-authentication</li>
84 </ul>
86 <p>Supported drivers:</p>
87 <ul>
88 <li>Linux drivers that support Linux Wireless Extensions v19 or newer with
89 WPA/WPA2 extensions</li>
90 <li>Host AP driver for Prism2/2.5/3</li>
91 <li>Linuxant DriverLoader with Windows NDIS driver supporting WPA</li>
92 <li>Agere Systems Inc. Linux Driver (Hermes-I/Hermes-II chipset)</li>
93 <li>madwifi (Atheros ar521x)</li>
94 <li>ATMEL AT76C5XXx</li>
95 <li>Linux ndiswrapper with Windows NDIS driver</li>
96 <li>Broadcom wl.o driver</li>
97 <li>Intel ipw2100 and ipw2200</li>
98 <li>Wired Ethernet drivers</li>
99 <li>BSD net80211 layer (e.g., Atheros driver) (FreeBSD 6-CURRENT)</li>
100 <li>Windows NDIS drivers (Windows; at least XP and 2000, others not tested)</li>
101 </ul>
103 <h3><a name="wpa_authenticator">WPA/RSN/EAP Authenticator (hostapd)</a></h3>
105 <p>More information is available on <a
106 href="hostapd/">hostapd's own page</a>.</p>
108 <p>Supported WPA/IEEE 802.11i features:</p>
109 <ul>
110 <li>WPA-PSK ("WPA-Personal")</li>
111 <li>WPA with EAP (e.g., with RADIUS authentication server) ("WPA-Enterprise")<br>
112 <li>key management for CCMP, TKIP, WEP104, WEP40</li>
113 <li>WPA and full IEEE 802.11i/RSN/WPA2</li>
114 <li>RSN: PMKSA caching, pre-authentication</li>
115 </ul>
117 <p>Supported drivers:</p>
118 <ul>
119 <li>Host AP driver for Prism2/2.5/3</li>
120 <li>madwifi (Atheros ar521x)</li>
121 <li>Prism54.org (PrismGT)</li>
122 <li>BSD net80211 layer (e.g., Atheros driver) (FreeBSD 6-CURRENT)</li>
123 </ul>
125 <h3><a name="download">Download</a></h3>
127 <p>
128 <b>Host AP driver</b><br>
129 Copyright (c) 2001-2002, SSH Communications Security Corp and
130 Jouni Malinen.<br>
131 Copyright (c) 2002-2007, Jouni Malinen and contributors.<br>
133 Author: Jouni Malinen <j@w1.fi>
134 </p>
136 <p>
137 <b>Host AP utils</b><br>
138 Copyright (c) 2002-2005, Jouni Malinen <j@w1.fi>
139 and contributors.
140 </p>
142 <p>
143 <b>hostapd</b><br>
144 Copyright (c) 2002-2008, Jouni Malinen <j@w1.fi>
145 and contributors.
146 </p>
148 <p>
149 <b>wpa_supplicant</b><br>
150 Copyright (c) 2003-2008, Jouni Malinen <j@w1.fi>
151 and contributors.
152 </p>
154 <p>
155 This program is free software; you can redistribute it and/or modify
156 it under the terms of the GNU General Public License version 2 as
157 published by the Free Software Foundation. See
158 <a href="/gitweb/gitweb.cgi?p=hostap.git;a=blob_plain;f=COPYING">COPYING</a>
159 for more details. hostapd and wpa_supplicant are alternatively
160 available under BSD license.
161 </p>
164 <p>
165 <b>Please see
166 <a href="/cgi-bin/viewcvs.cgi/*checkout*/hostap/README?rev=HEAD&content-type=text/plain">README</a>
167 for updated documentation of the driver.
168 Please also check <a href="/gitweb/gitweb.cgi?p=hostap.git;a=blob_plain;f=FAQ">FAQ</a> before sending problem reports.</b>
169 </p>
172 <p>
173 <b>Note!</b>
174 Host AP driver was added into the main kernel tree in Linux
175 v2.6.14. The version in the kernel tree should be used instead of this
176 external hostap-driver package. The external releases are only for
177 older kernel versions and all the future development will be in the
178 main kernel tree.
179 </p>
182 <ul>
183 <li><a href="releases.html">Release graph</a></li>
184 <li>Latest stable release:
185 <ul>
186 <li><a href="releases/hostapd-0.5.11.tar.gz">hostapd-0.5.11.tar.gz</a>
187 <li><a href="releases/wpa_supplicant-0.5.11.tar.gz">wpa_supplicant-0.5.11.tar.gz</a> (source code for all versions)
188 <li><a href="releases/wpa_supplicant-windows-bin-0.5.11.zip">wpa_supplicant-windows-bin-0.5.11.zip</a> (binaries for Windows)</li>
189 </ul>
190 <li>Older stable release:
191 <ul>
192 <li><a href="releases/hostap-driver-0.4.9.tar.gz">hostap-driver-0.4.9.tar.gz</a>
193 <li><a href="releases/hostap-utils-0.4.7.tar.gz">hostap-utils-0.4.7.tar.gz</a>
194 <li><a href="releases/hostapd-0.4.11.tar.gz">hostapd-0.4.11.tar.gz</a>
195 <li><a href="releases/wpa_supplicant-0.4.11.tar.gz">wpa_supplicant-0.4.11.tar.gz</a> (source code for all versions)
196 <li><a href="releases/wpa_supplicant-windows-bin-0.4.11.zip">wpa_supplicant-windows-bin-0.4.11.zip</a> (binaries for Windows)</li>
197 </ul>
198 <li>Older stable release:
199 <ul>
200 <li><a href="releases/hostap-driver-0.3.10.tar.gz">hostap-driver-0.3.10.tar.gz</a>
201 <li><a href="releases/hostap-utils-0.3.7.tar.gz">hostap-utils-0.3.7.tar.gz</a>
202 <li><a href="releases/hostapd-0.3.11.tar.gz">hostapd-0.3.11.tar.gz</a>
203 <li><a href="releases/wpa_supplicant-0.3.11.tar.gz">wpa_supplicant-0.3.11.tar.gz</a> (source code for all versions)
204 <li><a href="releases/wpa_supplicant-windows-bin-0.3.11.zip">wpa_supplicant-windows-bin-0.3.11.zip</a> (binaries for Windows)</li>
205 </ul>
206 <li>Obsolete stable release<BR>
207 (note: 0.2.x branch is not supported anymore - please upgrade to 0.4.x or 0.5.x):
208 <ul>
209 <li><a href="releases/hostap-driver-0.2.8.tar.gz">hostap-driver-0.2.8.tar.gz</a>
210 <li><a href="releases/hostap-utils-0.2.8.tar.gz">hostap-utils-0.2.8.tar.gz</a>
211 <li><a href="releases/hostapd-0.2.8.tar.gz">hostapd-0.2.8.tar.gz</a>
212 <li><a href="releases/wpa_supplicant-0.2.8.tar.gz">wpa_supplicant-0.2.8.tar.gz</a>
213 </ul>
214 <li>Latest development release:
215 <ul>
216 <li><a href="releases/hostapd-0.6.6.tar.gz">hostapd-0.6.6.tar.gz</a>
217 <li><a href="releases/wpa_supplicant-0.6.6.tar.gz">wpa_supplicant-0.6.6.tar.gz</a> (source code for all versions)</li>
218 <li><a href="releases/wpa_supplicant-windows-bin-0.6.6.zip">wpa_supplicant-windows-bin-0.6.6.zip</a> (binaries for Windows)</li>
219 <li><a href="wpa_supplicant/qt4/wpa_gui-qt433-windows-dll.zip">wpa_gui-qt433-windows-dll.zip</a> (Qt4 libraries from wpa_gui/Windows)</li>
220 </ul>
221 <li>ChangeLog:
222 <ul>
223 <li>hostap-driver:
224 <a href="/cgi-bin/viewcvs.cgi/*checkout*/hostap/ChangeLog?rev=HEAD&content-type=text/plain">[development branch]</a>
225 <a href="/cgi-bin/viewcvs.cgi/*checkout*/hostap/ChangeLog?rev=stable&content-type=text/plain">[stable branch]</a>
226 <li>hostap-utils:
227 <a href="/cgi-bin/viewcvs.cgi/*checkout*/hostap/utils/ChangeLog?rev=HEAD&content-type=text/plain">[development branch]</a>
228 <a href="/cgi-bin/viewcvs.cgi/*checkout*/hostap/utils/ChangeLog?rev=stable&content-type=text/plain">[stable branch]</a>
229 <li>hostapd:
230 <a href="/gitweb/gitweb.cgi?p=hostap.git;a=blob_plain;f=hostapd/ChangeLog">[development branch]</a>
231 <a href="/cgi-bin/viewcvs.cgi/*checkout*/hostap/hostapd/ChangeLog?rev=stable&content-type=text/plain">[stable branch]</a>
232 <li>wpa_supplicant:
233 <a href="/gitweb/gitweb.cgi?p=hostap.git;a=blob_plain;f=wpa_supplicant/ChangeLog">[development branch]</a>
234 <a href="/cgi-bin/viewcvs.cgi/*checkout*/hostap/wpa_supplicant/ChangeLog?rev=stable&content-type=text/plain">[stable branch]</a>
235 </ul>
236 <li><a href="releases/">Old releases</a>
237 <li><a href="http://lists.shmoo.com/mailman/listinfo/hostap">Mailing list</a>
238 <li><a href="http://lists.shmoo.com/pipermail/hostap/">New mailing list archives</a>
239 <li><a href="hostap/">Old mailing list archives</a>
240 <li><a href="htdig/">Search mailing list archives</a>
241 <li><a href="/gitweb/gitweb.cgi">Web interface to GIT repository (0.6.x and newer)</a></li>
242 <li><a href="/cgi-bin/viewcvs.cgi/hostap/">Web interface to CVS repository (0.5.x and older)</a></li>
243 <li><a href="releases/snapshots/">Snapshot releases from all active branches</a>
244 <li><a href="cvs.html">GIT and read-only anonymous CVS access (pserver)</a>
245 <li><a href="links.html">Host AP related links</a>
246 <li><a href="bugz/">Bug and feature request tracking</a></li>
247 </ul>
249 <h3>Wireless Tools for Linux</h3>
251 <p>
252 Please, note that you will need quite recent version of Wireless Tools
253 to use some features of the Host AP driver. Using the
254 <a href="http://www.hpl.hp.com/personal/Jean_Tourrilhes/Linux/Tools.html#latest">latest</a>
255 version of the tools is recommended. Some features might also require latest beta version.
256 </p>
258 <h3>Feedback, comments, mailing list</h3>
260 <p>
261 Any comments, reports on success/failure, ideas for further
262 improvement, feature requests, etc. are welcome at j@w1.fi.
263 Please note, that I often receive more email than I have time to answer.
264 Unfortunately, some messages may not get a reply, but I'll try to go
265 through my mail whenever time permits.
266 </p>
268 <p>
269 There is also a mailing list for Host AP related messages.
270 Since this list has a broader audience, your likelyhood of getting
271 responses is higher. This list is recommended for general questions
272 about Host AP driver and its development. In addition, I will send
273 release notes to it whenever a new version is available.
274 </p>
276 <p>
277 The mailing list information and web archive is at <a
278 href="http://lists.shmoo.com/mailman/listinfo/hostap">http://lists.shmoo.com/mailman/listinfo/hostap</a>.
279 Messages to hostap@shmoo.com will be delivered to the
280 subscribers. Please note, that due to large number of spam and virus
281 messages sent to the list address, the list is configured to accept
282 messages only from subscribed addresses. Messages from unsubscribed addresses
283 may be accepted manually, but their delivery will be delayed.
284 </p>
286 <p>
287 If you want to make sure your bug report of feature request does not
288 get lost, please report it through the bug tracking system as
289 <a href="bugz/enter_bug.cgi">a new bug/feature request</a>.
290 </p>
292 <hr>
293 <div>
294 <address><a href="mailto:j@w1.fi">Jouni Malinen</a></address>
295 <!-- Created: Mon May 27 20:08:41 EEST 2002 -->
296 <!-- hhmts start -->
297 Last modified: Fri Dec 26 15:37:35 EET 2008
298 <!-- hhmts end -->
299 </div>
300 </body>
301 </html>