diff --git a/hostapd/hostapd_cli.c b/hostapd/hostapd_cli.c
index 84e8641952d55ec0a83b21a11aab295e536f8f9a..05b4b3bc882750ac6d04dd025ec055a59f6de5fe 100644 (file)
--- a/hostapd/hostapd_cli.c
+++ b/hostapd/hostapd_cli.c
/*
* hostapd - command line interface for hostapd daemon
- * Copyright (c) 2004-2009, Jouni Malinen <j@w1.fi>
+ * Copyright (c) 2004-2011, Jouni Malinen <j@w1.fi>
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
#include "includes.h"
#include <dirent.h>
-#include "wpa_ctrl.h"
-#include "common.h"
-#include "version.h"
+#include "common/wpa_ctrl.h"
+#include "utils/common.h"
+#include "utils/eloop.h"
+#include "utils/edit.h"
+#include "common/version.h"
static const char *hostapd_cli_version =
"hostapd_cli v" VERSION_STR "\n"
-"Copyright (c) 2004-2009, Jouni Malinen <j@w1.fi> and contributors";
+"Copyright (c) 2004-2012, Jouni Malinen <j@w1.fi> and contributors";
static const char *hostapd_cli_license =
-"This program is free software. You can distribute it and/or modify it\n"
-"under the terms of the GNU General Public License version 2.\n"
-"\n"
-"Alternatively, this software may be distributed under the terms of the\n"
-"BSD license. See README and COPYING for more details.\n";
+"This software may be distributed under the terms of the BSD license.\n"
+"See README for more details.\n";
static const char *hostapd_cli_full_license =
-"This program is free software; you can redistribute it and/or modify\n"
-"it under the terms of the GNU General Public License version 2 as\n"
-"published by the Free Software Foundation.\n"
-"\n"
-"This program is distributed in the hope that it will be useful,\n"
-"but WITHOUT ANY WARRANTY; without even the implied warranty of\n"
-"MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the\n"
-"GNU General Public License for more details.\n"
-"\n"
-"You should have received a copy of the GNU General Public License\n"
-"along with this program; if not, write to the Free Software\n"
-"Foundation, Inc., 51 Franklin St, Fifth Floor, Boston, MA 02110-1301 USA\n"
-"\n"
-"Alternatively, this software may be distributed under the terms of the\n"
-"BSD license.\n"
+"This software may be distributed under the terms of the BSD license.\n"
"\n"
"Redistribution and use in source and binary forms, with or without\n"
"modification, are permitted provided that the following conditions are\n"
" sta <addr> get MIB variables for one station\n"
" all_sta get MIB variables for all stations\n"
" new_sta <addr> add a new station\n"
+" deauthenticate <addr> deauthenticate a station\n"
+" disassociate <addr> disassociate a station\n"
#ifdef CONFIG_IEEE80211W
" sa_query <addr> send SA Query to a station\n"
#endif /* CONFIG_IEEE80211W */
#ifdef CONFIG_WPS
-" wps_pin <uuid> <pin> [timeout] add WPS Enrollee PIN (Device Password)\n"
+" wps_pin <uuid> <pin> [timeout] [addr] add WPS Enrollee PIN\n"
+" wps_check_pin <PIN> verify PIN checksum\n"
" wps_pbc indicate button pushed to initiate PBC\n"
#ifdef CONFIG_WPS_OOB
" wps_oob <type> <path> <method> use WPS with out-of-band (UFD)\n"
#endif /* CONFIG_WPS_OOB */
+" wps_ap_pin <cmd> [params..] enable/disable AP PIN\n"
+" wps_config <SSID> <auth> <encr> <key> configure AP\n"
#endif /* CONFIG_WPS */
+" get_config show current configuration\n"
" help show this usage help\n"
" interface [ifname] show interfaces/select interface\n"
" level <debug level> change debug level\n"
static int hostapd_cli_attached = 0;
static const char *ctrl_iface_dir = "/var/run/hostapd";
static char *ctrl_ifname = NULL;
+static const char *pid_file = NULL;
+static const char *action_file = NULL;
static int ping_interval = 5;
+static int interactive = 0;
static void usage(void)
{
fprintf(stderr, "%s\n", hostapd_cli_version);
- fprintf(stderr,
- "\n"
- "usage: hostapd_cli [-p<path>] [-i<ifname>] [-hv] "
- "[-G<ping interval>] \\\n"
- " [command..]\n"
+ fprintf(stderr,
+ "\n"
+ "usage: hostapd_cli [-p<path>] [-i<ifname>] [-hvB] "
+ "[-a<path>] \\\n"
+ " [-G<ping interval>] [command..]\n"
"\n"
"Options:\n"
" -h help (show this usage text)\n"
" -v shown version information\n"
" -p<path> path to find control sockets (default: "
"/var/run/hostapd)\n"
+ " -a<file> run in daemon mode executing the action file "
+ "based on events\n"
+ " from hostapd\n"
+ " -B run a daemon in the background\n"
" -i<ifname> Interface to listen on (default: first "
"interface found in the\n"
" socket path)\n\n"
@@ -209,12 +207,63 @@ static int hostapd_cli_cmd_ping(struct wpa_ctrl *ctrl, int argc, char *argv[])
}
+static int hostapd_cli_cmd_relog(struct wpa_ctrl *ctrl, int argc, char *argv[])
+{
+ return wpa_ctrl_command(ctrl, "RELOG");
+}
+
+
static int hostapd_cli_cmd_mib(struct wpa_ctrl *ctrl, int argc, char *argv[])
{
return wpa_ctrl_command(ctrl, "MIB");
}
+static int hostapd_cli_exec(const char *program, const char *arg1,
+ const char *arg2)
+{
+ char *cmd;
+ size_t len;
+ int res;
+ int ret = 0;
+
+ len = os_strlen(program) + os_strlen(arg1) + os_strlen(arg2) + 3;
+ cmd = os_malloc(len);
+ if (cmd == NULL)
+ return -1;
+ res = os_snprintf(cmd, len, "%s %s %s", program, arg1, arg2);
+ if (res < 0 || (size_t) res >= len) {
+ os_free(cmd);
+ return -1;
+ }
+ cmd[len - 1] = '\0';
+#ifndef _WIN32_WCE
+ if (system(cmd) < 0)
+ ret = -1;
+#endif /* _WIN32_WCE */
+ os_free(cmd);
+
+ return ret;
+}
+
+
+static void hostapd_cli_action_process(char *msg, size_t len)
+{
+ const char *pos;
+
+ pos = msg;
+ if (*pos == '<') {
+ pos = os_strchr(pos, '>');
+ if (pos)
+ pos++;
+ else
+ pos = msg;
+ }
+
+ hostapd_cli_exec(action_file, ctrl_ifname, pos);
+}
+
+
static int hostapd_cli_cmd_sta(struct wpa_ctrl *ctrl, int argc, char *argv[])
{
char buf[64];
}
+static int hostapd_cli_cmd_deauthenticate(struct wpa_ctrl *ctrl, int argc,
+ char *argv[])
+{
+ char buf[64];
+ if (argc < 1) {
+ printf("Invalid 'deauthenticate' command - exactly one "
+ "argument, STA address, is required.\n");
+ return -1;
+ }
+ if (argc > 1)
+ os_snprintf(buf, sizeof(buf), "DEAUTHENTICATE %s %s",
+ argv[0], argv[1]);
+ else
+ os_snprintf(buf, sizeof(buf), "DEAUTHENTICATE %s", argv[0]);
+ return wpa_ctrl_command(ctrl, buf);
+}
+
+
+static int hostapd_cli_cmd_disassociate(struct wpa_ctrl *ctrl, int argc,
+ char *argv[])
+{
+ char buf[64];
+ if (argc < 1) {
+ printf("Invalid 'disassociate' command - exactly one "
+ "argument, STA address, is required.\n");
+ return -1;
+ }
+ if (argc > 1)
+ os_snprintf(buf, sizeof(buf), "DISASSOCIATE %s %s",
+ argv[0], argv[1]);
+ else
+ os_snprintf(buf, sizeof(buf), "DISASSOCIATE %s", argv[0]);
+ return wpa_ctrl_command(ctrl, buf);
+}
+
+
#ifdef CONFIG_IEEE80211W
static int hostapd_cli_cmd_sa_query(struct wpa_ctrl *ctrl, int argc,
char *argv[])
static int hostapd_cli_cmd_wps_pin(struct wpa_ctrl *ctrl, int argc,
char *argv[])
{
- char buf[64];
+ char buf[256];
if (argc < 2) {
printf("Invalid 'wps_pin' command - at least two arguments, "
"UUID and PIN, are required.\n");
return -1;
}
- if (argc > 2)
+ if (argc > 3)
+ snprintf(buf, sizeof(buf), "WPS_PIN %s %s %s %s",
+ argv[0], argv[1], argv[2], argv[3]);
+ else if (argc > 2)
snprintf(buf, sizeof(buf), "WPS_PIN %s %s %s",
argv[0], argv[1], argv[2]);
else
}
+static int hostapd_cli_cmd_wps_check_pin(struct wpa_ctrl *ctrl, int argc,
+ char *argv[])
+{
+ char cmd[256];
+ int res;
+
+ if (argc != 1 && argc != 2) {
+ printf("Invalid WPS_CHECK_PIN command: needs one argument:\n"
+ "- PIN to be verified\n");
+ return -1;
+ }
+
+ if (argc == 2)
+ res = os_snprintf(cmd, sizeof(cmd), "WPS_CHECK_PIN %s %s",
+ argv[0], argv[1]);
+ else
+ res = os_snprintf(cmd, sizeof(cmd), "WPS_CHECK_PIN %s",
+ argv[0]);
+ if (res < 0 || (size_t) res >= sizeof(cmd) - 1) {
+ printf("Too long WPS_CHECK_PIN command.\n");
+ return -1;
+ }
+ return wpa_ctrl_command(ctrl, cmd);
+}
+
+
static int hostapd_cli_cmd_wps_pbc(struct wpa_ctrl *ctrl, int argc,
char *argv[])
{
return wpa_ctrl_command(ctrl, cmd);
}
#endif /* CONFIG_WPS_OOB */
+
+
+static int hostapd_cli_cmd_wps_ap_pin(struct wpa_ctrl *ctrl, int argc,
+ char *argv[])
+{
+ char buf[64];
+ if (argc < 1) {
+ printf("Invalid 'wps_ap_pin' command - at least one argument "
+ "is required.\n");
+ return -1;
+ }
+ if (argc > 2)
+ snprintf(buf, sizeof(buf), "WPS_AP_PIN %s %s %s",
+ argv[0], argv[1], argv[2]);
+ else if (argc > 1)
+ snprintf(buf, sizeof(buf), "WPS_AP_PIN %s %s",
+ argv[0], argv[1]);
+ else
+ snprintf(buf, sizeof(buf), "WPS_AP_PIN %s", argv[0]);
+ return wpa_ctrl_command(ctrl, buf);
+}
+
+
+static int hostapd_cli_cmd_wps_config(struct wpa_ctrl *ctrl, int argc,
+ char *argv[])
+{
+ char buf[256];
+ char ssid_hex[2 * 32 + 1];
+ char key_hex[2 * 64 + 1];
+ int i;
+
+ if (argc < 1) {
+ printf("Invalid 'wps_config' command - at least two arguments "
+ "are required.\n");
+ return -1;
+ }
+
+ ssid_hex[0] = '\0';
+ for (i = 0; i < 32; i++) {
+ if (argv[0][i] == '\0')
+ break;
+ os_snprintf(&ssid_hex[i * 2], 3, "%02x", argv[0][i]);
+ }
+
+ key_hex[0] = '\0';
+ if (argc > 3) {
+ for (i = 0; i < 64; i++) {
+ if (argv[3][i] == '\0')
+ break;
+ os_snprintf(&key_hex[i * 2], 3, "%02x",
+ argv[3][i]);
+ }
+ }
+
+ if (argc > 3)
+ snprintf(buf, sizeof(buf), "WPS_CONFIG %s %s %s %s",
+ ssid_hex, argv[1], argv[2], key_hex);
+ else if (argc > 2)
+ snprintf(buf, sizeof(buf), "WPS_CONFIG %s %s %s",
+ ssid_hex, argv[1], argv[2]);
+ else
+ snprintf(buf, sizeof(buf), "WPS_CONFIG %s %s",
+ ssid_hex, argv[1]);
+ return wpa_ctrl_command(ctrl, buf);
+}
#endif /* CONFIG_WPS */
+static int hostapd_cli_cmd_ess_disassoc(struct wpa_ctrl *ctrl, int argc,
+ char *argv[])
+{
+ char buf[300];
+ int res;
+
+ if (argc < 2) {
+ printf("Invalid 'ess_disassoc' command - two arguments (STA "
+ "addr and URL) are needed\n");
+ return -1;
+ }
+
+ res = os_snprintf(buf, sizeof(buf), "ESS_DISASSOC %s %s",
+ argv[0], argv[1]);
+ if (res < 0 || res >= (int) sizeof(buf))
+ return -1;
+ return wpa_ctrl_command(ctrl, buf);
+}
+
+
+static int hostapd_cli_cmd_get_config(struct wpa_ctrl *ctrl, int argc,
+ char *argv[])
+{
+ return wpa_ctrl_command(ctrl, "GET_CONFIG");
+}
+
+
static int wpa_ctrl_command_sta(struct wpa_ctrl *ctrl, char *cmd,
char *addr, size_t addr_len)
{
static int hostapd_cli_cmd_quit(struct wpa_ctrl *ctrl, int argc, char *argv[])
{
hostapd_cli_quit = 1;
+ if (interactive)
+ eloop_terminate();
return 0;
}
}
+static int hostapd_cli_cmd_set(struct wpa_ctrl *ctrl, int argc, char *argv[])
+{
+ char cmd[256];
+ int res;
+
+ if (argc != 2) {
+ printf("Invalid SET command: needs two arguments (variable "
+ "name and value)\n");
+ return -1;
+ }
+
+ res = os_snprintf(cmd, sizeof(cmd), "SET %s %s", argv[0], argv[1]);
+ if (res < 0 || (size_t) res >= sizeof(cmd) - 1) {
+ printf("Too long SET command.\n");
+ return -1;
+ }
+ return wpa_ctrl_command(ctrl, cmd);
+}
+
+
+static int hostapd_cli_cmd_get(struct wpa_ctrl *ctrl, int argc, char *argv[])
+{
+ char cmd[256];
+ int res;
+
+ if (argc != 1) {
+ printf("Invalid GET command: needs one argument (variable "
+ "name)\n");
+ return -1;
+ }
+
+ res = os_snprintf(cmd, sizeof(cmd), "GET %s", argv[0]);
+ if (res < 0 || (size_t) res >= sizeof(cmd) - 1) {
+ printf("Too long GET command.\n");
+ return -1;
+ }
+ return wpa_ctrl_command(ctrl, cmd);
+}
+
+
struct hostapd_cli_cmd {
const char *cmd;
int (*handler)(struct wpa_ctrl *ctrl, int argc, char *argv[]);
static struct hostapd_cli_cmd hostapd_cli_commands[] = {
{ "ping", hostapd_cli_cmd_ping },
{ "mib", hostapd_cli_cmd_mib },
+ { "relog", hostapd_cli_cmd_relog },
{ "sta", hostapd_cli_cmd_sta },
{ "all_sta", hostapd_cli_cmd_all_sta },
{ "new_sta", hostapd_cli_cmd_new_sta },
+ { "deauthenticate", hostapd_cli_cmd_deauthenticate },
+ { "disassociate", hostapd_cli_cmd_disassociate },
#ifdef CONFIG_IEEE80211W
{ "sa_query", hostapd_cli_cmd_sa_query },
#endif /* CONFIG_IEEE80211W */
#ifdef CONFIG_WPS
{ "wps_pin", hostapd_cli_cmd_wps_pin },
+ { "wps_check_pin", hostapd_cli_cmd_wps_check_pin },
{ "wps_pbc", hostapd_cli_cmd_wps_pbc },
#ifdef CONFIG_WPS_OOB
{ "wps_oob", hostapd_cli_cmd_wps_oob },
#endif /* CONFIG_WPS_OOB */
+ { "wps_ap_pin", hostapd_cli_cmd_wps_ap_pin },
+ { "wps_config", hostapd_cli_cmd_wps_config },
#endif /* CONFIG_WPS */
+ { "ess_disassoc", hostapd_cli_cmd_ess_disassoc },
+ { "get_config", hostapd_cli_cmd_get_config },
{ "help", hostapd_cli_cmd_help },
{ "interface", hostapd_cli_cmd_interface },
{ "level", hostapd_cli_cmd_level },
{ "license", hostapd_cli_cmd_license },
{ "quit", hostapd_cli_cmd_quit },
+ { "set", hostapd_cli_cmd_set },
+ { "get", hostapd_cli_cmd_get },
{ NULL, NULL }
};
while (cmd->cmd) {
if (strncasecmp(cmd->cmd, argv[0], strlen(argv[0])) == 0) {
match = cmd;
+ if (os_strcasecmp(cmd->cmd, argv[0]) == 0) {
+ /* we have an exact match */
+ count = 1;
+ break;
+ }
count++;
}
cmd++;
}
-static void hostapd_cli_recv_pending(struct wpa_ctrl *ctrl, int in_read)
+static void hostapd_cli_recv_pending(struct wpa_ctrl *ctrl, int in_read,
+ int action_monitor)
{
int first = 1;
if (ctrl_conn == NULL)
size_t len = sizeof(buf) - 1;
if (wpa_ctrl_recv(ctrl, buf, &len) == 0) {
buf[len] = '\0';
- if (in_read && first)
- printf("\n");
- first = 0;
- printf("%s\n", buf);
+ if (action_monitor)
+ hostapd_cli_action_process(buf, len);
+ else {
+ if (in_read && first)
+ printf("\n");
+ first = 0;
+ printf("%s\n", buf);
+ }
} else {
printf("Could not read pending message.\n");
break;
}
-static void hostapd_cli_interactive(void)
-{
- const int max_args = 10;
- char cmd[256], *res, *argv[max_args], *pos;
- int argc;
+#define max_args 10
- printf("\nInteractive mode\n\n");
+static int tokenize_cmd(char *cmd, char *argv[])
+{
+ char *pos;
+ int argc = 0;
- do {
- hostapd_cli_recv_pending(ctrl_conn, 0);
- printf("> ");
- alarm(ping_interval);
- res = fgets(cmd, sizeof(cmd), stdin);
- alarm(0);
- if (res == NULL)
- break;
- pos = cmd;
- while (*pos != '\0') {
- if (*pos == '\n') {
- *pos = '\0';
- break;
- }
+ pos = cmd;
+ for (;;) {
+ while (*pos == ' ')
pos++;
+ if (*pos == '\0')
+ break;
+ argv[argc] = pos;
+ argc++;
+ if (argc == max_args)
+ break;
+ if (*pos == '"') {
+ char *pos2 = os_strrchr(pos, '"');
+ if (pos2)
+ pos = pos2 + 1;
}
- argc = 0;
- pos = cmd;
- for (;;) {
- while (*pos == ' ')
- pos++;
- if (*pos == '\0')
- break;
- argv[argc] = pos;
- argc++;
- if (argc == max_args)
- break;
- while (*pos != '\0' && *pos != ' ')
- pos++;
- if (*pos == ' ')
- *pos++ = '\0';
- }
- if (argc)
- wpa_request(ctrl_conn, argc, argv);
- } while (!hostapd_cli_quit);
-}
-
+ while (*pos != '\0' && *pos != ' ')
+ pos++;
+ if (*pos == ' ')
+ *pos++ = '\0';
+ }
-static void hostapd_cli_terminate(int sig)
-{
- hostapd_cli_close_connection();
- exit(0);
+ return argc;
}
-static void hostapd_cli_alarm(int sig)
+static void hostapd_cli_ping(void *eloop_ctx, void *timeout_ctx)
{
if (ctrl_conn && _wpa_ctrl_command(ctrl_conn, "PING", 0)) {
printf("Connection to hostapd lost - trying to reconnect\n");
}
}
if (ctrl_conn)
- hostapd_cli_recv_pending(ctrl_conn, 1);
- alarm(ping_interval);
+ hostapd_cli_recv_pending(ctrl_conn, 1, 0);
+ eloop_register_timeout(ping_interval, 0, hostapd_cli_ping, NULL, NULL);
+}
+
+
+static void hostapd_cli_eloop_terminate(int sig, void *signal_ctx)
+{
+ eloop_terminate();
+}
+
+
+static void hostapd_cli_edit_cmd_cb(void *ctx, char *cmd)
+{
+ char *argv[max_args];
+ int argc;
+ argc = tokenize_cmd(cmd, argv);
+ if (argc)
+ wpa_request(ctrl_conn, argc, argv);
+}
+
+
+static void hostapd_cli_edit_eof_cb(void *ctx)
+{
+ eloop_terminate();
+}
+
+
+static void hostapd_cli_interactive(void)
+{
+ printf("\nInteractive mode\n\n");
+
+ eloop_register_signal_terminate(hostapd_cli_eloop_terminate, NULL);
+ edit_init(hostapd_cli_edit_cmd_cb, hostapd_cli_edit_eof_cb,
+ NULL, NULL, NULL);
+ eloop_register_timeout(ping_interval, 0, hostapd_cli_ping, NULL, NULL);
+
+ eloop_run();
+
+ edit_deinit(NULL, NULL);
+ eloop_cancel_timeout(hostapd_cli_ping, NULL, NULL);
+}
+
+
+static void hostapd_cli_cleanup(void)
+{
+ hostapd_cli_close_connection();
+ if (pid_file)
+ os_daemonize_terminate(pid_file);
+
+ os_program_deinit();
+}
+
+
+static void hostapd_cli_action(struct wpa_ctrl *ctrl)
+{
+ fd_set rfds;
+ int fd, res;
+ struct timeval tv;
+ char buf[256];
+ size_t len;
+
+ fd = wpa_ctrl_get_fd(ctrl);
+
+ while (!hostapd_cli_quit) {
+ FD_ZERO(&rfds);
+ FD_SET(fd, &rfds);
+ tv.tv_sec = ping_interval;
+ tv.tv_usec = 0;
+ res = select(fd + 1, &rfds, NULL, NULL, &tv);
+ if (res < 0 && errno != EINTR) {
+ perror("select");
+ break;
+ }
+
+ if (FD_ISSET(fd, &rfds))
+ hostapd_cli_recv_pending(ctrl, 0, 1);
+ else {
+ len = sizeof(buf) - 1;
+ if (wpa_ctrl_request(ctrl, "PING", 4, buf, &len,
+ hostapd_cli_action_process) < 0 ||
+ len < 4 || os_memcmp(buf, "PONG", 4) != 0) {
+ printf("hostapd did not reply to PING "
+ "command - exiting\n");
+ break;
+ }
+ }
+ }
}
int main(int argc, char *argv[])
{
- int interactive;
int warning_displayed = 0;
int c;
+ int daemonize = 0;
+
+ if (os_program_init())
+ return -1;
for (;;) {
- c = getopt(argc, argv, "hG:i:p:v");
+ c = getopt(argc, argv, "a:BhG:i:p:v");
if (c < 0)
break;
switch (c) {
+ case 'a':
+ action_file = optarg;
+ break;
+ case 'B':
+ daemonize = 1;
+ break;
case 'G':
ping_interval = atoi(optarg);
break;
printf("%s\n", hostapd_cli_version);
return 0;
case 'i':
- free(ctrl_ifname);
- ctrl_ifname = strdup(optarg);
+ os_free(ctrl_ifname);
+ ctrl_ifname = os_strdup(optarg);
break;
case 'p':
ctrl_iface_dir = optarg;
}
}
- interactive = argc == optind;
+ interactive = (argc == optind) && (action_file == NULL);
if (interactive) {
printf("%s\n\n%s\n\n", hostapd_cli_version,
hostapd_cli_license);
}
+ if (eloop_init())
+ return -1;
+
for (;;) {
if (ctrl_ifname == NULL) {
struct dirent *dent;
DIR *dir = opendir(ctrl_iface_dir);
if (dir) {
while ((dent = readdir(dir))) {
- if (strcmp(dent->d_name, ".") == 0 ||
- strcmp(dent->d_name, "..") == 0)
+ if (os_strcmp(dent->d_name, ".") == 0
+ ||
+ os_strcmp(dent->d_name, "..") == 0)
continue;
printf("Selected interface '%s'\n",
dent->d_name);
- ctrl_ifname = strdup(dent->d_name);
+ ctrl_ifname = os_strdup(dent->d_name);
break;
}
closedir(dir);
printf("Could not connect to hostapd - re-trying\n");
warning_displayed = 1;
}
- sleep(1);
+ os_sleep(1, 0);
continue;
}
- signal(SIGINT, hostapd_cli_terminate);
- signal(SIGTERM, hostapd_cli_terminate);
- signal(SIGALRM, hostapd_cli_alarm);
-
- if (interactive) {
+ if (interactive || action_file) {
if (wpa_ctrl_attach(ctrl_conn) == 0) {
hostapd_cli_attached = 1;
} else {
printf("Warning: Failed to attach to hostapd.\n");
+ if (action_file)
+ return -1;
}
+ }
+
+ if (daemonize && os_daemonize(pid_file))
+ return -1;
+
+ if (interactive)
hostapd_cli_interactive();
- } else
+ else if (action_file)
+ hostapd_cli_action(ctrl_conn);
+ else
wpa_request(ctrl_conn, argc - optind, &argv[optind]);
- free(ctrl_ifname);
- hostapd_cli_close_connection();
+ os_free(ctrl_ifname);
+ eloop_destroy();
+ hostapd_cli_cleanup();
return 0;
}