index 970d97a34b942d3a4402e5a8da79a67ee9ba89dd..39b2147afbcaffea4071e5d5f376fafcfa626af9 100644 (file)
/*
* WPA Supplicant
- * Copyright (c) 2003-2011, Jouni Malinen <j@w1.fi>
+ * Copyright (c) 2003-2012, Jouni Malinen <j@w1.fi>
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
#include "rsn_supp/preauth.h"
#include "rsn_supp/pmksa_cache.h"
#include "common/wpa_ctrl.h"
-#include "mlme.h"
#include "common/ieee802_11_defs.h"
#include "p2p/p2p.h"
#include "blacklist.h"
const char *wpa_supplicant_version =
"wpa_supplicant v" VERSION_STR "\n"
-"Copyright (c) 2003-2011, Jouni Malinen <j@w1.fi> and contributors";
+"Copyright (c) 2003-2012, Jouni Malinen <j@w1.fi> and contributors";
const char *wpa_supplicant_license =
-"This program is free software. You can distribute it and/or modify it\n"
-"under the terms of the GNU General Public License version 2.\n"
-"\n"
-"Alternatively, this software may be distributed under the terms of the\n"
-"BSD license. See README and COPYING for more details.\n"
+"This software may be distributed under the terms of the BSD license.\n"
+"See README for more details.\n"
#ifdef EAP_TLS_OPENSSL
"\nThis product includes software developed by the OpenSSL Project\n"
"for use in the OpenSSL Toolkit (http://www.openssl.org/)\n"
#ifndef CONFIG_NO_STDOUT_DEBUG
/* Long text divided into parts in order to fit in C89 strings size limits. */
const char *wpa_supplicant_full_license1 =
-"This program is free software; you can redistribute it and/or modify\n"
-"it under the terms of the GNU General Public License version 2 as\n"
-"published by the Free Software Foundation.\n"
-"\n"
-"This program is distributed in the hope that it will be useful,\n"
-"but WITHOUT ANY WARRANTY; without even the implied warranty of\n"
-"MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the\n"
-"GNU General Public License for more details.\n"
-"\n";
+"";
const char *wpa_supplicant_full_license2 =
-"You should have received a copy of the GNU General Public License\n"
-"along with this program; if not, write to the Free Software\n"
-"Foundation, Inc., 51 Franklin St, Fifth Floor, Boston, MA 02110-1301 USA\n"
-"\n"
-"Alternatively, this software may be distributed under the terms of the\n"
-"BSD license.\n"
+"This software may be distributed under the terms of the BSD license.\n"
"\n"
"Redistribution and use in source and binary forms, with or without\n"
"modification, are permitted provided that the following conditions are\n"
}
+static void free_hw_features(struct wpa_supplicant *wpa_s)
+{
+ int i;
+ if (wpa_s->hw.modes == NULL)
+ return;
+
+ for (i = 0; i < wpa_s->hw.num_modes; i++) {
+ os_free(wpa_s->hw.modes[i].channels);
+ os_free(wpa_s->hw.modes[i].rates);
+ }
+
+ os_free(wpa_s->hw.modes);
+ wpa_s->hw.modes = NULL;
+}
+
+
static void wpa_supplicant_cleanup(struct wpa_supplicant *wpa_s)
{
bgscan_deinit(wpa_s);
wpa_s->l2_br = NULL;
}
- if (wpa_s->ctrl_iface) {
- wpa_supplicant_ctrl_iface_deinit(wpa_s->ctrl_iface);
- wpa_s->ctrl_iface = NULL;
- }
if (wpa_s->conf != NULL) {
struct wpa_ssid *ssid;
for (ssid = wpa_s->conf->ssid; ssid; ssid = ssid->next)
wpas_notify_network_removed(wpa_s, ssid);
- wpa_config_free(wpa_s->conf);
- wpa_s->conf = NULL;
}
os_free(wpa_s->confname);
wpa_supplicant_cancel_scan(wpa_s);
wpa_supplicant_cancel_auth_timeout(wpa_s);
-
- ieee80211_sta_deinit(wpa_s);
+ eloop_cancel_timeout(wpa_supplicant_stop_countermeasures, wpa_s, NULL);
+#ifdef CONFIG_DELAYED_MIC_ERROR_REPORT
+ eloop_cancel_timeout(wpa_supplicant_delayed_mic_error_report,
+ wpa_s, NULL);
+#endif /* CONFIG_DELAYED_MIC_ERROR_REPORT */
wpas_wps_deinit(wpa_s);
offchannel_deinit(wpa_s);
#endif /* CONFIG_OFFCHANNEL */
+ wpa_supplicant_cancel_sched_scan(wpa_s);
+
os_free(wpa_s->next_scan_freqs);
wpa_s->next_scan_freqs = NULL;
gas_query_deinit(wpa_s->gas);
wpa_s->gas = NULL;
+
+ free_hw_features(wpa_s);
}
static void wpa_supplicant_terminate(int sig, void *signal_ctx)
{
struct wpa_global *global = signal_ctx;
- struct wpa_supplicant *wpa_s;
- for (wpa_s = global->ifaces; wpa_s; wpa_s = wpa_s->next) {
- wpa_msg(wpa_s, MSG_INFO, WPA_EVENT_TERMINATING "- signal %d "
- "received", sig);
- }
wpa_supplicant_terminate_proc(global);
}
return -1;
}
- if (ssid->key_mgmt &
- (WPA_KEY_MGMT_PSK | WPA_KEY_MGMT_FT_PSK | WPA_KEY_MGMT_PSK_SHA256))
- {
+ if (wpa_key_mgmt_wpa_psk(ssid->key_mgmt)) {
wpa_sm_set_pmk(wpa_s->wpa, ssid->psk, PMK_LEN);
#ifndef CONFIG_NO_PBKDF2
if (bss && ssid->bssid_set && ssid->ssid_len == 0 &&
struct wpa_driver_capa capa;
int assoc_failed = 0;
struct wpa_ssid *old_ssid;
+#ifdef CONFIG_HT_OVERRIDES
+ struct ieee80211_ht_capabilities htcaps;
+ struct ieee80211_ht_capabilities htcaps_mask;
+#endif /* CONFIG_HT_OVERRIDES */
#ifdef CONFIG_IBSS_RSN
ibss_rsn_deinit(wpa_s->ibss_rsn);
wpa_ssid_txt(ssid->ssid, ssid->ssid_len));
os_memset(wpa_s->pending_bssid, 0, ETH_ALEN);
}
+ wpa_supplicant_cancel_sched_scan(wpa_s);
wpa_supplicant_cancel_scan(wpa_s);
/* Starting new association, so clear the possibly used WPA IE from the
if (bss && (wpa_bss_get_vendor_ie(bss, WPA_IE_VENDOR_TYPE) ||
wpa_bss_get_ie(bss, WLAN_EID_RSN)) &&
- (ssid->key_mgmt & (WPA_KEY_MGMT_IEEE8021X | WPA_KEY_MGMT_PSK |
- WPA_KEY_MGMT_FT_IEEE8021X |
- WPA_KEY_MGMT_FT_PSK |
- WPA_KEY_MGMT_IEEE8021X_SHA256 |
- WPA_KEY_MGMT_PSK_SHA256))) {
+ wpa_key_mgmt_wpa(ssid->key_mgmt)) {
int try_opportunistic;
try_opportunistic = ssid->proactive_key_caching &&
(ssid->proto & WPA_PROTO_RSN);
"key management and encryption suites");
return;
}
- } else if (ssid->key_mgmt &
- (WPA_KEY_MGMT_PSK | WPA_KEY_MGMT_IEEE8021X |
- WPA_KEY_MGMT_WPA_NONE | WPA_KEY_MGMT_FT_PSK |
- WPA_KEY_MGMT_FT_IEEE8021X | WPA_KEY_MGMT_PSK_SHA256 |
- WPA_KEY_MGMT_IEEE8021X_SHA256)) {
+ } else if (wpa_key_mgmt_wpa_any(ssid->key_mgmt)) {
wpa_ie_len = sizeof(wpa_ie);
if (wpa_supplicant_set_suites(wpa_s, NULL, ssid,
wpa_ie, &wpa_ie_len)) {
}
#endif /* CONFIG_P2P */
+#ifdef CONFIG_INTERWORKING
+ if (wpa_s->conf->interworking) {
+ u8 *pos = wpa_ie;
+ if (wpa_ie_len > 0 && pos[0] == WLAN_EID_RSN)
+ pos += 2 + pos[1];
+ os_memmove(pos + 6, pos, wpa_ie_len - (pos - wpa_ie));
+ wpa_ie_len += 6;
+ *pos++ = WLAN_EID_EXT_CAPAB;
+ *pos++ = 4;
+ *pos++ = 0x00;
+ *pos++ = 0x00;
+ *pos++ = 0x00;
+ *pos++ = 0x80; /* Bit 31 - Interworking */
+ }
+#endif /* CONFIG_INTERWORKING */
+
wpa_clear_keys(wpa_s, bss ? bss->bssid : NULL);
use_crypt = 1;
cipher_pairwise = cipher_suite2driver(wpa_s->pairwise_cipher);
params.ssid = ssid->ssid;
params.ssid_len = ssid->ssid_len;
}
+
+ if (ssid->mode == WPAS_MODE_IBSS && ssid->bssid_set &&
+ wpa_s->conf->ap_scan == 2) {
+ params.bssid = ssid->bssid;
+ params.fixed_bssid = 1;
+ }
+
if (ssid->mode == WPAS_MODE_IBSS && ssid->frequency > 0 &&
params.freq == 0)
params.freq = ssid->frequency; /* Initial channel for IBSS */
else
params.uapsd = -1;
- if (wpa_s->drv_flags & WPA_DRIVER_FLAGS_USER_SPACE_MLME)
- ret = ieee80211_sta_associate(wpa_s, ¶ms);
- else
- ret = wpa_drv_associate(wpa_s, ¶ms);
+#ifdef CONFIG_HT_OVERRIDES
+ os_memset(&htcaps, 0, sizeof(htcaps));
+ os_memset(&htcaps_mask, 0, sizeof(htcaps_mask));
+ params.htcaps = (u8 *) &htcaps;
+ params.htcaps_mask = (u8 *) &htcaps_mask;
+ wpa_supplicant_apply_ht_overrides(wpa_s, ssid, ¶ms);
+#endif /* CONFIG_HT_OVERRIDES */
+
+ ret = wpa_drv_associate(wpa_s, ¶ms);
if (ret < 0) {
wpa_msg(wpa_s, MSG_INFO, "Association request to the driver "
"failed");
u8 *addr = NULL;
if (!is_zero_ether_addr(wpa_s->bssid)) {
- if (wpa_s->drv_flags & WPA_DRIVER_FLAGS_USER_SPACE_MLME)
- ieee80211_sta_disassociate(wpa_s, reason_code);
- else
- wpa_drv_disassociate(wpa_s, wpa_s->bssid, reason_code);
+ wpa_drv_disassociate(wpa_s, wpa_s->bssid, reason_code);
addr = wpa_s->bssid;
}
u8 *addr = NULL;
if (!is_zero_ether_addr(wpa_s->bssid)) {
- if (wpa_s->drv_flags & WPA_DRIVER_FLAGS_USER_SPACE_MLME)
- ieee80211_sta_deauthenticate(wpa_s, reason_code);
- else
- wpa_drv_deauthenticate(wpa_s, wpa_s->bssid,
- reason_code);
+ wpa_drv_deauthenticate(wpa_s, wpa_s->bssid, reason_code);
addr = wpa_s->bssid;
}
{
struct wpa_ssid *other_ssid;
+ int disconnected = 0;
- if (ssid && ssid != wpa_s->current_ssid && wpa_s->current_ssid)
+ if (ssid && ssid != wpa_s->current_ssid && wpa_s->current_ssid) {
wpa_supplicant_disassociate(
wpa_s, WLAN_REASON_DEAUTH_LEAVING);
+ disconnected = 1;
+ }
/*
* Mark all other networks disabled or mark all networks enabled if no
if (was_disabled != other_ssid->disabled)
wpas_notify_network_enabled_changed(wpa_s, other_ssid);
}
+
+ if (ssid && ssid == wpa_s->current_ssid && wpa_s->current_ssid) {
+ /* We are already associated with the selected network */
+ wpa_printf(MSG_DEBUG, "Already associated with the "
+ "selected network - do nothing");
+ return;
+ }
+
+ if (ssid)
+ wpa_s->current_ssid = ssid;
wpa_s->connect_without_scan = NULL;
wpa_s->disconnected = 0;
wpa_s->reassociate = 1;
- wpa_supplicant_req_scan(wpa_s, 0, 0);
+ wpa_supplicant_req_scan(wpa_s, 0, disconnected ? 100000 : 0);
if (ssid)
wpas_notify_network_selected(wpa_s, ssid);
if (ap_scan < 0 || ap_scan > 2)
return -1;
+#ifdef ANDROID
+ if (ap_scan == 2 && ap_scan != wpa_s->conf->ap_scan &&
+ wpa_s->wpa_state >= WPA_ASSOCIATING &&
+ wpa_s->wpa_state < WPA_COMPLETED) {
+ wpa_printf(MSG_ERROR, "ap_scan = %d (%d) rejected while "
+ "associating", wpa_s->conf->ap_scan, ap_scan);
+ return 0;
+ }
+#endif /* ANDROID */
+
old_ap_scan = wpa_s->conf->ap_scan;
wpa_s->conf->ap_scan = ap_scan;
u8 bssid[ETH_ALEN];
int wired;
- if (wpa_s->drv_flags & WPA_DRIVER_FLAGS_USER_SPACE_MLME) {
- if (ieee80211_sta_get_ssid(wpa_s, ssid, &ssid_len)) {
- wpa_msg(wpa_s, MSG_WARNING, "Could not read SSID from "
- "MLME");
- return NULL;
- }
- } else {
- res = wpa_drv_get_ssid(wpa_s, ssid);
- if (res < 0) {
- wpa_msg(wpa_s, MSG_WARNING, "Could not read SSID from "
- "driver");
- return NULL;
- }
- ssid_len = res;
+ res = wpa_drv_get_ssid(wpa_s, ssid);
+ if (res < 0) {
+ wpa_msg(wpa_s, MSG_WARNING, "Could not read SSID from "
+ "driver");
+ return NULL;
}
+ ssid_len = res;
- if (wpa_s->drv_flags & WPA_DRIVER_FLAGS_USER_SPACE_MLME)
- os_memcpy(bssid, wpa_s->bssid, ETH_ALEN);
- else if (wpa_drv_get_bssid(wpa_s, bssid) < 0) {
+ if (wpa_drv_get_bssid(wpa_s, bssid) < 0) {
wpa_msg(wpa_s, MSG_WARNING, "Could not read BSSID from "
"driver");
return NULL;
}
+static int select_driver(struct wpa_supplicant *wpa_s, int i)
+{
+ struct wpa_global *global = wpa_s->global;
+
+ if (wpa_drivers[i]->global_init && global->drv_priv[i] == NULL) {
+ global->drv_priv[i] = wpa_drivers[i]->global_init();
+ if (global->drv_priv[i] == NULL) {
+ wpa_printf(MSG_ERROR, "Failed to initialize driver "
+ "'%s'", wpa_drivers[i]->name);
+ return -1;
+ }
+ }
+
+ wpa_s->driver = wpa_drivers[i];
+ wpa_s->global_drv_priv = global->drv_priv[i];
+
+ return 0;
+}
+
+
static int wpa_supplicant_set_driver(struct wpa_supplicant *wpa_s,
const char *name)
{
if (name == NULL) {
/* default to first driver in the list */
- wpa_s->driver = wpa_drivers[0];
- wpa_s->global_drv_priv = wpa_s->global->drv_priv[0];
- return 0;
+ return select_driver(wpa_s, 0);
}
do {
if (os_strlen(wpa_drivers[i]->name) == len &&
os_strncmp(driver, wpa_drivers[i]->name, len) ==
0) {
- wpa_s->driver = wpa_drivers[i];
- wpa_s->global_drv_priv =
- wpa_s->global->drv_priv[i];
- return 0;
+ /* First driver that succeeds wins */
+ if (select_driver(wpa_s, i) == 0)
+ return 0;
}
}
}
-/**
- * wpa_supplicant_driver_init - Initialize driver interface parameters
- * @wpa_s: Pointer to wpa_supplicant data
- * Returns: 0 on success, -1 on failure
- *
- * This function is called to initialize driver interface parameters.
- * wpa_drv_init() must have been called before this function to initialize the
- * driver interface.
- */
-int wpa_supplicant_driver_init(struct wpa_supplicant *wpa_s)
+int wpa_supplicant_update_mac_addr(struct wpa_supplicant *wpa_s)
{
- static int interface_count = 0;
-
if (wpa_s->driver->send_eapol) {
const u8 *addr = wpa_drv_get_mac_addr(wpa_s);
if (addr)
os_memcpy(wpa_s->own_addr, addr, ETH_ALEN);
} else if (!(wpa_s->drv_flags &
WPA_DRIVER_FLAGS_P2P_DEDICATED_INTERFACE)) {
+ l2_packet_deinit(wpa_s->l2);
wpa_s->l2 = l2_packet_init(wpa_s->ifname,
wpa_drv_get_mac_addr(wpa_s),
ETH_P_EAPOL,
wpa_dbg(wpa_s, MSG_DEBUG, "Own MAC address: " MACSTR,
MAC2STR(wpa_s->own_addr));
+ wpa_sm_set_own_addr(wpa_s->wpa, wpa_s->own_addr);
+
+ return 0;
+}
+
+
+/**
+ * wpa_supplicant_driver_init - Initialize driver interface parameters
+ * @wpa_s: Pointer to wpa_supplicant data
+ * Returns: 0 on success, -1 on failure
+ *
+ * This function is called to initialize driver interface parameters.
+ * wpa_drv_init() must have been called before this function to initialize the
+ * driver interface.
+ */
+int wpa_supplicant_driver_init(struct wpa_supplicant *wpa_s)
+{
+ static int interface_count = 0;
+
+ if (wpa_supplicant_update_mac_addr(wpa_s) < 0)
+ return -1;
if (wpa_s->bridge_ifname[0]) {
wpa_dbg(wpa_s, MSG_DEBUG, "Receiving packets from bridge "
wpa_drv_flush_pmkid(wpa_s);
wpa_s->prev_scan_ssid = WILDCARD_SSID_SCAN;
+ wpa_s->prev_scan_wildcard = 0;
+
if (wpa_supplicant_enabled_networks(wpa_s->conf)) {
- wpa_supplicant_req_scan(wpa_s, interface_count, 100000);
+ if (wpa_supplicant_delayed_sched_scan(wpa_s, interface_count,
+ 100000))
+ wpa_supplicant_req_scan(wpa_s, interface_count,
+ 100000);
interface_count++;
} else
wpa_supplicant_set_state(wpa_s, WPA_INACTIVE);
wpa_s->scan_interval = 5;
wpa_s->new_connection = 1;
wpa_s->parent = wpa_s;
+ wpa_s->sched_scanning = 0;
return wpa_s;
}
+#ifdef CONFIG_HT_OVERRIDES
+
+static int wpa_set_htcap_mcs(struct wpa_supplicant *wpa_s,
+ struct ieee80211_ht_capabilities *htcaps,
+ struct ieee80211_ht_capabilities *htcaps_mask,
+ const char *ht_mcs)
+{
+ /* parse ht_mcs into hex array */
+ int i;
+ const char *tmp = ht_mcs;
+ char *end = NULL;
+
+ /* If ht_mcs is null, do not set anything */
+ if (!ht_mcs)
+ return 0;
+
+ /* This is what we are setting in the kernel */
+ os_memset(&htcaps->supported_mcs_set, 0, IEEE80211_HT_MCS_MASK_LEN);
+
+ wpa_msg(wpa_s, MSG_DEBUG, "set_htcap, ht_mcs -:%s:-", ht_mcs);
+
+ for (i = 0; i < IEEE80211_HT_MCS_MASK_LEN; i++) {
+ errno = 0;
+ long v = strtol(tmp, &end, 16);
+ if (errno == 0) {
+ wpa_msg(wpa_s, MSG_DEBUG,
+ "htcap value[%i]: %ld end: %p tmp: %p",
+ i, v, end, tmp);
+ if (end == tmp)
+ break;
+
+ htcaps->supported_mcs_set[i] = v;
+ tmp = end;
+ } else {
+ wpa_msg(wpa_s, MSG_ERROR,
+ "Failed to parse ht-mcs: %s, error: %s\n",
+ ht_mcs, strerror(errno));
+ return -1;
+ }
+ }
+
+ /*
+ * If we were able to parse any values, then set mask for the MCS set.
+ */
+ if (i) {
+ os_memset(&htcaps_mask->supported_mcs_set, 0xff,
+ IEEE80211_HT_MCS_MASK_LEN - 1);
+ /* skip the 3 reserved bits */
+ htcaps_mask->supported_mcs_set[IEEE80211_HT_MCS_MASK_LEN - 1] =
+ 0x1f;
+ }
+
+ return 0;
+}
+
+
+static int wpa_disable_max_amsdu(struct wpa_supplicant *wpa_s,
+ struct ieee80211_ht_capabilities *htcaps,
+ struct ieee80211_ht_capabilities *htcaps_mask,
+ int disabled)
+{
+ u16 msk;
+
+ wpa_msg(wpa_s, MSG_DEBUG, "set_disable_max_amsdu: %d", disabled);
+
+ if (disabled == -1)
+ return 0;
+
+ msk = host_to_le16(HT_CAP_INFO_MAX_AMSDU_SIZE);
+ htcaps_mask->ht_capabilities_info |= msk;
+ if (disabled)
+ htcaps->ht_capabilities_info &= msk;
+ else
+ htcaps->ht_capabilities_info |= msk;
+
+ return 0;
+}
+
+
+static int wpa_set_ampdu_factor(struct wpa_supplicant *wpa_s,
+ struct ieee80211_ht_capabilities *htcaps,
+ struct ieee80211_ht_capabilities *htcaps_mask,
+ int factor)
+{
+ wpa_msg(wpa_s, MSG_DEBUG, "set_ampdu_factor: %d", factor);
+
+ if (factor == -1)
+ return 0;
+
+ if (factor < 0 || factor > 3) {
+ wpa_msg(wpa_s, MSG_ERROR, "ampdu_factor: %d out of range. "
+ "Must be 0-3 or -1", factor);
+ return -EINVAL;
+ }
+
+ htcaps_mask->a_mpdu_params |= 0x3; /* 2 bits for factor */
+ htcaps->a_mpdu_params &= ~0x3;
+ htcaps->a_mpdu_params |= factor & 0x3;
+
+ return 0;
+}
+
+
+static int wpa_set_ampdu_density(struct wpa_supplicant *wpa_s,
+ struct ieee80211_ht_capabilities *htcaps,
+ struct ieee80211_ht_capabilities *htcaps_mask,
+ int density)
+{
+ wpa_msg(wpa_s, MSG_DEBUG, "set_ampdu_density: %d", density);
+
+ if (density == -1)
+ return 0;
+
+ if (density < 0 || density > 7) {
+ wpa_msg(wpa_s, MSG_ERROR,
+ "ampdu_density: %d out of range. Must be 0-7 or -1.",
+ density);
+ return -EINVAL;
+ }
+
+ htcaps_mask->a_mpdu_params |= 0x1C;
+ htcaps->a_mpdu_params &= ~(0x1C);
+ htcaps->a_mpdu_params |= (density << 2) & 0x1C;
+
+ return 0;
+}
+
+
+static int wpa_set_disable_ht40(struct wpa_supplicant *wpa_s,
+ struct ieee80211_ht_capabilities *htcaps,
+ struct ieee80211_ht_capabilities *htcaps_mask,
+ int disabled)
+{
+ /* Masking these out disables HT40 */
+ u16 msk = host_to_le16(HT_CAP_INFO_SUPP_CHANNEL_WIDTH_SET |
+ HT_CAP_INFO_SHORT_GI40MHZ);
+
+ wpa_msg(wpa_s, MSG_DEBUG, "set_disable_ht40: %d", disabled);
+
+ if (disabled)
+ htcaps->ht_capabilities_info &= ~msk;
+ else
+ htcaps->ht_capabilities_info |= msk;
+
+ htcaps_mask->ht_capabilities_info |= msk;
+
+ return 0;
+}
+
+
+void wpa_supplicant_apply_ht_overrides(
+ struct wpa_supplicant *wpa_s, struct wpa_ssid *ssid,
+ struct wpa_driver_associate_params *params)
+{
+ struct ieee80211_ht_capabilities *htcaps;
+ struct ieee80211_ht_capabilities *htcaps_mask;
+
+ if (!ssid)
+ return;
+
+ params->disable_ht = ssid->disable_ht;
+ if (!params->htcaps || !params->htcaps_mask)
+ return;
+
+ htcaps = (struct ieee80211_ht_capabilities *) params->htcaps;
+ htcaps_mask = (struct ieee80211_ht_capabilities *) params->htcaps_mask;
+ wpa_set_htcap_mcs(wpa_s, htcaps, htcaps_mask, ssid->ht_mcs);
+ wpa_disable_max_amsdu(wpa_s, htcaps, htcaps_mask,
+ ssid->disable_max_amsdu);
+ wpa_set_ampdu_factor(wpa_s, htcaps, htcaps_mask, ssid->ampdu_factor);
+ wpa_set_ampdu_density(wpa_s, htcaps, htcaps_mask, ssid->ampdu_density);
+ wpa_set_disable_ht40(wpa_s, htcaps, htcaps_mask, ssid->disable_ht40);
+}
+
+#endif /* CONFIG_HT_OVERRIDES */
+
+
static int wpa_supplicant_init_iface(struct wpa_supplicant *wpa_s,
struct wpa_interface *iface)
{
return -1;
}
+ wpa_s->hw.modes = wpa_drv_get_hw_feature_data(wpa_s,
+ &wpa_s->hw.num_modes,
+ &wpa_s->hw.flags);
+
if (wpa_drv_get_capa(wpa_s, &capa) == 0) {
+ wpa_s->drv_capa_known = 1;
wpa_s->drv_flags = capa.flags;
- if (capa.flags & WPA_DRIVER_FLAGS_USER_SPACE_MLME) {
- if (ieee80211_sta_init(wpa_s))
- return -1;
- }
+ wpa_s->probe_resp_offloads = capa.probe_resp_offloads;
wpa_s->max_scan_ssids = capa.max_scan_ssids;
+ wpa_s->max_sched_scan_ssids = capa.max_sched_scan_ssids;
+ wpa_s->sched_scan_supported = capa.sched_scan_supported;
+ wpa_s->max_match_sets = capa.max_match_sets;
wpa_s->max_remain_on_chan = capa.max_remain_on_chan;
wpa_s->max_stations = capa.max_stations;
}
return -1;
}
- wpa_sm_set_own_addr(wpa_s->wpa, wpa_s->own_addr);
-
if (wpas_wps_init(wpa_s))
return -1;
static void wpa_supplicant_deinit_iface(struct wpa_supplicant *wpa_s,
- int notify)
+ int notify, int terminate)
{
if (wpa_s->drv_priv) {
wpa_supplicant_deauthenticate(wpa_s,
wpa_supplicant_cleanup(wpa_s);
+ if (wpa_s->drv_priv)
+ wpa_drv_deinit(wpa_s);
+
if (notify)
wpas_notify_iface_removed(wpa_s);
- if (wpa_s->drv_priv)
- wpa_drv_deinit(wpa_s);
+ if (terminate)
+ wpa_msg(wpa_s, MSG_INFO, WPA_EVENT_TERMINATING);
+
+ if (wpa_s->ctrl_iface) {
+ wpa_supplicant_ctrl_iface_deinit(wpa_s->ctrl_iface);
+ wpa_s->ctrl_iface = NULL;
+ }
+
+ if (wpa_s->conf != NULL) {
+ wpa_config_free(wpa_s->conf);
+ wpa_s->conf = NULL;
+ }
}
if (wpa_supplicant_init_iface(wpa_s, &t_iface)) {
wpa_printf(MSG_DEBUG, "Failed to add interface %s",
iface->ifname);
- wpa_supplicant_deinit_iface(wpa_s, 0);
+ wpa_supplicant_deinit_iface(wpa_s, 0, 0);
os_free(wpa_s);
return NULL;
}
/* Notify the control interfaces about new iface */
if (wpas_notify_iface_added(wpa_s)) {
- wpa_supplicant_deinit_iface(wpa_s, 1);
+ wpa_supplicant_deinit_iface(wpa_s, 1, 0);
os_free(wpa_s);
return NULL;
}
* %wpa_supplicant is terminated.
*/
int wpa_supplicant_remove_iface(struct wpa_global *global,
- struct wpa_supplicant *wpa_s)
+ struct wpa_supplicant *wpa_s,
+ int terminate)
{
struct wpa_supplicant *prev;
if (global->p2p_group_formation == wpa_s)
global->p2p_group_formation = NULL;
- wpa_supplicant_deinit_iface(wpa_s, 1);
+ wpa_supplicant_deinit_iface(wpa_s, 1, terminate);
os_free(wpa_s);
return 0;
if (params == NULL)
return NULL;
+#ifdef CONFIG_DRIVER_NDIS
+ {
+ void driver_ndis_init_ops(void);
+ driver_ndis_init_ops();
+ }
+#endif /* CONFIG_DRIVER_NDIS */
+
#ifndef CONFIG_NO_WPA_MSG
wpa_msg_register_ifname_cb(wpa_supplicant_msg_ifname_cb);
#endif /* CONFIG_NO_WPA_MSG */
wpa_supplicant_deinit(global);
return NULL;
}
- for (i = 0; wpa_drivers[i]; i++) {
- if (!wpa_drivers[i]->global_init)
- continue;
- global->drv_priv[i] = wpa_drivers[i]->global_init();
- if (global->drv_priv[i] == NULL) {
- wpa_printf(MSG_ERROR, "Failed to initialize driver "
- "'%s'", wpa_drivers[i]->name);
- wpa_supplicant_deinit(global);
- return NULL;
- }
- }
return global;
}
#endif /* CONFIG_P2P */
while (global->ifaces)
- wpa_supplicant_remove_iface(global, global->ifaces);
+ wpa_supplicant_remove_iface(global, global->ifaces, 1);
if (global->ctrl_iface)
wpa_supplicant_global_ctrl_iface_deinit(global->ctrl_iface);
}
-void ieee80211_sta_free_hw_features(struct hostapd_hw_modes *hw_features,
- size_t num_hw_features)
-{
- size_t i;
-
- if (hw_features == NULL)
- return;
-
- for (i = 0; i < num_hw_features; i++) {
- os_free(hw_features[i].channels);
- os_free(hw_features[i].rates);
- }
-
- os_free(hw_features);
-}
-
-
static void add_freq(int *freqs, int *num_freqs, int freq)
{
int i;
int count;
int *freqs = NULL;
+ /*
+ * Remove possible authentication timeout since the connection failed.
+ */
+ eloop_cancel_timeout(wpa_supplicant_timeout, wpa_s, NULL);
+
/*
* Add the failed BSSID into the blacklist and speed up next scan
* attempt if there could be other APs that could accept association.