]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - build-utilities/hostap.git/commit
Try to reconnect to the same BSS on recoverable disconnection
authorJouni Malinen <j@w1.fi>
Sun, 4 Dec 2011 19:57:14 +0000 (21:57 +0200)
committerJouni Malinen <j@w1.fi>
Sun, 4 Dec 2011 19:57:14 +0000 (21:57 +0200)
commitd00821e913eda00e3c61aaacc78687766f150d11
tree0d2f8c7ca74f0bff199ce4a0974114834adca8b1
parent536fd62dba5480a2490726f0e3a9bc38225b0904
Try to reconnect to the same BSS on recoverable disconnection

If the AP disconnects us with a reason code that indicates that it has
dropped the association, but could allow us to connect again, try to
reconnect to the same BSS without going through the full scan. This can
save quite a bit of time in some common use cases, e.g., when inactivity
timeout is used on the AP (and especially, when waking up from suspend
which has likely triggered some timeout on the AP).

Signed-hostap: Jouni Malinen <j@w1.fi>
wpa_supplicant/events.c