]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - build-utilities/hostap.git/commitdiff
Added the EAP-FAST patch for OpenSSL 0.9.8h
authorJouni Malinen <j@w1.fi>
Thu, 29 May 2008 07:47:03 +0000 (10:47 +0300)
committerJouni Malinen <j@w1.fi>
Thu, 29 May 2008 07:47:03 +0000 (10:47 +0300)
patches/openssl-0.9.8h-tls-extensions.patch [new file with mode: 0644]

diff --git a/patches/openssl-0.9.8h-tls-extensions.patch b/patches/openssl-0.9.8h-tls-extensions.patch
new file mode 100644 (file)
index 0000000..c68f227
--- /dev/null
@@ -0,0 +1,344 @@
+This patch adds support for TLS SessionTicket extension (RFC 5077) for
+the parts used by EAP-FAST (RFC 4851).
+
+This is based on the patch from Alexey Kobozev <akobozev@cisco.com>
+(sent to openssl-dev mailing list on Tue, 07 Jun 2005 15:40:58 +0300).
+
+OpenSSL 0.9.8h does not enable TLS extension support by default, so it
+will need to be enabled by adding enable-tlsext to config script
+command line.
+
+
+diff -upr openssl-0.9.8h.orig/ssl/s3_clnt.c openssl-0.9.8h/ssl/s3_clnt.c
+--- openssl-0.9.8h.orig/ssl/s3_clnt.c  2008-05-28 10:29:27.000000000 +0300
++++ openssl-0.9.8h/ssl/s3_clnt.c       2008-05-29 10:44:25.000000000 +0300
+@@ -752,6 +752,20 @@ int ssl3_get_server_hello(SSL *s)
+               goto f_err;
+               }
++#ifndef OPENSSL_NO_TLSEXT
++      /* check if we want to resume the session based on external pre-shared secret */
++      if (s->version >= TLS1_VERSION && s->tls_session_secret_cb)
++      {
++              SSL_CIPHER *pref_cipher=NULL;
++              s->session->master_key_length=sizeof(s->session->master_key);
++              if (s->tls_session_secret_cb(s, s->session->master_key, &s->session->master_key_length,
++                      NULL, &pref_cipher, s->tls_session_secret_cb_arg))
++              {
++                      s->session->cipher=pref_cipher ? pref_cipher : ssl_get_cipher_by_char(s,p+j);
++              }
++      }
++#endif /* OPENSSL_NO_TLSEXT */
++
+       if (j != 0 && j == s->session->session_id_length
+           && memcmp(p,s->session->session_id,j) == 0)
+           {
+@@ -2693,11 +2707,8 @@ static int ssl3_check_finished(SSL *s)
+       {
+       int ok;
+       long n;
+-      /* If we have no ticket or session ID is non-zero length (a match of
+-       * a non-zero session length would never reach here) it cannot be a
+-       * resumed session.
+-       */
+-      if (!s->session->tlsext_tick || s->session->session_id_length)
++      /* If we have no ticket it cannot be a resumed session. */
++      if (!s->session->tlsext_tick)
+               return 1;
+       /* this function is called when we really expect a Certificate
+        * message, so permit appropriate message length */
+diff -upr openssl-0.9.8h.orig/ssl/s3_srvr.c openssl-0.9.8h/ssl/s3_srvr.c
+--- openssl-0.9.8h.orig/ssl/s3_srvr.c  2008-04-30 19:11:32.000000000 +0300
++++ openssl-0.9.8h/ssl/s3_srvr.c       2008-05-28 18:49:34.000000000 +0300
+@@ -959,6 +959,59 @@ int ssl3_get_client_hello(SSL *s)
+                       SSLerr(SSL_F_SSL3_GET_CLIENT_HELLO,SSL_R_CLIENTHELLO_TLSEXT);
+                       goto err;
+               }
++
++      /* Check if we want to use external pre-shared secret for this
++       * handshake for not reused session only. We need to generate
++       * server_random before calling tls_session_secret_cb in order to allow
++       * SessionTicket processing to use it in key derivation. */
++      {
++              unsigned long Time;
++              unsigned char *pos;
++              Time=(unsigned long)time(NULL);                 /* Time */
++              pos=s->s3->server_random;
++              l2n(Time,pos);
++              if (RAND_pseudo_bytes(pos,SSL3_RANDOM_SIZE-4) <= 0)
++              {
++                      al=SSL_AD_INTERNAL_ERROR;
++                      goto f_err;
++              }
++      }
++
++      if (!s->hit && s->version >= TLS1_VERSION && s->tls_session_secret_cb)
++      {
++              SSL_CIPHER *pref_cipher=NULL;
++
++              s->session->master_key_length=sizeof(s->session->master_key);
++              if(s->tls_session_secret_cb(s, s->session->master_key, &s->session->master_key_length, 
++                      ciphers, &pref_cipher, s->tls_session_secret_cb_arg))
++              {
++                      s->hit=1;
++                      s->session->ciphers=ciphers;
++                      s->session->verify_result=X509_V_OK;
++                      
++                      ciphers=NULL;
++                      
++                      /* check if some cipher was preferred by call back */
++                      pref_cipher=pref_cipher ? pref_cipher : ssl3_choose_cipher(s, s->session->ciphers, SSL_get_ciphers(s));
++                      if (pref_cipher == NULL)
++                              {
++                              al=SSL_AD_HANDSHAKE_FAILURE;
++                              SSLerr(SSL_F_SSL3_GET_CLIENT_HELLO,SSL_R_NO_SHARED_CIPHER);
++                              goto f_err;
++                              }
++
++                      s->session->cipher=pref_cipher;
++
++                      if (s->cipher_list)
++                              sk_SSL_CIPHER_free(s->cipher_list);
++
++                      if (s->cipher_list_by_id)
++                              sk_SSL_CIPHER_free(s->cipher_list_by_id);
++
++                      s->cipher_list = sk_SSL_CIPHER_dup(s->session->ciphers);
++                      s->cipher_list_by_id = sk_SSL_CIPHER_dup(s->session->ciphers);
++              }
++      }
+ #endif
+       /* Worst case, we will use the NULL compression, but if we have other
+        * options, we will now look for them.  We have i-1 compression
+@@ -1097,16 +1150,22 @@ int ssl3_send_server_hello(SSL *s)
+       unsigned char *buf;
+       unsigned char *p,*d;
+       int i,sl;
+-      unsigned long l,Time;
++      unsigned long l;
++#ifdef OPENSSL_NO_TLSEXT
++      unsigned long Time;
++#endif
+       if (s->state == SSL3_ST_SW_SRVR_HELLO_A)
+               {
+               buf=(unsigned char *)s->init_buf->data;
++#ifdef OPENSSL_NO_TLSEXT
+               p=s->s3->server_random;
++              /* Generate server_random if it was not needed previously */
+               Time=(unsigned long)time(NULL);                 /* Time */
+               l2n(Time,p);
+               if (RAND_pseudo_bytes(p,SSL3_RANDOM_SIZE-4) <= 0)
+                       return -1;
++#endif
+               /* Do the message type and length last */
+               d=p= &(buf[4]);
+diff -upr openssl-0.9.8h.orig/ssl/ssl.h openssl-0.9.8h/ssl/ssl.h
+--- openssl-0.9.8h.orig/ssl/ssl.h      2008-04-30 19:11:32.000000000 +0300
++++ openssl-0.9.8h/ssl/ssl.h   2008-05-28 18:49:34.000000000 +0300
+@@ -343,6 +343,7 @@ extern "C" {
+  * 'struct ssl_st *' function parameters used to prototype callbacks
+  * in SSL_CTX. */
+ typedef struct ssl_st *ssl_crock_st;
++typedef struct tls_extension_st TLS_EXTENSION;
+ /* used to hold info on the particular ciphers used */
+ typedef struct ssl_cipher_st
+@@ -364,6 +365,8 @@ DECLARE_STACK_OF(SSL_CIPHER)
+ typedef struct ssl_st SSL;
+ typedef struct ssl_ctx_st SSL_CTX;
++typedef int (*tls_session_secret_cb_fn)(SSL *s, void *secret, int *secret_len, STACK_OF(SSL_CIPHER) *peer_ciphers, SSL_CIPHER **cipher, void *arg);
++
+ /* Used to hold functions for SSLv2 or SSLv3/TLSv1 functions */
+ typedef struct ssl_method_st
+       {
+@@ -1027,6 +1030,14 @@ struct ssl_st
+       /* RFC4507 session ticket expected to be received or sent */
+       int tlsext_ticket_expected;
++
++      /* TLS extensions */
++      TLS_EXTENSION *tls_extension;
++
++      /* TLS pre-shared secret session resumption */
++      tls_session_secret_cb_fn tls_session_secret_cb;
++      void *tls_session_secret_cb_arg;
++
+       SSL_CTX * initial_ctx; /* initial ctx, used to store sessions */
+ #define session_ctx initial_ctx
+ #else
+@@ -1625,6 +1636,12 @@ void *SSL_COMP_get_compression_methods(v
+ int SSL_COMP_add_compression_method(int id,void *cm);
+ #endif
++/* TLS extensions functions */
++int SSL_set_hello_extension(SSL *s, int ext_type, void *ext_data, int ext_len);
++
++/* Pre-shared secret session resumption functions */
++int SSL_set_session_secret_cb(SSL *s, tls_session_secret_cb_fn tls_session_secret_cb, void *arg);
++
+ /* BEGIN ERROR CODES */
+ /* The following lines are auto generated by the script mkerr.pl. Any changes
+  * made after this point may be overwritten when the script is next run.
+@@ -1815,6 +1832,7 @@ void ERR_load_SSL_strings(void);
+ #define SSL_F_TLS1_ENC                                         210
+ #define SSL_F_TLS1_SETUP_KEY_BLOCK                     211
+ #define SSL_F_WRITE_PENDING                            212
++#define SSL_F_SSL_SET_HELLO_EXTENSION                  213
+ /* Reason codes. */
+ #define SSL_R_APP_DATA_IN_HANDSHAKE                    100
+diff -upr openssl-0.9.8h.orig/ssl/ssl_err.c openssl-0.9.8h/ssl/ssl_err.c
+--- openssl-0.9.8h.orig/ssl/ssl_err.c  2007-10-12 03:00:30.000000000 +0300
++++ openssl-0.9.8h/ssl/ssl_err.c       2008-05-28 18:49:34.000000000 +0300
+@@ -251,6 +251,7 @@ static ERR_STRING_DATA SSL_str_functs[]=
+ {ERR_FUNC(SSL_F_TLS1_ENC),    "TLS1_ENC"},
+ {ERR_FUNC(SSL_F_TLS1_SETUP_KEY_BLOCK),        "TLS1_SETUP_KEY_BLOCK"},
+ {ERR_FUNC(SSL_F_WRITE_PENDING),       "WRITE_PENDING"},
++{ERR_FUNC(SSL_F_SSL_SET_HELLO_EXTENSION), "SSL_set_hello_extension"},
+ {0,NULL}
+       };
+diff -upr openssl-0.9.8h.orig/ssl/ssl_sess.c openssl-0.9.8h/ssl/ssl_sess.c
+--- openssl-0.9.8h.orig/ssl/ssl_sess.c 2007-10-17 20:30:15.000000000 +0300
++++ openssl-0.9.8h/ssl/ssl_sess.c      2008-05-28 18:49:34.000000000 +0300
+@@ -704,6 +704,52 @@ long SSL_CTX_get_timeout(const SSL_CTX *
+       return(s->session_timeout);
+       }
++#ifndef OPENSSL_NO_TLSEXT
++int SSL_set_session_secret_cb(SSL *s, int (*tls_session_secret_cb)(SSL *s, void *secret, int *secret_len, 
++      STACK_OF(SSL_CIPHER) *peer_ciphers, SSL_CIPHER **cipher, void *arg), void *arg)
++{
++      if (s == NULL) return(0);
++      s->tls_session_secret_cb = tls_session_secret_cb;
++      s->tls_session_secret_cb_arg = arg;
++      return(1);
++}
++
++int SSL_set_hello_extension(SSL *s, int ext_type, void *ext_data, int ext_len)
++{
++      if(s->version >= TLS1_VERSION)
++      {
++              if(s->tls_extension)
++              {
++                      OPENSSL_free(s->tls_extension);
++                      s->tls_extension = NULL;
++              }
++
++              s->tls_extension = OPENSSL_malloc(sizeof(TLS_EXTENSION) + ext_len);
++              if(!s->tls_extension)
++              {
++                      SSLerr(SSL_F_SSL_SET_HELLO_EXTENSION, ERR_R_MALLOC_FAILURE);
++                      return 0;
++              }
++
++              s->tls_extension->type = ext_type;
++
++              if(ext_data)
++              {
++                      s->tls_extension->length = ext_len;
++                      s->tls_extension->data = s->tls_extension + 1;
++                      memcpy(s->tls_extension->data, ext_data, ext_len);
++              } else {
++                      s->tls_extension->length = 0;
++                      s->tls_extension->data = NULL;
++              }
++
++              return 1;
++      }
++
++      return 0;
++}
++#endif /* OPENSSL_NO_TLSEXT */
++
+ typedef struct timeout_param_st
+       {
+       SSL_CTX *ctx;
+diff -upr openssl-0.9.8h.orig/ssl/t1_lib.c openssl-0.9.8h/ssl/t1_lib.c
+--- openssl-0.9.8h.orig/ssl/t1_lib.c   2008-05-28 10:26:33.000000000 +0300
++++ openssl-0.9.8h/ssl/t1_lib.c        2008-05-28 18:49:34.000000000 +0300
+@@ -106,6 +106,12 @@ int tls1_new(SSL *s)
+ void tls1_free(SSL *s)
+       {
++#ifndef OPENSSL_NO_TLSEXT
++      if(s->tls_extension)
++      {
++              OPENSSL_free(s->tls_extension);
++      }
++#endif
+       ssl3_free(s);
+       }
+@@ -175,8 +181,24 @@ unsigned char *ssl_add_clienthello_tlsex
+               int ticklen;
+               if (s->session && s->session->tlsext_tick)
+                       ticklen = s->session->tlsext_ticklen;
++              else if (s->session && s->tls_extension &&
++                      s->tls_extension->type == TLSEXT_TYPE_session_ticket &&
++                      s->tls_extension->data)
++              {
++                      ticklen = s->tls_extension->length;
++                      s->session->tlsext_tick = OPENSSL_malloc(ticklen);
++                      if (!s->session->tlsext_tick)
++                              return NULL;
++                      memcpy(s->session->tlsext_tick, s->tls_extension->data,
++                             ticklen);
++                      s->session->tlsext_ticklen = ticklen;
++              }
+               else
+                       ticklen = 0;
++              if (ticklen == 0 && s->tls_extension &&
++                  s->tls_extension->type == TLSEXT_TYPE_session_ticket &&
++                  s->tls_extension->data == NULL)
++                      goto skip_ext;
+               /* Check for enough room 2 for extension type, 2 for len
+                * rest for ticket
+                */
+@@ -190,6 +212,7 @@ unsigned char *ssl_add_clienthello_tlsex
+                       ret += ticklen;
+                       }
+               }
++              skip_ext:
+       if (s->tlsext_status_type == TLSEXT_STATUSTYPE_ocsp)
+               {
+@@ -774,6 +797,8 @@ int tls1_process_ticket(SSL *s, unsigned
+                               s->tlsext_ticket_expected = 1;
+                               return 0;       /* Cache miss */
+                               }
++                      if (s->tls_session_secret_cb)
++                              return 0;
+                       return tls_decrypt_ticket(s, p, size, session_id, len,
+                                                                       ret);
+                       }
+diff -upr openssl-0.9.8h.orig/ssl/tls1.h openssl-0.9.8h/ssl/tls1.h
+--- openssl-0.9.8h.orig/ssl/tls1.h     2008-04-30 19:11:33.000000000 +0300
++++ openssl-0.9.8h/ssl/tls1.h  2008-05-28 18:49:34.000000000 +0300
+@@ -398,6 +398,14 @@ SSL_CTX_callback_ctrl(ssl,SSL_CTRL_SET_T
+ #define TLS_MD_MASTER_SECRET_CONST    "\x6d\x61\x73\x74\x65\x72\x20\x73\x65\x63\x72\x65\x74"  /*master secret*/
+ #endif
++/* TLS extension struct */
++struct tls_extension_st
++{
++      unsigned short type;
++      unsigned short length;
++      void *data;
++};
++
+ #ifdef  __cplusplus
+ }
+ #endif
+diff -upr openssl-0.9.8h.orig/util/ssleay.num openssl-0.9.8h/util/ssleay.num
+--- openssl-0.9.8h.orig/util/ssleay.num        2007-08-13 01:31:16.000000000 +0300
++++ openssl-0.9.8h/util/ssleay.num     2008-05-28 18:49:34.000000000 +0300
+@@ -241,3 +241,5 @@ SSL_CTX_sess_get_remove_cb              
+ SSL_set_SSL_CTX                         290   EXIST::FUNCTION:
+ SSL_get_servername                      291   EXIST::FUNCTION:TLSEXT
+ SSL_get_servername_type                 292   EXIST::FUNCTION:TLSEXT
++SSL_set_hello_extension                       305     EXIST::FUNCTION:TLSEXT
++SSL_set_session_secret_cb             306     EXIST::FUNCTION:TLSEXT