summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 481234c)
raw | patch | inline | side by side (parent: 481234c)
author | Jouni Malinen <j@w1.fi> | |
Tue, 6 Dec 2011 19:13:54 +0000 (21:13 +0200) | ||
committer | Jouni Malinen <j@w1.fi> | |
Tue, 6 Dec 2011 19:13:54 +0000 (21:13 +0200) |
P2P use cases do not allow use of Label config method and the earlier
code for this has already been removed, but this documentation was not
updated at the same time.
Signed-hostap: Jouni Malinen <j@w1.fi>
code for this has already been removed, but this documentation was not
updated at the same time.
Signed-hostap: Jouni Malinen <j@w1.fi>
wpa_supplicant/README-P2P | patch | blob | history |
index 0c1ca03e76937b1c8172ee3ddcf90dc82b4acc83..4b713984b8bc65b93f01718c303dc4b40b7001d0 100644 (file)
us and "p2p_prov_disc 02:01:02:03:04:05 keypad" would request the peer
to enter a PIN that we display.
-p2p_connect <peer device address> <pbc|pin|PIN#> [label|display|keypad]
+p2p_connect <peer device address> <pbc|pin|PIN#> [display|keypad]
[persistent] [join|auth] [go_intent=<0..15>] [freq=<in MHz>]
Start P2P group formation with a discovered P2P peer. This includes
method. "pbc" string starts pushbutton method, "pin" string start PIN
method using an automatically generated PIN (which will be returned as
the command return code), PIN# means that a pre-selected PIN can be
-used (e.g., 12345670). [label|display|keypad] is used with PIN method
-to specify which PIN is used (label=PIN from local label,
-display=dynamically generated random PIN from local display,
-keypad=PIN entered from peer device label or display). "persistent"
+used (e.g., 12345670). [display|keypad] is used with PIN method
+to specify which PIN is used (display=dynamically generated random PIN
+from local display, keypad=PIN entered from peer display). "persistent"
parameter can be used to request a persistent group to be formed.
"join" indicates that this is a command to join an existing group as a