Preparations for 0.6.7 release
authorJouni Malinen <j@w1.fi>
Tue, 6 Jan 2009 18:11:15 +0000 (20:11 +0200)
committerJouni Malinen <j@w1.fi>
Tue, 6 Jan 2009 18:11:15 +0000 (20:11 +0200)
14 files changed:
hostapd/ChangeLog
hostapd/README
hostapd/hostapd.c
hostapd/hostapd_cli.c
src/common/version.h
wpa_supplicant/ChangeLog
wpa_supplicant/README
wpa_supplicant/README-Windows.txt
wpa_supplicant/wpa_cli.c
wpa_supplicant/wpa_supplicant.c
www/hostapd/index.html
www/index.html
www/versions.dot
www/wpa_supplicant/index.html

index 09b34cd9bf50260da1e447e79d51779cfe510c67..f85a4fb1187429b7900abae7062e9a32f9662d9f 100644 (file)
@@ -1,10 +1,11 @@
 ChangeLog for hostapd
 
-????-??-?? - v0.6.7
+2009-01-06 - v0.6.7
        * added support for Wi-Fi Protected Setup (WPS)
          (hostapd can now be configured to act as an integrated WPS Registrar
          and provision credentials for WPS Enrollees using PIN and PBC
-         methods; external WPS Registrars are not supported); WPS support can
+         methods; external wireless Registrar can configure the AP, but
+         external WLAN Manager Registrars are not supported); WPS support can
          be enabled by adding CONFIG_WPS=y into .config and setting the
          runtime configuration variables in hostapd.conf (see WPS section in
          the example configuration file); new hostapd_cli commands wps_pin and
index 674377470ccf9df4485397429bf69ce214707af0..eb9aa4815b4f5ad1fa0f5b1fa5b1772204cb8147 100644 (file)
@@ -2,7 +2,7 @@ hostapd - user space IEEE 802.11 AP and IEEE 802.1X/WPA/WPA2/EAP
          Authenticator and RADIUS authentication server
 ================================================================
 
-Copyright (c) 2002-2008, Jouni Malinen <j@w1.fi> and contributors
+Copyright (c) 2002-2009, Jouni Malinen <j@w1.fi> and contributors
 All Rights Reserved.
 
 This program is dual-licensed under both the GPL version 2 and BSD
index 1da0bf52acfdd3afe042aa0b800f07833a8a79a5..8f2ec4cb64f2fa6e76df533d697866bed472b6f1 100644 (file)
@@ -1,6 +1,6 @@
 /*
  * hostapd / Initialization and configuration
- * Copyright (c) 2002-2008, Jouni Malinen <j@w1.fi>
+ * Copyright (c) 2002-2009, Jouni Malinen <j@w1.fi>
  *
  * This program is free software; you can redistribute it and/or modify
  * it under the terms of the GNU General Public License version 2 as
@@ -1658,7 +1658,7 @@ static void show_version(void)
                "hostapd v" VERSION_STR "\n"
                "User space daemon for IEEE 802.11 AP management,\n"
                "IEEE 802.1X/WPA/WPA2/EAP/RADIUS Authenticator\n"
-               "Copyright (c) 2002-2008, Jouni Malinen <j@w1.fi> "
+               "Copyright (c) 2002-2009, Jouni Malinen <j@w1.fi> "
                "and contributors\n");
 }
 
index 68ff091cf50927973a8e7215cd84abb4e1e3d7cf..9c3e65b2a690848fd54148c70608bcde4a8717d0 100644 (file)
@@ -1,6 +1,6 @@
 /*
  * hostapd - command line interface for hostapd daemon
- * Copyright (c) 2004-2008, Jouni Malinen <j@w1.fi>
+ * Copyright (c) 2004-2009, Jouni Malinen <j@w1.fi>
  *
  * This program is free software; you can redistribute it and/or modify
  * it under the terms of the GNU General Public License version 2 as
@@ -22,7 +22,7 @@
 
 static const char *hostapd_cli_version =
 "hostapd_cli v" VERSION_STR "\n"
-"Copyright (c) 2004-2008, Jouni Malinen <j@w1.fi> and contributors";
+"Copyright (c) 2004-2009, Jouni Malinen <j@w1.fi> and contributors";
 
 
 static const char *hostapd_cli_license =
index cf137f9f42e497ed2eabaf3fc30009cd2cae9e18..7651b48a1e300ab9738562d45fc1ef78caacdcfa 100644 (file)
@@ -1,6 +1,6 @@
 #ifndef VERSION_H
 #define VERSION_H
 
-#define VERSION_STR "0.6.6"
+#define VERSION_STR "0.6.7"
 
 #endif /* VERSION_H */
index 361c17126e37a770bfb224b95339d9b4fff88bde..37ab7224b20d2b374d4b83f6cea84429d9afdc78 100644 (file)
@@ -1,6 +1,6 @@
 ChangeLog for wpa_supplicant
 
-????-??-?? - v0.6.7
+2009-01-06 - v0.6.7
        * added support for Wi-Fi Protected Setup (WPS)
          (wpa_supplicant can now be configured to act as a WPS Enrollee to
          enroll credentials for a network using PIN and PBC methods; in
index 643a727a8bc08d16e7ce92281f84b70673faca0f..778b0ba7270e224105426e6e9aa534a25e63d3c4 100644 (file)
@@ -1,7 +1,7 @@
 WPA Supplicant
 ==============
 
-Copyright (c) 2003-2008, Jouni Malinen <j@w1.fi> and contributors
+Copyright (c) 2003-2009, Jouni Malinen <j@w1.fi> and contributors
 All Rights Reserved.
 
 This program is dual-licensed under both the GPL version 2 and BSD
index e2b75bdde0bfacd28ae2230eb64bdbb3caa1642d..292223d2d5fea0ab5746da1bd41825c37b3b4626 100644 (file)
@@ -1,8 +1,7 @@
 wpa_supplicant for Windows
 ==========================
 
-Copyright (c) 2003-2008, Jouni Malinen <j@w1.fi> and
-contributors
+Copyright (c) 2003-2009, Jouni Malinen <j@w1.fi> and contributors
 All Rights Reserved.
 
 This program is dual-licensed under both the GPL version 2 and BSD
index c36277a0e2407bb33f1e032d6a3d7fde8318c107..c49b674011ac633e4663e67d22eee20940bc0502 100644 (file)
@@ -1,6 +1,6 @@
 /*
  * WPA Supplicant - command line interface for wpa_supplicant daemon
- * Copyright (c) 2004-2008, Jouni Malinen <j@w1.fi>
+ * Copyright (c) 2004-2009, Jouni Malinen <j@w1.fi>
  *
  * This program is free software; you can redistribute it and/or modify
  * it under the terms of the GNU General Public License version 2 as
@@ -31,7 +31,7 @@
 
 static const char *wpa_cli_version =
 "wpa_cli v" VERSION_STR "\n"
-"Copyright (c) 2004-2008, Jouni Malinen <j@w1.fi> and contributors";
+"Copyright (c) 2004-2009, Jouni Malinen <j@w1.fi> and contributors";
 
 
 static const char *wpa_cli_license =
index d23220d3a79979d9bcb9a0e0b087e6f2c0470e77..d2c45525e30643237c29bf336689c5d0ec42bf32 100644 (file)
@@ -1,6 +1,6 @@
 /*
  * WPA Supplicant
- * Copyright (c) 2003-2008, Jouni Malinen <j@w1.fi>
+ * Copyright (c) 2003-2009, Jouni Malinen <j@w1.fi>
  *
  * This program is free software; you can redistribute it and/or modify
  * it under the terms of the GNU General Public License version 2 as
@@ -42,7 +42,7 @@
 
 const char *wpa_supplicant_version =
 "wpa_supplicant v" VERSION_STR "\n"
-"Copyright (c) 2003-2008, Jouni Malinen <j@w1.fi> and contributors";
+"Copyright (c) 2003-2009, Jouni Malinen <j@w1.fi> and contributors";
 
 const char *wpa_supplicant_license =
 "This program is free software. You can distribute it and/or modify it\n"
index 0b89eb3afa2a886570a9bd146f1f0aead580dcaf..551d31b0e44d909971e5da9ed822f93206b432b3 100644 (file)
@@ -3,7 +3,7 @@
   <head>
     <title>hostapd: IEEE 802.11 AP, IEEE 802.1X/WPA/WPA2/EAP/RADIUS Authenticator</title>
     <meta name="description" content="hostapd (IEEE 802.1X, WPA, WPA2, RSN, IEEE 802.11i Authenticator and RADIUS authentication server)">
-    <meta name="keywords" content="WPA, WPA2, IEEE 802.11i, IEEE 802.1X, WPA Authenticator, hostapd, TKIP, CCMP, EAP-PEAP, EAP-TLS, EAP-TTLS, EAP-SIM, EAP-AKA, EAP-GTC, EAP-MSCHAPv2, EAP-MD5, EAP-PAX, EAP-PSK, EAP-FAST, IEEE 802.1X Supplicant, IEEE 802.1aa, EAPOL, RSN, pre-authentication, PMKSA caching, BSD WPA Authenticator, FreeBSD WPA Authenticator, RADIUS authentication server, EAP authenticator, EAP server, EAP-TNC, TNCS, IF-IMV, IF-TNCCS">
+    <meta name="keywords" content="WPA, WPA2, IEEE 802.11i, IEEE 802.1X, WPA Authenticator, hostapd, TKIP, CCMP, EAP-PEAP, EAP-TLS, EAP-TTLS, EAP-SIM, EAP-AKA, EAP-GTC, EAP-MSCHAPv2, EAP-MD5, EAP-PAX, EAP-PSK, EAP-FAST, IEEE 802.1X Supplicant, IEEE 802.1aa, EAPOL, RSN, pre-authentication, PMKSA caching, BSD WPA Authenticator, FreeBSD WPA Authenticator, RADIUS authentication server, EAP authenticator, EAP server, EAP-TNC, TNCS, IF-IMV, IF-TNCCS, WPS">
     <meta http-equiv="Content-Type" content="text/html; charset=iso-8859-1">
   </head>
 
@@ -33,6 +33,7 @@ RADIUS backend authentication server) ("WPA-Enterprise")</li>
 <li>RSN: PMKSA caching, pre-authentication</li>
 <li>RADIUS accounting</li>
 <li>RADIUS authentication server with EAP</li>
+<li>Wi-Fi Protected Setup (WPS)</li>
 </ul>
 
 <h4>Supported EAP methods (integrated EAP server and RADIUS authentication server)</h4>
@@ -59,7 +60,7 @@ RADIUS backend authentication server) ("WPA-Enterprise")</li>
 <li>EAP-SAKE</li>
 <li>EAP-FAST</li>
 <li>EAP-IKEv2</li>
-<li>EAP-GPSK (experimental)</li>
+<li>EAP-GPSK</li>
 </ul>
 
 <p>Following methods are also supported, but since they do not generate keying
@@ -89,7 +90,7 @@ available in <a href="/gitweb/gitweb.cgi?p=hostap.git;a=blob_plain;f=hostapd/eap
 
 <p>
 <b>hostapd</b><br>
-Copyright (c) 2002-2008, Jouni Malinen &lt;j@w1.fi&gt;
+Copyright (c) 2002-2009, Jouni Malinen &lt;j@w1.fi&gt;
 and contributors.
 </p>
 
@@ -132,7 +133,7 @@ for the current documentation.</b></p>
 </ul>
 <li>Latest development release:
 <ul>
-<li><a href="../releases/hostapd-0.6.6.tar.gz">hostapd-0.6.6.tar.gz</a></li>
+<li><a href="../releases/hostapd-0.6.7.tar.gz">hostapd-0.6.7.tar.gz</a></li>
 </ul>
 <li>ChangeLog:
 <ul>
@@ -261,7 +262,7 @@ bug/feature request</a>.
     <address><a href="mailto:j@w1.fi">Jouni Malinen</a></address>
 <!-- Created: Sun Jan  2 17:20:17 PST 2005 -->
 <!-- hhmts start -->
-Last modified: Fri Dec 26 15:37:54 EET 2008
+Last modified: Tue Jan  6 20:05:09 EET 2009
 <!-- hhmts end -->
     </div>
   </body>
index 2f67c734c9014fdcdda60c68d8ea848d8e5ed181..0f0a4a976ae8c1af8ace94641b2b9f508ded5e9b 100644 (file)
@@ -141,13 +141,13 @@ and contributors.
 
 <p>
 <b>hostapd</b><br>
-Copyright (c) 2002-2008, Jouni Malinen &lt;j@w1.fi&gt;
+Copyright (c) 2002-2009, Jouni Malinen &lt;j@w1.fi&gt;
 and contributors.
 </p>
 
 <p>
 <b>wpa_supplicant</b><br>
-Copyright (c) 2003-2008, Jouni Malinen &lt;j@w1.fi&gt;
+Copyright (c) 2003-2009, Jouni Malinen &lt;j@w1.fi&gt;
 and contributors.
 </p>
 
@@ -213,9 +213,10 @@ main kernel tree.
 </ul>
 <li>Latest development release:
 <ul>
-<li><a href="releases/hostapd-0.6.6.tar.gz">hostapd-0.6.6.tar.gz</a>
-<li><a href="releases/wpa_supplicant-0.6.6.tar.gz">wpa_supplicant-0.6.6.tar.gz</a> (source code for all versions)</li>
-<li><a href="releases/wpa_supplicant-windows-bin-0.6.6.zip">wpa_supplicant-windows-bin-0.6.6.zip</a> (binaries for Windows)</li>
+<li><a href="releases/hostapd-0.6.7.tar.gz">hostapd-0.6.7.tar.gz</a>
+<li><a href="releases/wpa_supplicant-0.6.7.tar.gz">wpa_supplicant-0.6.7.tar.gz</a> (source code for all versions)</li>
+<li><a href="releases/wpa_supplicant-0.6.7.exe">wpa_supplicant-0.6.7.exe</a> (binary installer for Windows)</li>
+<li><a href="releases/wpa_supplicant-windows-bin-0.6.7.zip">wpa_supplicant-windows-bin-0.6.7.zip</a> (binaries for Windows)</li>
 <li><a href="wpa_supplicant/qt4/wpa_gui-qt433-windows-dll.zip">wpa_gui-qt433-windows-dll.zip</a> (Qt4 libraries from wpa_gui/Windows)</li>
 </ul>
 <li>ChangeLog:
@@ -294,7 +295,7 @@ get lost, please report it through the bug tracking system as
     <address><a href="mailto:j@w1.fi">Jouni Malinen</a></address>
 <!-- Created: Mon May 27 20:08:41 EEST 2002 -->
 <!-- hhmts start -->
-Last modified: Fri Dec 26 15:37:35 EET 2008
+Last modified: Tue Jan  6 20:03:17 EET 2009
 <!-- hhmts end -->
     </div>
   </body>
index d24abe95e03bb7b15b1060a6704eb3498c853e53..4a0a5a89c2d641cde7b3c2c21bb40baeb353350d 100644 (file)
@@ -43,6 +43,7 @@ digraph versions {
        v064 [label="0.6.4  hw\n2008-08-10"]
        v065 [label="0.6.5  hw\n2008-11-01"]
        v066 [label="0.6.6  hw\n2008-11-23"]
+       v067 [label="0.6.7  hw\n2009-01-06"]
 
 # stable releases
 
@@ -75,7 +76,7 @@ digraph versions {
        v024 -> v030 -> v031 -> v032 -> v033 -> v034 -> v035 -> v036 -> v037
        v037 -> v040 -> v041 -> v042 -> v043 -> v044 -> v045 -> v046 -> v047
        v047 -> v050 -> v051 -> v052 -> v053 -> v054 -> v055 -> v056 -> v057
-       v057 -> v060 -> v061 -> v062 -> v063 -> v064 -> v065 -> v066
+       v057 -> v060 -> v061 -> v062 -> v063 -> v064 -> v065 -> v066 -> v067
 
        {rank=same; v001 v024}
        {rank=same; v030 v037}
index cfb128a3faecba122c7a669f8cb3428d54507a47..05042a0cbd7f34dcf7b965f1d39ce93a3d626edb 100644 (file)
@@ -3,7 +3,7 @@
   <head>
     <title>Linux WPA Supplicant (IEEE 802.1X, WPA, WPA2, RSN, IEEE 802.11i)</title>
     <meta name="description" content="WPA Supplicant for Linux, BSD, and Windows (IEEE 802.1X, WPA, WPA2, RSN, IEEE 802.11i)">
-    <meta name="keywords" content="WPA, WPA2, IEEE 802.11i, IEEE 802.1X, WPA Supplicant, wpa_supplicant, TKIP, CCMP, EAP-PEAP, EAP-TLS, EAP-TTLS, EAP-SIM, EAP-AKA, EAP-PSK, EAP-GTC, EAP-MSCHAPv2, EAP-MD5, EAP-FAST, EAP-PAX, EAP-IKEv2IEEE 802.1X Supplicant, IEEE 802.1aa, EAPOL, RSN, pre-authentication, PMKSA caching, BSD WPA Supplicant, FreeBSD WPA Supplicant, wireless, WinXP WPA Supplicant, EAP-TNC, TNCC, IF-IMC, IF-TNCCS">
+    <meta name="keywords" content="WPA, WPA2, IEEE 802.11i, IEEE 802.1X, WPA Supplicant, wpa_supplicant, TKIP, CCMP, EAP-PEAP, EAP-TLS, EAP-TTLS, EAP-SIM, EAP-AKA, EAP-PSK, EAP-GTC, EAP-MSCHAPv2, EAP-MD5, EAP-FAST, EAP-PAX, EAP-IKEv2IEEE 802.1X Supplicant, IEEE 802.1aa, EAPOL, RSN, pre-authentication, PMKSA caching, BSD WPA Supplicant, FreeBSD WPA Supplicant, wireless, WinXP WPA Supplicant, EAP-TNC, TNCC, IF-IMC, IF-TNCCS, WPS">
     <meta http-equiv="Content-Type" content="text/html; charset=iso-8859-1">
   </head>
 
@@ -41,6 +41,7 @@ build for x86 target).</p>
 <li>key management for CCMP, TKIP, WEP104, WEP40</li>
 <li>WPA and full IEEE 802.11i/RSN/WPA2</li>
 <li>RSN: PMKSA caching, pre-authentication</li>
+<li>Wi-Fi Protected Setup (WPS)</li>
 </ul>
 
 <h4>Supported EAP methods (IEEE 802.1X Supplicant)</h4>
@@ -69,7 +70,7 @@ build for x86 target).</p>
 <li>EAP-PAX</li>
 <li>EAP-SAKE</li>
 <li>EAP-IKEv2</li>
-<li>EAP-GPSK (experimental)</li>
+<li>EAP-GPSK</li>
 <li>LEAP (note: requires special support from the driver)</li>
 </ul>
 
@@ -138,7 +139,7 @@ other drivers.</p>
 
 <p>
 <b>wpa_supplicant</b><br>
-Copyright (c) 2003-2008, Jouni Malinen &lt;j@w1.fi&gt;
+Copyright (c) 2003-2009, Jouni Malinen &lt;j@w1.fi&gt;
 and contributors.
 </p>
 
@@ -186,8 +187,9 @@ has some more information about the Windows port of wpa_supplicant.</p>
 </ul>
 <li>Latest development release:
 <ul>
-<li><a href="../releases/wpa_supplicant-0.6.6.tar.gz">wpa_supplicant-0.6.6.tar.gz</a> (source code for all versions)</li>
-<li><a href="../releases/wpa_supplicant-windows-bin-0.6.6.zip">wpa_supplicant-windows-bin-0.6.6.zip</a> (binaries for Windows)</li>
+<li><a href="../releases/wpa_supplicant-0.6.7.tar.gz">wpa_supplicant-0.6.7.tar.gz</a> (source code for all versions)</li>
+<li><a href="../releases/wpa_supplicant-0.6.7.exe">wpa_supplicant-0.6.7.exe</a> (binary installer for Windows)</li>
+<li><a href="../releases/wpa_supplicant-windows-bin-0.6.7.zip">wpa_supplicant-windows-bin-0.6.7.zip</a> (binaries for Windows)</li>
 <li><a href="qt4/wpa_gui-qt433-windows-dll.zip">wpa_gui-qt433-windows-dll.zip</a> (Qt4 libraries from wpa_gui/Windows)</li>
 </ul>
 <li>ChangeLog:
@@ -351,7 +353,7 @@ bug/feature request</a>.
     <address><a href="mailto:j@w1.fi">Jouni Malinen</a></address>
 <!-- Created: Sat May 22 21:41:58 PDT 2004 -->
 <!-- hhmts start -->
-Last modified: Fri Dec 26 15:37:46 EET 2008
+Last modified: Tue Jan  6 20:06:04 EET 2009
 <!-- hhmts end -->
     </div>
   </body>